SE - Secure Element#
Secure Element peripheral API.
Abstraction of the Secure Element's mailbox interface.
For series 2 devices with a part number that is xG23 or higher, the following step is necessary for basic operation:
Clock enable:
CMU_ClockEnable(cmuClock_SEMAILBOX, true);
Note
The high-level SE API has been moved to the SE manager, and the implementation in em_se should not be used.
Using the SE's mailbox is not thread-safe in EMLIB, and accessing the SE's mailbox both in regular and IRQ context is not safe. SE operations should be performed using the SE manager if possible.
Modules#
Typedefs#
Possible responses to a command.
Functions#
Write to FIFO.
Add input data to a command.
Add output data to a command.
Add a parameter to a command.
Execute the passed command.
Check whether the running command has completed.
Read the status of the previously executed command.
Wait for completion of the current command.
Disable one or more SE interrupts.
Enable one or more SE interrupts.
Macros#
Response status codes for the Secure Element.
Command executed successfully or signature was successfully validated.
Maximum amount of parameters supported by the hardware FIFO.
Stop datatransfer.
Discard datatransfer.
Realign datatransfer.
Datatransfer Const Address.
Stop Length Mask.
Maximum amount of parameters for largest command in defined command set.
Default initialization of data transfer struct.
Default initialization of command struct.
Function Documentation#
writeToFifo#
void writeToFifo (uint32_t value)
Write to FIFO.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | value | Value to write to FIFO |
SE_addDataInput#
void SE_addDataInput (SE_Command_t * command, SE_DataTransfer_t * data)
Add input data to a command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SE_Command_t * | [in] | command | Pointer to an SE command structure. |
| SE_DataTransfer_t * | [in] | data | Pointer to a data transfer structure. |
This function adds a buffer of input data to the given SE command structure The buffer gets appended by reference at the end of the list of already added buffers.
Note
Note that this function does not copy either the data buffer or the buffer structure, so make sure to keep the data object in scope until the command has been executed by the secure element.
SE_addDataOutput#
void SE_addDataOutput (SE_Command_t * command, SE_DataTransfer_t * data)
Add output data to a command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SE_Command_t * | [in] | command | Pointer to an SE command structure. |
| SE_DataTransfer_t * | [in] | data | Pointer to a data transfer structure. |
This function adds a buffer of output data to the given command structure The buffer gets appended by reference at the end of the list of already added buffers.
Note
Note that this function does not copy either the data buffer or the buffer structure, so make sure to keep the data object in scope until the command has been executed by the secure element.
SE_addParameter#
void SE_addParameter (SE_Command_t * command, uint32_t parameter)
Add a parameter to a command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SE_Command_t * | [in] | command | Pointer to a filled-out SE command structure. |
| uint32_t | [in] | parameter | Parameter to add. |
This function adds a parameter word to the passed command.
Note
Make sure to not exceed SE_MAX_PARAMETERS.
SE_executeCommand#
void SE_executeCommand (SE_Command_t * command)
Execute the passed command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| SE_Command_t * | [in] | command | Pointer to a filled-out SE command structure. |
This function starts the execution of the passed command by the secure element. When started, wait for the RXINT interrupt flag, or call SE_waitCommandCompletion to busy-wait. After completion, you have to call SE_readCommandResponse to get the command's execution status.
SE_isCommandCompleted#
bool SE_isCommandCompleted (void )
Check whether the running command has completed.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function polls the SE-to-host mailbox interrupt flag.
Returns
True if a command has completed and the result is available
SE_readCommandResponse#
SE_Response_t SE_readCommandResponse (void )
Read the status of the previously executed command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function reads the status of the previously executed command.
Note
The command response needs to be read for every executed command, and can only be read once per executed command (FIFO behavior).
Returns
One of the SE_RESPONSE return codes: SE_RESPONSE_OK when the command was executed successfully or a signature was successfully verified.
SE_waitCommandCompletion#
void SE_waitCommandCompletion (void )
Wait for completion of the current command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function "busy"-waits until the execution of the ongoing instruction has completed.
SE_disableInterrupt#
void SE_disableInterrupt (uint32_t flags)
Disable one or more SE interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | flags | SE interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the Secure Element module (SE_CONFIGURATION_(TX/RX)INTEN). |
SE_enableInterrupt#
void SE_enableInterrupt (uint32_t flags)
Enable one or more SE interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | flags | SE interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the Secure Element module (SEMAILBOX_CONFIGURATION_TXINTEN or SEMAILBOX_CONFIGURATION_RXINTEN). |