You are viewing documentation for version:
PDFSE Command structure to which all commands to the SE must adhere.
Public Attribute Documentation#
command#
uint32_t SE_Command_t::command
SE Command.
data_in#
SE_DataTransfer_t* SE_Command_t::data_in
Input data.
data_out#
SE_DataTransfer_t* SE_Command_t::data_out
Output data.
parameters#
uint32_t SE_Command_t::parameters[SE_MAX_PARAMETERS]
Parameters.
num_parameters#
size_t SE_Command_t::num_parameters
Number of parameters.