System Initialization and Action Processing#
System Initialization and Action Processing.
System Init#
System Init provides a function for initializing the system and the products:
This function calls a set of functions that are automatically generated and located in autogen/sl_event_handler.c. Handlers can be registered for the following events using the Event Handler API provided by the Event Handler component:
platform_init -> sl_platform_init()
driver_init -> sl_driver_init()
service_init -> sl_service_init()
stack_init -> sl_stack_init()
internal_app_init -> sl_internal_app_init()
These events are fired in the order listed above when sl_system_init() is called.
System Kernel#
System Kernel component provides a function for starting the kernel:
This function calls a functions that is automatically generated and located in $autogen/sl_event_handler.c. Handlers can be registered for the following events using the Event Handler API provided by the Event Handler component:
kernel_start -> sl_kernel_start()
The event is fired when sl_system_kernel_start() is called.
System Process Action#
System Process Action component provides a function for running the products from a super loop:
This function calls a set of functions that are automatically generated and located in $autogen/sl_event_handler.c. Handlers can be registered for the following events using the Event Handler API provided by the Event Handler component:
platform_process_action -> sl_platform_process_action()
service_process_action -> sl_service_process_action()
stack_process_action -> sl_stack_process_action()
internal_app_process_action -> sl_internal_process_action()
These events are fired in the order listed above when sl_system_process_action() is called.
Usage example:
#if defined(SL_COMPONENT_CATALOG_PRESENT)
#include "sl_component_catalog.h"
#endif
#include "sl_system_init.h"
#include "sl_power_manager.h"
#include "app.h"
#if defined(SL_CATALOG_KERNEL_PRESENT)
#include "sl_system_kernel.h"
#else
#include "sl_system_process_action.h"
#endif
int main(void)
{
// Initialize Silicon Labs device, system, service(s) and protocol stack(s).
// Note that if the kernel is present, processing task(s) will be created by
// this call.
sl_system_init();
// Initialize the application.
app_init();
#if defined(SL_CATALOG_KERNEL_PRESENT)
// Start the kernel. Task(s) created in app_init() will start running.
sl_system_kernel_start();
#else
do {
// Do not remove this call: Silicon Labs components process action routine
// must be called from the super loop.
sl_system_process_action();
// Application process.
app_process_action();
// Let the CPU go to sleep if the system allow it.
sl_power_manager_sleep();
} while (1);
#endif // SL_CATALOG_KERNEL_PRESENT
}
Functions#
Start the kernel.
Initialize Silicon Labs products.
System processing action.
Function Documentation#
sl_system_kernel_start#
void sl_system_kernel_start (void )
Start the kernel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_system_init#
void sl_system_init (void )
Initialize Silicon Labs products.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_system_process_action#
void sl_system_process_action (void )
System processing action.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |