UARTDRV - UART Driver#
Universal Asynchronous Receiver/Transmitter Driver.
The source files for the UART driver library, uartdrv.c and uartdrv.h, are in the emdrv/uartdrv folder.
Introduction#
The UART driver supports the UART capabilities of the USART, UART, and LEUART peripherals. The driver is fully reentrant and supports multiple driver instances. The driver does not buffer or queue data. However, it queues UART transmit and receive operations. Both blocking and non-blocking transfer functions are available. Non-blocking transfer functions report transfer completion with callback functions. Transfers are done using DMA. Simple direct/forced transmit and receive functions are also available. Note that these functions are blocking and not suitable for low energy applications because they use CPU polling.
UART hardware flow control (CTS/RTS) is fully supported by the driver. UART software flow control (XON/XOFF) is partially supported by the driver. For more information about flow control support, see Flow Control Support.
Note
Transfer completion callback functions are called from within the DMA interrupt handler with interrupts disabled.
Configuration Options#
Some properties of the UARTDRV driver are compile-time configurable. These properties are set in a uartdrv_config.h file. A template for this file, containing default values, is in the emdrv/config folder. To configure UARTDRV for your application, provide a custom configuration file, or override the defines on the compiler command line. These are the available configuration parameters with default values defined.
// Set to 1 to enable hardware flow control.
#define EMDRV_UARTDRV_FLOW_CONTROL_ENABLE 1
// Maximum number of driver instances.
#define EMDRV_UARTDRV_MAX_DRIVER_INSTANCES 4
// UART software flow control code: request peer to start Tx.
#define UARTDRV_FC_SW_XON 0x11
// UART software flow control code: request peer to stop Tx.
#define UARTDRV_FC_SW_XOFF 0x13
The properties of each UART driver instance are set at run-time via the UARTDRV_InitUart_t data structure input parameter to the UARTDRV_InitUart() function for UART and USART peripherals, and the UARTDRV_InitLeuart_t data structure input parameter to the UARTDRV_InitLeuart() function for LEUART peripherals.
The API#
This section contains brief descriptions of the functions in the API. For more information on input and output parameters and return values, click on the hyperlinked function names. Most functions return an error code, ECODE_EMDRV_UARTDRV_OK is returned on success, see ecode.h and uartdrv.h for other error codes.
The application code must include uartdrv.h header file.
UARTDRV_InitUart(), UARTDRV_InitLeuart() and UARTDRV_DeInit()
These functions initialize and deinitialize the UARTDRV driver. Typically, UARTDRV_InitUart() (for UART/USART) or UARTDRV_InitLeuart() (for LEUART) are called once in the startup code.
UARTDRV_GetReceiveStatus() and UARTDRV_GetTransmitStatus()
Query the status of a current transmit or receive operations. Reports number of items (frames) transmitted and remaining.
UARTDRV_GetReceiveDepth() and UARTDRV_GetTransmitDepth()
Get the number of queued receive or transmit operations.
UARTDRV_Transmit(), UARTDRV_Receive()
UARTDRV_TransmitB(), UARTDRV_ReceiveB()
UARTDRV_ForceTransmit() and UARTDRV_ForceReceive()
Blocking and non-blocking transfer functions are included. The blocking versions have an uppercase B (for Blocking) at the end of their function name. Blocking functions do not return before the transfer is complete. The non-blocking functions signal a transfer completion with a callback function. UARTDRV_ForceTransmit() and UARTDRV_ForceReceive() are also blocking. These two functions access the UART peripheral directly without using DMA or interrupts. UARTDRV_ForceTransmit() does not respect flow control. UARTDRV_ForceReceive() forces RTS low.
UARTDRV_Abort()
Abort current transmit or receive operations and remove all queued operations.
UARTDRV_FlowControlSet(), UARTDRV_FlowControlGetSelfStatus(), UARTDRV_FlowControlSetPeerStatus() and UARTDRV_FlowControlGetPeerStatus()
Set and get flow control status of self or peer device. Note that the return value from these two functions depends on the flow control mode set by UARTDRV_FlowControlSet(), UARTDRV_InitUart(), or UARTDRV_InitLeuart().
UARTDRV_FlowControlIgnoreRestrain()
Enables transmission when restrained by flow control.
UARTDRV_PauseTransmit() and UARTDRV_ResumeTransmit()
Pause a currently active transmit operation by preventing the DMA from loading the UART FIFO. Will not override HW flow control state (if applicable), but can be used in conjunction.
Flow Control Support#
If UART flow control is not required, make sure that EMDRV_UARTDRV_FLOW_CONTROL_ENABLE is set to 0. This reduces the code size and complexity of the driver.
Both hardware and software flow control are supported. To enable either of these, set EMDRV_UARTDRV_FLOW_CONTROL_ENABLE to 1 in uartdrv_config.h.
Hardware Flow Control#
UART hardware flow control uses two additional pins for flow control handshaking, the clear-to-send (CTS) and ready-to-send (RTS) pins. RTS is an output and CTS is an input. These are active-low signals. When CTS is high, the UART transmitter should stop sending frames. A receiver should set RTS high when it is no longer capable of receiving data.
Peripheral Hardware Flow Control#
Newer devices natively support CTS/RTS in the USART peripheral hardware. To enable hardware flow control, perform the following steps:
Set EMDRV_UARTDRV_FLOW_CONTROL_ENABLE to 1.
In the UARTDRV_InitUart_t struct passed to UARTDRV_InitUart(), set UARTDRV_InitUart_t.fcType = uartdrvFlowControlHwUart.
Define the pins for CTS and RTS by setting ctsPort, ctsPin, rtsPort and rtsPin in the init struct.
Also define the CTS and RTS locations by setting portLocationCts and portLocationRts in the init struct.
GPIO Hardware Flow Control#
To support hardware flow control on devices that don't have UART CTS/RTS hardware support, the driver includes the GPIOINT driver to emulate a hardware implementation of UART CTS/RTS flow control on these devices.
To enable hardware flow control, perform the following steps:
Set EMDRV_UARTDRV_FLOW_CONTROL_ENABLE to 1.
UART/USART: In the UARTDRV_InitUart_t struct passed to UARTDRV_InitUart(), set UARTDRV_InitUart_t.fcType = uartdrvFlowControlHw.
LEUART: In the UARTDRV_InitLeuart_t struct passed to UARTDRV_InitLeuart(), set UARTDRV_InitLeuart_t::fcType = uartdrvFlowControlHw.
Define the pins for CTS and RTS by setting ctsPort, ctsPin, rtsPort and rtsPin in the same init struct.
Note
Because of the limitations in GPIO interrupt hardware, you cannot select CTS pins in multiple driver instances with the same pin number. For example, pin A0 and B0 cannot serve as CTS pins in two concurrent driver instances.
RTS is set high whenever there are no Rx operations queued. The UART transmitter is halted when the CTS pin goes high. The transmitter completes the current frame before halting. DMA transfers are also halted.
Software Flow Control#
UART software flow control uses in-band signaling, meaning the receiver sends special flow control characters to the transmitter and thereby removes the need for dedicated wires for flow control. The two symbols UARTDRV_FC_SW_XON and UARTDRV_FC_SW_XOFF are defined in uartdrv_config.h.
To enable support for software flow control, perform the following steps:
Set EMDRV_UARTDRV_FLOW_CONTROL_ENABLE to 1.
UART/USART: In the UARTDRV_InitUart_t structure passed to UARTDRV_InitUart(), set UARTDRV_InitUart_t.fcType = uartdrvFlowControlSw.
LEUART: In the UARTDRV_InitLeuart_t structure passed to UARTDRV_InitLeuart(), set UARTDRV_InitLeuart_t::fcType = uartdrvFlowControlSw.
Note
Software flow control is partial only.
The application must monitor buffers and make decisions on when to send XON/ XOFF. XON/XOFF can be sent to the peer using UARTDRV_FlowControlSet(). Though UARTDRV_FlowControlSet() will pause the active transmit operation to send a flow control character, there is no way to guarantee the order. If the application implements a specific packet format where the flow control codes may appear only in fixed positions, the application should not use UARTDRV_FlowControlSet() but implement read and write of XON/XOFF into packet buffers. If the application code fully implements all the flow control logic, EMDRV_UARTDRV_FLOW_CONTROL_ENABLE should be set to 0 to reduce code space.
Example#
Modules#
Enumerations#
UARTDRV Flow Control method.
Flow Control state.
Transfer abort type.
Typedefs#
A UART transfer count.
A UART status return type. Bitfield of UARTDRV_STATUS_* values.
UARTDRV transfer completion callback function.
Handle pointer.
Functions#
Initialize a EUART driver instance.
Deinitialize a UART driver instance.
Return the status of the UART peripheral associated with a given handle.
Check the status of the UART and gather information about any ongoing receive operations.
Check the status of the UART and gather information about any ongoing transmit operations.
Return the number of queued receive operations.
Returns the number of queued transmit operations.
Start a non-blocking transmit.
Start a non-blocking receive.
Start a blocking transmit.
Start a blocking receive.
Direct transmit without interrupts or callback.
Direct receive without interrupts or callback.
Abort ongoing UART transfers.
Pause an ongoing transmit operation.
Resume a paused transmit operation.
Check the self flow control status.
Check the peer's flow control status.
Set UART flow control state.
Set peer UART flow control state.
Enable transmission when restrained by flow control.
Macros#
Macros to define FIFO and buffer queues.
Enumeration Documentation#
UARTDRV_FlowControlType_t#
UARTDRV_FlowControlType_t
UARTDRV Flow Control method.
| Enumerator | |
|---|---|
| uartdrvFlowControlNone | None. |
| uartdrvFlowControlSw | Software XON/XOFF. |
| uartdrvFlowControlHw | nRTS/nCTS hardware handshake |
| uartdrvFlowControlHwUart | UART peripheral controls nRTS/nCTS. |
UARTDRV_FlowControlState_t#
UARTDRV_FlowControlState_t
Flow Control state.
| Enumerator | |
|---|---|
| uartdrvFlowControlOn | XON or nRTS/nCTS low. |
| uartdrvFlowControlOff | XOFF or nRTS/nCTS high. |
| uartdrvFlowControlAuto | This driver controls the state. |
UARTDRV_AbortType_t#
UARTDRV_AbortType_t
Transfer abort type.
| Enumerator | |
|---|---|
| uartdrvAbortTransmit | Abort current and queued transmit operations. |
| uartdrvAbortReceive | Abort current and queued receive operations. |
| uartdrvAbortAll | Abort all current and queued operations. |
Typedef Documentation#
UARTDRV_Status_t#
typedef uint32_t UARTDRV_Status_t
A UART status return type. Bitfield of UARTDRV_STATUS_* values.
UARTDRV_Callback_t#
typedef void(* UARTDRV_Callback_t) (struct UARTDRV_HandleData *handle, Ecode_t transferStatus, uint8_t *data, UARTDRV_Count_t transferCount) )(struct UARTDRV_HandleData *handle, Ecode_t transferStatus, uint8_t *data, UARTDRV_Count_t transferCount)
UARTDRV transfer completion callback function.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | handle | The UARTDRV device handle used to start the transfer. | |
| [in] | transferStatus | Completion status of the transfer operation. | |
| [in] | data | A pointer to the transfer data buffer. | |
| [in] | transferCount | A number of bytes transferred. |
Called when a transfer is complete. An application should check the transferStatus and itemsTransferred values.
Function Documentation#
UARTDRV_InitLeuart#
Ecode_t UARTDRV_InitLeuart (UARTDRV_Handle_t handle, const UARTDRV_InitLeuart_t * initData)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | N/A | handle | |
| const UARTDRV_InitLeuart_t * | N/A | initData |
UARTDRV_InitEuart#
Ecode_t UARTDRV_InitEuart (UARTDRV_Handle_t handle, const UARTDRV_InitEuart_t * initData)
Initialize a EUART driver instance.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [out] | handle | Pointer to a UARTDRV handle, refer to UARTDRV_Handle_t. |
| const UARTDRV_InitEuart_t * | [in] | initData | Pointer to an initialization data structure, refer to UARTDRV_InitEuart_t. |
Returns
ECODE_EMDRV_UARTDRV_OK on success. On failure an appropriate UARTDRV Ecode_t is returned.
UARTDRV_DeInit#
Ecode_t UARTDRV_DeInit (UARTDRV_Handle_t handle)
Deinitialize a UART driver instance.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
Returns
ECODE_EMDRV_UARTDRV_OK on success. On failure, an appropriate UARTDRV Ecode_t is returned.
UARTDRV_GetPeripheralStatus#
UARTDRV_Status_t UARTDRV_GetPeripheralStatus (UARTDRV_Handle_t handle)
Return the status of the UART peripheral associated with a given handle.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
Returns
UART status value
UARTDRV_GetReceiveStatus#
UARTDRV_Status_t UARTDRV_GetReceiveStatus (UARTDRV_Handle_t handle, uint8_t ** buffer, UARTDRV_Count_t * itemsReceived, UARTDRV_Count_t * itemsRemaining)
Check the status of the UART and gather information about any ongoing receive operations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
| uint8_t ** | [out] | buffer | Pointer to the current data buffer. |
| UARTDRV_Count_t * | [out] | itemsReceived | Current bytes received count. |
| UARTDRV_Count_t * | [out] | itemsRemaining | Current bytes remaining count. |
Returns
UART status.
UARTDRV_GetTransmitStatus#
UARTDRV_Status_t UARTDRV_GetTransmitStatus (UARTDRV_Handle_t handle, uint8_t ** buffer, UARTDRV_Count_t * itemsSent, UARTDRV_Count_t * itemsRemaining)
Check the status of the UART and gather information about any ongoing transmit operations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
| uint8_t ** | [out] | buffer | Pointer to the current data buffer. |
| UARTDRV_Count_t * | [out] | itemsSent | Current bytes sent count. |
| UARTDRV_Count_t * | [out] | itemsRemaining | Current bytes remaining count. |
Returns
UART status.
UARTDRV_GetReceiveDepth#
uint8_t UARTDRV_GetReceiveDepth (UARTDRV_Handle_t handle)
Return the number of queued receive operations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
Returns
The number of queued operations.
UARTDRV_GetTransmitDepth#
uint8_t UARTDRV_GetTransmitDepth (UARTDRV_Handle_t handle)
Returns the number of queued transmit operations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
Returns
The number of queued operations.
UARTDRV_Transmit#
Ecode_t UARTDRV_Transmit (UARTDRV_Handle_t handle, uint8_t * data, UARTDRV_Count_t count, UARTDRV_Callback_t callback)
Start a non-blocking transmit.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
| uint8_t * | [in] | data | A transmit data buffer. |
| UARTDRV_Count_t | [in] | count | A number of bytes to transmit. |
| UARTDRV_Callback_t | [in] | callback | A transfer completion callback. |
Returns
ECODE_EMDRV_UARTDRV_OK on success.
UARTDRV_Receive#
Ecode_t UARTDRV_Receive (UARTDRV_Handle_t handle, uint8_t * data, UARTDRV_Count_t count, UARTDRV_Callback_t callback)
Start a non-blocking receive.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
| uint8_t * | [in] | data | A receive data buffer. |
| UARTDRV_Count_t | [in] | count | A number of bytes received. |
| UARTDRV_Callback_t | [in] | callback | A transfer completion callback. |
Returns
ECODE_EMDRV_UARTDRV_OK on success.
UARTDRV_TransmitB#
Ecode_t UARTDRV_TransmitB (UARTDRV_Handle_t handle, uint8_t * data, UARTDRV_Count_t count)
Start a blocking transmit.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
| uint8_t * | [in] | data | A transmit data buffer. |
| UARTDRV_Count_t | [in] | count | A number of bytes to transmit. |
Returns
ECODE_EMDRV_UARTDRV_OK on success.
UARTDRV_ReceiveB#
Ecode_t UARTDRV_ReceiveB (UARTDRV_Handle_t handle, uint8_t * data, UARTDRV_Count_t count)
Start a blocking receive.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
| uint8_t * | [in] | data | A receive data buffer. |
| UARTDRV_Count_t | [in] | count | A number of bytes received. |
Returns
ECODE_EMDRV_UARTDRV_OK on success.
UARTDRV_ForceTransmit#
Ecode_t UARTDRV_ForceTransmit (UARTDRV_Handle_t handle, uint8_t * data, UARTDRV_Count_t count)
Direct transmit without interrupts or callback.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
| uint8_t * | [in] | data | Pointer to the buffer. |
| UARTDRV_Count_t | [in] | count | A number of bytes to transmit. |
This is a blocking function. that ignores flow control if enabled.
Returns
ECODE_EMDRV_UARTDRV_OK on success.
UARTDRV_ForceReceive#
UARTDRV_Count_t UARTDRV_ForceReceive (UARTDRV_Handle_t handle, uint8_t * data, UARTDRV_Count_t maxCount)
Direct receive without interrupts or callback.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
| uint8_t * | [in] | data | pointer to buffer. |
| UARTDRV_Count_t | [in] | maxCount | Maximum number of bytes to receive. |
This is a blocking function.
Returns
Number of bytes received.
UARTDRV_Abort#
Ecode_t UARTDRV_Abort (UARTDRV_Handle_t handle, UARTDRV_AbortType_t type)
Abort ongoing UART transfers.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
| UARTDRV_AbortType_t | [in] | type | Abort type – whether to abort only Tx, only Rx, or both. |
All ongoing or queued operations of the given abort type will be aborted.
Returns
ECODE_EMDRV_UARTDRV_OK on success, ECODE_EMDRV_UARTDRV_IDLE if the UART is idle. On failure, an appropriate UARTDRV Ecode_t is returned.
UARTDRV_PauseTransmit#
Ecode_t UARTDRV_PauseTransmit (UARTDRV_Handle_t handle)
Pause an ongoing transmit operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
Returns
ECODE_EMDRV_UARTDRV_OK on success. On failure, an appropriate UARTDRV Ecode_t is returned.
UARTDRV_ResumeTransmit#
Ecode_t UARTDRV_ResumeTransmit (UARTDRV_Handle_t handle)
Resume a paused transmit operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
Returns
ECODE_EMDRV_UARTDRV_OK on success. On failure, an appropriate UARTDRV Ecode_t is returned.
UARTDRV_FlowControlGetSelfStatus#
UARTDRV_FlowControlState_t UARTDRV_FlowControlGetSelfStatus (UARTDRV_Handle_t handle)
Check the self flow control status.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
Returns
Returns uartdrvFlowControlOn if requesting to send.
UARTDRV_FlowControlGetPeerStatus#
UARTDRV_FlowControlState_t UARTDRV_FlowControlGetPeerStatus (UARTDRV_Handle_t handle)
Check the peer's flow control status.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
Returns
Returns uartdrvFlowControlOn if clear to send.
UARTDRV_FlowControlSet#
Ecode_t UARTDRV_FlowControlSet (UARTDRV_Handle_t handle, UARTDRV_FlowControlState_t state)
Set UART flow control state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
| UARTDRV_FlowControlState_t | [in] | state | Flow control state. |
Set nRTS pin if hardware flow control is enabled. Send XON/XOFF if software flow control is enabled.
Returns
ECODE_EMDRV_UARTDRV_OK on success.
UARTDRV_FlowControlSetPeerStatus#
Ecode_t UARTDRV_FlowControlSetPeerStatus (UARTDRV_Handle_t handle, UARTDRV_FlowControlState_t state)
Set peer UART flow control state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
| UARTDRV_FlowControlState_t | [in] | state | Flow control state. |
Pause/resume transmit accordingly. Only for manual software flow control.
Returns
ECODE_EMDRV_UARTDRV_OK on success.
UARTDRV_FlowControlIgnoreRestrain#
Ecode_t UARTDRV_FlowControlIgnoreRestrain (UARTDRV_Handle_t handle)
Enable transmission when restrained by flow control.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| UARTDRV_Handle_t | [in] | handle | Pointer to a UART driver handle. |
Returns
ECODE_EMDRV_UARTDRV_OK on success.