LCD Controller Initialization structure.

Public Attributes#

bool

Enable controller at end of initialization.

Mux configuration.

Bias configuration.

Wave configuration.

Mode of operation.

uint8_t

Frame rate divider.

int

Contrast level.

uint32_t

Clock Prescaler.

Public Attribute Documentation#

enable#

bool LCD_Init_TypeDef::enable

Enable controller at end of initialization.


Definition at line 373 of file platform/emlib/inc/em_lcd.h

mux#

LCD_Mux_TypeDef LCD_Init_TypeDef::mux

Mux configuration.


Definition at line 375 of file platform/emlib/inc/em_lcd.h

bias#

LCD_Bias_TypeDef LCD_Init_TypeDef::bias

Bias configuration.


Definition at line 377 of file platform/emlib/inc/em_lcd.h

wave#

LCD_Wave_TypeDef LCD_Init_TypeDef::wave

Wave configuration.


Definition at line 379 of file platform/emlib/inc/em_lcd.h

mode#

LCD_Mode_Typedef LCD_Init_TypeDef::mode

Mode of operation.


Definition at line 388 of file platform/emlib/inc/em_lcd.h

chargeRedistribution#

LCD_ChargeRedistribution_TypeDef LCD_Init_TypeDef::chargeRedistribution

Charge redistribution cycles.


Definition at line 390 of file platform/emlib/inc/em_lcd.h

frameRateDivider#

uint8_t LCD_Init_TypeDef::frameRateDivider

Frame rate divider.


Definition at line 392 of file platform/emlib/inc/em_lcd.h

contrastLevel#

int LCD_Init_TypeDef::contrastLevel

Contrast level.


Definition at line 394 of file platform/emlib/inc/em_lcd.h

clockPrescaler#

uint32_t LCD_Init_TypeDef::clockPrescaler

Clock Prescaler.


Definition at line 397 of file platform/emlib/inc/em_lcd.h