LFRCO Initialization#
Initialize the LFRCO oscillator.
Initialize the low frequency RC oscillator. On Series 2 devices with precision mode support, the precision mode is configured in the configuration header sl_device_init_lfrco_config.h. On other devices, there is nothing to configure.
If using Simplicity Studio, this configuration header is also configurable through the Project Configurator, by selecting the "Device Init: LFRCO" configuration component.
Functions#
sl_status_t
sl_device_init_lfrco(void)
Initialize LFRCO.
Function Documentation#
sl_device_init_lfrco#
sl_status_t sl_device_init_lfrco (void )
Initialize LFRCO.
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Initialize the low frequency RC oscillator. On devices that support high precision mode, this function configures the precision mode based on the configuration option SL_DEVICE_INIT_LFRCO_PRECISION.
Returns
Status code
Return values
SL_STATUS_OK: LFRCO initialized successfully