LED#
Sample API funtions for controlling LEDs.
When specifying an LED to use, always use the BOARDLEDx definitions that are defined within the BOARD_HEADER.
See led.h for source code.
Typedefs#
Ensures that the definitions from the BOARD_HEADER are always used as parameters to the LED functions.
Functions#
Configures GPIOs pertaining to the control of LEDs.
Atomically wraps an XOR or similar operation for a single GPIO pin attached to an LED.
Turns on (sets) a GPIO pin connected to an LED so that the LED turns on.
Turns off (clears) a GPIO pin connected to an LED, which turns off the LED.
Called by the stack to indicate activity over the radio (for both transmission and reception).
Typedef Documentation#
HalBoardLed#
typedef enum HalBoardLedPins HalBoardLed
Ensures that the definitions from the BOARD_HEADER are always used as parameters to the LED functions.
Function Documentation#
halInternalInitLed#
void halInternalInitLed (void )
Configures GPIOs pertaining to the control of LEDs.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
halToggleLed#
void halToggleLed (HalBoardLed led)
Atomically wraps an XOR or similar operation for a single GPIO pin attached to an LED.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| HalBoardLed | N/A | led | Identifier (from BOARD_HEADER) for the LED to be toggled.  | 
halSetLed#
void halSetLed (HalBoardLed led)
Turns on (sets) a GPIO pin connected to an LED so that the LED turns on.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| HalBoardLed | N/A | led | Identifier (from BOARD_HEADER) for the LED to turn on.  | 
halClearLed#
void halClearLed (HalBoardLed led)
Turns off (clears) a GPIO pin connected to an LED, which turns off the LED.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| HalBoardLed | N/A | led | Identifier (from BOARD_HEADER) for the LED to turn off.  | 
halStackIndicateActivity#
void halStackIndicateActivity (bool turnOn)
Called by the stack to indicate activity over the radio (for both transmission and reception).
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| bool | N/A | turnOn | See Usage.  | 
It is called once with turnOn true and shortly thereafter with turnOn false.
Typically does something interesting, such as change the state of an LED.