This structure defines a variety of information about the attached external EEPROM device.

Public Attributes#

uint32_t

The version of this data structure.

uint16_t

A bitmask describing the capabilites of this particular external EEPROM.

uint16_t

Maximum time it takes to erase a page.

uint16_t

Maximum time it takes to erase the entire part.

uint32_t

The size of a single erasable page in bytes.

uint32_t

The total size of the external EEPROM in bytes.

char *

Pointer to a string describing the attached external EEPROM.

uint8_t

The number of bytes in a word for the external EEPROM.

Public Attribute Documentation#

version#

uint32_t HalEepromInformationType::version

The version of this data structure.


capabilitiesMask#

uint16_t HalEepromInformationType::capabilitiesMask

A bitmask describing the capabilites of this particular external EEPROM.


pageEraseMs#

uint16_t HalEepromInformationType::pageEraseMs

Maximum time it takes to erase a page.

(in 1024Hz Milliseconds)


partEraseTime#

uint16_t HalEepromInformationType::partEraseTime

Maximum time it takes to erase the entire part.

(in 1024Hz Milliseconds). Can be changed to be in seconds using EEPROM_CAPABILITIES_PART_ERASE_SECONDS


pageSize#

uint32_t HalEepromInformationType::pageSize

The size of a single erasable page in bytes.


partSize#

uint32_t HalEepromInformationType::partSize

The total size of the external EEPROM in bytes.


partDescription#

char* HalEepromInformationType::partDescription

Pointer to a string describing the attached external EEPROM.


wordSizeBytes#

uint8_t HalEepromInformationType::wordSizeBytes

The number of bytes in a word for the external EEPROM.