Struct representing energy mode transition event information.
Public Attributes#
Mask of the transitions on which the callback should be called.
Function that must be called when the event occurs.
Public Attribute Documentation#
event_mask#
const sl_power_manager_em_transition_event_t sl_power_manager_em_transition_event_info_t::event_mask
Mask of the transitions on which the callback should be called.
on_event#
const sl_power_manager_em_transition_on_event_t sl_power_manager_em_transition_event_info_t::on_event
Function that must be called when the event occurs.