HFXO initialization structure.
Initialization values should be obtained from a configuration tool, application note or crystal data sheet. 
Public Attributes#
Core bias change timeout.
Steady state timeout duration for first lock.
Steady state timeout duration.
XO pin startup tuning capacitance.
XI pin startup tuning capacitance.
Core bias startup current.
Core bias intermediate startup current.
Core degeneration control.
Fixed tuning capacitance on XI/XO.
Tuning capacitance on XO.
Tuning capacitance on XI.
Core bias current.
Enable XI internal DC bias.
Oscillator mode.
Force XO pin to ground.
Force XI pin to ground.
Disable on-demand requests.
Force oscillator enable.
Lock register access.
Public Attribute Documentation#
timeoutCbLsb#
CMU_HfxoCbLsbTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutCbLsb
Core bias change timeout.
timeoutSteadyFirstLock#
CMU_HfxoSteadyStateTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutSteadyFirstLock
Steady state timeout duration for first lock.
timeoutSteady#
CMU_HfxoSteadyStateTimeout_TypeDef CMU_HFXOInit_TypeDef::timeoutSteady
Steady state timeout duration.
imCoreBiasStartup#
uint8_t CMU_HFXOInit_TypeDef::imCoreBiasStartup
Core bias intermediate startup current.
ctuneFixAna#
CMU_HfxoCtuneFixCap_TypeDef CMU_HFXOInit_TypeDef::ctuneFixAna
Fixed tuning capacitance on XI/XO.