You are viewing documentation for version:
LFXO initialization structure.
Initialization values should be obtained from a configuration tool, application note or crystal data sheet.
Public Attributes#
uint8_t
Internal capacitance tuning.
bool
EM4 wakeup on failure enable.
bool
Oscillator failure detection enable.
bool
Disable on-demand requests.
Public Attribute Documentation#
gain#
uint8_t CMU_LFXOInit_TypeDef::gain
Startup gain.
capTune#
uint8_t CMU_LFXOInit_TypeDef::capTune
Internal capacitance tuning.
timeout#
CMU_LfxoStartupDelay_TypeDef CMU_LFXOInit_TypeDef::timeout
Startup delay.
mode#
CMU_LfxoOscMode_TypeDef CMU_LFXOInit_TypeDef::mode
Oscillator mode.
highAmplitudeEn#
bool CMU_LFXOInit_TypeDef::highAmplitudeEn
High amplitude enable.
agcEn#
bool CMU_LFXOInit_TypeDef::agcEn
AGC enable.
failDetEM4WUEn#
bool CMU_LFXOInit_TypeDef::failDetEM4WUEn
EM4 wakeup on failure enable.
failDetEn#
bool CMU_LFXOInit_TypeDef::failDetEn
Oscillator failure detection enable.
disOnDemand#
bool CMU_LFXOInit_TypeDef::disOnDemand
Disable on-demand requests.
forceEn#
bool CMU_LFXOInit_TypeDef::forceEn
Force oscillator enable.
regLock#
bool CMU_LFXOInit_TypeDef::regLock
Lock register access.