You are viewing documentation for version:
BURTC initialization structure for Series 2 devices.
Public Attributes#
bool
Start BURTC after initialization.
bool
If true, counter will keep running under debug halt.
bool
Set if Compare Value 0 is also top value (counter restart)
bool
Enable EM4 wakeup on compare match.
bool
Enable EM4 wakeup on counter overflow.
Public Attribute Documentation#
start#
bool BURTC_Init_TypeDef::start
Start BURTC after initialization.
debugRun#
bool BURTC_Init_TypeDef::debugRun
If true, counter will keep running under debug halt.
clkDiv#
uint32_t BURTC_Init_TypeDef::clkDiv
Clock divider.
Supported range is 1-32768
compare0Top#
bool BURTC_Init_TypeDef::compare0Top
Set if Compare Value 0 is also top value (counter restart)
em4comp#
bool BURTC_Init_TypeDef::em4comp
Enable EM4 wakeup on compare match.
em4overflow#
bool BURTC_Init_TypeDef::em4overflow
Enable EM4 wakeup on counter overflow.