EUSART - Extended USART#
Extended Universal Synchronous/Asynchronous Receiver/Transmitter.
Introduction#
This module contains functions to control the Enhanced Universal Synchronous / Asynchronous Receiver / Transmitter controller(s) (EUSART) peripheral of Silicon Labs' 32-bit MCUs and SoCs. EUSART can be used as a UART and can, therefore, be connected to an external transceiver to communicate with another host using the serial link.
It supports full duplex asynchronous UART communication as well as RS-485, SPI, MicroWire, and 3-wire. It can also interface with ISO7816 Smart-Cards, and IrDA devices.
EUSART has a wide selection of operating modes, frame formats, and baud rates. All features are supported through the API of this module.
This module does not support DMA configuration. UARTDRV and SPIDRV drivers provide full support for DMA and more.
Example#
EUSART Async TX example:
{
  EUSART_UartInit_TypeDef init = EUSART_UART_INIT_DEFAULT_HF;
  // Configure the clocks.
  CMU_ClockSelectSet(cmuClock_EUSART0CLK, cmuSelect_EM01GRPCCLK);
  CMU_ClockEnable(cmuClock_EUSART0CLK, true);
  // Initialize the EUSART
  EUSART_UartInitHf(EUSART0, &init);
  EUSART_Tx(EUSART0, data);
}
EUSART Sync SPI Transaction example:
{
  EUSART_SpiInit_TypeDef init_master = EUSART_SPI_MASTER_INIT_DEFAULT_HF;
  // Configure the clocks.
  CMU_ClockSelectSet(cmuClock_EM01GRPCCLK, cmuSelect_HFRCODPLL);
  CMU_ClockEnable(cmuClock_EUSART1, true);
  CMU_ClockEnable(cmuClock_GPIO, true);
  //Configure the SPI ports
  GPIO_PinModeSet(sclk_port, sclk_pin, gpioModePushPull, 0);
  GPIO_PinModeSet(mosi_port, mosi_pin, gpioModePushPull, 0);
  GPIO_PinModeSet(mosi_port, miso_pin, gpioModeInput, 0);
  // Connect EUSART to ports
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].TXROUTE = (mosi_port << _GPIO_EUSART_TXROUTE_PORT_SHIFT)
                                                   | (mosi_pin << _GPIO_EUSART_TXROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].RXROUTE = (miso_port << _GPIO_EUSART_RXROUTE_PORT_SHIFT)
                                                   | (miso_pin << _GPIO_EUSART_RXROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].SCLKROUTE = (sclk_port << _GPIO_EUSART_SCLKROUTE_PORT_SHIFT)
                                                   | (sclk_pin << _GPIO_EUSART_SCLKROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].ROUTEEN = GPIO_EUSART_ROUTEEN_TXPEN | GPIO_EUSART_ROUTEEN_SCLKPEN;
  // Initialize the EUSART
  EUSART_SpiInit(EUSART1, &init_master);
  EUSART_Spi_TxRx(EUSART1, data);
}
EM2 guidelines for non EM2-Capable instances#
Note
- EUSART instances located in the PD1 power domain are non EM2-capable. The EUSART_EM2_CAPABLE() and EUSART_NOT_EM2_CAPABLE() macros can be used to determine whether or not a EUSART instance is EM2-Capable. 
Follow theses steps when entering in EM2:
- Wait for the current transaction to complete with TXCIF interrupt 
- Disable TX and RX using TXDIS and RXDIS cmd 
- Poll for EUSARTn_SYNCBUSY.TXDIS and EUSARTn_SYNCBUSY.RXDIS to go low 
- Wait for EUSARTn_STATUS.TXENS and EUSARTn_STATUS.RXENS to go low 
- Disable SCLKPEN and CSPEN in GPIO if they were previously enabled 
- Enter EM2 
On wakeup from EM2, EUSART transmitter/receiver and relevant GPIO (SCLKPEN and CSPEN) must be re-enabled. For example:
{
  // Enable TX and RX
  EUSART_Enable(EUSART0, eusartEnable);
  BUS_RegMaskedWrite(&GPIO->EUSARTROUTE[EUSART_NUM(EUSART0)].ROUTEEN,
                     _GPIO_EUSART_ROUTEEN_TXPEN_MASK | _GPIO_EUSART_ROUTEEN_SCLKPEN_MASK,
                     GPIO_EUSART_ROUTEEN_TXPEN | GPIO_EUSART_ROUTEEN_SCLKPEN);
}
Modules#
EUSART_SpiAdvancedInit_TypeDef
Enumerations#
Enable selection.
Data bit selection.
Parity selection.
Stop bits selection.
Oversampling selection, used for asynchronous operation.
HW flow control config.
Loopback enable.
Majority vote enable.
Block reception enable.
TX output tristate enable.
IrDA filter enable.
Pulse width selection for IrDA mode.
PRS trigger enable.
IO polarity selection.
Auto TX delay transmission.
RX FIFO Interrupt ans Status Watermark.
TX FIFO Interrupt and Status Watermark.
Clock polarity/phase mode.
Chip select polarity.
Typedefs#
PRS Channel type.
Functions#
Initialize EUSART when used in UART mode with the high frequency clock.
Initialize EUSART when used in UART mode with the low frequency clock.
Initialize EUSART when used in IrDA mode with the high or low frequency clock.
Initialize EUSART when used in SPI mode.
Configure EUSART to its reset state.
Enable/disable EUSART receiver and/or transmitter.
Receive one 8 bit frame, (or part of 9 bit frame).
Receive one 8-16 bit frame with extended information.
Transmit one frame.
Transmit one 8-9 bit frame with extended control.
Transmit one 8-16 bit frame and return received data.
Configure the baudrate (or as close as possible to a specified baudrate).
Get the current baudrate.
Enable/Disable reception operation until the configured start frame is received.
Enable/Disable the tristating of the transmitter output.
Initialize the automatic enabling of transmissions and/or reception using the PRS as a trigger.
Get EUSART STATUS register.
Clear one or more pending EUSART interrupts.
Disable one or more EUSART interrupts.
Enable one or more EUSART interrupts.
Get pending EUSART interrupt flags.
Get enabled and pending EUSART interrupt flags.
Set one or more pending EUSART interrupts from SW.
Macros#
Define EUSART FIFO Depth information.
Default configuration for EUSART initialization structure in UART mode with high-frequency clock.
Default start frame configuration, i.e. feature disabled.
Default configuration for EUSART advanced initialization structure.
Default configuration for EUSART initialization structure in UART mode with low-frequency clock.
Default configuration for EUSART initialization structure in IrDA mode with high-frequency clock.
Default configuration for EUSART initialization structure in IrDA mode with low-frequency clock.
Default advanced configuration for EUSART initialization structure in SPI mode with high-frequency clock.
Default configuration for EUSART initialization structure in SPI master mode with high-frequency clock.
Default configuration for EUSART initialization structure in SPI slave mode with high-frequency clock.
Enumeration Documentation#
EUSART_Enable_TypeDef#
EUSART_Enable_TypeDef
Enable selection.
| Enumerator | |
|---|---|
| eusartDisable | Disable the peripheral. | 
| eusartEnableRx | Enable receiver only, transmitter disabled. | 
| eusartEnableTx | Enable transmitter only, receiver disabled. | 
| eusartEnable | Enable both receiver and transmitter. | 
EUSART_Databits_TypeDef#
EUSART_Databits_TypeDef
Data bit selection.
| Enumerator | |
|---|---|
| eusartDataBits7 | 7 data bits. | 
| eusartDataBits8 | 8 data bits. | 
| eusartDataBits9 | 9 data bits. | 
| eusartDataBits10 | 10 data bits, SPI mode only. | 
| eusartDataBits11 | 11 data bits, SPI mode only. | 
| eusartDataBits12 | 12 data bits, SPI mode only. | 
| eusartDataBits13 | 13 data bits, SPI mode only. | 
| eusartDataBits14 | 14 data bits, SPI mode only. | 
| eusartDataBits15 | 15 data bits, SPI mode only. | 
| eusartDataBits16 | 16 data bits, SPI mode only. | 
EUSART_Parity_TypeDef#
EUSART_Parity_TypeDef
Parity selection.
| Enumerator | |
|---|---|
| eusartNoParity | No parity. | 
| eusartEvenParity | Even parity. | 
| eusartOddParity | Odd parity. | 
EUSART_Stopbits_TypeDef#
EUSART_Stopbits_TypeDef
Stop bits selection.
| Enumerator | |
|---|---|
| eusartStopbits0p5 | 0.5 stop bits. | 
| eusartStopbits1p5 | 1.5 stop bits. | 
| eusartStopbits1 | 1 stop bits. | 
| eusartStopbits2 | 2 stop bits. | 
EUSART_OVS_TypeDef#
EUSART_OVS_TypeDef
Oversampling selection, used for asynchronous operation.
| Enumerator | |
|---|---|
| eusartOVS16 | 16x oversampling (normal). | 
| eusartOVS8 | 8x oversampling. | 
| eusartOVS6 | 6x oversampling. | 
| eusartOVS4 | 4x oversampling. | 
| eusartOVS0 | Oversampling disabled. | 
EUSART_HwFlowControl_TypeDef#
EUSART_HwFlowControl_TypeDef
HW flow control config.
| Enumerator | |
|---|---|
| eusartHwFlowControlNone | No HW Flow Control. | 
| eusartHwFlowControlCts | CTS HW Flow Control. | 
| eusartHwFlowControlRts | RTS HW Flow Control. | 
| eusartHwFlowControlCtsAndRts | CTS and RTS HW Flow Control. | 
EUSART_LoopbackEnable_TypeDef#
EUSART_LoopbackEnable_TypeDef
Loopback enable.
| Enumerator | |
|---|---|
| eusartLoopbackEnable | Enable loopback. | 
| eusartLoopbackDisable | Disable loopback. | 
EUSART_MajorityVote_TypeDef#
EUSART_MajorityVote_TypeDef
Majority vote enable.
| Enumerator | |
|---|---|
| eusartMajorityVoteEnable | Enable majority vote for 16x, 8x and 6x oversampling modes. | 
| eusartMajorityVoteDisable | Disable majority vote for 16x, 8x and 6x oversampling modes. | 
EUSART_BlockRx_TypeDef#
EUSART_BlockRx_TypeDef
Block reception enable.
| Enumerator | |
|---|---|
| eusartBlockRxEnable | Block reception enable, resulting in all incoming frames being discarded. | 
| eusartBlockRxDisable | Block reception disable, resulting in all incoming frames being loaded into the RX FIFO. | 
EUSART_TristateTx_TypeDef#
EUSART_TristateTx_TypeDef
TX output tristate enable.
| Enumerator | |
|---|---|
| eusartTristateTxEnable | Tristates the transmitter output. | 
| eusartTristateTxDisable | Disables tristating of the transmitter output. | 
EUSART_IrDARxFilterEnable_TypeDef#
EUSART_IrDARxFilterEnable_TypeDef
IrDA filter enable.
| Enumerator | |
|---|---|
| eusartIrDARxFilterEnable | Enable filter on demodulator. | 
| eusartIrDARxFilterDisable | Disable filter on demodulator. | 
EUSART_IrDAPulseWidth_Typedef#
EUSART_IrDAPulseWidth_Typedef
Pulse width selection for IrDA mode.
| Enumerator | |
|---|---|
| eusartIrDAPulseWidthOne | IrDA pulse width is 1/16 for OVS=X16 and 1/8 for OVS=X8. | 
| eusartIrDAPulseWidthTwo | IrDA pulse width is 2/16 for OVS=X16 and 2/8 for OVS=X8. | 
| eusartIrDAPulseWidthThree | IrDA pulse width is 3/16 for OVS=X16 and 3/8 for OVS=X8. | 
| eusartIrDAPulseWidthFour | IrDA pulse width is 4/16 for OVS=X16 and 4/8 for OVS=X8. | 
EUSART_PrsTriggerEnable_TypeDef#
EUSART_PrsTriggerEnable_TypeDef
PRS trigger enable.
| Enumerator | |
|---|---|
| eusartPrsTriggerDisable | Disable trigger on both receiver and transmitter. | 
| eusartPrsTriggerEnableRx | Enable receive trigger only, transmit disabled. | 
| eusartPrsTriggerEnableTx | Enable transmit trigger only, receive disabled. | 
| eusartPrsTriggerEnableRxTx | Enable trigger on both receive and transmit. | 
EUSART_InvertIO_TypeDef#
EUSART_InvertIO_TypeDef
IO polarity selection.
| Enumerator | |
|---|---|
| eusartInvertIODisable | Disable inversion on both RX and TX signals. | 
| eusartInvertRxEnable | Invert RX signal, before receiver. | 
| eusartInvertTxEnable | Invert TX signal, after transmitter. | 
| eusartInvertIOEnable | Enable trigger on both receive and transmit. | 
EUSART_AutoTxDelay_TypeDef#
EUSART_AutoTxDelay_TypeDef
Auto TX delay transmission.
| Enumerator | |
|---|---|
| eusartAutoTxDelayNone | Frames are transmitted immediately. | 
| eusartAutoTxDelaySingle | Transmission of new frames is delayed by a single bit period. | 
| eusartAutoTxDelayDouble | Transmission of new frames is delayed by a two bit periods. | 
| eusartAutoTxDelayTripple | Transmission of new frames is delayed by a three bit periods. | 
EUSART_RxFifoWatermark_TypeDef#
EUSART_RxFifoWatermark_TypeDef
RX FIFO Interrupt ans Status Watermark.
| Enumerator | |
|---|---|
| eusartRxFiFoWatermark1Frame | |
| eusartRxFiFoWatermark2Frame | |
| eusartRxFiFoWatermark3Frame | |
| eusartRxFiFoWatermark4Frame | |
| eusartRxFiFoWatermark5Frame | |
| eusartRxFiFoWatermark6Frame | |
| eusartRxFiFoWatermark7Frame | |
| eusartRxFiFoWatermark8Frame | |
| eusartRxFiFoWatermark9Frame | |
| eusartRxFiFoWatermark10Frame | |
| eusartRxFiFoWatermark11Frame | |
| eusartRxFiFoWatermark12Frame | |
| eusartRxFiFoWatermark13Frame | |
| eusartRxFiFoWatermark14Frame | |
| eusartRxFiFoWatermark15Frame | |
| eusartRxFiFoWatermark16Frame | |
EUSART_TxFifoWatermark_TypeDef#
EUSART_TxFifoWatermark_TypeDef
TX FIFO Interrupt and Status Watermark.
| Enumerator | |
|---|---|
| eusartTxFiFoWatermark1Frame | |
| eusartTxFiFoWatermark2Frame | |
| eusartTxFiFoWatermark3Frame | |
| eusartTxFiFoWatermark4Frame | |
| eusartTxFiFoWatermark5Frame | |
| eusartTxFiFoWatermark6Frame | |
| eusartTxFiFoWatermark7Frame | |
| eusartTxFiFoWatermark8Frame | |
| eusartTxFiFoWatermark9Frame | |
| eusartTxFiFoWatermark10Frame | |
| eusartTxFiFoWatermark11Frame | |
| eusartTxFiFoWatermark12Frame | |
| eusartTxFiFoWatermark13Frame | |
| eusartTxFiFoWatermark14Frame | |
| eusartTxFiFoWatermark15Frame | |
| eusartTxFiFoWatermark16Frame | |
EUSART_ClockMode_TypeDef#
EUSART_ClockMode_TypeDef
Clock polarity/phase mode.
| Enumerator | |
|---|---|
| eusartClockMode0 | Clock idle low, sample on rising edge. | 
| eusartClockMode1 | Clock idle low, sample on falling edge. | 
| eusartClockMode2 | Clock idle high, sample on falling edge. | 
| eusartClockMode3 | Clock idle high, sample on rising edge. | 
EUSART_CsPolarity_TypeDef#
EUSART_CsPolarity_TypeDef
Chip select polarity.
| Enumerator | |
|---|---|
| eusartCsActiveLow | Chip select active low. | 
| eusartCsActiveHigh | Chip select active high. | 
Typedef Documentation#
Function Documentation#
EUSART_UartInitHf#
void EUSART_UartInitHf (EUSART_TypeDef * eusart, const EUSART_UartInit_TypeDef * init)
Initialize EUSART when used in UART mode with the high frequency clock.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| const EUSART_UartInit_TypeDef * | N/A | init | A pointer to the initialization structure. | 
Initialize EUSART when used in UART mode with the high frequency clock.
EUSART_UartInitLf#
void EUSART_UartInitLf (EUSART_TypeDef * eusart, const EUSART_UartInit_TypeDef * init)
Initialize EUSART when used in UART mode with the low frequency clock.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| const EUSART_UartInit_TypeDef * | N/A | init | A pointer to the initialization structure. | 
Initialize EUSART when used in UART mode with the low frequency clock.
Note
- (1) When EUSART oversampling is set to eusartOVS0 (Disable), the peripheral clock frequency must be at least three times higher than the chosen baud rate. In LF, max input clock is 32768 (LFXO or LFRCO), thus 32768 / 3 ~ 9600 baudrate. 
EUSART_IrDAInit#
void EUSART_IrDAInit (EUSART_TypeDef * eusart, const EUSART_IrDAInit_TypeDef * irdaInit)
Initialize EUSART when used in IrDA mode with the high or low frequency clock.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| const EUSART_IrDAInit_TypeDef * | N/A | irdaInit | A pointer to the initialization structure. | 
Initialize EUSART when used in IrDA mode with the high or low frequency clock.
EUSART_SpiInit#
void EUSART_SpiInit (EUSART_TypeDef * eusart, const EUSART_SpiInit_TypeDef * init)
Initialize EUSART when used in SPI mode.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| const EUSART_SpiInit_TypeDef * | N/A | init | A pointer to the initialization structure. | 
Initialize EUSART when used in SPI mode.
EUSART_Reset#
void EUSART_Reset (EUSART_TypeDef * eusart)
Configure EUSART to its reset state.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
Configure EUSART to its reset state.
EUSART_Enable#
void EUSART_Enable (EUSART_TypeDef * eusart, EUSART_Enable_TypeDef enable)
Enable/disable EUSART receiver and/or transmitter.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| EUSART_Enable_TypeDef | N/A | enable | Select the status for the receiver and transmitter. | 
Enable/disable EUSART receiver and/or transmitter.
EUSART_Rx#
uint8_t EUSART_Rx (EUSART_TypeDef * eusart)
Receive one 8 bit frame, (or part of 9 bit frame).
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
Note
- This function is normally used to receive one frame when operating with frame length of 8 bits. See EUSART_RxExt() for reception of 9 bit frames. Notice that possible parity/stop bits are not considered a part of the specified frame bit length. 
- This function will stall if buffer is empty until data is received. 
Returns
- Data received. 
Receive one 8 bit frame, (or part of 9 bit frame).
Note
- (1) Handles the case where the RX Fifo Watermark has been set to N frames, and when N is greater than one. Attempt to read a frame from the RX Fifo. If the read is unsuccessful (i.e. no frames in the RX fifo), the RXFU interrupt flag is set. If the flag is set, wait to read again until the RXFL status flag is set, indicating there are N frames in the RX Fifo, where N is equal to the RX watermark level. Once there are N frames in the Fifo, read and return one frame. For consecutive N-1 reads there will be data available in the Fifo. Therefore, the RXUF interrupt will not be triggered eliminating delays between reads and sending N data frames in "bursts". 
EUSART_RxExt#
uint16_t EUSART_RxExt (EUSART_TypeDef * eusart)
Receive one 8-16 bit frame with extended information.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
Note
- This function is normally used to receive one frame and additional RX status information. 
- This function will stall if buffer is empty until data is received. 
Returns
- Data received and receive status. 
Receive one 8-16 bit frame with extended information.
EUSART_Tx#
void EUSART_Tx (EUSART_TypeDef * eusart, uint8_t data)
Transmit one frame.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| uint8_t | N/A | data | Data to transmit. | 
Note
- Depending on the frame length configuration, 8 (least significant) bits from - dataare transmitted. If the frame length is 9, 8 bits are transmitted from- data. See EUSART_TxExt() for transmitting 9 bit frame with full control of all 9 bits.
- This function will stall if the 4 frame FIFO is full, until the buffer becomes available. 
Transmit one frame.
EUSART_TxExt#
void EUSART_TxExt (EUSART_TypeDef * eusart, uint16_t data)
Transmit one 8-9 bit frame with extended control.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| uint16_t | N/A | data | Data to transmit. | 
Note
- Possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length. 
- This function will stall if buffer is full until the buffer becomes available. 
Transmit one 8-9 bit frame with extended control.
EUSART_Spi_TxRx#
uint16_t EUSART_Spi_TxRx (EUSART_TypeDef * eusart, uint16_t data)
Transmit one 8-16 bit frame and return received data.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| uint16_t | N/A | data | Data to transmit. | 
Returns
- Data received and receive status. 
Note
- SPI master mode only. 
- This function will stall if the TX buffer is full until the buffer becomes available. 
Transmit one 8-16 bit frame and return received data.
EUSART_BaudrateSet#
void EUSART_BaudrateSet (EUSART_TypeDef * eusart, uint32_t refFreq, uint32_t baudrate)
Configure the baudrate (or as close as possible to a specified baudrate).
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| uint32_t | N/A | refFreq | The EUSART reference clock frequency in Hz that will be used. If set to 0, the currently configured peripheral clock is used. | 
| uint32_t | N/A | baudrate | A baudrate to try to achieve. | 
Configure the baudrate (or as close as possible to a specified baudrate).
Note
- (1) When the oversampling is disabled, the peripheral clock frequency must be at least three times higher than the chosen baud rate. 
EUSART_BaudrateGet#
uint32_t EUSART_BaudrateGet (EUSART_TypeDef * eusart)
Get the current baudrate.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
Returns
- The current baudrate. 
Get the current baudrate.
EUSART_RxBlock#
void EUSART_RxBlock (EUSART_TypeDef * eusart, EUSART_BlockRx_TypeDef enable)
Enable/Disable reception operation until the configured start frame is received.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| EUSART_BlockRx_TypeDef | N/A | enable | Select the receiver blocking status. | 
Enable/Disable reception operation until the configured start frame is received.
EUSART_TxTristateSet#
void EUSART_TxTristateSet (EUSART_TypeDef * eusart, EUSART_TristateTx_TypeDef enable)
Enable/Disable the tristating of the transmitter output.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| EUSART_TristateTx_TypeDef | N/A | enable | Select the transmitter tristate status. | 
Enable/Disable the tristating of the transmitter output.
EUSART_PrsTriggerEnable#
void EUSART_PrsTriggerEnable (EUSART_TypeDef * eusart, const EUSART_PrsTriggerInit_TypeDef * init)
Initialize the automatic enabling of transmissions and/or reception using the PRS as a trigger.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| const EUSART_PrsTriggerInit_TypeDef * | N/A | init | Pointer to the initialization structure. | 
Note
- Initialize EUSART with EUSART_UartInitHf() or EUSART_UartInitLf() before enabling the PRS trigger. 
Initialize the automatic enabling of transmissions and/or reception using the PRS as a trigger.
EUSART_StatusGet#
uint32_t EUSART_StatusGet (EUSART_TypeDef * eusart)
Get EUSART STATUS register.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
Returns
- STATUS register value. 
EUSART_IntClear#
void EUSART_IntClear (EUSART_TypeDef * eusart, uint32_t flags)
Clear one or more pending EUSART interrupts.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| uint32_t | N/A | flags | Pending EUSART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn). | 
EUSART_IntDisable#
void EUSART_IntDisable (EUSART_TypeDef * eusart, uint32_t flags)
Disable one or more EUSART interrupts.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| uint32_t | N/A | flags | Pending EUSART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn). | 
EUSART_IntEnable#
void EUSART_IntEnable (EUSART_TypeDef * eusart, uint32_t flags)
Enable one or more EUSART interrupts.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| uint32_t | N/A | flags | Pending EUSART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn). | 
EUSART_IntGet#
uint32_t EUSART_IntGet (EUSART_TypeDef * eusart)
Get pending EUSART interrupt flags.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
Returns
- Pending EUSART interrupt sources. 
EUSART_IntGetEnabled#
uint32_t EUSART_IntGetEnabled (EUSART_TypeDef * eusart)
Get enabled and pending EUSART interrupt flags.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
Useful for handling more interrupt sources in the same interrupt handler.
Returns
- Pending and enabled EUSART interrupt sources. 
EUSART_IntSet#
void EUSART_IntSet (EUSART_TypeDef * eusart, uint32_t flags)
Set one or more pending EUSART interrupts from SW.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| EUSART_TypeDef * | N/A | eusart | Pointer to the EUSART peripheral register block. | 
| uint32_t | N/A | flags | Interrupt source(s) to set to pending. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn). |