Capsense initialization structure.
Public Attributes#
uint32_t
Bias current.
Hysteresis level.
A resistor used in the capacitive sensing circuit.
uint32_t
VDD division factor.
bool
If true, ACMP is enabled after configuration.
Public Attribute Documentation#
biasProg#
uint32_t ACMP_CapsenseInit_TypeDef::biasProg
Bias current.
See the ACMP chapter about bias and response time in the reference manual for details.
hysteresisLevel#
ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel
Hysteresis level.
resistor#
ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor
A resistor used in the capacitive sensing circuit.
For values see the device data sheet.
vrefDiv#
uint32_t ACMP_CapsenseInit_TypeDef::vrefDiv
VDD division factor.
VREFOUT = VREFIN * (VREFDIV / 63). Valid values are in the 0-63 range.