RFF PLL initialization structure.
When using this structure you need to modify the X, Y and N factor and the desired host target frequency to match the components placed on the board (namely the RFFPLL reference clock). X, Y, N values for a 39MHz HFXO:
- Formula for host clock output: frequency = (freq HFXO * dividerN / 2) / dividerY 
- Formula for radio clock output: freq = (freq HFXO * dividerN / 2) / (dividerX / 2) 
Public Attributes#
uint32_t
Host target frequency.
bool
Disable on-demand requests.
bool
Force oscillator enable.
bool
Enable register lock.
uint8_t
Divider Y for digital.
uint8_t
Divider X for Radio.
uint8_t
Feedback divider N.