IrDA Initialization structure.
Public Attributes#
General EUSART initialization structure.
bool
Enable the IrDA low frequency mode. Only RX operation are enabled.
Set to enable filter on IrDA demodulator.
Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.
Public Attribute Documentation#
irDALowFrequencyEnable#
bool EUSART_IrDAInit_TypeDef::irDALowFrequencyEnable
Enable the IrDA low frequency mode. Only RX operation are enabled.
irDARxFilterEnable#
EUSART_IrDARxFilterEnable_TypeDef EUSART_IrDAInit_TypeDef::irDARxFilterEnable
Set to enable filter on IrDA demodulator.
irDAPulseWidth#
EUSART_IrDAPulseWidth_Typedef EUSART_IrDAInit_TypeDef::irDAPulseWidth
Configure the pulse width generated by the IrDA modulator as a fraction of the configured EUSART bit period.