You are viewing documentation for version:
Struct representing an instance of the CLI storage RAM. 
Public Attributes#
The CLI instance associated with this instance. 
char *
The string that define the end of definition. 
size_t
The number of command lines that can be stored in RAM. 
size_t
The next free line in RAM. 
char *
Pointer to the RAM buffer. 
bool
True if the command shell execute when defined. 
bool
True when definition is in progress. 
bool
True when execute is in progress. 
Public Attribute Documentation#
cli_handle#
sl_cli_handle_t cli_storage_ram_t::cli_handle
The CLI instance associated with this instance. 
prompt#
char* cli_storage_ram_t::prompt
The command prompt. 
end_string#
char* cli_storage_ram_t::end_string
The string that define the end of definition. 
ram_size#
size_t cli_storage_ram_t::ram_size
The number of command lines that can be stored in RAM. 
ram_next#
size_t cli_storage_ram_t::ram_next
The next free line in RAM. 
ram_buffer#
char* cli_storage_ram_t::ram_buffer
Pointer to the RAM buffer. 
execute_while_define#
bool cli_storage_ram_t::execute_while_define
True if the command shell execute when defined. 
define_in_progress#
bool cli_storage_ram_t::define_in_progress
True when definition is in progress. 
execute_in_progress#
bool cli_storage_ram_t::execute_in_progress
True when execute is in progress.