TIMER compare/capture initialization structure.

Public Attributes#

Compare/capture channel mode.

Select Compare/Capture channel input.

uint8_t

Sets the watermark level of generation of fifo interrupt and DMA requests.

bool

Compare output initial state.

bool

PRS output configuration.

bool

Enable digital filter.

bool

Invert output from compare/capture channel.

Public Attribute Documentation#

channel_mode#

sl_hal_timer_channel_mode_t sl_hal_timer_channel_config_t::channel_mode

Compare/capture channel mode.


input_type#

sl_hal_timer_channel_input_type_t sl_hal_timer_channel_config_t::input_type

Select Compare/Capture channel input.


compare_match_output_action#

sl_hal_timer_channel_output_action_t sl_hal_timer_channel_config_t::compare_match_output_action

Counter match output action.


compare_underflow_output_action#

sl_hal_timer_channel_output_action_t sl_hal_timer_channel_config_t::compare_underflow_output_action

Counter underflow output action.


compare_overflow_output_action#

sl_hal_timer_channel_output_action_t sl_hal_timer_channel_config_t::compare_overflow_output_action

Counter overflow output action.


input_capture_event#

sl_hal_timer_channel_input_event_t sl_hal_timer_channel_config_t::input_capture_event

Input capture event control.


input_capture_edge#

sl_hal_timer_channel_input_edge_t sl_hal_timer_channel_config_t::input_capture_edge

Input capture edge select.


input_watermark_level#

uint8_t sl_hal_timer_channel_config_t::input_watermark_level

Sets the watermark level of generation of fifo interrupt and DMA requests.


output_initial_state#

bool sl_hal_timer_channel_config_t::output_initial_state

Compare output initial state.

Only used in Output Compare and PWM mode. When true, the compare/PWM output is set high when the counter is disabled. When counting resumes, this value will represent the initial value for the compare/PWM output. If the bit is cleared, the output will be cleared when the counter is disabled.


prs_output#

bool sl_hal_timer_channel_config_t::prs_output

PRS output configuration.

PRS output from a timer can either be a pulse output or a level output that follows the CC out value. if set, prs outputs a level that follows cc out value.


filter#

bool sl_hal_timer_channel_config_t::filter

Enable digital filter.


output_invert#

bool sl_hal_timer_channel_config_t::output_invert

Invert output from compare/capture channel.