PCNT - Pulse Counter#
Example#
The following example demonstrates basic usage of the PCNT peripheral in oversampling single input mode.
void pcnt_basic_example(void)
{
// Configure PCNT with default settings for single input oversampling mode
sl_hal_pcnt_config_t config = SL_HAL_PCNT_CONFIG_DEFAULT(SL_HAL_PCNT_MODE_OVS_SINGLE);
// Initialize PCNT with our configuration
sl_hal_pcnt_init(PCNT0, &config);
// Enable the PCNT peripheral
sl_hal_pcnt_enable(PCNT0);
// Start the main counter
sl_hal_pcnt_start_main_counter(PCNT0);
// Wait for synchronization to complete
sl_hal_pcnt_wait_sync(PCNT0);
// Check if counter is running by reading status
uint32_t status = sl_hal_pcnt_get_status(PCNT0);
bool is_running = status & PCNT_STATUS_CNTRUNNING;
if (is_running) {
// Read current counter value
uint32_t count_initial = sl_hal_pcnt_get_main_counter(PCNT0);
// Optionally set counter to a specific value
uint32_t count_new = count_initial + 10;
sl_hal_pcnt_set_main_counter(PCNT0, count_new);
// Read the updated counter value
uint32_t count_after = sl_hal_pcnt_get_main_counter(PCNT0);
// Application processing...
// Reset the counter when needed
sl_hal_pcnt_reset_counters(PCNT0);
// Counter value should now be 0
count_after = sl_hal_pcnt_get_main_counter(PCNT0);
}
// Stop the counter when done
sl_hal_pcnt_stop_main_counter(PCNT0);
sl_hal_pcnt_wait_sync(PCNT0);
// Verify counter is stopped
status = sl_hal_pcnt_get_status(PCNT0);
is_running = status & PCNT_STATUS_CNTRUNNING;
// Clean up - disable PCNT when no longer needed
sl_hal_pcnt_disable(PCNT0);
}
Modules#
Enumerations#
PCNT mode.
Counter event selection.
Functions#
Initialize the pulse counter (PCNT).
Reset the PCNT to the same state that it was in after a hardware reset.
Enable the PCNT.
Disable PCNT.
Returns if the PCNT module is enabled or not.
Wait for disabling to finish.
Wait for ongoing sync of register(s) to the low-frequency domain to complete.
Get status values for the PCNT.
Enable one or more PCNT interrupts.
Disable one or more PCNT interrupts.
Clear one or more pending PCNT interrupts.
Set one or more pending PCNT interrupts from SW.
Get pending PCNT interrupt flags.
Get enabled and pending PCNT interrupt flags.
Lock PCNT registers.
Unlock PCNT registers.
Set the top value buffer.
Get the top value buffer.
Set the top value.
Get the top value.
Start PCNT main counter.
Stop PCNT main counter.
Set a counter value.
Get the main counter value.
Start PCNT auxiliary counter.
Stop PCNT auxiliary counter.
Get the auxiliary counter value.
Reset PCNT counters.
Macros#
Check if PCNT module is valid.
Return PCNT module max count.
Default configuration for PCNT initialization structure.
Enumeration Documentation#
sl_hal_pcnt_mode_t#
sl_hal_pcnt_mode_t
PCNT mode.
| Enumerator | |
|---|---|
| SL_HAL_PCNT_MODE_OVS_SINGLE | Single input LFACLK oversampling mode (available in EM0-EM3). |
| SL_HAL_PCNT_MODE_EXT_CLK_SINGLE | Externally clocked single input counter mode (available in EM0-EM3). |
| SL_HAL_PCNT_MODE_EXT_CLK_QUAD | Externally clocked quadrature decoder mode (available in EM0-EM3). |
| SL_HAL_PCNT_MODE_OVS_QUAD_1X | LFACLK oversampling quadrature decoder 1X mode (available in EM0-EM3). |
| SL_HAL_PCNT_MODE_OVS_QUAD_2X | LFACLK oversampling quadrature decoder 2X mode (available in EM0-EM3). |
| SL_HAL_PCNT_MODE_OVS_QUAD_4X | LFACLK oversampling quadrature decoder 4X mode (available in EM0-EM3). |
sl_hal_pcnt_count_event_t#
sl_hal_pcnt_count_event_t
Counter event selection.
| Enumerator | |
|---|---|
| SL_HAL_PCNT_COUNT_EVENT_BOTH | Counts up on up-count and down on down-count events. |
| SL_HAL_PCNT_COUNT_EVENT_UP | Only counts up on up-count events. |
| SL_HAL_PCNT_COUNT_EVENT_DOWN | Only counts down on down-count events. |
Function Documentation#
sl_hal_pcnt_init#
void sl_hal_pcnt_init (PCNT_TypeDef * pcnt, const sl_hal_pcnt_config_t * init)
Initialize the pulse counter (PCNT).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
| const sl_hal_pcnt_config_t * | [in] | init | Pointer to the initialization structure. |
Notice that the EM23GRPACLK must be enabled in all modes, since some basic setup is done with this clock even if the external pin clock usage mode is chosen. The pulse counter clock for the selected instance must also be enabled prior to initialization.
Notice that pins used by the PCNT module must be properly configured by the user explicitly through setting the ROUTE register for the PCNT to work as intended.
sl_hal_pcnt_reset#
void sl_hal_pcnt_reset (PCNT_TypeDef * pcnt)
Reset the PCNT to the same state that it was in after a hardware reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
sl_hal_pcnt_enable#
void sl_hal_pcnt_enable (PCNT_TypeDef * pcnt)
Enable the PCNT.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
sl_hal_pcnt_disable#
void sl_hal_pcnt_disable (PCNT_TypeDef * pcnt)
Disable PCNT.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
sl_hal_pcnt_is_enabled#
bool sl_hal_pcnt_is_enabled (PCNT_TypeDef * pcnt)
Returns if the PCNT module is enabled or not.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
Returns
Returns true if the module is enabled.
sl_hal_pcnt_wait_ready#
void sl_hal_pcnt_wait_ready (PCNT_TypeDef * pcnt)
Wait for disabling to finish.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
sl_hal_pcnt_wait_sync#
void sl_hal_pcnt_wait_sync (PCNT_TypeDef * pcnt)
Wait for ongoing sync of register(s) to the low-frequency domain to complete.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
sl_hal_pcnt_get_status#
uint32_t sl_hal_pcnt_get_status (PCNT_TypeDef * pcnt)
Get status values for the PCNT.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
Returns
Current status values.
sl_hal_pcnt_enable_interrupts#
void sl_hal_pcnt_enable_interrupts (PCNT_TypeDef * pcnt, uint32_t flags)
Enable one or more PCNT interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
| uint32_t | [in] | flags | PCNT interrupt source(s) to enable. Use one or more valid interrupt flags for the PCNT module (PCNT_IF_nnn) OR'ed together. |
sl_hal_pcnt_disable_interrupts#
void sl_hal_pcnt_disable_interrupts (PCNT_TypeDef * pcnt, uint32_t flags)
Disable one or more PCNT interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
| uint32_t | [in] | flags | PCNT interrupt source(s) to disable. Use one or more valid interrupt flags for the PCNT module (PCNT_IF_nnn) OR'ed together. |
sl_hal_pcnt_clear_interrupts#
void sl_hal_pcnt_clear_interrupts (PCNT_TypeDef * pcnt, uint32_t flags)
Clear one or more pending PCNT interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
| uint32_t | [in] | flags | Pending PCNT interrupt source(s) to clear. Use one or more valid interrupt flags for the PCNT module (PCNT_IF_nnn) OR'ed together. |
sl_hal_pcnt_set_interrupts#
void sl_hal_pcnt_set_interrupts (PCNT_TypeDef * pcnt, uint32_t flags)
Set one or more pending PCNT interrupts from SW.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
| uint32_t | [in] | flags | PCNT interrupt source(s) to set to pending. Use one or more valid interrupt flags for the PCNT module (PCNT_IF_nnn) OR'ed together. |
sl_hal_pcnt_get_pending_interrupts#
uint32_t sl_hal_pcnt_get_pending_interrupts (PCNT_TypeDef * pcnt)
Get pending PCNT interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
Note
Event bits are not cleared by this function.
Returns
PCNT interrupt source(s) pending. Returns one or more valid interrupt flags for the PCNT module (PCNT_IF_nnn) OR'ed together.
sl_hal_pcnt_get_enabled_pending_interrupts#
uint32_t sl_hal_pcnt_get_enabled_pending_interrupts (PCNT_TypeDef * pcnt)
Get enabled and pending PCNT interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
Useful for handling more interrupt sources in the same interrupt handler.
Note
Interrupt flags are not cleared by this function.
Returns
Pending and enabled PCNT interrupt sources. The return value is the bitwise AND combination of
the OR combination of enabled interrupt sources in PCNTx_IEN_nnn register (PCNTx_IEN_nnn) and
the OR combination of valid interrupt flags of the PCNT module (PCNTx_IF_nnn).
sl_hal_pcnt_lock#
void sl_hal_pcnt_lock (PCNT_TypeDef * pcnt)
Lock PCNT registers.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
Note
When PCNT registers are locked PCNT_CFG, PCNT_EN, PCNT_SWRST, PCNT_CMD, PCNT_CTRL, PCNT_OVSCTRL, PCNT_CNT, PCNT_TOP, and PCNT_TOPB registers cannot be written to.
sl_hal_pcnt_unlock#
void sl_hal_pcnt_unlock (PCNT_TypeDef * pcnt)
Unlock PCNT registers.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to thePCNT peripheral register block. |
sl_hal_pcnt_set_top_buffer#
void sl_hal_pcnt_set_top_buffer (PCNT_TypeDef * pcnt, uint32_t value)
Set the top value buffer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
| uint32_t | [in] | value | Value to set in top value buffer register. |
When top value buffer register is updated, value is loaded into top value register at the next wrap around. This feature is useful in order to update top value safely when PCNT is running. This won't happen if SL_HAL_PCNT_COUNT_EVENT_BOTH is used.
sl_hal_pcnt_get_top_buffer#
uint32_t sl_hal_pcnt_get_top_buffer (PCNT_TypeDef * pcnt)
Get the top value buffer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
Returns
Current top value buffer.
sl_hal_pcnt_set_top#
void sl_hal_pcnt_set_top (PCNT_TypeDef * pcnt, uint32_t value)
Set the top value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
| uint32_t | [in] | value | Value to set in top value register. |
sl_hal_pcnt_get_top#
uint32_t sl_hal_pcnt_get_top (PCNT_TypeDef * pcnt)
Get the top value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
Returns
Current top value.
sl_hal_pcnt_start_main_counter#
void sl_hal_pcnt_start_main_counter (PCNT_TypeDef * pcnt)
Start PCNT main counter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
This function will send a start command to the PCNT peripheral. The PCNT peripheral will use some LF clock ticks before the command is executed. The sl_hal_pcnt_wait_sync() function can be used to wait for the start command to be executed.
sl_hal_pcnt_stop_main_counter#
void sl_hal_pcnt_stop_main_counter (PCNT_TypeDef * pcnt)
Stop PCNT main counter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
This function will send a stop command to the PCNT peripheral. The PCNT peripheral will use some LF clock ticks before the command is executed. The sl_hal_pcnt_wait_sync() function can be used to wait for the stop command to be executed.
sl_hal_pcnt_set_main_counter#
void sl_hal_pcnt_set_main_counter (PCNT_TypeDef * pcnt, uint32_t value)
Set a counter value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
| uint32_t | [in] | value | Value to set in counter register. |
Note
This function could stall until synchronization to low-frequency domain is completed. For that reason, it should normally not be used when an external clock is used for the PCNT module, since stall time may be undefined.
sl_hal_pcnt_get_main_counter#
uint32_t sl_hal_pcnt_get_main_counter (PCNT_TypeDef * pcnt)
Get the main counter value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
Returns
Current main counter value.
sl_hal_pcnt_start_aux_counter#
void sl_hal_pcnt_start_aux_counter (PCNT_TypeDef * pcnt)
Start PCNT auxiliary counter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
This function will send a start command to the PCNT peripheral. The PCNT peripheral will use some LF clock ticks before the command is executed. The sl_hal_pcnt_wait_sync() function can be used to wait for the start command to be executed.
sl_hal_pcnt_stop_aux_counter#
void sl_hal_pcnt_stop_aux_counter (PCNT_TypeDef * pcnt)
Stop PCNT auxiliary counter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
This function will send a stop command to the PCNT peripheral. The PCNT peripheral will use some LF clock ticks before the command is executed. The sl_hal_pcnt_wait_sync() function can be used to wait for the stop command to be executed.
sl_hal_pcnt_get_aux_counter#
uint32_t sl_hal_pcnt_get_aux_counter (PCNT_TypeDef * pcnt)
Get the auxiliary counter value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | Pointer to the PCNT peripheral register block. |
Returns
Current auxiliary counter value.
sl_hal_pcnt_reset_counters#
void sl_hal_pcnt_reset_counters (PCNT_TypeDef * pcnt)
Reset PCNT counters.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| PCNT_TypeDef * | [in] | pcnt | A pointer to the PCNT peripheral register block. |
Macro Definition Documentation#
SL_HAL_PCNT_CONFIG_DEFAULT#
#define SL_HAL_PCNT_CONFIG_DEFAULTValue:
Default configuration for PCNT initialization structure.