PCNT initialization structure.
Public Attributes#
Mode to operate in.
Selects whether the main counter responds to up-count events, down-count events or both.
Selects whether the auxiliary counter responds to up-count events, down-count events or both.
Polarity of incoming edge.
Counting direction, only applicable for OVS_SINGLE and EXT_CLK_SINGLE modes.
Set to true to enable S1 to determine the direction of counting in OVS_SINGLE or EXT_CLK_SINGLE modes.
Enable/disable PCNT counting during debug halt.
Set to true to enable hysteresis.
Set to true if a PRS channel is used as input to S0IN in PCNTx_INPUT register.
Set to true if a PRS channel is used as input to S1IN in PCNTx_INPUT register.
Enable digital pulse width filter, only available in OVS_SINGLE and OVS_QUAD modes.
When set, removes flutter from Quad decoder inputs S0IN and S1IN.
Used only in OVS_SINGLE and OVS_QUAD modes.
Public Attribute Documentation#
main_count_event#
sl_hal_pcnt_count_event_t sl_hal_pcnt_config_t::main_count_event
Selects whether the main counter responds to up-count events, down-count events or both.
aux_count_event#
sl_hal_pcnt_count_event_t sl_hal_pcnt_config_t::aux_count_event
Selects whether the auxiliary counter responds to up-count events, down-count events or both.
negative_edge#
bool sl_hal_pcnt_config_t::negative_edge
Polarity of incoming edge.
In EXT_CLK_SINGLE mode: if false, positive edges are counted, otherwise negative edges.
In EXT_CLK_QUAD mode: if true, counting direction is inverted.
count_down#
bool sl_hal_pcnt_config_t::count_down
Counting direction, only applicable for OVS_SINGLE and EXT_CLK_SINGLE modes.
If true, counting up, otherwise counting down.
s1_count_direction#
bool sl_hal_pcnt_config_t::s1_count_direction
Set to true to enable S1 to determine the direction of counting in OVS_SINGLE or EXT_CLK_SINGLE modes.
When S1 is high, the count direction is given by count_down, and when S1 is low, the count direction is the opposite.
debug_halt#
bool sl_hal_pcnt_config_t::debug_halt
Enable/disable PCNT counting during debug halt.
Only in OVS_SINGLE and OVS_QUAD modes.
hysteresis_enable#
bool sl_hal_pcnt_config_t::hysteresis_enable
Set to true to enable hysteresis.
When enabled, PCNT will always overflow and underflow to TOP/2.
s0_prs_enable#
bool sl_hal_pcnt_config_t::s0_prs_enable
Set to true if a PRS channel is used as input to S0IN in PCNTx_INPUT register.
s1_prs_enable#
bool sl_hal_pcnt_config_t::s1_prs_enable
Set to true if a PRS channel is used as input to S1IN in PCNTx_INPUT register.
filter_enable#
bool sl_hal_pcnt_config_t::filter_enable
Enable digital pulse width filter, only available in OVS_SINGLE and OVS_QUAD modes.
flutter_remove#
bool sl_hal_pcnt_config_t::flutter_remove
When set, removes flutter from Quad decoder inputs S0IN and S1IN.
Available only in OVS_SINGLE and OVS_QUAD modes.
filter_lenght#
uint8_t sl_hal_pcnt_config_t::filter_lenght
Used only in OVS_SINGLE and OVS_QUAD modes.
To use this, enable filter by setting filter_enable to true.
Filter length = (filter_lenght + 5) LFACLK cycles.