DALI Initialization structure.

Public Attributes#

bool

Enable the DALI low frequency mode.

Number of TX data bits in frame.

Number of RX data bits in frame.

General EUSART initialization structure.

Public Attribute Documentation#

dali_low_frequency_enable#

bool sl_hal_eusart_dali_config_t::dali_low_frequency_enable

Enable the DALI low frequency mode.


tx_data_bits#

sl_hal_eusart_dali_data_bits_t sl_hal_eusart_dali_config_t::tx_data_bits

Number of TX data bits in frame.


rx_data_bits#

sl_hal_eusart_dali_data_bits_t sl_hal_eusart_dali_config_t::rx_data_bits

Number of RX data bits in frame.


eusart_init#

sl_hal_eusart_uart_config_t sl_hal_eusart_dali_config_t::eusart_init

General EUSART initialization structure.