TIMER compare/capture initialization structure.
Public Attributes#
Compare/capture channel mode.
Select Compare/Capture channel input.
Counter match output action.
Counter underflow output action.
Counter overflow output action.
Input capture event control.
Input capture edge select.
Sets the watermark level of generation of fifo interrupt and DMA requests.
Compare output initial state.
PRS output configuration.
Enable digital filter.
Invert output from compare/capture channel.
Public Attribute Documentation#
channel_mode#
sl_hal_timer_channel_mode_t sl_hal_timer_channel_config_t::channel_mode
Compare/capture channel mode.
input_type#
sl_hal_timer_channel_input_type_t sl_hal_timer_channel_config_t::input_type
Select Compare/Capture channel input.
compare_match_output_action#
sl_hal_timer_channel_output_action_t sl_hal_timer_channel_config_t::compare_match_output_action
Counter match output action.
compare_underflow_output_action#
sl_hal_timer_channel_output_action_t sl_hal_timer_channel_config_t::compare_underflow_output_action
Counter underflow output action.
compare_overflow_output_action#
sl_hal_timer_channel_output_action_t sl_hal_timer_channel_config_t::compare_overflow_output_action
Counter overflow output action.
input_capture_event#
sl_hal_timer_channel_input_event_t sl_hal_timer_channel_config_t::input_capture_event
Input capture event control.
input_capture_edge#
sl_hal_timer_channel_input_edge_t sl_hal_timer_channel_config_t::input_capture_edge
Input capture edge select.
input_watermark_level#
uint8_t sl_hal_timer_channel_config_t::input_watermark_level
Sets the watermark level of generation of fifo interrupt and DMA requests.
output_initial_state#
bool sl_hal_timer_channel_config_t::output_initial_state
Compare output initial state.
Only used in Output Compare and PWM mode. When true, the compare/PWM output is set high when the counter is disabled. When counting resumes, this value will represent the initial value for the compare/PWM output. If the bit is cleared, the output will be cleared when the counter is disabled.
prs_output#
bool sl_hal_timer_channel_config_t::prs_output
PRS output configuration.
PRS output from a timer can either be a pulse output or a level output that follows the CC out value. if set, prs outputs a level that follows cc out value.
output_invert#
bool sl_hal_timer_channel_config_t::output_invert
Invert output from compare/capture channel.