EUSART - Enhanced USART#

Enhanced Universal Synchronous/Asynchronous Receiver/Transmitter.


Introduction#

This module contains functions to control the Enhanced Universal Synchronous / Asynchronous Receiver / Transmitter controller(s) (EUSART) peripheral of Silicon Labs' 32-bit MCUs and SoCs. EUSART can be used as a UART and can, therefore, be connected to an external transceiver to communicate with another host using the serial link.

It supports full duplex asynchronous UART communication as well as RS-485, SPI, MicroWire, and 3-wire. It can also interface with ISO7816 Smart-Cards, and IrDA devices.

EUSART has a wide selection of operating modes, frame formats, and baud rates. All features are supported through the API of this module.

This module does not support DMA configuration. UARTDRV and SPIDRV drivers provide full support for DMA and more.


Example#

EUSART Asynchronous UART TX example:

{
  #define GPIO_TX    PB0

  sl_hal_eusart_uart_config_t config = SL_HAL_EUSART_UART_INIT_DEFAULT_HF;

  // Configure the clocks.
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_EUSART0);
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_GPIO);

  // Calculate and configure the eusart's clock divider.
  uint32_t baudrate = 38400;  // Desired baudrate.
  sl_clock_branch_t clock_branch = sl_device_peripheral_get_clock_branch(SL_PERIPHERAL_EUSART0);
  uint32_t freq;
  sl_clock_manager_get_clock_branch_frequency(clock_branch, &freq);
  config.clock_div = sl_hal_eusart_uart_calculate_clock_div(freq, baudrate, config.oversampling);

  // Configure the EUSART port.
  sl_gpio_set_pin_mode(GPIO_TX, SL_GPIO_MODE_PUSH_PULL, 0);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART0)].TXROUTE = (GPIO_TX->port << _GPIO_EUSART_TXROUTE_PORT_SHIFT)
                                                 | (GPIO_TX->pin << _GPIO_EUSART_TXROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART0)].ROUTEEN = GPIO_EUSART_ROUTEEN_TXPEN;

  // Initialize the EUSART.
  sl_hal_eusart_init_uart_hf(EUSART0, &config);
  sl_hal_eusart_enable(EUSART0);
  sl_hal_eusart_enable_tx(EUSART0);

  uint16_t data = 0xFF;
  sl_hal_eusart_tx(EUSART0, data);
}

EUSART Synchronous SPI Initialization example:

{
  #define GPIO_MOSI    PC0
  #define GPIO_MISO    PC1
  #define GPIO_SCLK    PC2

  sl_hal_eusart_spi_config_t config = SL_HAL_EUSART_SPI_MASTER_INIT_DEFAULT_HF;
  // Clock idle low, sample on falling edge.
  config.clock_mode = SL_HAL_EUSART_CLOCK_MODE_1;

  // Configure the clocks.
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_EUSART1);
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_GPIO);

  // Calculate and configure the eusart's clock divider.
  uint32_t baudrate  = 1000000;  // Desired baudrate.
  sl_clock_branch_t clock_branch = sl_device_peripheral_get_clock_branch(SL_PERIPHERAL_EUSART1);
  uint32_t freq;
  sl_clock_manager_get_clock_branch_frequency(clock_branch, &freq);
  config.clock_div = sl_hal_eusart_spi_calculate_clock_div(freq, baudrate);

  // Configure the SPI ports.
  sl_gpio_set_pin_mode(GPIO_MOSI, SL_GPIO_MODE_PUSH_PULL, 0);
  sl_gpio_set_pin_mode(GPIO_MISO, SL_GPIO_MODE_INPUT, 0);
  sl_gpio_set_pin_mode(GPIO_SCLK, SL_GPIO_MODE_PUSH_PULL, 0);

  // Connect EUSART to ports.
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].TXROUTE = (GPIO_MOSI->port << _GPIO_EUSART_TXROUTE_PORT_SHIFT)
                                                   | (GPIO_MOSI->pin << _GPIO_EUSART_TXROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].RXROUTE = (GPIO_MISO->port << _GPIO_EUSART_RXROUTE_PORT_SHIFT)
                                                   | (GPIO_MISO->pin << _GPIO_EUSART_RXROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].SCLKROUTE = (GPIO_SCLK->port << _GPIO_EUSART_SCLKROUTE_PORT_SHIFT)
                                                   | (GPIO_SCLK->pin << _GPIO_EUSART_SCLKROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].ROUTEEN = GPIO_EUSART_ROUTEEN_TXPEN | GPIO_EUSART_ROUTEEN_RXPEN | GPIO_EUSART_ROUTEEN_SCLKPEN;

  // Initialize the EUSART.
  sl_hal_eusart_init_spi(EUSART1, &config);
  sl_hal_eusart_enable(EUSART1);
  sl_hal_eusart_enable_rx(EUSART1);
  sl_hal_eusart_enable_tx(EUSART1);
}

Modules#

sl_hal_eusart_uart_advanced_config_t

sl_hal_eusart_uart_config_t

sl_hal_eusart_irda_config_t

sl_hal_eusart_dali_config_t

sl_hal_eusart_spi_advanced_config_t

sl_hal_eusart_spi_config_t

Enumerations#

enum
SL_HAL_EUSART_DATA_BITS_7 = _EUSART_FRAMECFG_DATABITS_SEVEN
SL_HAL_EUSART_DATA_BITS_8 = _EUSART_FRAMECFG_DATABITS_EIGHT
SL_HAL_EUSART_DATA_BITS_9 = _EUSART_FRAMECFG_DATABITS_NINE
SL_HAL_EUSART_DATA_BITS_10 = _EUSART_FRAMECFG_DATABITS_TEN
SL_HAL_EUSART_DATA_BITS_11 = _EUSART_FRAMECFG_DATABITS_ELEVEN
SL_HAL_EUSART_DATA_BITS_12 = _EUSART_FRAMECFG_DATABITS_TWELVE
SL_HAL_EUSART_DATA_BITS_13 = _EUSART_FRAMECFG_DATABITS_THIRTEEN
SL_HAL_EUSART_DATA_BITS_14 = _EUSART_FRAMECFG_DATABITS_FOURTEEN
SL_HAL_EUSART_DATA_BITS_15 = _EUSART_FRAMECFG_DATABITS_FIFTEEN
SL_HAL_EUSART_DATA_BITS_16 = _EUSART_FRAMECFG_DATABITS_SIXTEEN
}

Data bit selection.

enum
SL_HAL_EUSART_NO_PARITY = _EUSART_FRAMECFG_PARITY_NONE
SL_HAL_EUSART_EVEN_PARITY = _EUSART_FRAMECFG_PARITY_EVEN
SL_HAL_EUSART_ODD_PARITY = _EUSART_FRAMECFG_PARITY_ODD
}

Parity selection.

enum
SL_HAL_EUSART_STOP_BITS_0P5 = _EUSART_FRAMECFG_STOPBITS_HALF
SL_HAL_EUSART_STOP_BITS_1P5 = _EUSART_FRAMECFG_STOPBITS_ONEANDAHALF
SL_HAL_EUSART_STOP_BITS_1 = _EUSART_FRAMECFG_STOPBITS_ONE
SL_HAL_EUSART_STOP_BITS_2 = _EUSART_FRAMECFG_STOPBITS_TWO
}

Stop bits selection.

enum
SL_HAL_EUSART_OVS_16 = _EUSART_CFG0_OVS_X16
SL_HAL_EUSART_OVS_8 = _EUSART_CFG0_OVS_X8
SL_HAL_EUSART_OVS_6 = _EUSART_CFG0_OVS_X6
SL_HAL_EUSART_OVS_4 = _EUSART_CFG0_OVS_X4
SL_HAL_EUSART_OVS_0 = _EUSART_CFG0_OVS_DISABLE
}

Oversampling selection, used for asynchronous operation.

enum
SL_HAL_EUSART_LOOPBACK_ENABLE = _EUSART_CFG0_LOOPBK_ENABLE
SL_HAL_EUSART_LOOPBACK_DISABLE = _EUSART_CFG0_LOOPBK_DISABLE
}

Loopback enable.

enum
SL_HAL_EUSART_MAJORITY_VOTE_ENABLE = 0
SL_HAL_EUSART_MAJORITY_VOTE_DISABLE = 1
}

Majority vote enable.

enum
SL_HAL_EUSART_HW_FLOW_CONTROL_NONE = 0
SL_HAL_EUSART_HW_FLOW_CONTROL_CTS
SL_HAL_EUSART_HW_FLOW_CONTROL_RTS
SL_HAL_EUSART_HW_FLOW_CONTROL_CTS_RTS
}

Hardware flow control configuration.

enum
SL_HAL_EUSART_INVERT_IO_DISABLE = (EUSART_CFG0_RXINV_DISABLE | EUSART_CFG0_TXINV_DISABLE) >> _EUSART_CFG0_RXINV_SHIFT
SL_HAL_EUSART_INVERT_IO_RX_ENABLE = EUSART_CFG0_RXINV_ENABLE >> _EUSART_CFG0_RXINV_SHIFT
SL_HAL_EUSART_INVERT_IO_TX_ENABLE = EUSART_CFG0_TXINV_ENABLE >> _EUSART_CFG0_RXINV_SHIFT
SL_HAL_EUSART_INVERT_IO_RXTX_ENABLE = (EUSART_CFG0_RXINV_ENABLE | EUSART_CFG0_TXINV_ENABLE) >> _EUSART_CFG0_RXINV_SHIFT
}

IO polarity selection.

enum
SL_HAL_EUSART_AUTO_TX_DELAY_NONE = _EUSART_TIMINGCFG_TXDELAY_NONE
SL_HAL_EUSART_AUTO_TX_DELAY_SINGLE = _EUSART_TIMINGCFG_TXDELAY_SINGLE
SL_HAL_EUSART_AUTO_TX_DELAY_DOUBLE = _EUSART_TIMINGCFG_TXDELAY_DOUBLE
SL_HAL_EUSART_AUTO_TX_DELAY_TRIPPLE = _EUSART_TIMINGCFG_TXDELAY_TRIPPLE
}

Auto TX delay transmission.

enum
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_ONE = _EUSART_CFG1_RXFIW_ONEFRAME
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_TWO = _EUSART_CFG1_RXFIW_TWOFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_THREE = _EUSART_CFG1_RXFIW_THREEFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_FOUR = _EUSART_CFG1_RXFIW_FOURFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_FIVE = _EUSART_CFG1_RXFIW_FIVEFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_SIX = _EUSART_CFG1_RXFIW_SIXFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_SEVEN = _EUSART_CFG1_RXFIW_SEVENFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_EIGHT = _EUSART_CFG1_RXFIW_EIGHTFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_NINE = _EUSART_CFG1_RXFIW_NINEFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_TEN = _EUSART_CFG1_RXFIW_TENFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_ELEVEN = _EUSART_CFG1_RXFIW_ELEVENFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_TWELVE = _EUSART_CFG1_RXFIW_TWELVEFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_THIRTEEN = _EUSART_CFG1_RXFIW_THIRTEENFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_FOURTEEN = _EUSART_CFG1_RXFIW_FOURTEENFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_FIFTEEN = _EUSART_CFG1_RXFIW_FIFTEENFRAMES
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_SIXTEEN = _EUSART_CFG1_RXFIW_SIXTEENFRAMES
}

FIFO Interrupt and Status Watermark.

enum
SL_HAL_EUSART_IRDA_MODE_HF
SL_HAL_EUSART_IRDA_MODE_LF
}

IrDA frequency mode (high/low frequency).

enum
SL_HAL_EUSART_PULSE_WIDTH_ONE = _EUSART_IRHFCFG_IRHFPW_ONE
SL_HAL_EUSART_PULSE_WIDTH_TWO = _EUSART_IRHFCFG_IRHFPW_TWO
SL_HAL_EUSART_PULSE_WIDTH_THREE = _EUSART_IRHFCFG_IRHFPW_THREE
SL_HAL_EUSART_PULSE_WIDTH_FOUR = _EUSART_IRHFCFG_IRHFPW_FOUR
}

Pulse width selection for IrDA mode.

enum
SL_HAL_EUSART_CS_TIME_ZERO = _EUSART_TIMINGCFG_CSSETUP_ZERO
SL_HAL_EUSART_CS_TIME_ONE = _EUSART_TIMINGCFG_CSSETUP_ONE
SL_HAL_EUSART_CS_TIME_TWO = _EUSART_TIMINGCFG_CSSETUP_TWO
SL_HAL_EUSART_CS_TIME_THREE = _EUSART_TIMINGCFG_CSSETUP_THREE
SL_HAL_EUSART_CS_TIME_FOUR = _EUSART_TIMINGCFG_CSSETUP_FOUR
SL_HAL_EUSART_CS_TIME_FIVE = _EUSART_TIMINGCFG_CSSETUP_FIVE
SL_HAL_EUSART_CS_TIME_SIX = _EUSART_TIMINGCFG_CSSETUP_SIX
SL_HAL_EUSART_CS_TIME_SEVEN = _EUSART_TIMINGCFG_CSSETUP_SEVEN
}

Chip select assertion/de-assertion time.

enum
SL_HAL_EUSART_ICS_TIME_ZERO = _EUSART_TIMINGCFG_ICS_ZERO
SL_HAL_EUSART_ICS_TIME_ONE = _EUSART_TIMINGCFG_ICS_ONE
SL_HAL_EUSART_ICS_TIME_TWO = _EUSART_TIMINGCFG_ICS_TWO
SL_HAL_EUSART_ICS_TIME_THREE = _EUSART_TIMINGCFG_ICS_THREE
SL_HAL_EUSART_ICS_TIME_FOUR = _EUSART_TIMINGCFG_ICS_FOUR
SL_HAL_EUSART_ICS_TIME_FIVE = _EUSART_TIMINGCFG_ICS_FIVE
SL_HAL_EUSART_ICS_TIME_SIX = _EUSART_TIMINGCFG_ICS_SIX
SL_HAL_EUSART_ICS_TIME_SEVEN = _EUSART_TIMINGCFG_ICS_SEVEN
}

Inter-character spacing after each TX frame while TX FIFO is not empty.

enum
SL_HAL_EUSART_CS_ACTIVE_LOW = _EUSART_CFG2_CSINV_AL
SL_HAL_EUSART_CS_ACTIVE_HIGH = _EUSART_CFG2_CSINV_AH
}

Chip select polarity.

enum
SL_HAL_EUSART_CLOCK_MODE_0 = (EUSART_CFG2_CLKPOL_IDLELOW | EUSART_CFG2_CLKPHA_SAMPLELEADING) >> _EUSART_CFG2_CLKPOL_SHIFT
SL_HAL_EUSART_CLOCK_MODE_1 = (EUSART_CFG2_CLKPOL_IDLELOW | EUSART_CFG2_CLKPHA_SAMPLETRAILING) >> _EUSART_CFG2_CLKPOL_SHIFT
SL_HAL_EUSART_CLOCK_MODE_2 = (EUSART_CFG2_CLKPOL_IDLEHIGH | EUSART_CFG2_CLKPHA_SAMPLELEADING) >> _EUSART_CFG2_CLKPOL_SHIFT
SL_HAL_EUSART_CLOCK_MODE_3 = (EUSART_CFG2_CLKPOL_IDLEHIGH | EUSART_CFG2_CLKPHA_SAMPLETRAILING) >> _EUSART_CFG2_CLKPOL_SHIFT
}

Clock polarity/phase mode.

enum
SL_HAL_EUSART_DALI_DATA_BITS_8 = _EUSART_DALICFG_DALITXDATABITS_EIGHT
SL_HAL_EUSART_DALI_DATA_BITS_9 = _EUSART_DALICFG_DALITXDATABITS_NINE
SL_HAL_EUSART_DALI_DATA_BITS_10 = _EUSART_DALICFG_DALITXDATABITS_TEN
SL_HAL_EUSART_DALI_DATA_BITS_11 = _EUSART_DALICFG_DALITXDATABITS_ELEVEN
SL_HAL_EUSART_DALI_DATA_BITS_12 = _EUSART_DALICFG_DALITXDATABITS_TWELVE
SL_HAL_EUSART_DALI_DATA_BITS_13 = _EUSART_DALICFG_DALITXDATABITS_THIRTEEN
SL_HAL_EUSART_DALI_DATA_BITS_14 = _EUSART_DALICFG_DALITXDATABITS_FOURTEEN
SL_HAL_EUSART_DALI_DATA_BITS_15 = _EUSART_DALICFG_DALITXDATABITS_FIFTEEN
SL_HAL_EUSART_DALI_DATA_BITS_16 = _EUSART_DALICFG_DALITXDATABITS_SIXTEEN
SL_HAL_EUSART_DALI_DATA_BITS_17 = _EUSART_DALICFG_DALITXDATABITS_SEVENTEEN
SL_HAL_EUSART_DALI_DATA_BITS_18 = _EUSART_DALICFG_DALITXDATABITS_EIGHTEEN
SL_HAL_EUSART_DALI_DATA_BITS_19 = _EUSART_DALICFG_DALITXDATABITS_NINETEEN
SL_HAL_EUSART_DALI_DATA_BITS_20 = _EUSART_DALICFG_DALITXDATABITS_TWENTY
SL_HAL_EUSART_DALI_DATA_BITS_21 = _EUSART_DALICFG_DALITXDATABITS_TWENTYONE
SL_HAL_EUSART_DALI_DATA_BITS_22 = _EUSART_DALICFG_DALITXDATABITS_TWENTYTWO
SL_HAL_EUSART_DALI_DATA_BITS_23 = _EUSART_DALICFG_DALITXDATABITS_TWENTYTHREE
SL_HAL_EUSART_DALI_DATA_BITS_24 = _EUSART_DALICFG_DALITXDATABITS_TWENTYFOUR
SL_HAL_EUSART_DALI_DATA_BITS_25 = _EUSART_DALICFG_DALITXDATABITS_TWENTYFIVE
SL_HAL_EUSART_DALI_DATA_BITS_26 = _EUSART_DALICFG_DALITXDATABITS_TWENTYSIX
SL_HAL_EUSART_DALI_DATA_BITS_27 = _EUSART_DALICFG_DALITXDATABITS_TWENTYSEVEN
SL_HAL_EUSART_DALI_DATA_BITS_28 = _EUSART_DALICFG_DALITXDATABITS_TWENTYEIGHT
SL_HAL_EUSART_DALI_DATA_BITS_29 = _EUSART_DALICFG_DALITXDATABITS_TWENTYNINE
SL_HAL_EUSART_DALI_DATA_BITS_30 = _EUSART_DALICFG_DALITXDATABITS_THIRTY
SL_HAL_EUSART_DALI_DATA_BITS_31 = _EUSART_DALICFG_DALITXDATABITS_THIRTYONE
SL_HAL_EUSART_DALI_DATA_BITS_32 = _EUSART_DALICFG_DALITXDATABITS_THIRTYTWO
}

DALI RX/TX databits (8-32).

Functions#

void
sl_hal_eusart_init_uart_hf(EUSART_TypeDef *eusart, const sl_hal_eusart_uart_config_t *config)

Initialize EUSART when used in UART mode with the high frequency clock.

void
sl_hal_eusart_init_uart_lf(EUSART_TypeDef *eusart, const sl_hal_eusart_uart_config_t *config)

Initialize EUSART when used in UART mode with the low frequency clock.

void
sl_hal_eusart_init_irda(EUSART_TypeDef *eusart, const sl_hal_eusart_irda_config_t *irda_config)

Initialize EUSART when used in IrDA mode with the high or low frequency clock.

void
sl_hal_eusart_init_dali(EUSART_TypeDef *eusart, const sl_hal_eusart_dali_config_t *dali_config)

Initialize EUSART when used in DALI mode with the high or low frequency clock.

void
sl_hal_eusart_init_spi(EUSART_TypeDef *eusart, const sl_hal_eusart_spi_config_t *config)

Initialize EUSART when used in SPI mode.

void
sl_hal_eusart_reset(EUSART_TypeDef *eusart)

Configure EUSART to its reset state.

uint16_t
sl_hal_eusart_rx(EUSART_TypeDef *eusart)

Receive one 8 bits frame, (or part of 9 bit frame).

uint16_t
sl_hal_eusart_rx_extended(EUSART_TypeDef *eusart)

Receive one 8-16 bit frame with extended information.

void
sl_hal_eusart_tx(EUSART_TypeDef *eusart, uint16_t data)

Transmit one 8 bits frame.

void
sl_hal_eusart_tx_extended(EUSART_TypeDef *eusart, uint16_t data)

Transmit one 8-9 bit frame with extended control.

uint16_t
sl_hal_eusart_spi_tx_rx(EUSART_TypeDef *eusart, uint16_t data)

Transmit one 8-16 bit frame and return received data.

void
sl_hal_eusart_dali_tx(EUSART_TypeDef *eusart, uint32_t data)

Transmit one DALI frame.

uint32_t
sl_hal_eusart_dali_rx(EUSART_TypeDef *eusart)

Receive one 8-32 bit DALI frame.

uint32_t
sl_hal_eusart_spi_calculate_clock_div(uint32_t ref_freq, uint32_t baudrate)

Calculate SPI clock divider using given reference frequency and baudrate.

uint32_t
sl_hal_eusart_uart_calculate_clock_div(uint32_t ref_freq, uint32_t baudrate, sl_hal_eusart_ovs_t ovs)

Calculate UART clock divider using given reference frequency, oversampling and baudrate.

uint32_t
sl_hal_eusart_uart_calculate_baudrate(uint32_t div, sl_hal_eusart_ovs_t ovs, uint32_t freq)

Get the calculated baudrate from the current EUSART configuration and clock.

uint32_t
sl_hal_eusart_spi_calculate_baudrate(uint32_t div, uint32_t freq)

Get the calculated baudrate from the current EUSART configuration and clock.

void
sl_hal_eusart_wait_sync(EUSART_TypeDef *eusart, uint32_t mask)

Wait for ongoing sync of register(s) to the low-frequency domain to complete.

void
sl_hal_eusart_enable(EUSART_TypeDef *eusart)

Enable EUSART.

void
sl_hal_eusart_disable(EUSART_TypeDef *eusart)

Disable EUSART.

void
sl_hal_eusart_wait_ready(EUSART_TypeDef *eusart)

Wait for disabling to finish.

void
sl_hal_eusart_enable_rx(EUSART_TypeDef *eusart)

Enable EUSART receiver.

void
sl_hal_eusart_disable_rx(EUSART_TypeDef *eusart)

Disable EUSART receiver.

void
sl_hal_eusart_enable_tx(EUSART_TypeDef *eusart)

Enable EUSART transmitter.

void
sl_hal_eusart_disable_tx(EUSART_TypeDef *eusart)

Disable EUSART transmitter.

void
sl_hal_eusart_enable_block_rx(EUSART_TypeDef *eusart)

Enable reception operation until the configured start frame is received.

void
sl_hal_eusart_disable_block_rx(EUSART_TypeDef *eusart)

Disable reception operation until the configured start frame is received.

void
sl_hal_eusart_enable_tx_tristate(EUSART_TypeDef *eusart)

Enable the tristating of the transmitter output.

void
sl_hal_eusart_disable_tx_tristate(EUSART_TypeDef *eusart)

Disable the tristating of the transmitter output.

void
sl_hal_eusart_clear_rx(EUSART_TypeDef *eusart)

Clear RX FIFO.

void
sl_hal_eusart_clear_tx(EUSART_TypeDef *eusart)

Clear TX FIFO.

uint32_t
sl_hal_eusart_get_status(EUSART_TypeDef *eusart)

Get EUSART STATUS register.

void
sl_hal_eusart_uart_set_clock_div(EUSART_TypeDef *eusart, uint32_t clock_divider)

Set UART mode clock divider.

uint32_t
sl_hal_eusart_uart_get_clock_div(EUSART_TypeDef *eusart)

Get UART mode clock divider.

sl_hal_eusart_uart_get_oversampling(EUSART_TypeDef *eusart)

Get UART mode oversampling value.

void
sl_hal_eusart_clear_interrupts(EUSART_TypeDef *eusart, uint32_t flags)

Clear one or more pending EUSART interrupts.

void
sl_hal_eusart_disable_interrupts(EUSART_TypeDef *eusart, uint32_t flags)

Disable one or more EUSART interrupts.

void
sl_hal_eusart_enable_interrupts(EUSART_TypeDef *eusart, uint32_t flags)

Enable one or more EUSART interrupts.

uint32_t
sl_hal_eusart_get_pending_interrupts(EUSART_TypeDef *eusart)

Get pending EUSART interrupt flags.

uint32_t

Get enabled and pending EUSART interrupt flags.

void
sl_hal_eusart_set_interrupts(EUSART_TypeDef *eusart, uint32_t flags)

Set one or more pending EUSART interrupts from SW.

Macros#

#define
SL_HAL_EUSART_REF_VALID (ref)

Check if EUSART insance is valid.

#define
SL_HAL_EUSART_UART_INIT_DEFAULT_HF undefined

Default configuration for EUSART initialization structure in UART mode with high-frequency clock.

#define
SL_HAL_EUSART_UART_INIT_DEFAULT_LF undefined

Default configuration for EUSART initialization structure in UART mode with low-frequency clock.

#define
SL_HAL_EUSART_UART_ADVANCED_INIT_DEFAULT undefined

Default configuration for EUSART advanced initialization structure in UART mode..

#define
SL_HAL_EUSART_SPI_MASTER_INIT_DEFAULT_HF undefined

Default configuration for EUSART initialization structure in SPI master mode with high-frequency clock.

#define
SL_HAL_EUSART_SPI_SLAVE_INIT_DEFAULT_HF undefined

Default configuration for EUSART initialization structure in SPI slave mode with high-frequency clock.

#define
SL_HAL_EUSART_SPI_ADVANCED_INIT_DEFAULT undefined

Default advanced configuration for EUSART initialization structure in SPI mode with high-frequency clock.

#define
SL_HAL_EUSART_IRDA_INIT_DEFAULT_HF undefined

Default configuration for EUSART initialization structure in IrDA mode with high-frequency clock.

#define
SL_HAL_EUSART_IRDA_INIT_DEFAULT_LF undefined

Default configuration for EUSART initialization structure in IrDA mode with low-frequency clock.

#define
SL_HAL_EUSART_DALI_ADVANCED_INIT_DEFAULT undefined

Default configuration for EUSART initialization structure in DALI mode with high-frequency clock.

#define
SL_HAL_EUSART_DALI_INIT_DEFAULT_HF undefined

Default configuration for EUSART initialization structure in DALI mode with high-frequency clock.

#define
SL_HAL_EUSART_DALI_INIT_DEFAULT_LF undefined

Default configuration for EUSART initialization structure in DALI mode with low-frequency clock.

Enumeration Documentation#

sl_hal_eusart_data_bits_t#

sl_hal_eusart_data_bits_t

Data bit selection.

Enumerator
SL_HAL_EUSART_DATA_BITS_7

7 data bits.

SL_HAL_EUSART_DATA_BITS_8

8 data bits.

SL_HAL_EUSART_DATA_BITS_9

9 data bits.

SL_HAL_EUSART_DATA_BITS_10

10 data bits, SPI mode only.

SL_HAL_EUSART_DATA_BITS_11

11 data bits, SPI mode only.

SL_HAL_EUSART_DATA_BITS_12

12 data bits, SPI mode only.

SL_HAL_EUSART_DATA_BITS_13

13 data bits, SPI mode only.

SL_HAL_EUSART_DATA_BITS_14

14 data bits, SPI mode only.

SL_HAL_EUSART_DATA_BITS_15

15 data bits, SPI mode only.

SL_HAL_EUSART_DATA_BITS_16

16 data bits, SPI mode only.


sl_hal_eusart_parity_t#

sl_hal_eusart_parity_t

Parity selection.

Enumerator
SL_HAL_EUSART_NO_PARITY

No parity.

SL_HAL_EUSART_EVEN_PARITY

Even parity.

SL_HAL_EUSART_ODD_PARITY

Odd parity.


sl_hal_eusart_stop_bits_t#

sl_hal_eusart_stop_bits_t

Stop bits selection.

Enumerator
SL_HAL_EUSART_STOP_BITS_0P5

0.5 stop bits.

SL_HAL_EUSART_STOP_BITS_1P5

1.5 stop bits.

SL_HAL_EUSART_STOP_BITS_1

1 stop bits.

SL_HAL_EUSART_STOP_BITS_2

2 stop bits.


sl_hal_eusart_ovs_t#

sl_hal_eusart_ovs_t

Oversampling selection, used for asynchronous operation.

Enumerator
SL_HAL_EUSART_OVS_16

16x oversampling (normal).

SL_HAL_EUSART_OVS_8

8x oversampling.

SL_HAL_EUSART_OVS_6

6x oversampling.

SL_HAL_EUSART_OVS_4

4x oversampling.

SL_HAL_EUSART_OVS_0

Oversampling disabled.


sl_hal_eusart_loopback_t#

sl_hal_eusart_loopback_t

Loopback enable.

Enumerator
SL_HAL_EUSART_LOOPBACK_ENABLE

Enable loopback.

SL_HAL_EUSART_LOOPBACK_DISABLE

Disable loopback.


sl_hal_eusart_majority_vote_t#

sl_hal_eusart_majority_vote_t

Majority vote enable.

Enumerator
SL_HAL_EUSART_MAJORITY_VOTE_ENABLE

Enable majority vote for 16x, 8x and 6x oversampling modes.

SL_HAL_EUSART_MAJORITY_VOTE_DISABLE

Disable majority vote for 16x, 8x and 6x oversampling modes.


sl_hal_eusart_hw_flow_control_t#

sl_hal_eusart_hw_flow_control_t

Hardware flow control configuration.

Enumerator
SL_HAL_EUSART_HW_FLOW_CONTROL_NONE

No Hardware Flow Control.

SL_HAL_EUSART_HW_FLOW_CONTROL_CTS

CTS Hardware Flow Control.

SL_HAL_EUSART_HW_FLOW_CONTROL_RTS

RTS Hardware Flow Control.

SL_HAL_EUSART_HW_FLOW_CONTROL_CTS_RTS

CTS and RTS Hardware Flow Control.


sl_hal_eusart_invert_io_t#

sl_hal_eusart_invert_io_t

IO polarity selection.

Enumerator
SL_HAL_EUSART_INVERT_IO_DISABLE

Disable inversion on both RX and TX signals.

SL_HAL_EUSART_INVERT_IO_RX_ENABLE

Invert RX signal, before receiver.

SL_HAL_EUSART_INVERT_IO_TX_ENABLE

Invert TX signal, after transmitter.

SL_HAL_EUSART_INVERT_IO_RXTX_ENABLE

Enable trigger on both receive and transmit.


sl_hal_eusart_auto_tx_delay_t#

sl_hal_eusart_auto_tx_delay_t

Auto TX delay transmission.

Enumerator
SL_HAL_EUSART_AUTO_TX_DELAY_NONE

Frames are transmitted immediately.

SL_HAL_EUSART_AUTO_TX_DELAY_SINGLE

Transmission of new frames is delayed by a single bit period.

SL_HAL_EUSART_AUTO_TX_DELAY_DOUBLE

Transmission of new frames is delayed by a two bit periods.

SL_HAL_EUSART_AUTO_TX_DELAY_TRIPPLE

Transmission of new frames is delayed by a three bit periods.


sl_hal_eusart_fifo_interrupt_watermark_t#

sl_hal_eusart_fifo_interrupt_watermark_t

FIFO Interrupt and Status Watermark.

Enumerator
SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_ONE

Interrupt and status level are set after 1 frame.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_TWO

Interrupt and status level are set after 2 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_THREE

Interrupt and status level are set after 3 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_FOUR

Interrupt and status level are set after 4 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_FIVE

Interrupt and status level are set after 5 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_SIX

Interrupt and status level are set after 6 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_SEVEN

Interrupt and status level are set after 7 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_EIGHT

Interrupt and status level are set after 8 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_NINE

Interrupt and status level are set after 9 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_TEN

Interrupt and status level are set after 10 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_ELEVEN

Interrupt and status level are set after 11 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_TWELVE

Interrupt and status level are set after 12 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_THIRTEEN

Interrupt and status level are set after 13 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_FOURTEEN

Interrupt and status level are set after 14 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_FIFTEEN

Interrupt and status level are set after 15 frames.

SL_HAL_EUSART_FIFO_INTERRUPT_WATERMARK_FRAMES_SIXTEEN

Interrupt and status level are set after 16 frames.


sl_hal_eusart_irda_frequency_mode_t#

sl_hal_eusart_irda_frequency_mode_t

IrDA frequency mode (high/low frequency).

Enumerator
SL_HAL_EUSART_IRDA_MODE_HF

High frequency mode.

SL_HAL_EUSART_IRDA_MODE_LF

Low frequency mode.


sl_hal_eusart_irda_pulse_width_t#

sl_hal_eusart_irda_pulse_width_t

Pulse width selection for IrDA mode.

Enumerator
SL_HAL_EUSART_PULSE_WIDTH_ONE

IrDA pulse width is 1/16 for OVS=X16 and 1/8 for OVS=X8.

SL_HAL_EUSART_PULSE_WIDTH_TWO

IrDA pulse width is 2/16 for OVS=X16 and 2/8 for OVS=X8.

SL_HAL_EUSART_PULSE_WIDTH_THREE

IrDA pulse width is 3/16 for OVS=X16 and 3/8 for OVS=X8.

SL_HAL_EUSART_PULSE_WIDTH_FOUR

IrDA pulse width is 4/16 for OVS=X16 and 4/8 for OVS=X8.


sl_hal_eusart_cs_time_t#

sl_hal_eusart_cs_time_t

Chip select assertion/de-assertion time.

Enumerator
SL_HAL_EUSART_CS_TIME_ZERO

Chip select is asserted/de-asserted half or 1 baud-time before transmission.

SL_HAL_EUSART_CS_TIME_ONE

Chip select is asserted/de-asserted 1 additional baud-time before transmission.

SL_HAL_EUSART_CS_TIME_TWO

Chip select is asserted/de-asserted 2 additional baud-time before transmission.

SL_HAL_EUSART_CS_TIME_THREE

Chip select is asserted/de-asserted 3 additional baud-time before transmission.

SL_HAL_EUSART_CS_TIME_FOUR

Chip select is asserted/de-asserted 4 additional baud-time before transmission.

SL_HAL_EUSART_CS_TIME_FIVE

Chip select is asserted/de-asserted 5 additional baud-time before transmission.

SL_HAL_EUSART_CS_TIME_SIX

Chip select is asserted/de-asserted 6 additional baud-time before transmission.

SL_HAL_EUSART_CS_TIME_SEVEN

Chip select is asserted/de-asserted 7 additional baud-time before transmission.


sl_hal_eusart_inter_character_space_t#

sl_hal_eusart_inter_character_space_t

Inter-character spacing after each TX frame while TX FIFO is not empty.

Enumerator
SL_HAL_EUSART_ICS_TIME_ZERO

There is no space between characters..

SL_HAL_EUSART_ICS_TIME_ONE

Create a space on 1 baud-times between frames.

SL_HAL_EUSART_ICS_TIME_TWO

Create a space on 2 baud-times between frames.

SL_HAL_EUSART_ICS_TIME_THREE

Create a space on 3 baud-times between frames.

SL_HAL_EUSART_ICS_TIME_FOUR

Create a space on 4 baud-times between frames.

SL_HAL_EUSART_ICS_TIME_FIVE

Create a space on 5 baud-times between frames.

SL_HAL_EUSART_ICS_TIME_SIX

Create a space on 6 baud-times between frames.

SL_HAL_EUSART_ICS_TIME_SEVEN

Create a space on 7 baud-times between frames.


sl_hal_eusart_cs_polarity_t#

sl_hal_eusart_cs_polarity_t

Chip select polarity.

Enumerator
SL_HAL_EUSART_CS_ACTIVE_LOW

Chip select active low.

SL_HAL_EUSART_CS_ACTIVE_HIGH

Chip select active high.


sl_hal_eusart_clock_mode_t#

sl_hal_eusart_clock_mode_t

Clock polarity/phase mode.

Enumerator
SL_HAL_EUSART_CLOCK_MODE_0

Clock idle low, sample on rising edge.

SL_HAL_EUSART_CLOCK_MODE_1

Clock idle low, sample on falling edge.

SL_HAL_EUSART_CLOCK_MODE_2

Clock idle high, sample on falling edge.

SL_HAL_EUSART_CLOCK_MODE_3

Clock idle high, sample on rising edge.


sl_hal_eusart_dali_data_bits_t#

sl_hal_eusart_dali_data_bits_t

DALI RX/TX databits (8-32).

Enumerator
SL_HAL_EUSART_DALI_DATA_BITS_8

Each frame contains 8 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_9

Each frame contains 9 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_10

Each frame contains 10 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_11

Each frame contains 11 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_12

Each frame contains 12 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_13

Each frame contains 13 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_14

Each frame contains 14 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_15

Each frame contains 15 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_16

Each frame contains 16 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_17

Each frame contains 17 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_18

Each frame contains 18 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_19

Each frame contains 19 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_20

Each frame contains 20 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_21

Each frame contains 21 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_22

Each frame contains 22 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_23

Each frame contains 23 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_24

Each frame contains 24 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_25

Each frame contains 25 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_26

Each frame contains 26 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_27

Each frame contains 27 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_28

Each frame contains 28 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_29

Each frame contains 29 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_30

Each frame contains 30 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_31

Each frame contains 31 data bits.

SL_HAL_EUSART_DALI_DATA_BITS_32

Each frame contains 32 data bits.


Function Documentation#

sl_hal_eusart_init_uart_hf#

void sl_hal_eusart_init_uart_hf (EUSART_TypeDef * eusart, const sl_hal_eusart_uart_config_t * config)

Initialize EUSART when used in UART mode with the high frequency clock.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

const sl_hal_eusart_uart_config_t *[in]config

A pointer to the initialization structure.


sl_hal_eusart_init_uart_lf#

void sl_hal_eusart_init_uart_lf (EUSART_TypeDef * eusart, const sl_hal_eusart_uart_config_t * config)

Initialize EUSART when used in UART mode with the low frequency clock.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

const sl_hal_eusart_uart_config_t *[in]config

A pointer to the initialization structure.

Note

  • (1) When EUSART oversampling is set to SL_HAL_EUSART_OVS_0 (Disable), the peripheral clock frequency must be at least three times higher than the chosen baud rate. In LF, max input clock is 32768 (LFXO or LFRCO), thus 32768 / 3 ~ 9600 baudrate. Number of stop bits must be 1 or 2. Data bits must be less than 9 bits. Majority Vote must be disabled.


sl_hal_eusart_init_irda#

void sl_hal_eusart_init_irda (EUSART_TypeDef * eusart, const sl_hal_eusart_irda_config_t * irda_config)

Initialize EUSART when used in IrDA mode with the high or low frequency clock.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

const sl_hal_eusart_irda_config_t *[in]irda_config

A pointer to the initialization structure.


sl_hal_eusart_init_dali#

void sl_hal_eusart_init_dali (EUSART_TypeDef * eusart, const sl_hal_eusart_dali_config_t * dali_config)

Initialize EUSART when used in DALI mode with the high or low frequency clock.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

const sl_hal_eusart_dali_config_t *[in]dali_config

A pointer to the initialization structure.

Note

  • When EUSART oversampling is set to SL_HAL_EUSART_OVS_0 (Disable), the peripheral clock frequency must be at least three times higher than the chosen baud rate. In LF, max input clock is 32768 (LFXO or LFRCO), thus 32768 / 3 ~ 9600 baudrate.


sl_hal_eusart_init_spi#

void sl_hal_eusart_init_spi (EUSART_TypeDef * eusart, const sl_hal_eusart_spi_config_t * config)

Initialize EUSART when used in SPI mode.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

const sl_hal_eusart_spi_config_t *[in]config

A pointer to the initialization structure.


sl_hal_eusart_reset#

void sl_hal_eusart_reset (EUSART_TypeDef * eusart)

Configure EUSART to its reset state.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_rx#

uint16_t sl_hal_eusart_rx (EUSART_TypeDef * eusart)

Receive one 8 bits frame, (or part of 9 bit frame).

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

Note

  • This function will stall if buffer is empty until data is received.

Returns

  • Data received.


sl_hal_eusart_rx_extended#

uint16_t sl_hal_eusart_rx_extended (EUSART_TypeDef * eusart)

Receive one 8-16 bit frame with extended information.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

Note

  • This function is normally used to receive one frame and additional RX status information.

  • This function will stall if buffer is empty until data is received.

Returns

  • Data received and receive status.


sl_hal_eusart_tx#

void sl_hal_eusart_tx (EUSART_TypeDef * eusart, uint16_t data)

Transmit one 8 bits frame.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

uint16_t[in]data

Data to transmit.

Note

  • This function will stall if the 4 frame FIFO is full, until the buffer becomes available.


sl_hal_eusart_tx_extended#

void sl_hal_eusart_tx_extended (EUSART_TypeDef * eusart, uint16_t data)

Transmit one 8-9 bit frame with extended control.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

uint16_t[in]data

Data to transmit.

Note

  • Possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.

  • This function will stall if buffer is full until the buffer becomes available.


sl_hal_eusart_spi_tx_rx#

uint16_t sl_hal_eusart_spi_tx_rx (EUSART_TypeDef * eusart, uint16_t data)

Transmit one 8-16 bit frame and return received data.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

uint16_t[in]data

Data to transmit.

Returns

  • Data received and receive status.

Note

  • SPI master mode only.

  • This function will stall if the TX buffer is full until the buffer becomes available.


sl_hal_eusart_dali_tx#

void sl_hal_eusart_dali_tx (EUSART_TypeDef * eusart, uint32_t data)

Transmit one DALI frame.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

uint32_t[in]data

Data to transmit.

Note

  • Depending on the TXdatabits configuration, N (least significant) bits from data are transmitted.

  • This function will stall if the 16 frame FIFO is full, until the buffer becomes available.


sl_hal_eusart_dali_rx#

uint32_t sl_hal_eusart_dali_rx (EUSART_TypeDef * eusart)

Receive one 8-32 bit DALI frame.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

Note

  • This function is normally used to receive one DALI frame.

  • This function will stall if the 16 frame FIFO is empty until new data is received.

Returns

  • Data received. Depending on the RXdatabits configuration, N (least significant) bits are returned.


sl_hal_eusart_spi_calculate_clock_div#

uint32_t sl_hal_eusart_spi_calculate_clock_div (uint32_t ref_freq, uint32_t baudrate)

Calculate SPI clock divider using given reference frequency and baudrate.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]ref_freq

Peripheral clock frequency.

uint32_t[in]baudrate

Transmission speed of the SPI interface.

Returns

  • Eusart clock divider for desired baud rate.


sl_hal_eusart_uart_calculate_clock_div#

uint32_t sl_hal_eusart_uart_calculate_clock_div (uint32_t ref_freq, uint32_t baudrate, sl_hal_eusart_ovs_t ovs)

Calculate UART clock divider using given reference frequency, oversampling and baudrate.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]ref_freq

Peripheral clock frequency.

uint32_t[in]baudrate

Transmission speed of the UART interface.

sl_hal_eusart_ovs_t[in]ovs

Oversampling rate.

Returns

  • Eusart clock divider for desired baud rate.


sl_hal_eusart_uart_calculate_baudrate#

uint32_t sl_hal_eusart_uart_calculate_baudrate (uint32_t div, sl_hal_eusart_ovs_t ovs, uint32_t freq)

Get the calculated baudrate from the current EUSART configuration and clock.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]div

CLKDIV register value of the EUSART.

sl_hal_eusart_ovs_t[in]ovs

Oversample value of the EUSART.

uint32_t[in]freq

The clock branch frequency to calculate the baudrate.

Returns

  • The baudrate


sl_hal_eusart_spi_calculate_baudrate#

uint32_t sl_hal_eusart_spi_calculate_baudrate (uint32_t div, uint32_t freq)

Get the calculated baudrate from the current EUSART configuration and clock.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]div

clkdiv register value of the EUSART.

uint32_t[in]freq

The clock branch frequency to calculate the baudrate.

Returns

  • The baudrate.


sl_hal_eusart_wait_sync#

void sl_hal_eusart_wait_sync (EUSART_TypeDef * eusart, uint32_t mask)

Wait for ongoing sync of register(s) to the low-frequency domain to complete.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

uint32_t[in]mask

Bitmask for SYNCBUSY register - indicates which register(s) to wait for synchronization to complete


sl_hal_eusart_enable#

void sl_hal_eusart_enable (EUSART_TypeDef * eusart)

Enable EUSART.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_disable#

void sl_hal_eusart_disable (EUSART_TypeDef * eusart)

Disable EUSART.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_wait_ready#

void sl_hal_eusart_wait_ready (EUSART_TypeDef * eusart)

Wait for disabling to finish.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_enable_rx#

void sl_hal_eusart_enable_rx (EUSART_TypeDef * eusart)

Enable EUSART receiver.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_disable_rx#

void sl_hal_eusart_disable_rx (EUSART_TypeDef * eusart)

Disable EUSART receiver.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_enable_tx#

void sl_hal_eusart_enable_tx (EUSART_TypeDef * eusart)

Enable EUSART transmitter.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_disable_tx#

void sl_hal_eusart_disable_tx (EUSART_TypeDef * eusart)

Disable EUSART transmitter.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_enable_block_rx#

void sl_hal_eusart_enable_block_rx (EUSART_TypeDef * eusart)

Enable reception operation until the configured start frame is received.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_disable_block_rx#

void sl_hal_eusart_disable_block_rx (EUSART_TypeDef * eusart)

Disable reception operation until the configured start frame is received.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_enable_tx_tristate#

void sl_hal_eusart_enable_tx_tristate (EUSART_TypeDef * eusart)

Enable the tristating of the transmitter output.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_disable_tx_tristate#

void sl_hal_eusart_disable_tx_tristate (EUSART_TypeDef * eusart)

Disable the tristating of the transmitter output.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_clear_rx#

void sl_hal_eusart_clear_rx (EUSART_TypeDef * eusart)

Clear RX FIFO.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_clear_tx#

void sl_hal_eusart_clear_tx (EUSART_TypeDef * eusart)

Clear TX FIFO.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.


sl_hal_eusart_get_status#

uint32_t sl_hal_eusart_get_status (EUSART_TypeDef * eusart)

Get EUSART STATUS register.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

Returns

  • STATUS register value.


sl_hal_eusart_uart_set_clock_div#

void sl_hal_eusart_uart_set_clock_div (EUSART_TypeDef * eusart, uint32_t clock_divider)

Set UART mode clock divider.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

uint32_t[in]clock_divider

Clock divider value.


sl_hal_eusart_uart_get_clock_div#

uint32_t sl_hal_eusart_uart_get_clock_div (EUSART_TypeDef * eusart)

Get UART mode clock divider.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

ointer to the EUSART peripheral register block.

Returns

  • Clock divider value.


sl_hal_eusart_uart_get_oversampling#

sl_hal_eusart_ovs_t sl_hal_eusart_uart_get_oversampling (EUSART_TypeDef * eusart)

Get UART mode oversampling value.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

Returns

  • Oversampling value.


sl_hal_eusart_clear_interrupts#

void sl_hal_eusart_clear_interrupts (EUSART_TypeDef * eusart, uint32_t flags)

Clear one or more pending EUSART interrupts.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

uint32_t[in]flags

Pending EUSART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn).


sl_hal_eusart_disable_interrupts#

void sl_hal_eusart_disable_interrupts (EUSART_TypeDef * eusart, uint32_t flags)

Disable one or more EUSART interrupts.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

uint32_t[in]flags

Pending EUSART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn).


sl_hal_eusart_enable_interrupts#

void sl_hal_eusart_enable_interrupts (EUSART_TypeDef * eusart, uint32_t flags)

Enable one or more EUSART interrupts.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

uint32_t[in]flags

Pending EUSART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn).


sl_hal_eusart_get_pending_interrupts#

uint32_t sl_hal_eusart_get_pending_interrupts (EUSART_TypeDef * eusart)

Get pending EUSART interrupt flags.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

Returns

  • Pending EUSART interrupt sources.


sl_hal_eusart_get_enabled_pending_interrupts#

uint32_t sl_hal_eusart_get_enabled_pending_interrupts (EUSART_TypeDef * eusart)

Get enabled and pending EUSART interrupt flags.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

ointer to the EUSART peripheral register block.

Note

  • Useful for handling more interrupt sources in the same interrupt handler.

Returns

  • Pending and enabled EUSART interrupt sources.


sl_hal_eusart_set_interrupts#

void sl_hal_eusart_set_interrupts (EUSART_TypeDef * eusart, uint32_t flags)

Set one or more pending EUSART interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
EUSART_TypeDef *[in]eusart

Pointer to the EUSART peripheral register block.

uint32_t[in]flags

Interrupt source(s) to set to pending. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn).