IrDA mode initialization structure. Inherited from asynchronous mode initialization structure.
Public Attributes#
bool
Set to invert Rx signal before IrDA demodulator.
bool
Set to enable filter on IrDA demodulator.
Configure the pulse width generated by the IrDA modulator as a fraction of the configured USART bit period.
General Asynchronous initialization structure.
Public Attribute Documentation#
ir_rx_inv#
bool sl_hal_usart_irda_config_t::ir_rx_inv
Set to invert Rx signal before IrDA demodulator.
ir_pulse_width#
sl_hal_usart_irda_pulse_width_t sl_hal_usart_irda_config_t::ir_pulse_width
Configure the pulse width generated by the IrDA modulator as a fraction of the configured USART bit period.
async#
sl_hal_usart_async_config_t sl_hal_usart_irda_config_t::async
General Asynchronous initialization structure.