TIMER - Timer/Counter#


Introduction#

This module contains functions to control the TIMER peripheral of Silicon Labs' 32-bit MCUs and SoCs. The general purpose timer has 3 or 4 compare/capture channels for input capture and compare/Pulse-Width Modulation (PWM) output. The TIMER module may be 16 or 32 bits wide. Some timers also include a Dead-Time Insertion module suitable for motor control applications.

Refer to the device data sheet to determine the capabilities (capture/compare channel count, width, and DTI) of each timer instance.


Examples#

TIMER enable counter example:

{
  // Enable the clock for the timer.
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_TIMER0);

  // Initialize a timer and enable it.
  sl_hal_timer_config_t init = SL_HAL_TIMER_CONFIG_DEFAULT;
  sl_hal_timer_init(TIMER0, &init);
  sl_hal_timer_enable(TIMER0);

  // Get counter value.
  uint32_t counter_value = sl_hal_timer_get_counter(TIMER0);

  // Start counter.
  sl_hal_timer_start(TIMER0);

  // [User code]

  // Get a new counter value.
  uint32_t new_counter_value = sl_hal_timer_get_counter(TIMER0);

  // Stop counter.
  sl_hal_timer_stop(TIMER0);

  sl_hal_timer_disable(TIMER0);
}

TIMER interrupt example:

// Global irq flag.
static volatile uint32_t irq_flag = 0;

// Example IRQHandler.
void TIMER0_IRQHandler(void)
{
  // Get all pending and enabled interrupts.
  uint32_t pending = sl_hal_timer_get_enabled_pending_interrupts(TIMER0);

  // Handle different IRQ flags here, execute callbacks, etc.
  if (pending) {
    sl_hal_timer_clear_interrupts(TIMER0, pending);
    irq_flag = pending;
  }
}

void timer_example(void)
{
  // Enable the clock for the timer.
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_TIMER0);

  // Initialize a timer and enable it.
  sl_hal_timer_config_t init = SL_HAL_TIMER_CONFIG_DEFAULT;
  sl_hal_timer_init(TIMER0, &init);
  sl_hal_timer_enable(TIMER0);

  sl_hal_timer_clear_interrupts(TIMER0, _TIMER_IF_MASK);
  sl_hal_timer_enable_interrupts(TIMER0, _TIMER_IEN_MASK);
  sl_interrupt_manager_enable_irq(TIMER0_IRQn);

  sl_hal_timer_start(TIMER0);

  // Wait until we get the flag.
  while (!irq_flag) ;

  // Cleanup.
  sl_hal_timer_stop(TIMER0);
  sl_interrupt_manager_disable_irq(TIMER0_IRQn);
  sl_hal_timer_reset(TIMER0);
  sl_clock_manager_disable_bus_clock(SL_BUS_CLOCK_TIMER0);
}

TIMER buffer update mode example:

void timer_buffer_update_example(void)
{
  // Enable the clock for the timer
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_TIMER0);

  // Initialize timer with update mode enabled
  sl_hal_timer_config_t init = SL_HAL_TIMER_CONFIG_DEFAULT;
  init.enable_update_mode = true;  // Enable manual update mode

  // Initialize a channel for PWM operation
  sl_hal_timer_channel_config_t channel_config = SL_HAL_TIMER_CHANNEL_CONFIG_PWM;

  // Configure timer and channel
  sl_hal_timer_init(TIMER0, &init);
  sl_hal_timer_channel_init(TIMER0, 0, &channel_config);

  // Set initial parameters
  sl_hal_timer_set_top(TIMER0, 10000);                // Set PWM period
  sl_hal_timer_channel_set_compare(TIMER0, 0, 5000);  // 50% duty cycle

  // Enable timer and start counting
  sl_hal_timer_enable(TIMER0);
  sl_hal_timer_wait_sync(TIMER0);
  sl_hal_timer_start(TIMER0);

  // Change PWM parameters using buffer registers
  uint32_t new_compare_value = 7500;       // New PWM compare value (75% duty cycle)
  uint32_t new_phase_value = 1000;         // New phase value
  uint8_t new_dither_value = 8;            // New dither value

  // Write to buffer registers (not immediately applied)
  sl_hal_timer_channel_set_compare_buffer(TIMER0, 0, new_compare_value);
  sl_hal_timer_channel_set_phase_buffer(TIMER0, 0, new_phase_value);
  sl_hal_timer_channel_set_dither_buffer(TIMER0, 0, new_dither_value);

  // With update_mode enabled, buffer values are only marked for
  // transfer after explicitly calling sl_hal_timer_channel_update_registers()
  sl_hal_timer_channel_update_registers(TIMER0);

  // Check if buffer values are pending transfer
  uint32_t status = sl_hal_timer_get_status2(TIMER0);
  if ((status & _TIMER_STATUS2_PHASEBV0_MASK) &&
      (status & _TIMER_STATUS2_DITHERBV0_MASK)) {
    // Buffer values are pending transfer at next overflow/underflow
  }

  // Optionally force an update event soon by setting counter close to overflow
  sl_hal_timer_set_counter(TIMER0, 0xffff0000);

  // Wait for synchronization and transfer to complete
  sl_hal_timer_wait_sync(TIMER0);

  // Verify buffer values have been transferred
  status = sl_hal_timer_get_status2(TIMER0);
  if (!(status & _TIMER_STATUS2_PHASEBV0_MASK) &&
      !(status & _TIMER_STATUS2_DITHERBV0_MASK)) {
    // Buffer values have been transferred to active registers

    // Read active register values to confirm
    uint32_t current_compare = sl_hal_timer_channel_get_compare(TIMER0, 0);
    uint32_t current_phase = sl_hal_timer_channel_get_phase(TIMER0, 0);
    uint32_t current_dither = sl_hal_timer_channel_get_dither(TIMER0, 0);
  }

  // Cleanup
  sl_hal_timer_stop(TIMER0);
  sl_hal_timer_disable(TIMER0);
  sl_clock_manager_disable_bus_clock(SL_BUS_CLOCK_TIMER0);
}

Note

  • When update_mode is disabled (default), buffer values are automatically transferred to active registers at the next update event (overflow/underflow). When update_mode is enabled, sl_hal_timer_channel_update_registers() must be called to mark buffers for transfer at the next update event.

Modules#

sl_hal_timer_config_t

sl_hal_timer_channel_config_t

sl_hal_timer_dti_config_t

Enumerations#

enum
SL_HAL_TIMER_CHANNEL_MODE_OFF = _TIMER_CC_CFG_MODE_OFF
SL_HAL_TIMER_CHANNEL_MODE_CAPTURE = _TIMER_CC_CFG_MODE_INPUTCAPTURE
SL_HAL_TIMER_CHANNEL_MODE_COMPARE = _TIMER_CC_CFG_MODE_OUTPUTCOMPARE
SL_HAL_TIMER_CHANNEL_MODE_PWM = _TIMER_CC_CFG_MODE_PWM
}

Timer compare/capture mode.

enum
SL_HAL_TIMER_CLKSEL_HFPERCLK = _TIMER_CFG_CLKSEL_PRESCEM01GRPACLK
SL_HAL_TIMER_CLKSEL_CC1 = _TIMER_CFG_CLKSEL_CC1
SL_HAL_TIMER_CLKSEL_CASCADE = _TIMER_CFG_CLKSEL_TIMEROUF
}

Clock select.

enum
SL_HAL_TIMER_CHANNEL_EDGE_RISING = _TIMER_CC_CTRL_ICEDGE_RISING
SL_HAL_TIMER_CHANNEL_EDGE_FALLING = _TIMER_CC_CTRL_ICEDGE_FALLING
SL_HAL_TIMER_CHANNEL_EDGE_BOTH = _TIMER_CC_CTRL_ICEDGE_BOTH
SL_HAL_TIMER_CHANNEL_EDGE_NONE = _TIMER_CC_CTRL_ICEDGE_NONE
}

Input capture edge select.

enum
SL_HAL_TIMER_CHANNEL_EVENT_EVERY_EDGE = _TIMER_CC_CTRL_ICEVCTRL_EVERYEDGE
SL_HAL_TIMER_CHANNEL_EVENT_EVERY_SECONDE_EDGE = _TIMER_CC_CTRL_ICEVCTRL_EVERYSECONDEDGE
SL_HAL_TIMER_CHANNEL_EVENT_RISING = _TIMER_CC_CTRL_ICEVCTRL_RISING
SL_HAL_TIMER_CHANNEL_EVENT_FALLING = _TIMER_CC_CTRL_ICEVCTRL_FALLING
}

Input capture event control.

enum
SL_HAL_TIMER_INPUT_ACTION_NONE = _TIMER_CTRL_FALLA_NONE
SL_HAL_TIMER_INPUT_ACTION_START = _TIMER_CTRL_FALLA_START
SL_HAL_TIMER_INPUT_ACTION_STOP = _TIMER_CTRL_FALLA_STOP
SL_HAL_TIMER_INPUT_ACTION_RELOAD_START = _TIMER_CTRL_FALLA_RELOADSTART
}

Input edge action.

enum
SL_HAL_TIMER_MODE_UP = _TIMER_CFG_MODE_UP
SL_HAL_TIMER_MODE_DOWN = _TIMER_CFG_MODE_DOWN
SL_HAL_TIMER_MODE_UPDOWN = _TIMER_CFG_MODE_UPDOWN
SL_HAL_TIMER_MODE_QDEC = _TIMER_CFG_MODE_QDEC
}

Timer mode.

enum
SL_HAL_TIMER_CHANNEL_OUTPUT_ACTION_NONE = _TIMER_CC_CTRL_CUFOA_NONE
SL_HAL_TIMER_CHANNEL_OUTPUT_ACTION_TOGGLE = _TIMER_CC_CTRL_CUFOA_TOGGLE
SL_HAL_TIMER_CHANNEL_OUTPUT_ACTION_CLEAR = _TIMER_CC_CTRL_CUFOA_CLEAR
SL_HAL_TIMER_CHANNEL_OUTPUT_ACTION_SET = _TIMER_CC_CTRL_CUFOA_SET
}

Compare/capture output action.

enum
SL_HAL_TIMER_PRESCALER_DIV1 = _TIMER_CFG_PRESC_DIV1
SL_HAL_TIMER_PRESCALER_DIV2 = _TIMER_CFG_PRESC_DIV2
SL_HAL_TIMER_PRESCALER_DIV4 = _TIMER_CFG_PRESC_DIV4
SL_HAL_TIMER_PRESCALER_DIV8 = _TIMER_CFG_PRESC_DIV8
SL_HAL_TIMER_PRESCALER_DIV16 = _TIMER_CFG_PRESC_DIV16
SL_HAL_TIMER_PRESCALER_DIV32 = _TIMER_CFG_PRESC_DIV32
SL_HAL_TIMER_PRESCALER_DIV64 = _TIMER_CFG_PRESC_DIV64
SL_HAL_TIMER_PRESCALER_DIV128 = _TIMER_CFG_PRESC_DIV128
SL_HAL_TIMER_PRESCALER_DIV256 = _TIMER_CFG_PRESC_DIV256
SL_HAL_TIMER_PRESCALER_DIV512 = _TIMER_CFG_PRESC_DIV512
SL_HAL_TIMER_PRESCALER_DIV1024 = _TIMER_CFG_PRESC_DIV1024
}

Prescaler.

enum
SL_HAL_TIMER_CHANNEL_INPUT_PIN = _TIMER_CC_CFG_INSEL_PIN
SL_HAL_TIMER_CHANNEL_INPUT_PRS_SYNC = _TIMER_CC_CFG_INSEL_PRSSYNC
SL_HAL_TIMER_CHANNEL_INPUT_PRS_ASYNC_LEVEL = _TIMER_CC_CFG_INSEL_PRSASYNCLEVEL
SL_HAL_TIMER_CHANNEL_INPUT_PRS_ASYNC_PULSE = _TIMER_CC_CFG_INSEL_PRSASYNCPULSE
}

Input type.

enum
SL_HAL_TIMER_DTI_FAULT_ACTION_NONE = _TIMER_DTFCFG_DTFA_NONE
SL_HAL_TIMER_DTI_FAULT_ACTION_INACTIVE = _TIMER_DTFCFG_DTFA_INACTIVE
SL_HAL_TIMER_DTI_FAULT_ACTION_CLEAR = _TIMER_DTFCFG_DTFA_CLEAR
SL_HAL_TIMER_DTI_FAULT_ACTION_TRISTATE = _TIMER_DTFCFG_DTFA_TRISTATE
}

DT (Dead Time) Fault Actions.

Functions#

void
sl_hal_timer_init(TIMER_TypeDef *timer, const sl_hal_timer_config_t *init)

Initialize TIMER.

void
sl_hal_timer_channel_init(TIMER_TypeDef *timer, uint8_t channel, const sl_hal_timer_channel_config_t *init)

Initialize the TIMER compare/capture channel.

void
sl_hal_timer_dti_init(TIMER_TypeDef *timer, const sl_hal_timer_dti_config_t *init)

Initialize the TIMER DTI unit.

void
sl_hal_timer_reset(TIMER_TypeDef *timer)

Reset the TIMER to the same state that it was in after a hardware reset.

void
sl_hal_timer_wait_sync(TIMER_TypeDef *timer)

Wait for ongoing sync of register(s) to the low-frequency domain to complete.

void
sl_hal_timer_wait_ready(TIMER_TypeDef *timer)

Wait for disabling to finish.

void
sl_hal_timer_enable(TIMER_TypeDef *timer)

Enable TIMER.

void
sl_hal_timer_disable(TIMER_TypeDef *timer)

Disable TIMER.

void
sl_hal_timer_start(TIMER_TypeDef *timer)

Start TIMER.

void
sl_hal_timer_stop(TIMER_TypeDef *timer)

Stop TIMER.

void

Sends software command to update channel registers in the following update event using software.

uint32_t
sl_hal_timer_channel_get_capture(TIMER_TypeDef *timer, uint8_t channel)

Get capture value for the capture channel.

uint32_t
sl_hal_timer_channel_get_capture_buffer(TIMER_TypeDef *timer, uint8_t channel)

Get the buffered capture value for capture channel.

uint32_t
sl_hal_timer_channel_get_compare(TIMER_TypeDef *timer, uint8_t channel)

Get compare value for the compare channel.

uint32_t
sl_hal_timer_channel_get_compare_buffer(TIMER_TypeDef *timer, uint8_t channel)

Get the buffered compare value for compare channel.

void
sl_hal_timer_channel_set_compare_buffer(TIMER_TypeDef *timer, uint8_t channel, uint32_t value)

Set the compare value buffer for the compare/capture channel when operating in compare or PWM mode.

void
sl_hal_timer_channel_set_compare(TIMER_TypeDef *timer, uint8_t channel, uint32_t value)

Set the compare value for compare/capture channel when operating in compare or PWM mode.

void
sl_hal_timer_channel_set_phase(TIMER_TypeDef *timer, uint8_t channel, uint32_t phase)

Update timer phase value.

uint32_t
sl_hal_timer_channel_get_phase(TIMER_TypeDef *timer, uint8_t channel)

Get timer phase value.

void
sl_hal_timer_channel_set_phase_buffer(TIMER_TypeDef *timer, uint8_t channel, uint32_t phase)

Update timer phase buffer value.

uint32_t
sl_hal_timer_channel_get_phase_buffer(TIMER_TypeDef *timer, uint8_t channel)

Get timer phase buffer value.

void
sl_hal_timer_channel_set_dither(TIMER_TypeDef *timer, uint8_t channel, uint8_t dither)

Update timer dither value.

uint8_t
sl_hal_timer_channel_get_dither(TIMER_TypeDef *timer, uint8_t channel)

Get timer dither value.

void
sl_hal_timer_channel_set_dither_buffer(TIMER_TypeDef *timer, uint8_t channel, uint8_t dither)

Update timer dither buffer value.

uint8_t
sl_hal_timer_channel_get_dither_buffer(TIMER_TypeDef *timer, uint8_t channel)

Get timer dither buffer value.

uint32_t
sl_hal_timer_get_counter(TIMER_TypeDef *timer)

Get the TIMER counter value.

void
sl_hal_timer_set_counter(TIMER_TypeDef *timer, uint32_t value)

Set the TIMER counter value.

void
sl_hal_timer_set_top_buffer(TIMER_TypeDef *timer, uint32_t value)

Set the top value buffer for the timer.

void
sl_hal_timer_set_top(TIMER_TypeDef *timer, uint32_t value)

Set the top value for timer.

uint32_t
sl_hal_timer_get_top(TIMER_TypeDef *timer)

Get the top value setting for the timer.

uint32_t
sl_hal_timer_get_status(TIMER_TypeDef *timer)

Get status values for the timer.

uint32_t
sl_hal_timer_get_status2(TIMER_TypeDef *timer)

Get status2 values for the timer.

void
sl_hal_timer_lock(TIMER_TypeDef *timer)

Lock some TIMER registers to protect them from being modified.

void
sl_hal_timer_unlock(TIMER_TypeDef *timer)

Unlock some TIMER registers to be able to modify registers.

void
sl_hal_timer_dti_enable(TIMER_TypeDef *timer)

Enable DTI unit.

void
sl_hal_timer_dti_disable(TIMER_TypeDef *timer)

Disable DTI unit.

uint32_t
sl_hal_timer_dti_get_fault(TIMER_TypeDef *timer)

Get DTI fault source flags status.

void
sl_hal_timer_dti_clear_fault(TIMER_TypeDef *timer, uint32_t flags)

Clear DTI fault source flags.

void
sl_hal_timer_dti_unlock(TIMER_TypeDef *timer)

Unlock timer DTI to enable writing to locked registers again.

void
sl_hal_timer_dti_lock(TIMER_TypeDef *timer)

Lock timer DTI to disable writing to registers.

void
sl_hal_timer_clear_interrupts(TIMER_TypeDef *timer, uint32_t flags)

Clear one or more pending TIMER interrupts.

void
sl_hal_timer_disable_interrupts(TIMER_TypeDef *timer, uint32_t flags)

Disable one or more TIMER interrupts.

void
sl_hal_timer_enable_interrupts(TIMER_TypeDef *timer, uint32_t flags)

Enable one or more TIMER interrupts.

uint32_t

Get pending TIMER interrupt flags.

uint32_t

Get enabled and pending TIMER interrupt flags.

void
sl_hal_timer_set_interrupts(TIMER_TypeDef *timer, uint32_t flags)

Set one or more pending TIMER interrupts from SW.

Macros#

#define

Check if TIMER instance is valid.

#define

Return TIMER instance max count.

#define

Return TIMER instance channel count.

#define

Check if TIMER instance supports DTI.

#define

Default configuration for TIMER initialization structure.

#define

Default configuration for TIMER compare/capture initialization structure.

#define

PWM mode configuration for TIMER compare/capture initialization structure.

#define

Default configuration for TIMER DTI initialization structure.

Enumeration Documentation#

sl_hal_timer_channel_mode_t#

sl_hal_timer_channel_mode_t

Timer compare/capture mode.

Enumerator
SL_HAL_TIMER_CHANNEL_MODE_OFF

Channel turned off.

SL_HAL_TIMER_CHANNEL_MODE_CAPTURE

Input capture.

SL_HAL_TIMER_CHANNEL_MODE_COMPARE

Output compare.

SL_HAL_TIMER_CHANNEL_MODE_PWM

Pulse-Width modulation.


sl_hal_timer_clock_select_t#

sl_hal_timer_clock_select_t

Clock select.

Enumerator
SL_HAL_TIMER_CLKSEL_HFPERCLK

Prescaled EM01GRPA clock.

SL_HAL_TIMER_CLKSEL_CC1

Compare/Capture Channel 1 Input.

SL_HAL_TIMER_CLKSEL_CASCADE

Cascaded clocked by underflow or overflow by lower numbered timer.


sl_hal_timer_channel_input_edge_t#

sl_hal_timer_channel_input_edge_t

Input capture edge select.

Enumerator
SL_HAL_TIMER_CHANNEL_EDGE_RISING

Rising edges detected.

SL_HAL_TIMER_CHANNEL_EDGE_FALLING

Falling edges detected.

SL_HAL_TIMER_CHANNEL_EDGE_BOTH

Both edges detected.

SL_HAL_TIMER_CHANNEL_EDGE_NONE

No edge detection, leave signal as is.


sl_hal_timer_channel_input_event_t#

sl_hal_timer_channel_input_event_t

Input capture event control.

Enumerator
SL_HAL_TIMER_CHANNEL_EVENT_EVERY_EDGE

PRS output pulse, interrupt flag, and DMA request set on every capture.

SL_HAL_TIMER_CHANNEL_EVENT_EVERY_SECONDE_EDGE

PRS output pulse, interrupt flag, and DMA request set on every second capture.

SL_HAL_TIMER_CHANNEL_EVENT_RISING

PRS output pulse, interrupt flag, and DMA request set on rising edge (if input capture edge = BOTH).

SL_HAL_TIMER_CHANNEL_EVENT_FALLING

PRS output pulse, interrupt flag, and DMA request set on falling edge (if input capture edge = BOTH).


sl_hal_timer_input_edge_action_t#

sl_hal_timer_input_edge_action_t

Input edge action.

Enumerator
SL_HAL_TIMER_INPUT_ACTION_NONE

No action taken.

SL_HAL_TIMER_INPUT_ACTION_START

Start counter without reload.

SL_HAL_TIMER_INPUT_ACTION_STOP

Stop counter without reload.

SL_HAL_TIMER_INPUT_ACTION_RELOAD_START

Reload and start counter.


sl_hal_timer_mode_t#

sl_hal_timer_mode_t

Timer mode.

Enumerator
SL_HAL_TIMER_MODE_UP

Up-counting.

SL_HAL_TIMER_MODE_DOWN

Down-counting.

SL_HAL_TIMER_MODE_UPDOWN

Up/down-counting.

SL_HAL_TIMER_MODE_QDEC

Quadrature decoder.


sl_hal_timer_channel_output_action_t#

sl_hal_timer_channel_output_action_t

Compare/capture output action.

Enumerator
SL_HAL_TIMER_CHANNEL_OUTPUT_ACTION_NONE

No action.

SL_HAL_TIMER_CHANNEL_OUTPUT_ACTION_TOGGLE

Toggle on event.

SL_HAL_TIMER_CHANNEL_OUTPUT_ACTION_CLEAR

Clear on event.

SL_HAL_TIMER_CHANNEL_OUTPUT_ACTION_SET

Set on event.


sl_hal_timer_prescaler_t#

sl_hal_timer_prescaler_t

Prescaler.

Enumerator
SL_HAL_TIMER_PRESCALER_DIV1

Divide by 1.

SL_HAL_TIMER_PRESCALER_DIV2

Divide by 2.

SL_HAL_TIMER_PRESCALER_DIV4

Divide by 4.

SL_HAL_TIMER_PRESCALER_DIV8

Divide by 8.

SL_HAL_TIMER_PRESCALER_DIV16

Divide by 16.

SL_HAL_TIMER_PRESCALER_DIV32

Divide by 32.

SL_HAL_TIMER_PRESCALER_DIV64

Divide by 64.

SL_HAL_TIMER_PRESCALER_DIV128

Divide by 128.

SL_HAL_TIMER_PRESCALER_DIV256

Divide by 256.

SL_HAL_TIMER_PRESCALER_DIV512

Divide by 512.

SL_HAL_TIMER_PRESCALER_DIV1024

Divide by 1024.


sl_hal_timer_channel_input_type_t#

sl_hal_timer_channel_input_type_t

Input type.

Enumerator
SL_HAL_TIMER_CHANNEL_INPUT_PIN

No PRS input.

SL_HAL_TIMER_CHANNEL_INPUT_PRS_SYNC

Synchronous PRS selected.

SL_HAL_TIMER_CHANNEL_INPUT_PRS_ASYNC_LEVEL

Asynchronous level PRS selected.

SL_HAL_TIMER_CHANNEL_INPUT_PRS_ASYNC_PULSE

Asynchronous pulse PRS selected.


sl_hal_timer_dti_fault_action_t#

sl_hal_timer_dti_fault_action_t

DT (Dead Time) Fault Actions.

Enumerator
SL_HAL_TIMER_DTI_FAULT_ACTION_NONE

No action on fault.

SL_HAL_TIMER_DTI_FAULT_ACTION_INACTIVE

Set outputs inactive.

SL_HAL_TIMER_DTI_FAULT_ACTION_CLEAR

Clear outputs.

SL_HAL_TIMER_DTI_FAULT_ACTION_TRISTATE

Tristate outputs.


Function Documentation#

sl_hal_timer_init#

void sl_hal_timer_init (TIMER_TypeDef * timer, const sl_hal_timer_config_t * init)

Initialize TIMER.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

A pointer to the TIMER peripheral register block.

const sl_hal_timer_config_t *[in]init

A pointer to the TIMER initialization structure used to configure TIMER.

Notice that the counter top must be configured separately with, for instance sl_hal_timer_set_top(). In addition, compare/capture and dead-time insertion initialization must be initialized separately if used, which should probably be done prior to using this function if configuring the TIMER to start when initialization is completed.


sl_hal_timer_channel_init#

void sl_hal_timer_channel_init (TIMER_TypeDef * timer, uint8_t channel, const sl_hal_timer_channel_config_t * init)

Initialize the TIMER compare/capture channel.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

A pointer to the TIMER peripheral register block.

uint8_t[in]channel

A compare/capture channel to initialize for.

const sl_hal_timer_channel_config_t *[in]init

A pointer to the TIMER initialization structure.

Notice that if operating the channel in compare mode, the OC and OCB register must be set separately, as required.


sl_hal_timer_dti_init#

void sl_hal_timer_dti_init (TIMER_TypeDef * timer, const sl_hal_timer_dti_config_t * init)

Initialize the TIMER DTI unit.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

A pointer to the TIMER peripheral register block.

const sl_hal_timer_dti_config_t *[in]init

A pointer to the TIMER DTI initialization structure.


sl_hal_timer_reset#

void sl_hal_timer_reset (TIMER_TypeDef * timer)

Reset the TIMER to the same state that it was in after a hardware reset.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

A pointer to the TIMER peripheral register block.

Note

  • The ROUTE register is NOT reset by this function to allow for a centralized setup of this feature.


sl_hal_timer_wait_sync#

void sl_hal_timer_wait_sync (TIMER_TypeDef * timer)

Wait for ongoing sync of register(s) to the low-frequency domain to complete.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the timer peripheral register block.


sl_hal_timer_wait_ready#

void sl_hal_timer_wait_ready (TIMER_TypeDef * timer)

Wait for disabling to finish.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.


sl_hal_timer_enable#

void sl_hal_timer_enable (TIMER_TypeDef * timer)

Enable TIMER.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.


sl_hal_timer_disable#

void sl_hal_timer_disable (TIMER_TypeDef * timer)

Disable TIMER.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.


sl_hal_timer_start#

void sl_hal_timer_start (TIMER_TypeDef * timer)

Start TIMER.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.


sl_hal_timer_stop#

void sl_hal_timer_stop (TIMER_TypeDef * timer)

Stop TIMER.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.


sl_hal_timer_channel_update_registers#

void sl_hal_timer_channel_update_registers (TIMER_TypeDef * timer)

Sends software command to update channel registers in the following update event using software.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Note

  • If timer enable_update_mode is false, channel registers are updated automatically, and this API will do nothing. This function is only useful when enable_update_mode is true.


sl_hal_timer_channel_get_capture#

uint32_t sl_hal_timer_channel_get_capture (TIMER_TypeDef * timer, uint8_t channel)

Get capture value for the capture channel.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

Capture channel to access.

Returns

  • Current capture value.


sl_hal_timer_channel_get_capture_buffer#

uint32_t sl_hal_timer_channel_get_capture_buffer (TIMER_TypeDef * timer, uint8_t channel)

Get the buffered capture value for capture channel.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

Capture channel to access.

Returns

  • Current buffered capture value.


sl_hal_timer_channel_get_compare#

uint32_t sl_hal_timer_channel_get_compare (TIMER_TypeDef * timer, uint8_t channel)

Get compare value for the compare channel.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

Compare channel to access.

Returns

  • Current compare value.


sl_hal_timer_channel_get_compare_buffer#

uint32_t sl_hal_timer_channel_get_compare_buffer (TIMER_TypeDef * timer, uint8_t channel)

Get the buffered compare value for compare channel.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

Compare channel to access.

Returns

  • Current buffered compare value.


sl_hal_timer_channel_set_compare_buffer#

void sl_hal_timer_channel_set_compare_buffer (TIMER_TypeDef * timer, uint8_t channel, uint32_t value)

Set the compare value buffer for the compare/capture channel when operating in compare or PWM mode.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

Compare/capture channel to access.

uint32_t[in]value

Value to set in compare value buffer register.

The compare value buffer holds the value which will be written to TIMERn_CCx_CCV on an update event if the buffer has been updated since the last event.


sl_hal_timer_channel_set_compare#

void sl_hal_timer_channel_set_compare (TIMER_TypeDef * timer, uint8_t channel, uint32_t value)

Set the compare value for compare/capture channel when operating in compare or PWM mode.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

Compare/capture channel to access.

uint32_t[in]value

Value to set in compare value register.


sl_hal_timer_channel_set_phase#

void sl_hal_timer_channel_set_phase (TIMER_TypeDef * timer, uint8_t channel, uint32_t phase)

Update timer phase value.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

A compare/capture channel to set phase for.

uint32_t[in]phase

Phase value that determines the value at which CC output is set to 1 in PWM upcout mode.


sl_hal_timer_channel_get_phase#

uint32_t sl_hal_timer_channel_get_phase (TIMER_TypeDef * timer, uint8_t channel)

Get timer phase value.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

A compare/capture channel to get phase value from.

Returns

  • TIMER CC phase value.


sl_hal_timer_channel_set_phase_buffer#

void sl_hal_timer_channel_set_phase_buffer (TIMER_TypeDef * timer, uint8_t channel, uint32_t phase)

Update timer phase buffer value.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

A compare/capture channel to set phase for.

uint32_t[in]phase

Phase value to write to the phase buffer. The phase buffer value is written to the phase register automatically or via software command using sl_hal_timer_channel_update_registers.


sl_hal_timer_channel_get_phase_buffer#

uint32_t sl_hal_timer_channel_get_phase_buffer (TIMER_TypeDef * timer, uint8_t channel)

Get timer phase buffer value.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

A compare/capture channel to get phase value from.

Returns

  • TIMER CC phase buffer value.


sl_hal_timer_channel_set_dither#

void sl_hal_timer_channel_set_dither (TIMER_TypeDef * timer, uint8_t channel, uint8_t dither)

Update timer dither value.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

A compare/capture channel to set dither for.

uint8_t[in]dither

Dither value that determines the number of PWM pulses to add the dithering to, out of 2^DITHERWIDTH pulses.


sl_hal_timer_channel_get_dither#

uint8_t sl_hal_timer_channel_get_dither (TIMER_TypeDef * timer, uint8_t channel)

Get timer dither value.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

A compare/capture channel to get dither value from.

Returns

  • TIMER CC dither value.


sl_hal_timer_channel_set_dither_buffer#

void sl_hal_timer_channel_set_dither_buffer (TIMER_TypeDef * timer, uint8_t channel, uint8_t dither)

Update timer dither buffer value.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

A compare/capture channel to set dither buffer value for.

uint8_t[in]dither

The dither buffer value is written to the dither register automatically or via software command using sl_hal_timer_channel_update_registers.


sl_hal_timer_channel_get_dither_buffer#

uint8_t sl_hal_timer_channel_get_dither_buffer (TIMER_TypeDef * timer, uint8_t channel)

Get timer dither buffer value.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint8_t[in]channel

A compare/capture channel to get dither buffer value from.

Returns

  • TIMER CC buffer dither value.


sl_hal_timer_get_counter#

uint32_t sl_hal_timer_get_counter (TIMER_TypeDef * timer)

Get the TIMER counter value.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to TIMER peripheral register block.

Returns

  • Current TIMER counter value.


sl_hal_timer_set_counter#

void sl_hal_timer_set_counter (TIMER_TypeDef * timer, uint32_t value)

Set the TIMER counter value.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]value

Value to set counter to.


sl_hal_timer_set_top_buffer#

void sl_hal_timer_set_top_buffer (TIMER_TypeDef * timer, uint32_t value)

Set the top value buffer for the timer.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]value

Value to set in top value buffer register.

When top value buffer register is updated, value is loaded into top value register at the next wrap around. This feature is useful in order to update top value safely when timer is running.


sl_hal_timer_set_top#

void sl_hal_timer_set_top (TIMER_TypeDef * timer, uint32_t value)

Set the top value for timer.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]value

Value to set in top value register.


sl_hal_timer_get_top#

uint32_t sl_hal_timer_get_top (TIMER_TypeDef * timer)

Get the top value setting for the timer.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Returns

  • Current top value.


sl_hal_timer_get_status#

uint32_t sl_hal_timer_get_status (TIMER_TypeDef * timer)

Get status values for the timer.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Returns

  • Current status values.


sl_hal_timer_get_status2#

uint32_t sl_hal_timer_get_status2 (TIMER_TypeDef * timer)

Get status2 values for the timer.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Returns

  • Current status2 values.


sl_hal_timer_lock#

void sl_hal_timer_lock (TIMER_TypeDef * timer)

Lock some TIMER registers to protect them from being modified.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to TIMER peripheral register block.

Refer to the reference manual for TIMER registers that will be locked.

Note

  • If locking the TIMER registers, they must be unlocked prior to using any TIMER API function that modifies TIMER registers protected by the lock.


sl_hal_timer_unlock#

void sl_hal_timer_unlock (TIMER_TypeDef * timer)

Unlock some TIMER registers to be able to modify registers.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to TIMER peripheral register block.

Refer to the reference manual for TIMER registers that will be unlocked.

Note

  • Unlock prior to using any TIMER API function that modifies TIMER registers protected by the lock.


sl_hal_timer_dti_enable#

void sl_hal_timer_dti_enable (TIMER_TypeDef * timer)

Enable DTI unit.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Make sure to enable the DTI before enabling the timer.


sl_hal_timer_dti_disable#

void sl_hal_timer_dti_disable (TIMER_TypeDef * timer)

Disable DTI unit.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Make sure to disable the DTI before enabling the timer.


sl_hal_timer_dti_get_fault#

uint32_t sl_hal_timer_dti_get_fault (TIMER_TypeDef * timer)

Get DTI fault source flags status.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Note

  • Event bits are not cleared by this function.

Returns

  • Status of the DTI fault source flags. Returns one or more valid DTI fault source flags (TIMER_DTFAULT_nnn) OR'ed together.


sl_hal_timer_dti_clear_fault#

void sl_hal_timer_dti_clear_fault (TIMER_TypeDef * timer, uint32_t flags)

Clear DTI fault source flags.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]flags

DTI fault source(s) to clear. Use one or more valid DTI fault source flags (TIMER_DTFAULT_nnn) OR'ed together.


sl_hal_timer_dti_unlock#

void sl_hal_timer_dti_unlock (TIMER_TypeDef * timer)

Unlock timer DTI to enable writing to locked registers again.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.


sl_hal_timer_dti_lock#

void sl_hal_timer_dti_lock (TIMER_TypeDef * timer)

Lock timer DTI to disable writing to registers.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.


sl_hal_timer_clear_interrupts#

void sl_hal_timer_clear_interrupts (TIMER_TypeDef * timer, uint32_t flags)

Clear one or more pending TIMER interrupts.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]flags

Pending TIMER interrupt source(s) to clear. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.


sl_hal_timer_disable_interrupts#

void sl_hal_timer_disable_interrupts (TIMER_TypeDef * timer, uint32_t flags)

Disable one or more TIMER interrupts.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]flags

TIMER interrupt source(s) to disable. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.


sl_hal_timer_enable_interrupts#

void sl_hal_timer_enable_interrupts (TIMER_TypeDef * timer, uint32_t flags)

Enable one or more TIMER interrupts.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]flags

TIMER interrupt source(s) to enable. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using TIMER_IntClear() prior to enabling the interrupt.


sl_hal_timer_get_pending_interrupts#

uint32_t sl_hal_timer_get_pending_interrupts (TIMER_TypeDef * timer)

Get pending TIMER interrupt flags.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Note

  • Event bits are not cleared by this function.

Returns

  • TIMER interrupt source(s) pending. Returns one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.


sl_hal_timer_get_enabled_pending_interrupts#

uint32_t sl_hal_timer_get_enabled_pending_interrupts (TIMER_TypeDef * timer)

Get enabled and pending TIMER interrupt flags.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Interrupt flags are not cleared by this function.

Returns

  • Pending and enabled TIMER interrupt sources. The return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in TIMERx_IEN_nnn register (TIMERx_IEN_nnn) and

    • the OR combination of valid interrupt flags of the TIMER module (TIMERx_IF_nnn).


sl_hal_timer_set_interrupts#

void sl_hal_timer_set_interrupts (TIMER_TypeDef * timer, uint32_t flags)

Set one or more pending TIMER interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
TIMER_TypeDef *[in]timer

Pointer to the TIMER peripheral register block.

uint32_t[in]flags

TIMER interrupt source(s) to set to pending. Use one or more valid interrupt flags for the TIMER module (TIMER_IF_nnn) OR'ed together.


Macro Definition Documentation#

SL_HAL_TIMER_REF_VALID#

#define SL_HAL_TIMER_REF_VALID
Value:
(timer_ref)

Check if TIMER instance is valid.


SL_HAL_TIMER_MAX_COUNT#

#define SL_HAL_TIMER_MAX_COUNT
Value:
(timer_ref)

Return TIMER instance max count.


SL_HAL_TIMER_CHANNEL_NUM#

#define SL_HAL_TIMER_CHANNEL_NUM
Value:
(timer_ref)

Return TIMER instance channel count.


SL_HAL_TIMER_SUPPORTS_DTI#

#define SL_HAL_TIMER_SUPPORTS_DTI
Value:
(timer_ref)

Check if TIMER instance supports DTI.


SL_HAL_TIMER_CONFIG_DEFAULT#

#define SL_HAL_TIMER_CONFIG_DEFAULT
Value:
{ \
(sl_hal_timer_mode_t)_TIMER_CFG_MODE_DEFAULT, /* Up-counting. */ \
(sl_hal_timer_clock_select_t)_TIMER_CFG_CLKSEL_DEFAULT, /* Select HFPER / HFPERB clock. */ \
(sl_hal_timer_prescaler_t)_TIMER_CFG_PRESC_DEFAULT, /* No prescaling. */ \
(sl_hal_timer_input_edge_action_t)_TIMER_CTRL_RISEA_DEFAULT, /* No action on rising input edge. */ \
(sl_hal_timer_input_edge_action_t)_TIMER_CTRL_FALLA_DEFAULT, /* No action on falling input edge. */ \
(bool)_TIMER_CFG_SYNC_DEFAULT, /* Not started/stopped/reloaded by other timers. */ \
(bool)_TIMER_CFG_OSMEN_DEFAULT, /* Disable one shot. */ \
(bool)_TIMER_CFG_QDM_DEFAULT, /* Select default X2 quadrature decode mode (if used). */ \
(bool)_TIMER_CFG_DEBUGRUN_DEFAULT, /* Stop counter during debug halt. */ \
(bool)_TIMER_CFG_DMACLRACT_DEFAULT, /* Stop counter during debug halt. */ \
(bool)_TIMER_CFG_RETIMEEN_DEFAULT, /* Disable retime. */ \
(bool)_TIMER_CFG_DISSYNCOUT_DEFAULT, /* Disable ability to start/stop/reload other timers. */ \
(bool)_TIMER_CFG_ATI_DEFAULT, /* No ATI. */ \
(bool)_TIMER_CFG_RSSCOIST_DEFAULT, /* RSSCOIST is disabled. */ \
(bool)_TIMER_CTRL_X2CNT_DEFAULT, /* Not 2x count mode. */ \
(bool)_TIMER_CFG_UPDATEMODE_DEFAULT /* Automatic write from CCB to CC registers. */ \
}

Default configuration for TIMER initialization structure.


SL_HAL_TIMER_CHANNEL_CONFIG_DEFAULT#

#define SL_HAL_TIMER_CHANNEL_CONFIG_DEFAULT
Value:
{ \
(uint32_t)_TIMER_CC_PHASE_PHASE_DEFAULT, /* No phase value. */ \
(uint32_t)_TIMER_CC_DITHER_DITHER_DEFAULT, /* No dither value. */ \
(sl_hal_timer_channel_mode_t)_TIMER_CC_CFG_MODE_DEFAULT, /* Disable compare/capture channel. */ \
(sl_hal_timer_channel_input_type_t)_TIMER_CC_CFG_INSEL_DEFAULT, /* Select PIN. */ \
(sl_hal_timer_channel_output_action_t)_TIMER_CC_CTRL_CMOA_DEFAULT, /* No action on match. */ \
(sl_hal_timer_channel_output_action_t)_TIMER_CC_CTRL_CUFOA_DEFAULT, /* No action on underflow. */ \
(sl_hal_timer_channel_output_action_t)_TIMER_CC_CTRL_COFOA_DEFAULT, /* No action on overflow. */ \
(sl_hal_timer_channel_input_event_t)_TIMER_CC_CTRL_ICEVCTRL_DEFAULT, /* Event on every capture. */ \
(sl_hal_timer_channel_input_edge_t)_TIMER_CC_CTRL_ICEDGE_DEFAULT, /* Use default PRS output configuration. */ \
(uint8_t)_TIMER_CC_CFG_ICFWL_DEFAULT, /* Disable watermark level check. */ \
(bool)_TIMER_CC_CFG_COIST_DEFAULT, /* Clear output when counter disabled. */ \
(bool)_TIMER_CC_CFG_PRSCONF_DEFAULT, /* Use default PRS output configuration. */ \
(bool)_TIMER_CC_CFG_FILT_DEFAULT, /* Disable filter. */ \
(bool)_TIMER_CC_CTRL_OUTINV_DEFAULT, /* Do not invert output. */ \
}

Default configuration for TIMER compare/capture initialization structure.


SL_HAL_TIMER_CHANNEL_CONFIG_PWM#

#define SL_HAL_TIMER_CHANNEL_CONFIG_PWM
Value:
{ \
(uint32_t)_TIMER_CC_PHASE_PHASE_DEFAULT, /* No phase value. */ \
(uint32_t)_TIMER_CC_DITHER_DITHER_DEFAULT, /* No dither value. */ \
SL_HAL_TIMER_CHANNEL_MODE_PWM, /* Set PWM mode. */ \
(sl_hal_timer_channel_input_type_t)_TIMER_CC_CFG_INSEL_DEFAULT, /* Select PIN. */ \
SL_HAL_TIMER_CHANNEL_OUTPUT_ACTION_TOGGLE, /* Toggle on match. */ \
(sl_hal_timer_channel_output_action_t)_TIMER_CC_CTRL_CUFOA_DEFAULT, /* No action on underflow. */ \
(sl_hal_timer_channel_output_action_t)_TIMER_CC_CTRL_COFOA_DEFAULT, /* No action on overflow. */ \
(sl_hal_timer_channel_input_event_t)_TIMER_CC_CTRL_ICEVCTRL_DEFAULT, /* Event on every capture. */ \
(sl_hal_timer_channel_input_edge_t)_TIMER_CC_CTRL_ICEDGE_DEFAULT, /* Use default PRS output configuration. */ \
(uint8_t)_TIMER_CC_CFG_ICFWL_DEFAULT, /* Disable watermark level check. */ \
(bool)_TIMER_CC_CFG_COIST_DEFAULT, /* Clear output when counter disabled. */ \
(bool)_TIMER_CC_CFG_PRSCONF_DEFAULT, /* Use default PRS output configuration. */ \
(bool)_TIMER_CC_CFG_FILT_DEFAULT, /* Disable filter. */ \
false, /* Do not invert output. */ \
}

PWM mode configuration for TIMER compare/capture initialization structure.


SL_HAL_TIMER_DTI_CONFIG_DEFAULT#

#define SL_HAL_TIMER_DTI_CONFIG_DEFAULT
Value:
{ \
(bool)_TIMER_DTCFG_DTDAS_DEFAULT, /* No auto restart when debugger exits. */ \
(bool)_TIMER_DTCFG_DTAR_DEFAULT, /* Stop DTI output on channel 0 when timer stops. */ \
(bool)_TIMER_DTCFG_DTFATS_DEFAULT, /* Disable safe state when timer stops. */ \
(bool)_TIMER_DTCFG_DTPRSEN_DEFAULT, /* No PRS source selected. */ \
(bool)_TIMER_DTCTRL_DTCINV_DEFAULT, /* CDTI[0|1|2] outputs are not inverted. */ \
(bool)_TIMER_DTCTRL_DTIPOL_DEFAULT, /* CC[0|1|2] outputs are active high. */ \
(bool)_TIMER_DTFCFG_DTLOCKUPFEN_DEFAULT, /* Disable core lockup as fault source. */ \
(bool)_TIMER_DTFCFG_DTDBGFEN_DEFAULT, /* Disable debugger as fault source. */ \
(bool)_TIMER_DTFCFG_DTPRS0FEN_DEFAULT, /* Disable PRS fault source 0. */ \
(bool)_TIMER_DTFCFG_DTPRS1FEN_DEFAULT, /* Disable PRS fault source 1. */ \
(sl_hal_timer_prescaler_t)_TIMER_DTTIMECFG_DTPRESC_DEFAULT, /* No prescaling. */ \
(uint8_t)_TIMER_DTTIMECFG_DTRISET_DEFAULT, /* No rise time. */ \
(uint8_t)_TIMER_DTTIMECFG_DTFALLT_DEFAULT, /* No rise time. */ \
(uint32_t)0, /* Disable output generation for all channels. */ \
(sl_hal_timer_dti_fault_action_t)_TIMER_DTFCFG_DTFA_DEFAULT, /* No fault action. */ \
}

Default configuration for TIMER DTI initialization structure.