You are viewing documentation for version:
Dimensions of the display. 
Public Attributes#
uint16_t
Horizontal size of the display, in pixels. 
uint16_t
Vertical size of the display, in pixels. 
uint16_t
X coordinate of the top left corner of the clipping area. 
uint16_t
Y coordinate of the top left corner of the clipping area. 
uint16_t
Width of the clipping area. 
uint16_t
Height of the clipping area. 
Public Attribute Documentation#
xSize#
uint16_t DMD_DisplayGeometry::xSize
Horizontal size of the display, in pixels. 
ySize#
uint16_t DMD_DisplayGeometry::ySize
Vertical size of the display, in pixels. 
xClipStart#
uint16_t DMD_DisplayGeometry::xClipStart
X coordinate of the top left corner of the clipping area. 
yClipStart#
uint16_t DMD_DisplayGeometry::yClipStart
Y coordinate of the top left corner of the clipping area. 
clipWidth#
uint16_t DMD_DisplayGeometry::clipWidth
Width of the clipping area. 
clipHeight#
uint16_t DMD_DisplayGeometry::clipHeight
Height of the clipping area.