USART - Synchronous/Asynchronous Serial#
Universal Synchronous/Asynchronous Receiver/Transmitter Peripheral API.
Introduction#
The Universal Synchronous/Asynchronous Receiver/Transmitter (USART) is a very flexible serial I/O module. It supports full duplex asynchronous UART communication as well as RS-485, SPI, MicroWire, and 3-wire. It can also interface with ISO7816 Smart-Cards, and IrDA devices.
The USART has a wide selection of operating modes, frame formats, and baud rates. All features are supported through the API of this module.
Triple buffering and DMA support makes high data-rates possible with minimal CPU intervention. It is possible to transmit and receive large frames while the MCU remains in EM1 Sleep.
This module does not support DMA configuration. The UARTDRV and SPIDRV drivers provide full support for DMA and more.
The following steps are necessary for basic operation:
Note
UARTDRV supports all types of UART flow control. Software assisted hardware flow control is available for parts without true UART hardware flow control.
Example#
USART Asynchronous UART TX example:
{
#define GPIO_TX PB0
sl_hal_usart_async_init_t init = SL_HAL_USART_INIT_ASYNC_DEFAULT;
// Configure the clocks.
sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_USART0);
sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_GPIO);
// Calculate and configure the usart's clock divider.
uint32_t baudrate = 38400; // Desired baudrate.
sl_clock_branch_t clock_branch = sl_device_peripheral_get_clock_branch(SL_PERIPHERAL_USART0);
uint32_t freq;
sl_clock_manager_get_clock_branch_frequency(clock_branch, &freq);
init.clock_div = sl_hal_usart_async_calculate_clock_div(freq, baudrate, init.oversampling);
// Configure the USART port.
sl_gpio_set_pin_mode(GPIO_TX, SL_GPIO_MODE_PUSH_PULL, 0);
GPIO->USARTROUTE[USART_NUM(USART0)].TXROUTE = (GPIO_TX->port << _GPIO_USART_TXROUTE_PORT_SHIFT)
| (GPIO_TX->pin << _GPIO_USART_TXROUTE_PIN_SHIFT);
GPIO->USARTROUTE[USART_NUM(USART0)].ROUTEEN = GPIO_USART_ROUTEEN_TXPEN;
// Initialize the USART.
sl_hal_usart_init_async(USART0, &init);
sl_hal_usart_enable(USART0);
sl_hal_usart_enable_tx(USART0);
uint16_t data = 0xFF;
sl_hal_usart_tx(USART0, data);
}
USART Synchronous SPI Initialization example:
{
#define GPIO_MOSI PC0
#define GPIO_MISO PC1
#define GPIO_SCLK PC2
sl_hal_usart_sync_init_t init = SL_HAL_USART_INIT_SYNC_DEFAULT;
// Operate as SPI master.
init.master = true;
// Clock idle low, sample on falling edge.
init.clock_mode = SL_HAL_USART_CLOCK_MODE_1;
// Configure the clocks.
sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_USART1);
sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_GPIO);
// Calculate and configure the usart's clock divider.
uint32_t baudrate = 1000000; // Desired baudrate.
sl_clock_branch_t clock_branch = sl_device_peripheral_get_clock_branch(SL_PERIPHERAL_USART1);
uint32_t freq;
sl_clock_manager_get_clock_branch_frequency(clock_branch, &freq);
init.clock_div = sl_hal_usart_sync_calculate_clock_div(freq, baudrate);
// Configure the SPI ports.
sl_gpio_set_pin_mode(GPIO_MOSI, SL_GPIO_MODE_PUSH_PULL, 0);
sl_gpio_set_pin_mode(GPIO_MISO, SL_GPIO_MODE_INPUT, 0);
sl_gpio_set_pin_mode(GPIO_SCLK, SL_GPIO_MODE_PUSH_PULL, 0);
// Connect USART to ports.
GPIO->USARTROUTE[USART_NUM(USART1)].TXROUTE = (GPIO_MOSI->port << _GPIO_USART_TXROUTE_PORT_SHIFT)
| (GPIO_MOSI->pin << _GPIO_USART_TXROUTE_PIN_SHIFT);
GPIO->USARTROUTE[USART_NUM(USART1)].RXROUTE = (GPIO_MISO->port << _GPIO_USART_RXROUTE_PORT_SHIFT)
| (GPIO_MISO->pin << _GPIO_USART_RXROUTE_PIN_SHIFT);
GPIO->USARTROUTE[USART_NUM(USART1)].CLKROUTE = (GPIO_SCLK->port << _GPIO_USART_CLKROUTE_PORT_SHIFT)
| (GPIO_SCLK->pin << _GPIO_USART_CLKROUTE_PIN_SHIFT);
GPIO->USARTROUTE[USART_NUM(USART1)].ROUTEEN = GPIO_USART_ROUTEEN_TXPEN | GPIO_USART_ROUTEEN_RXPEN | GPIO_USART_ROUTEEN_CLKPEN;
// Initialize the USART.
sl_hal_usart_init_sync(USART1, &init);
sl_hal_usart_enable(USART1);
sl_hal_usart_enable_rx(USART1);
sl_hal_usart_enable_tx(USART1);
}
Modules#
Enumerations#
Databit selection.
Oversampling selection, used for asynchronous operation.
Parity selection, mainly used for asynchronous operation.
Stop bits selection, used for asynchronous operation.
Majority vote enable.
Hardware Flow Control Selection.
Clock polarity/phase mode.
Pulse width selection for IrDA mode.
I2S format selection.
I2S frame data justify.
Functions#
Initialize USART/UART for normal asynchronous mode.
Calculate baudrate for USART/UART given reference frequency, clock division, and oversampling rate.
Calculate UART clock divider using given reference frequency, oversampling and baudrate.
Initialize USART for synchronous mode.
Calculate baudrate for USART/UART (sync mode) given reference frequency, clock division.
Calculate UART (sync mode) clock divider using given reference frequency and baudrate.
Initialize USART for asynchronous IrDA mode.
Initialize USART for I2S mode.
Reset USART/UART to the same state that it was in after a hardware reset.
Transmit one 4-9 bit frame.
Perform one 8 bit frame SPI transfer.
Transmit two 4-9 bit frames or one 10-16 bit frame.
Transmit two 4-9 bit frames or one 10-16 bit frame with extended control.
Transmit one 4-9 bit frame with extended control.
Enable automatic enabling of reception using the PRS as a trigger.
Disable automatic enabling of reception using the PRS as a trigger.
Enable automatic enabling of transmission using the PRS as a trigger.
Disable automatic enabling of transmission using the PRS as a trigger.
Set UART mode clock divider.
Get UART mode clock divider.
Enable USART.
Disable USART.
Enable USART receiver.
Disable USART receiver.
Enable USART transmitter.
Disable USART transmitter.
Clear RX FIFO.
Clear TX FIFO.
Receive one 4-8 bit frame, (or part of 10-16 bit frame).
Receive two 4-8 bit frames or one 10-16 bit frame.
Receive two 4-9 bit frames, or one 10-16 bit frame with extended information.
Receive one 4-9 bit frame (or part of 10-16 bit frame) with extended information.
Receive one 4-8 bit frame, (or part of 10-16 bit frame).
Receive two 4-8 bit frames, or one 10-16 bit frame.
Receive two 4-9 bit frames, or one 10-16 bit frame with extended information.
Receive one 4-9 bit frame, (or part of 10-16 bit frame) with extended information.
Clear one or more pending USART interrupts.
Disable one or more USART interrupts.
Enable one or more USART interrupts.
Get pending USART interrupt flags.
Get enabled and pending USART interrupt flags.
Set one or more pending USART interrupts from SW.
Get USART STATUS register.
Macros#
Validation of USART register block pointer reference for assert statements. */.
Default configuration for USART asynchronous initialization structure.
Default configuration for USART sync initialization structure.
Default configuration for USART IRDA initialization structure.
Default USART Sync configuration for series 2 devices.
Enumeration Documentation#
sl_hal_usart_data_bits_t#
sl_hal_usart_data_bits_t
Databit selection.
| Enumerator | |
|---|---|
| SL_HAL_USART_DATA_BITS_4 | 4 data bits (not available for UART). |
| SL_HAL_USART_DATA_BITS_5 | 5 data bits (not available for UART). |
| SL_HAL_USART_DATA_BITS_6 | 6 data bits (not available for UART). |
| SL_HAL_USART_DATA_BITS_7 | 7 data bits (not available for UART). |
| SL_HAL_USART_DATA_BITS_8 | 8 data bits. |
| SL_HAL_USART_DATA_BITS_9 | 9 data bits. |
| SL_HAL_USART_DATA_BITS_10 | 10 data bits (not available for UART). |
| SL_HAL_USART_DATA_BITS_11 | 11 data bits (not available for UART). |
| SL_HAL_USART_DATA_BITS_12 | 12 data bits (not available for UART). |
| SL_HAL_USART_DATA_BITS_13 | 13 data bits (not available for UART). |
| SL_HAL_USART_DATA_BITS_14 | 14 data bits (not available for UART). |
| SL_HAL_USART_DATA_BITS_15 | 15 data bits (not available for UART). |
| SL_HAL_USART_DATA_BITS_16 | 16 data bits (not available for UART). |
sl_hal_usart_ovs_t#
sl_hal_usart_ovs_t
Oversampling selection, used for asynchronous operation.
| Enumerator | |
|---|---|
| SL_HAL_USART_OVS_16 | 16x oversampling (normal). |
| SL_HAL_USART_OVS_8 | 8x oversampling. |
| SL_HAL_USART_OVS_6 | 6x oversampling. |
| SL_HAL_USART_OVS_4 | 4x oversampling. |
sl_hal_usart_parity_t#
sl_hal_usart_parity_t
Parity selection, mainly used for asynchronous operation.
| Enumerator | |
|---|---|
| SL_HAL_USART_NO_PARITY | No parity. |
| SL_HAL_USART_EVEN_PARITY | Even parity. |
| SL_HAL_USART_ODD_PARITY | Odd parity. |
sl_hal_usart_stop_bits_t#
sl_hal_usart_stop_bits_t
Stop bits selection, used for asynchronous operation.
| Enumerator | |
|---|---|
| SL_HAL_USART_STOP_BITS_0P5 | 0.5 stop bits. |
| SL_HAL_USART_STOP_BITS_1 | 1 stop bits. |
| SL_HAL_USART_STOP_BITS_1P5 | 1.5 stop bits. |
| SL_HAL_USART_STOP_BITS_2 | 2 stop bits. |
sl_hal_usart_majority_vote_t#
sl_hal_usart_majority_vote_t
Majority vote enable.
| Enumerator | |
|---|---|
| SL_HAL_USART_MAJORITY_VOTE_ENABLE | Enable majority vote for 16x, 8x and 6x oversampling modes. |
| SL_HAL_USART_MAJORITY_VOTE_DISABLE | Disable majority vote for 16x, 8x and 6x oversampling modes. |
sl_hal_usart_hw_flow_control_t#
sl_hal_usart_hw_flow_control_t
Hardware Flow Control Selection.
| Enumerator | |
|---|---|
| SL_HAL_USART_HW_FLOW_CONTROL_NONE | No hardware flow control. |
| SL_HAL_USART_HW_FLOW_CONTROL_CTS | CTS signal is enabled for TX flow control. |
| SL_HAL_USART_HW_FLOW_CONTROL_RTS | RTS signal is enabled for RX flow control. |
| SL_HAL_USART_HW_FLOW_CONTROL_CTS_RTS | CTS and RTS signals are enabled for TX and RX flow control. |
sl_hal_usart_clock_mode_t#
sl_hal_usart_clock_mode_t
Clock polarity/phase mode.
| Enumerator | |
|---|---|
| SL_HAL_USART_CLOCK_MODE_0 | Clock idle low, sample on rising edge. |
| SL_HAL_USART_CLOCK_MODE_1 | Clock idle low, sample on falling edge. |
| SL_HAL_USART_CLOCK_MODE_2 | Clock idle high, sample on falling edge. |
| SL_HAL_USART_CLOCK_MODE_3 | Clock idle high, sample on rising edge. |
sl_hal_usart_irda_pulse_width_t#
sl_hal_usart_irda_pulse_width_t
Pulse width selection for IrDA mode.
| Enumerator | |
|---|---|
| SL_HAL_USART_PULSE_WIDTH_ONE | IrDA pulse width is 1/16 for OVS=0 and 1/8 for OVS=1. |
| SL_HAL_USART_PULSE_WIDTH_TWO | IrDA pulse width is 2/16 for OVS=0 and 2/8 for OVS=1. |
| SL_HAL_USART_PULSE_WIDTH_THREE | IrDA pulse width is 3/16 for OVS=0 and 3/8 for OVS=1. |
| SL_HAL_USART_PULSE_WIDTH_FOUR | IrDA pulse width is 4/16 for OVS=0 and 4/8 for OVS=1. |
sl_hal_usart_i2s_format_t#
sl_hal_usart_i2s_format_t
I2S format selection.
| Enumerator | |
|---|---|
| SL_HAL_USART_I2S_FORMAT_W32D32 | 32-bit word, 32-bit data. |
| SL_HAL_USART_I2S_FORMAT_W32D24M | 32-bit word, 32-bit data with 8 lsb masked. |
| SL_HAL_USART_I2S_FORMAT_W32D24 | 32-bit word, 24-bit data. |
| SL_HAL_USART_I2S_FORMAT_W32D16 | 32-bit word, 16-bit data. |
| SL_HAL_USART_I2S_FORMAT_W32D8 | 32-bit word, 8-bit data. |
| SL_HAL_USART_I2S_FORMAT_W16D16 | 16-bit word, 16-bit data. |
| SL_HAL_USART_I2S_FORMAT_W16D8 | 16-bit word, 8-bit data. |
| SL_HAL_USART_I2S_FORMAT_W8D8 | 8-bit word, 8-bit data. |
sl_hal_usart_i2s_justify_t#
sl_hal_usart_i2s_justify_t
I2S frame data justify.
| Enumerator | |
|---|---|
| SL_HAL_USART_JUSTIFY_LEFT | Data is left-justified within the frame. |
| SL_HAL_USART_JUSTIFY_RIGHT | Data is right-justified within the frame. |
Function Documentation#
sl_hal_usart_init_async#
void sl_hal_usart_init_async (USART_TypeDef * usart, const sl_hal_usart_async_init_t * init)
Initialize USART/UART for normal asynchronous mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART/UART peripheral register block. |
| const sl_hal_usart_async_init_t * | [in] | init | A pointer to the initialization structure used to configure the basic async setup. |
This function will configure basic settings to operate in normal asynchronous mode.
A special control setup not covered by this function must be done after using this function by direct modification of the CTRL register.
Notice that pins used by the USART/UART module must be properly configured by the user explicitly for the USART/UART to work as intended. (When configuring pins, remember to consider the sequence of configuration to avoid unintended pulses/glitches on output pins.)
sl_hal_usart_async_calculate_baudrate#
uint32_t sl_hal_usart_async_calculate_baudrate (uint32_t ref_freq, uint32_t clk_div, sl_hal_usart_ovs_t ovs)
Calculate baudrate for USART/UART given reference frequency, clock division, and oversampling rate.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | ref_freq | USART/UART HF peripheral frequency used. |
| uint32_t | [in] | clk_div | A clock division factor to be used. |
| sl_hal_usart_ovs_t | [in] | ovs | Oversample value of the USART. |
This function returns the baudrate that a USART/UART module will use if configured with the given frequency, clock divider, and mode. Notice that this function will not use the hardware configuration. It can be used to determine if a given configuration is sufficiently accurate for the application.
Returns
Baudrate with given settings.
sl_hal_usart_async_calculate_clock_div#
uint32_t sl_hal_usart_async_calculate_clock_div (uint32_t ref_freq, uint32_t baudrate, sl_hal_usart_ovs_t ovs)
Calculate UART clock divider using given reference frequency, oversampling and baudrate.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | ref_freq | Peripheral clock frequency. |
| uint32_t | [in] | baudrate | Transmission speed of the UART interface. |
| sl_hal_usart_ovs_t | [in] | ovs | Oversampling rate. |
Returns
USART clock divider for desired baud rate.
sl_hal_usart_init_sync#
void sl_hal_usart_init_sync (USART_TypeDef * usart, const sl_hal_usart_sync_init_t * init)
Initialize USART for synchronous mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART peripheral register block. (UART does not support this mode.) |
| const sl_hal_usart_sync_init_t * | [in] | init | A pointer to the initialization structure used to configure basic async setup. |
This function will configure basic settings to operate in synchronous mode.
A special control setup not covered by this function must be done after using this function by direct modification of the CTRL register.
Notice that pins used by the USART module must be properly configured by the user explicitly for the USART to work as intended. (When configuring pins remember to consider the sequence of configuration to avoid unintended pulses/glitches on output pins.)
sl_hal_usart_sync_calculate_baudrate#
uint32_t sl_hal_usart_sync_calculate_baudrate (uint32_t ref_freq, uint32_t clk_div)
Calculate baudrate for USART/UART (sync mode) given reference frequency, clock division.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | ref_freq | USART/UART HF peripheral frequency used. |
| uint32_t | [in] | clk_div | A clock division factor to be used. |
This function returns the baudrate that a USART/UART module will use if configured with the given frequency, clock divider, and mode. Notice that this function will not use the hardware configuration. It can be used to determine if a given configuration is sufficiently accurate for the application.
Returns
Baudrate with given settings.
sl_hal_usart_sync_calculate_clock_div#
uint32_t sl_hal_usart_sync_calculate_clock_div (uint32_t ref_freq, uint32_t baudrate)
Calculate UART (sync mode) clock divider using given reference frequency and baudrate.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | ref_freq | Peripheral clock frequency. |
| uint32_t | [in] | baudrate | Transmission speed of the USART/UART interface. |
Returns
USART clock divider for desired baud rate.
sl_hal_usart_init_irda#
void sl_hal_usart_init_irda (USART_TypeDef * usart, const sl_hal_usart_irda_init_t * init)
Initialize USART for asynchronous IrDA mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART peripheral register block. |
| const sl_hal_usart_irda_init_t * | [in] | init | A pointer to the initialization structure used to configure async IrDA setup. |
This function will configure basic settings to operate in asynchronous IrDA mode.
A special control setup not covered by this function must be done after using this function by direct modification of the CTRL and IRCTRL registers.
Notice that pins used by the USART/UART module must be properly configured by the user explicitly for the USART/UART to work as intended. (When configuring pins, remember to consider the sequence of configuration to avoid unintended pulses/glitches on output pins.)
Note
Not all USART instances support IrDA.
sl_hal_usart_init_i2s#
void sl_hal_usart_init_i2s (USART_TypeDef * usart, const sl_hal_usart_i2s_init_t * init)
Initialize USART for I2S mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART peripheral register block. (UART does not support this mode.) |
| const sl_hal_usart_i2s_init_t * | [in] | init | A pointer to the initialization structure used to configure the basic I2S setup. |
This function will configure basic settings to operate in I2S mode.
A special control setup not covered by this function must be done after using this function by direct modification of the CTRL and I2SCTRL registers.
Notice that pins used by the USART module must be properly configured by the user explicitly for the USART to work as intended. (When configuring pins, remember to consider the sequence of configuration to avoid unintended pulses/glitches on output pins.)
Note
This function does not apply to all USART's.
sl_hal_usart_reset#
void sl_hal_usart_reset (USART_TypeDef * usart)
Reset USART/UART to the same state that it was in after a hardware reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to USART/UART peripheral register block. |
sl_hal_usart_tx#
void sl_hal_usart_tx (USART_TypeDef * usart, uint8_t data)
Transmit one 4-9 bit frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART/UART peripheral register block. |
| uint8_t | [in] | data | Data to transmit. See details above for more information. |
Depending on the frame length configuration, 4-8 (least significant) bits from data are transmitted. If the frame length is 9, 8 bits are transmitted from data and one bit as specified by CTRL register, BIT8DV field. See sl_hal_usart_tx_ext() for transmitting 9 bit frame with full control of all 9 bits.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
Note
This function will stall if the buffer is full until the buffer becomes available.
sl_hal_usart_spi_transfer#
uint8_t sl_hal_usart_spi_transfer (USART_TypeDef * usart, uint8_t data)
Perform one 8 bit frame SPI transfer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART peripheral register block. |
| uint8_t | [in] | data | Data to transmit. |
Note
This function will stall if the transmit buffer is full. When a transmit buffer becomes available, data is written and the function will wait until data is fully transmitted. The SPI return value is then read out and returned.
Returns
Data received.
sl_hal_usart_tx_double#
void sl_hal_usart_tx_double (USART_TypeDef * usart, uint16_t data)
Transmit two 4-9 bit frames or one 10-16 bit frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART/UART peripheral register block. |
| uint16_t | [in] | data | Data to transmit, the least significant byte holds the frame transmitted first. See details above for more info. |
Depending on the frame length configuration, 4-8 (least significant) bits from each byte in data are transmitted. If frame length is 9, 8 bits are transmitted from each byte in data adding one bit as specified by the CTRL register, BIT8DV field, to each byte. See sl_hal_usart_tx_double_ext() for transmitting two 9 bit frames with full control of all 9 bits.
If the frame length is 10-16, 10-16 (least significant) bits from data are transmitted.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
Note
This function will stall if the buffer is full until the buffer becomes available.
sl_hal_usart_tx_double_ext#
void sl_hal_usart_tx_double_ext (USART_TypeDef * usart, uint32_t data)
Transmit two 4-9 bit frames or one 10-16 bit frame with extended control.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART/UART peripheral register block. |
| uint32_t | [in] | data | Data to transmit with extended control. Contains two 16 bit words concatenated. Least significant word holds the frame transmitted first. If the frame length is 4-9, two frames with 4-9 least significant bits from each 16 bit word are transmitted. |
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
Note
This function will stall if the buffer is full until the buffer becomes available.
If the frame length is 10-16 bits, 8 data bits are taken from the least significant 16 bit word and the remaining bits from the other 16 bit word.
Additional control bits are available as documented in the reference manual (set to 0 if not used). For 10-16 bit frame length, these control bits are taken from the most significant 16 bit word.
sl_hal_usart_tx_ext#
void sl_hal_usart_tx_ext (USART_TypeDef * usart, uint16_t data)
Transmit one 4-9 bit frame with extended control.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART/UART peripheral register block. |
| uint16_t | [in] | data | Data to transmit with extended control. Least significant bit contains frame bits. Additional control bits are available as documented in the reference manual (set to 0 if not used). |
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
Note
This function will stall if the buffer is full until the buffer becomes available.
sl_hal_usart_enable_rx_prs_trigger#
void sl_hal_usart_enable_rx_prs_trigger (USART_TypeDef * usart, uint8_t channel)
Enable automatic enabling of reception using the PRS as a trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART peripheral register block. |
| uint8_t | [in] | channel | PRS channel to use. |
sl_hal_usart_disable_rx_prs_trigger#
void sl_hal_usart_disable_rx_prs_trigger (USART_TypeDef * usart)
Disable automatic enabling of reception using the PRS as a trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART peripheral register block. |
sl_hal_usart_enable_tx_prs_trigger#
void sl_hal_usart_enable_tx_prs_trigger (USART_TypeDef * usart, uint8_t channel)
Enable automatic enabling of transmission using the PRS as a trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART peripheral register block. |
| uint8_t | [in] | channel | PRS channel number. |
sl_hal_usart_disable_tx_prs_trigger#
void sl_hal_usart_disable_tx_prs_trigger (USART_TypeDef * usart)
Disable automatic enabling of transmission using the PRS as a trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART peripheral register block. |
sl_hal_usart_async_set_clock_div#
void sl_hal_usart_async_set_clock_div (USART_TypeDef * usart, uint32_t clock_div)
Set UART mode clock divider.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART peripheral register block. |
| uint32_t | [in] | clock_div | Clock divider value. |
sl_hal_usart_async_get_clock_div#
uint32_t sl_hal_usart_async_get_clock_div (USART_TypeDef * usart)
Get UART mode clock divider.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART peripheral register block. |
Returns
Clock divider value.
sl_hal_usart_enable#
void sl_hal_usart_enable (USART_TypeDef * usart)
Enable USART.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART peripheral register block. |
sl_hal_usart_disable#
void sl_hal_usart_disable (USART_TypeDef * usart)
Disable USART.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART peripheral register block. |
sl_hal_usart_enable_rx#
void sl_hal_usart_enable_rx (USART_TypeDef * usart)
Enable USART receiver.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART peripheral register block. |
sl_hal_usart_disable_rx#
void sl_hal_usart_disable_rx (USART_TypeDef * usart)
Disable USART receiver.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART peripheral register block. |
sl_hal_usart_enable_tx#
void sl_hal_usart_enable_tx (USART_TypeDef * usart)
Enable USART transmitter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART peripheral register block. |
sl_hal_usart_disable_tx#
void sl_hal_usart_disable_tx (USART_TypeDef * usart)
Disable USART transmitter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART peripheral register block. |
sl_hal_usart_clear_rx#
void sl_hal_usart_clear_rx (USART_TypeDef * usart)
Clear RX FIFO.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART peripheral register block. |
sl_hal_usart_clear_tx#
void sl_hal_usart_clear_tx (USART_TypeDef * usart)
Clear TX FIFO.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART peripheral register block. |
sl_hal_usart_rx#
uint8_t sl_hal_usart_rx (USART_TypeDef * usart)
Receive one 4-8 bit frame, (or part of 10-16 bit frame).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART/UART peripheral register block. |
This function is normally used to receive one frame when operating with frame length 4-8 bits. See sl_hal_usart_rx_ext() for reception of 9 bit frames.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
Note
This function will stall if the buffer is empty until data is received. Alternatively, the user can explicitly check whether data is available. If data is available, call sl_hal_usart_rx_data_get() to read the RXDATA register directly.
Returns
Data received.
sl_hal_usart_rx_double#
uint16_t sl_hal_usart_rx_double (USART_TypeDef * usart)
Receive two 4-8 bit frames or one 10-16 bit frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART/UART peripheral register block. |
This function is normally used to receive one frame when operating with frame length 10-16 bits. See sl_hal_usart_rx_double_ext() for reception of two 9 bit frames.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
Note
This function will stall if the buffer is empty until data is received. Alternatively, the user can explicitly check whether data is available. If data is available, call sl_hal_usart_rx_double_get() to read the RXDOUBLE register directly.
Returns
Data received.
sl_hal_usart_rx_double_ext#
uint32_t sl_hal_usart_rx_double_ext (USART_TypeDef * usart)
Receive two 4-9 bit frames, or one 10-16 bit frame with extended information.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART/UART peripheral register block. |
This function is normally used to receive one frame when operating with frame length 10-16 bits and additional RX status information is required.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
Note
This function will stall if buffer is empty until data is received. Alternatively, the user can explicitly check whether data is available. If data is available, call sl_hal_usart_rx_double_x_get() to read the RXDOUBLEX register directly.
Returns
Data received.
sl_hal_usart_rx_ext#
uint16_t sl_hal_usart_rx_ext (USART_TypeDef * usart)
Receive one 4-9 bit frame (or part of 10-16 bit frame) with extended information.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART/UART peripheral register block. |
This function is normally used to receive one frame when operating with frame length 4-9 bits and additional RX status information is required.
Notice that possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.
Note
This function will stall if the buffer is empty until data is received. Alternatively, the user can explicitly check whether data is available. If data is available, call sl_hal_usart_rx_data_get() to read the RXDATAX register directly.
Returns
Data received.
sl_hal_usart_rx_data_get#
uint8_t sl_hal_usart_rx_data_get (USART_TypeDef * usart)
Receive one 4-8 bit frame, (or part of 10-16 bit frame).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to USART/UART peripheral register block. |
This function is used to quickly receive one 4-8 bits frame by reading the RXDATA register directly, without checking the STATUS register for the RXDATAV flag. This can be useful from the RXDATAV interrupt handler, i.e., waiting is superfluous, in order to quickly read the received data. Please refer to sl_hal_usart_rx_ext() for reception of 9 bit frames.
Note
Because this function does not check whether the RXDATA register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g., when handling an RXDATAV interrupt. The sl_hal_usart_rx() is normally a better choice if the validity of the RXDATA register is not certain.
Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
Returns
Data received.
sl_hal_usart_rx_double_get#
uint16_t sl_hal_usart_rx_double_get (USART_TypeDef * usart)
Receive two 4-8 bit frames, or one 10-16 bit frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to USART/UART peripheral register block. |
This function is used to quickly receive one 10-16 bits frame or two 4-8 bit frames by reading the RXDOUBLE register directly, without checking the STATUS register for the RXDATAV flag. This can be useful from the RXDATAV interrupt handler, i.e., waiting is superfluous, in order to quickly read the received data. This function is normally used to receive one frame when operating with frame length 10-16 bits. Please refer to sl_hal_usart_rx_double_x_get() for reception of two 9 bit frames.
Note
Because this function does not check whether the RXDOUBLE register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g., when handling an RXDATAV interrupt. The sl_hal_usart_rx_double() is normally a better choice if the validity of the RXDOUBLE register is not certain.
Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
Returns
Data received.
sl_hal_usart_rx_double_x_get#
uint32_t sl_hal_usart_rx_double_x_get (USART_TypeDef * usart)
Receive two 4-9 bit frames, or one 10-16 bit frame with extended information.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to USART/UART peripheral register block. |
This function is used to quickly receive one 10-16 bits frame or two 4-9 bit frames by reading the RXDOUBLEX register directly, without checking the STATUS register for the RXDATAV flag. This can be useful from the RXDATAV interrupt handler, i.e., waiting is superfluous, in order to quickly read the received data.
Note
Because this function does not check whether the RXDOUBLEX register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g., when handling an RXDATAV interrupt. The sl_hal_usart_rx_double_ext() is normally a better choice if the validity of the RXDOUBLEX register is not certain.
Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
Returns
Data received.
sl_hal_usart_rx_data_x_get#
uint16_t sl_hal_usart_rx_data_x_get (USART_TypeDef * usart)
Receive one 4-9 bit frame, (or part of 10-16 bit frame) with extended information.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to USART/UART peripheral register block. |
This function is used to quickly receive one 4-9 bit frame, (or part of 10-16 bit frame) with extended information by reading the RXDATAX register directly, without checking the STATUS register for the RXDATAV flag. This can be useful from the RXDATAV interrupt handler, i.e., waiting is superfluous, in order to quickly read the received data.
Note
Because this function does not check whether the RXDATAX register actually holds valid data, it should only be used in situations when it is certain that there is valid data, ensured by some external program routine, e.g., when handling an RXDATAV interrupt. The sl_hal_usart_rx_ext() is normally a better choice if the validity of the RXDATAX register is not certain.
Notice that possible parity/stop bits in asynchronous mode are not considered part of specified frame bit length.
Returns
Data received.
sl_hal_usart_clear_interrupts#
void sl_hal_usart_clear_interrupts (USART_TypeDef * usart, uint32_t flags)
Clear one or more pending USART interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART/UART peripheral register block. |
| uint32_t | [in] | flags | Pending USART/UART interrupt source(s) to clear. Use one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together. |
sl_hal_usart_disable_interrupts#
void sl_hal_usart_disable_interrupts (USART_TypeDef * usart, uint32_t flags)
Disable one or more USART interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART/UART peripheral register block. |
| uint32_t | [in] | flags | USART/UART interrupt source(s) to disable. Use one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together. |
sl_hal_usart_enable_interrupts#
void sl_hal_usart_enable_interrupts (USART_TypeDef * usart, uint32_t flags)
Enable one or more USART interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART/UART peripheral register block. |
| uint32_t | [in] | flags | USART/UART interrupt source(s) to enable. Use one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together. |
Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using USART_IntClear() prior to enabling the interrupt.
sl_hal_usart_get_pending_interrupts#
uint32_t sl_hal_usart_get_pending_interrupts (USART_TypeDef * usart)
Get pending USART interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART/UART peripheral register block. |
Note
The event bits are not cleared by the use of this function.
Returns
USART/UART interrupt source(s) pending. Returns one or more valid interrupt flags for the USART module (USART_IF_nnn) OR'ed together.
sl_hal_usart_get_enabled_pending_interrupts#
uint32_t sl_hal_usart_get_enabled_pending_interrupts (USART_TypeDef * usart)
Get enabled and pending USART interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | Pointer to the USART/UART peripheral register block. |
Useful for handling more interrupt sources in the same interrupt handler.
Note
Interrupt flags are not cleared by the use of this function.
Returns
Pending and enabled USART interrupt sources. The return value is the bitwise AND combination of
the OR combination of enabled interrupt sources in USARTx_IEN_nnn register (USARTx_IEN_nnn) and
the OR combination of valid interrupt flags of the USART module (USARTx_IF_nnn).
sl_hal_usart_set_interrupts#
void sl_hal_usart_set_interrupts (USART_TypeDef * usart, uint32_t flags)
Set one or more pending USART interrupts from SW.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART/UART peripheral register block. |
| uint32_t | [in] | flags | USART/UART interrupt source(s) to set to pending. Use one or more valid interrupt flags for the USART module(USART_IF_nnn) OR'ed together. |
sl_hal_usart_get_status#
uint32_t sl_hal_usart_get_status (USART_TypeDef * usart)
Get USART STATUS register.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| USART_TypeDef * | [in] | usart | A pointer to the USART/UART peripheral register block. |
Returns
STATUS register value.
Macro Definition Documentation#
SL_HAL_USART_REF_VALID#
#define SL_HAL_USART_REF_VALIDValue:
(ref)
Validation of USART register block pointer reference for assert statements. */.
SL_HAL_USART_INIT_ASYNC_DEFAULT#
#define SL_HAL_USART_INIT_ASYNC_DEFAULTValue:
Default configuration for USART asynchronous initialization structure.
SL_HAL_USART_INIT_SYNC_DEFAULT#
#define SL_HAL_USART_INIT_SYNC_DEFAULTValue:
Default configuration for USART sync initialization structure.
SL_HAL_USART_INIT_IRDA_DEFAULT#
#define SL_HAL_USART_INIT_IRDA_DEFAULTValue:
Default configuration for USART IRDA initialization structure.
SL_HAL_USART_INIT_I2S_DEFAULT#
#define SL_HAL_USART_INIT_I2S_DEFAULTValue:
Default USART Sync configuration for series 2 devices.