LDMA - Linked DMA#
Linked Direct Memory Access (LDMA) Peripheral API.
Introduction#
LDMA API functions provide full support for the LDMA peripheral.
LDMA supports these LDMA transfer types:
Memory to memory.
Memory to peripheral.
Peripheral to memory.
Peripheral to peripheral.
Constant value to memory.
LDMA supports linked lists of LDMA descriptors allowing:
Circular and ping-pong buffer transfers.
Scatter-gather transfers.
Looped transfers.
LDMA has some advanced features:
Intra-channel synchronization (SYNC), allowing hardware events to pause and restart a LDMA sequence.
Immediate-write (WRI), allowing LDMA to write a constant anywhere in the memory map.
Complex flow control allowing if-else constructs.
Basic understanding of LDMA controller is assumed. Please refer to the reference manual for further details. The LDMA examples described in the reference manual are particularly helpful in understanding LDMA operations.
In order to use the LDMA controller, the initialization function sl_hal_ldma_init() must have been executed once (normally during system initialization).
LDMA transfers are initialized by a call to sl_hal_ldma_init_transfer(), transfer properties are controlled by the contents of sl_hal_ldma_transfer_init_t and sl_hal_ldma_descriptor_t structure parameters. The LDMA transfers can then be initiated by calling sl_hal_ldma_start_transfer(). The sl_hal_ldma_descriptor_t structure parameter may be a pointer to an array of descriptors, descriptors in array should be linked together as needed.
Transfer and descriptor initialization macros are provided for the most common transfer types. Due to the flexibility of LDMA peripheral, only a small subset of all possible initializer macros are provided, users should create new ones when needed.
Example#
A simple memory to memory transfer:
{
// Enable bus clock.
sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_LDMA0);
// Two buffers used in the memory-to-memory transfers.
static volatile uint32_t src[4];
static volatile uint32_t dst[4];
static const sl_hal_ldma_transfer_init_t transferCfg = SL_HAL_LDMA_TRANSFER_CFG_MEMORY();
static const sl_hal_ldma_descriptor_t desc = SL_HAL_LDMA_DESCRIPTOR_SINGLE_M2M(SL_HAL_LDMA_CTRL_SIZE_WORD, src, dst, 4);
// Initialize the LDMA with default values.
sl_hal_ldma_init_t initCfg = SL_HAL_LDMA_INIT_DEFAULT;
sl_hal_ldma_init(LDMA0, &initCfg);
// Start the memory transfer.
uint8_t channel = 0;
sl_hal_ldma_init_transfer(LDMA0, channel, &transferCfg, &desc);
sl_hal_ldma_start_transfer(LDMA0, channel);
while (!sl_hal_ldma_transfer_is_done(LDMA0, channel)) {
// Wait until the transfer is over.
}
}
A linked list of three memory-to-memory transfers:
{
// Enable bus clock.
sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_LDMA0);
// Two buffers used in the memory-to-memory transfers.
static volatile uint32_t src[12];
static volatile uint32_t dst[12];
// A transfer consisting of 3 descriptors linked together and each descriptor
// transfers 4 words from the source to the destination.
static const sl_hal_ldma_transfer_init_t transferCfg = SL_HAL_LDMA_TRANSFER_CFG_MEMORY();
static const sl_hal_ldma_descriptor_t descList[] =
{
SL_HAL_LDMA_DESCRIPTOR_LINKREL_M2M(SL_HAL_LDMA_CTRL_SIZE_WORD, src, dst, 4, 1),
SL_HAL_LDMA_DESCRIPTOR_LINKREL_M2M(SL_HAL_LDMA_CTRL_SIZE_WORD, src + 4, dst + 4, 4, 1),
SL_HAL_LDMA_DESCRIPTOR_SINGLE_M2M(SL_HAL_LDMA_CTRL_SIZE_WORD, src + 8, dst + 8, 4)
};
// Initialize the LDMA with default values.
sl_hal_ldma_init_t initCfg = SL_HAL_LDMA_INIT_DEFAULT;
sl_hal_ldma_init(LDMA0, &initCfg);
// Start the linked memory transfer.
uint8_t channel = 0;
sl_hal_ldma_init_transfer(LDMA0, channel, &transferCfg, descList);
sl_hal_ldma_start_transfer(LDMA0, channel);
while (!sl_hal_ldma_transfer_is_done(LDMA0, channel)) {
// Wait until the transfer is over.
}
}
LDMA from serial port peripheral to memory:
{
// Enable bus clock.
sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_LDMA0);
// Two buffer used in the transfer from EUSART0.
static volatile uint8_t dst[4];
// The LDMA transfer should be triggered by the EUSART0 RX data available signal.
static const sl_hal_ldma_transfer_init_t eusart0RxTransfer =
SL_HAL_LDMA_TRANSFER_CFG_PERIPHERAL(SL_HAL_LDMA_PERIPHERAL_SIGNAL_EUSART0_RXFL);
// Transfer 4 bytes from the EUSART0 RX FIFO to memory.
static const sl_hal_ldma_descriptor_t eusart0RxDesc =
SL_HAL_LDMA_DESCRIPTOR_SINGLE_P2M(SL_HAL_LDMA_CTRL_SIZE_BYTE, // Transfer size
&EUSART0->RXDATA, // Peripheral address
dst, // Destination (SRAM)
4); // Number of byte transfers
// Initialize the LDMA with default values.
sl_hal_ldma_init_t initCfg = SL_HAL_LDMA_INIT_DEFAULT;
sl_hal_ldma_init(LDMA0, &initCfg);
// Start the peripheral transfer which is triggered by the EUSART0
// peripheral RXFL signal.
uint8_t channel = 0;
sl_hal_ldma_init_transfer(LDMA0, channel, &eusart0RxTransfer, &eusart0RxDesc);
sl_hal_ldma_start_transfer(LDMA0, channel);
while (!sl_hal_ldma_transfer_is_done(LDMA0, channel)) {
// Wait until the transfer is over.
}
}
Ping-pong LDMA from serial port peripheral to memory:
{
// Enable bus clock.
sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_LDMA0);
// Two buffers used in the ping-pong transfer from EUSART0.
static volatile uint8_t buffer0[5];
static volatile uint8_t buffer1[5];
// The LDMA transfer should be triggered by the EUSART0 RX data available signal.
static const sl_hal_ldma_transfer_init_t eusart0RxTransfer =
SL_HAL_LDMA_TRANSFER_CFG_PERIPHERAL(SL_HAL_LDMA_PERIPHERAL_SIGNAL_EUSART0_RXFL);
// Both descriptors transfer 5 bytes from the EUSART0 RX data register into
// one of the buffers. Note that the first descriptor uses a relative address
// of 1 to link to the next descriptor, while the last descriptor uses a
// relative address of -1 to link to the first descriptor.
static const sl_hal_ldma_descriptor_t rxLoopDesc[] =
{
SL_HAL_LDMA_DESCRIPTOR_LINKREL_P2M(SL_HAL_LDMA_CTRL_SIZE_BYTE, &EUSART0->RXDATA, buffer0, 5, 1),
SL_HAL_LDMA_DESCRIPTOR_LINKREL_P2M(SL_HAL_LDMA_CTRL_SIZE_BYTE, &EUSART0->RXDATA, buffer1, 5, -1)
};
// Initialize the LDMA with default values.
sl_hal_ldma_init_t initCfg = SL_HAL_LDMA_INIT_DEFAULT;
sl_hal_ldma_init(LDMA0, &initCfg);
// Start the peripheral transfer which is triggered by the EUSART0
// peripheral RXFL signal.
uint8_t channel = 0;
sl_hal_ldma_init_transfer(LDMA0, channel, &eusart0RxTransfer, rxLoopDesc);
sl_hal_ldma_start_transfer(LDMA0, channel);
}
Note
LDMA peripheral module does not implement LDMA interrupt handler. A template for an LDMA IRQ handler is included here as an example. For series 2, a single IRQ handler is shared by all channels.
void LDMA_IRQHandler(void) { //Get all pending and enabled interrupts. uint32_t pending = sl_hal_ldma_get_enabled_pending_interrupts(LDMA); while (pending & LDMA_IF_ERROR) { // Loop here on an LDMA error to enable debugging. } // Iterate over all LDMA channels. for (uint32_t channel = 0; channel < DMA_CHAN_COUNT; channel++) { uint32_t mask = 0x1 << channel; if (pending & mask) { // Clear interrupt flag. sl_hal_ldma_clear_interrupts(LDMA, mask); // Do more stuff here, execute callbacks, etc. } } }For series 3, every channel has its own IRQ handler. Here is an example handler for channel 0.
void LDMA0_CHNL0_IRQHandler(void) { // Get all pending and enabled interrupts. uint32_t pending = sl_hal_ldma_get_enabled_pending_interrupts(LDMA0); while (pending & LDMA_IF_ERROR0) { // Loop here on an LDMA error to enable debugging. } if (pending & LDMA_IF_DONE0) { // Clear interrupt flag. sl_hal_ldma_clear_interrupts(LDMA0, LDMA_IF_DONE0); // Do more stuff here, execute callbacks, etc. } }
Modules#
sl_hal_ldma_descriptor_extend_t
Enumerations#
Controls the number of unit data transfers per arbitration cycle, providing a means to balance LDMA channels' load on the controller.
LDMA structure type.
LDMA transfer block or cycle selector.
Source address increment unit size.
LDMA transfer unit size.
Destination address increment unit size.
Source addressing mode.
Destination addressing mode.
LDMA link load address mode.
Insert extra arbitration slots to increase channel arbitration priority.
Source address increment sign.
Destination address increment sign.
Structure fetch operation bus port.
Source operation bus port.
Destination operation bus port.
Rules table mode (interleaving destination).
Peripherals that can trigger LDMA transfers.
Functions#
Initialize an extended LDMA transfer.
Initialize a LDMA transfer.
Initialize a LDMA transfer.
Start a LDMA transfer.
Stop a LDMA transfer.
Check if a LDMA transfer has completed.
Get the number of items remaining in a transfer.
Wait for the LDMA to complete disabling procedure.
Enable LDMA.
Enable LDMA channel.
Disable LDMA.
Disable LDMA channel.
Gets LDMA STATUS register value.
Reset the LDMA.
Check if a certain channel is enabled.
Enable an LDMA channel request.
Disable an LDMA channel request.
Clear one or more pending LDMA interrupts for LDMA channels 0 to 15.
Disable one or more LDMA interrupts for LDMA channels 0 to 15.
Enable one or more LDMA interrupts for LDMA channels 0 to 15.
Get pending LDMA interrupt flags for LDMA channels 0 to 15.
Set one or more pending LDMA interrupts for LDMA channels 0 to 15.
Get enabled and pending LDMA interrupt flags for LDMA channels 0 to 7.
Macros#
Size in words of a non-extended LDMA descriptor.
Size in words of an extended LDMA descriptor.
Maximum transfer size possible per descriptor.
Maximum transfer size possible per extended descriptor.
Converts a sl_hal_ldma_descriptor_t pointer to the value suitable to write to the link_addr field of a sl_hal_ldma_descriptor_t.
Converts a sl_hal_ldma_descriptor_t link_addr field value back to a sl_hal_ldma_descriptor_t pointer.
Default value for BUS PORT for sl_hal_ldma_transfer_init_t struct initializer.
XFER_COUNT suitable for sl_hal_ldma_descriptor_extend_t.
Default value for extended descriptor for sl_hal_ldma_descriptor_extend_t struct initializer.
Default LDMA initialization structure.
Generic LDMA transfer configuration for memory to memory transfers.
Generic LDMA transfer configuration for looped memory to memory transfers.
Generic LDMA transfer configuration for memory to/from peripheral transfers.
Generic LDMA transfer configuration for looped memory to/from peripheral transfers.
LDMA descriptor initializer for single memory to memory transfer.
LDMA descriptor initializer for single peripheral to memory transfer.
LDMA descriptor initializer for single peripheral to peripheral transfer.
LDMA descriptor initializer for single memory to peripheral transfer.
LDMA descriptor initializer for linked memory to memory transfer.
LDMA descriptor initializer for linked peripheral to memory transfer.
LDMA descriptor initializer for linked memory to peripheral word transfer.
LDMA descriptor initializer for linked peripheral to peripheral word transfer.
LDMA descriptor initializer for linked peripheral to peripheral word transfer.
LDMA descriptor initializer for linked peripheral to memory transfer.
LDMA descriptor initializer for linked memory to peripheral transfer.
LDMA descriptor initializer for linked peripheral to peripheral transfer.
LDMA descriptor initializer for Immediate WRITE transfer.
LDMA descriptor initializer for Immediate WRITE transfer.
LDMA descriptor initializer for Immediate WRITE transfer.
LDMA descriptor initializer for SYNC transfer.
LDMA descriptor initializer for SYNC transfer.
LDMA descriptor initializer for SYNC transfer.
Initializer for the destination interleaving portion of the LDMA extended descriptor.
LDMA descriptor initializer for single memory to memory transfer.
LDMA descriptor initializer for single peripheral to memory transfer.
LDMA descriptor initializer for single memory to peripheral transfer.
LDMA descriptor initializer for linked memory to memory transfer.
LDMA descriptor initializer for linked peripheral to memory transfer.
LDMA descriptor initializer for linked memory to peripheral word transfer.
LDMA descriptor initializer for linked memory to memory transfer.
LDMA descriptor initializer for linked peripheral to memory transfer.
LDMA descriptor initializer for linked memory to peripheral transfer.
Enumeration Documentation#
sl_hal_ldma_ctrl_block_size_t#
sl_hal_ldma_ctrl_block_size_t
Controls the number of unit data transfers per arbitration cycle, providing a means to balance LDMA channels' load on the controller.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_1 | One transfer per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_2 | Two transfers per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_3 | Three transfers per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_4 | Four transfers per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_6 | Six transfers per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_8 | Eight transfers per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_16 | 16 transfers per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_32 | 32 transfers per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_64 | 64 transfers per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_128 | 128 transfers per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_256 | 256 transfers per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_512 | 512 transfers per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_UNIT_1024 | 1024 transfers per arbitration. |
| SL_HAL_LDMA_CTRL_BLOCK_SIZE_ALL | Lock arbitration during transfer. |
sl_hal_ldma_ctrl_struct_type_t#
sl_hal_ldma_ctrl_struct_type_t
LDMA structure type.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CTRL_STRUCT_TYPE_XFER | TRANSFER transfer type. |
| SL_HAL_LDMA_CTRL_STRUCT_TYPE_SYNC | SYNCHRONIZE transfer type. |
| SL_HAL_LDMA_CTRL_STRUCT_TYPE_WRITE | WRITE transfer type. |
sl_hal_ldma_ctrl_req_mode_t#
sl_hal_ldma_ctrl_req_mode_t
LDMA transfer block or cycle selector.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CTRL_REQ_MODE_BLOCK | Each LDMA request trigger transfer of one block. |
| SL_HAL_LDMA_CTRL_REQ_MODE_ALL | A LDMA request trigger transfer of a complete cycle. |
sl_hal_ldma_ctrl_src_inc_t#
sl_hal_ldma_ctrl_src_inc_t
Source address increment unit size.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CTRL_SRC_INC_ONE | Increment source address by one unit data size. |
| SL_HAL_LDMA_CTRL_SRC_INC_TWO | Increment source address by two unit data sizes. |
| SL_HAL_LDMA_CTRL_SRC_INC_FOUR | Increment source address by four unit data sizes. |
| SL_HAL_LDMA_CTRL_SRC_INC_NONE | Do not increment source address. |
sl_hal_ldma_ctrl_size_t#
sl_hal_ldma_ctrl_size_t
LDMA transfer unit size.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CTRL_SIZE_BYTE | Each unit transfer is a byte. |
| SL_HAL_LDMA_CTRL_SIZE_HALF | Each unit transfer is a half-word. |
| SL_HAL_LDMA_CTRL_SIZE_WORD | Each unit transfer is a word. |
sl_hal_ldma_ctrl_dst_inc_t#
sl_hal_ldma_ctrl_dst_inc_t
Destination address increment unit size.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CTRL_DST_INC_ONE | Increment destination address by one unit data size. |
| SL_HAL_LDMA_CTRL_DST_INC_TWO | Increment destination address by two unit data sizes. |
| SL_HAL_LDMA_CTRL_DST_INC_FOUR | Increment destination address by four unit data sizes. |
| SL_HAL_LDMA_CTRL_DST_INC_NONE | Do not increment destination address. |
sl_hal_ldma_ctrl_src_addr_mode_t#
sl_hal_ldma_ctrl_src_addr_mode_t
Source addressing mode.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CTRL_SRC_ADDR_MODE_ABS | Address fetched from a linked structure is absolute. |
| SL_HAL_LDMA_CTRL_SRC_ADDR_MODE_REL | Address fetched from a linked structure is relative. |
sl_hal_ldma_ctrl_dst_addr_mode_t#
sl_hal_ldma_ctrl_dst_addr_mode_t
Destination addressing mode.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CTRL_DST_ADDR_MODE_ABS | Address fetched from a linked structure is absolute. |
| SL_HAL_LDMA_CTRL_DST_ADDR_MODE_REL | Address fetched from a linked structure is relative. |
sl_hal_ldma_link_mode_t#
sl_hal_ldma_link_mode_t
LDMA link load address mode.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_LINK_MODE_ABS | Link address is an absolute address value. |
| SL_HAL_LDMA_LINK_MODE_REL | Link address is a two's complement relative address. |
sl_hal_ldma_cfg_arb_slots_t#
sl_hal_ldma_cfg_arb_slots_t
Insert extra arbitration slots to increase channel arbitration priority.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CFG_ARBSLOTS_ONE | One arbitration slot selected. |
| SL_HAL_LDMA_CFG_ARBSLOTS_TWO | Two arbitration slots selected. |
| SL_HAL_LDMA_CFG_ARBSLOTS_FOUR | Four arbitration slots selected. |
| SL_HAL_LDMA_CFG_ARBSLOTS_EIGHT | Eight arbitration slots selected. |
sl_hal_ldma_cfg_src_inc_sign_t#
sl_hal_ldma_cfg_src_inc_sign_t
Source address increment sign.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CFG_SRC_INC_SIGN_POS | Increment source address. |
| SL_HAL_LDMA_CFG_SRC_INC_SIGN_NEG | Decrement source address. |
sl_hal_ldma_cfg_dst_inc_sign_t#
sl_hal_ldma_cfg_dst_inc_sign_t
Destination address increment sign.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CFG_DST_INC_SIGN_POS | Increment destination address. |
| SL_HAL_LDMA_CFG_DST_INC_SIGN_NEG | Decrement destination address. |
sl_hal_ldma_cfg_struct_bus_port_t#
sl_hal_ldma_cfg_struct_bus_port_t
Structure fetch operation bus port.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CFG_STRUCT_BUS_PORT_0 | AHB Master 0 port. |
| SL_HAL_LDMA_CFG_STRUCT_BUS_PORT_1 | AHB Master 1 port. |
sl_hal_ldma_cfg_src_bus_port_t#
sl_hal_ldma_cfg_src_bus_port_t
Source operation bus port.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CFG_SRC_BUS_PORT_0 | AHB Master 0 port. |
| SL_HAL_LDMA_CFG_SRC_BUS_PORT_1 | AHB Master 1 port. |
sl_hal_ldma_cfg_dst_bus_port_t#
sl_hal_ldma_cfg_dst_bus_port_t
Destination operation bus port.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_CFG_DST_BUS_PORT_0 | AHB Master 0 port. |
| SL_HAL_LDMA_CFG_DST_BUS_PORT_1 | AHB Master 1 port. |
sl_hal_ldma_rules_table_mode_t#
sl_hal_ldma_rules_table_mode_t
Rules table mode (interleaving destination).
| Enumerator | |
|---|---|
| SL_HAL_LDMA_MODE_ABSOLUTE | Address by value in rules. Size of WORD. |
| SL_HAL_LDMA_MODE_RELATIVE_16 | Address by adding rules to DST. Size of HALFWORD. |
| SL_HAL_LDMA_MODE_RELATIVE_8 | Address by adding rules to DST. Size of BYTE. |
sl_hal_ldma_peripheral_signal_t#
sl_hal_ldma_peripheral_signal_t
Peripherals that can trigger LDMA transfers.
| Enumerator | |
|---|---|
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_NONE | No peripheral selected for LDMA triggering. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_LDMAXBAR0_PRSREQ0 | Trigger on PRS REQ0. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_LDMAXBAR0_PRSREQ1 | Trigger on PRS REQ1. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER0_CC0 | Trigger on TIMER0_CC0. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER0_CC1 | Trigger on TIMER0_CC1. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER0_CC2 | Trigger on TIMER0_CC2. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER0_UFOF | Trigger on TIMER0_UFOF. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER1_CC0 | Trigger on TIMER1_CC0. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER1_CC1 | Trigger on TIMER1_CC1. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER1_CC2 | Trigger on TIMER1_CC2. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER1_UFOF | Trigger on TIMER1_UFOF. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER2_CC0 | Trigger on TIMER2_CC0. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER2_CC1 | Trigger on TIMER2_CC1. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER2_CC2 | Trigger on TIMER2_CC2. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER2_UFOF | Trigger on TIMER2_UFOF. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER2_CC3 | Trigger on TIMER2_CC3. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER2_CC4 | Trigger on TIMER2_CC4. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER2_CC5 | Trigger on TIMER2_CC5. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER2_CC6 | Trigger on TIMER2_CC6. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER3_CC0 | Trigger on TIMER3_CC0. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER3_CC1 | Trigger on TIMER3_CC1. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER3_CC2 | Trigger on TIMER3_CC2. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER3_UFOF | Trigger on TIMER3_UFOF. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER3_CC3 | Trigger on TIMER3_CC3. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER3_CC4 | Trigger on TIMER3_CC4. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER3_CC5 | Trigger on TIMER3_CC5. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_TIMER3_CC6 | Trigger on TIMER3_CC6. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_I2C0_RXDATAV | Trigger on I2C0_RXDATAV. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_I2C0_TXBL | Trigger on I2C0_TXBL. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_I2C1_RXDATAV | Trigger on I2C1_RXDATAV. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_I2C1_TXBL | Trigger on I2C1_TXBL. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_I2C2_RXDATAV | Trigger on I2C2_RXDATAV. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_I2C2_TXBL | Trigger on I2C2_TXBL. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_ADC0_SCAN | Trigger on ADC0_SCAN. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_EUSART0_RXFL | Trigger on EUSART0_RXFL. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_EUSART0_TXFL | Trigger on EUSART0_TXFL. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_EUSART1_RXFL | Trigger on EUSART1_RXFL. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_EUSART1_TXFL | Trigger on EUSART1_TXFL. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_EUSART2_RXFL | Trigger on EUSART2_RXFL. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_EUSART2_TXFL | Trigger on EUSART2_TXFL. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_PIXELRZ0REQ_TXF | Trigger on PIXELRZ0REQ_TXF. |
| SL_HAL_LDMA_PERIPHERAL_SIGNAL_PIXELRZ1REQ_TXF | Trigger on PIXELRZ1REQ_TXF. |
Function Documentation#
sl_hal_ldma_init#
void sl_hal_ldma_init (LDMA_TypeDef * ldma, const sl_hal_ldma_init_t * init)
Initialize an extended LDMA transfer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| const sl_hal_ldma_init_t * | [in] | init | A pointer to the initialization structure used to configure the LDMA. |
This function will disable all the LDMA channels. This function will also set the LDMA IRQ priority to a user-configurable priority. The LDMA interrupt priority is configured using the sl_hal_ldma__t structure.
sl_hal_ldma_init_transfer#
void sl_hal_ldma_init_transfer (LDMA_TypeDef * ldma, uint32_t channel, const sl_hal_ldma_transfer_init_t * transfer_init, const sl_hal_ldma_descriptor_t * descriptor)
Initialize a LDMA transfer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | channel | A LDMA channel to stop. |
| const sl_hal_ldma_transfer_init_t * | [in] | transfer_init | The initialization structure used to configure the transfer. |
| const sl_hal_ldma_descriptor_t * | [in] | descriptor | The transfer descriptor, which can be an array of descriptors linked together. Each descriptor's fields stored in RAM will be loaded into the certain hardware registers at the proper time to perform the LDMA transfer. |
Note
If the descriptor is allocated on the stack, its content may change unpredictably when the function exits. To prevent this, declare the descriptor as a static or global variable, or allocate memory for it using
malloc. Ensure that the memory location of the descriptor remains stable until the LDMA transfer is complete, as the LDMA controller may load the descriptor at any time.
sl_hal_ldma_init_transfer_extend#
void sl_hal_ldma_init_transfer_extend (LDMA_TypeDef * ldma, uint32_t channel, const sl_hal_ldma_transfer_init_t * transfer_init, const sl_hal_ldma_descriptor_extend_t * descriptor_extend)
Initialize a LDMA transfer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | channel | A LDMA channel to stop. |
| const sl_hal_ldma_transfer_init_t * | [in] | transfer_init | The initialization structure used to configure the transfer. |
| const sl_hal_ldma_descriptor_extend_t * | [in] | descriptor_extend | The transfer extended descriptor, which can be an array of descriptors linked together. Each descriptor's fields stored in RAM will be loaded into the certain hardware registers at the proper time to perform the LDMA transfer. |
sl_hal_ldma_start_transfer#
void sl_hal_ldma_start_transfer (LDMA_TypeDef * ldma, uint32_t channel)
Start a LDMA transfer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | channel | A DMA channel. |
sl_hal_ldma_stop_transfer#
void sl_hal_ldma_stop_transfer (LDMA_TypeDef * ldma, uint32_t channel)
Stop a LDMA transfer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | channel | A LDMA channel to stop. |
Note
The LDMA will complete the current AHB burst transfer before stopping.
sl_hal_ldma_transfer_is_done#
bool sl_hal_ldma_transfer_is_done (LDMA_TypeDef * ldma, uint32_t channel)
Check if a LDMA transfer has completed.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | channel | A LDMA channel to check. |
Returns
True if transfer has completed, false if not.
sl_hal_ldma_transfer_remaining_count#
uint32_t sl_hal_ldma_transfer_remaining_count (LDMA_TypeDef * ldma, uint32_t channel)
Get the number of items remaining in a transfer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | channel | The channel number of the transfer to check. |
Note
This function does not take into account that a LDMA transfer with a chain of linked transfers might be ongoing. It will only check the count for the current transfer.
Returns
A number of items remaining in the transfer.
sl_hal_ldma_wait_ready#
void sl_hal_ldma_wait_ready (LDMA_TypeDef * ldma)
Wait for the LDMA to complete disabling procedure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
sl_hal_ldma_enable#
void sl_hal_ldma_enable (LDMA_TypeDef * ldma)
Enable LDMA.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
sl_hal_ldma_enable_channel#
void sl_hal_ldma_enable_channel (LDMA_TypeDef * ldma, uint32_t channel)
Enable LDMA channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | channel | A LDMA channel. |
sl_hal_ldma_disable#
void sl_hal_ldma_disable (LDMA_TypeDef * ldma)
Disable LDMA.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
sl_hal_ldma_disable_channel#
void sl_hal_ldma_disable_channel (LDMA_TypeDef * ldma, uint32_t channel)
Disable LDMA channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | channel | A LDMA channel. |
sl_hal_ldma_get_status#
uint32_t sl_hal_ldma_get_status (LDMA_TypeDef * ldma)
Gets LDMA STATUS register value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
Returns
Current STATUS register value.
sl_hal_ldma_reset#
void sl_hal_ldma_reset (LDMA_TypeDef * ldma)
Reset the LDMA.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
sl_hal_ldma_channel_is_enabled#
bool sl_hal_ldma_channel_is_enabled (LDMA_TypeDef * ldma, uint32_t channel)
Check if a certain channel is enabled.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | channel | LDMA channel to check. |
Returns
return true if the LDMA channel is enabled and false if the channel is not enabled.
sl_hal_ldma_enable_channel_request#
void sl_hal_ldma_enable_channel_request (LDMA_TypeDef * ldma, uint32_t channel)
Enable an LDMA channel request.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | channel | LDMA channel to enable requests. |
Use this function to enable an LDMA channel request. This will prevent the LDMA from proceeding after its current transaction is disabled.
sl_hal_ldma_disable_channel_request#
void sl_hal_ldma_disable_channel_request (LDMA_TypeDef * ldma, uint32_t channel)
Disable an LDMA channel request.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | channel | LDMA channel to disable requests. |
Use this function to disable an LDMA channel request. This will prevent the LDMA from proceeding after its current transaction is disabled.
sl_hal_ldma_clear_interrupts#
void sl_hal_ldma_clear_interrupts (LDMA_TypeDef * ldma, uint32_t flags)
Clear one or more pending LDMA interrupts for LDMA channels 0 to 15.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | flags | Pending LDMA interrupt sources to clear. Use one or more valid interrupt flags for the LDMA peripheral module. The flags are one LDMA_IF_ERRORx flag for each channel (x = a supported channel number) and one LDMA_IF_DONEx flag for each channel (x = a supported channel number). For series 2 devices, use LDMA_IF_ERROR and LDMA_IF_DONEx. |
Note
For series 2 devices, there is only one LDMA_IF_ERROR shared across all channels. Use the appropriate flags to clear these interrupts.
sl_hal_ldma_disable_interrupts#
void sl_hal_ldma_disable_interrupts (LDMA_TypeDef * ldma, uint32_t flags)
Disable one or more LDMA interrupts for LDMA channels 0 to 15.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | flags | LDMA interrupt sources to disable. Use one or more valid interrupt flags for LDMA peripheral module. The flags are one LDMA_IEN_ERROR flag for all the channels and one LDMA_IEN_DONEx flag for each channel (x = a supported channel number). |
sl_hal_ldma_enable_interrupts#
void sl_hal_ldma_enable_interrupts (LDMA_TypeDef * ldma, uint32_t flags)
Enable one or more LDMA interrupts for LDMA channels 0 to 15.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | flags | LDMA interrupt sources to enable. Use one or more valid interrupt flags for LDMA peripheral module. The flags are one LDMA_IEN_ERROR flag for all channels and one LDMA_IEN_DONEx flag for each channel (x = a supported channel number). |
Note
Depending on the use, a pending interrupt may already be set before to enabling the interrupt. To ignore a pending interrupt, consider using sl_hal_ldma_clear_interrupts() prior to enabling the interrupt.
sl_hal_ldma_get_pending_interrupts#
uint32_t sl_hal_ldma_get_pending_interrupts (LDMA_TypeDef * ldma)
Get pending LDMA interrupt flags for LDMA channels 0 to 15.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
Note
Event bits are not cleared by the use of this function. For series 2 devices, there is only one LDMA_IF_ERROR shared across all channels. Use the appropriate flags to clear these interrupts.
Returns
Pending LDMA interrupt sources. Returns one or more valid interrupt flags for the LDMA module. The flags are one LDMA_IF_ERRORx flag for each channel (x = a supported channel number) and one LDMA_IF_DONEx flag for each channel (x = a supported channel number). For series 2 devices, use LDMA_IF_ERROR and LDMA_IF_DONEx.
sl_hal_ldma_set_interrupts#
void sl_hal_ldma_set_interrupts (LDMA_TypeDef * ldma, uint32_t flags)
Set one or more pending LDMA interrupts for LDMA channels 0 to 15.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
| uint32_t | [in] | flags | LDMA interrupt sources to set to pending. Use one or more valid interrupt flags for LDMA peripheral module. The flags are one LDMA_IF_ERRORx flag for each channel (x = a supported channel number) and one LDMA_IF_DONEx flag for each channel (x = a supported channel number). For series 2 devices, use LDMA_IF_ERROR and LDMA_IF_DONEx. |
Note
For series 2 devices, there is only one LDMA_IF_ERROR shared across all channels. Use the appropriate flags to clear these interrupts.
sl_hal_ldma_get_enabled_pending_interrupts#
uint32_t sl_hal_ldma_get_enabled_pending_interrupts (LDMA_TypeDef * ldma)
Get enabled and pending LDMA interrupt flags for LDMA channels 0 to 7.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LDMA_TypeDef * | [in] | ldma | A LDMA peripheral module. |
Useful for handling more interrupt sources in the same interrupt handler.
Note
Interrupt flags are not cleared by the use of this function.
Returns
Pending and enabled LDMA interrupt sources
Macro Definition Documentation#
SL_HAL_LDMA_DESCRIPTOR_NON_EXTEND_SIZE_WORD#
#define SL_HAL_LDMA_DESCRIPTOR_NON_EXTEND_SIZE_WORDValue:
4
Size in words of a non-extended LDMA descriptor.
SL_HAL_LDMA_DESCRIPTOR_EXTEND_SIZE_WORD#
#define SL_HAL_LDMA_DESCRIPTOR_EXTEND_SIZE_WORDValue:
7
Size in words of an extended LDMA descriptor.
SL_HAL_LDMA_DESCRIPTOR_MAX_XFER_SIZE#
#define SL_HAL_LDMA_DESCRIPTOR_MAX_XFER_SIZEValue:
((_LDMA_CH_CTRL_XFERCNT_MASK >> _LDMA_CH_CTRL_XFERCNT_SHIFT) + 1)
Maximum transfer size possible per descriptor.
SL_HAL_LDMA_DESCRIPTOR_EXTEND_MAX_XFER_SIZE#
#define SL_HAL_LDMA_DESCRIPTOR_EXTEND_MAX_XFER_SIZEValue:
SL_HAL_LDMA_DESCRIPTOR_MAX_XFER_SIZE
Maximum transfer size possible per extended descriptor.
SL_HAL_LDMA_DESCRIPTOR_LINKABS_ADDR_TO_LINKADDR#
#define SL_HAL_LDMA_DESCRIPTOR_LINKABS_ADDR_TO_LINKADDRValue:
(addr)
Converts a sl_hal_ldma_descriptor_t pointer to the value suitable to write to the link_addr field of a sl_hal_ldma_descriptor_t.
SL_HAL_LDMA_DESCRIPTOR_LINKABS_LINKADDR_TO_ADDR#
#define SL_HAL_LDMA_DESCRIPTOR_LINKABS_LINKADDR_TO_ADDRValue:
(link_addr)
Converts a sl_hal_ldma_descriptor_t link_addr field value back to a sl_hal_ldma_descriptor_t pointer.
SL_HAL_LDMA_CFG_BUS_PORT_DEFAULT#
#define SL_HAL_LDMA_CFG_BUS_PORT_DEFAULTValue:
Default value for BUS PORT for sl_hal_ldma_transfer_init_t struct initializer.
SL_HAL_LDMA_EXTEND_XFER_COUNT#
#define SL_HAL_LDMA_EXTEND_XFER_COUNTValue:
(count)
XFER_COUNT suitable for sl_hal_ldma_descriptor_extend_t.
SL_HAL_LDMA_EXTEND_DEFAULT#
#define SL_HAL_LDMA_EXTEND_DEFAULTValue:
Default value for extended descriptor for sl_hal_ldma_descriptor_extend_t struct initializer.
SL_HAL_LDMA_INIT_DEFAULT#
#define SL_HAL_LDMA_INIT_DEFAULTValue:
Default LDMA initialization structure.
SL_HAL_LDMA_TRANSFER_CFG_MEMORY#
#define SL_HAL_LDMA_TRANSFER_CFG_MEMORYValue:
Generic LDMA transfer configuration for memory to memory transfers.
SL_HAL_LDMA_TRANSFER_CFG_MEMORY_LOOP#
#define SL_HAL_LDMA_TRANSFER_CFG_MEMORY_LOOPValue:
Generic LDMA transfer configuration for looped memory to memory transfers.
SL_HAL_LDMA_TRANSFER_CFG_PERIPHERAL#
#define SL_HAL_LDMA_TRANSFER_CFG_PERIPHERALValue:
Generic LDMA transfer configuration for memory to/from peripheral transfers.
SL_HAL_LDMA_TRANSFER_CFG_PERIPHERAL_LOOP#
#define SL_HAL_LDMA_TRANSFER_CFG_PERIPHERAL_LOOPValue:
Generic LDMA transfer configuration for looped memory to/from peripheral transfers.
SL_HAL_LDMA_DESCRIPTOR_SINGLE_M2M#
#define SL_HAL_LDMA_DESCRIPTOR_SINGLE_M2MValue:
LDMA descriptor initializer for single memory to memory transfer.
SL_HAL_LDMA_DESCRIPTOR_SINGLE_P2M#
#define SL_HAL_LDMA_DESCRIPTOR_SINGLE_P2MValue:
LDMA descriptor initializer for single peripheral to memory transfer.
SL_HAL_LDMA_DESCRIPTOR_SINGLE_P2P#
#define SL_HAL_LDMA_DESCRIPTOR_SINGLE_P2PValue:
LDMA descriptor initializer for single peripheral to peripheral transfer.
SL_HAL_LDMA_DESCRIPTOR_SINGLE_M2P#
#define SL_HAL_LDMA_DESCRIPTOR_SINGLE_M2PValue:
LDMA descriptor initializer for single memory to peripheral transfer.
SL_HAL_LDMA_DESCRIPTOR_LINKABS_M2M#
#define SL_HAL_LDMA_DESCRIPTOR_LINKABS_M2MValue:
LDMA descriptor initializer for linked memory to memory transfer.
Link address must be an absolute address.
Note
The link_addr member of the transfer descriptor is not initialized. link_addr must be initialized by using the proper bits right-shift to get the correct bits from the absolute address. _LDMA_CH_LINK_LINKADDR_SHIFT should be used for that operation:
desc.link_addr = ((int32_t)&next_desc) >> _LDMA_CH_LINK_LINKADDR_SHIFT;
The opposite bit shift (left) must be done if link_addr is read.
SL_HAL_LDMA_DESCRIPTOR_LINKABS_P2M#
#define SL_HAL_LDMA_DESCRIPTOR_LINKABS_P2MValue:
LDMA descriptor initializer for linked peripheral to memory transfer.
Link address must be an absolute address.
Note
The link_addr member of the transfer descriptor is not initialized. link_addr must be initialized by using the proper bits right-shift to get the correct bits from the absolute address. _LDMA_CH_LINK_LINKADDR_SHIFT should be used for that operation:
desc.link_addr = ((int32_t)&next_desc) >> _LDMA_CH_LINK_LINKADDR_SHIFT;
The opposite bit shift (left) must be done if link_addr is read.
SL_HAL_LDMA_DESCRIPTOR_LINKABS_M2P#
#define SL_HAL_LDMA_DESCRIPTOR_LINKABS_M2PValue:
LDMA descriptor initializer for linked memory to peripheral word transfer.
Link address must be an absolute address.
Note
The link_addr member of the transfer descriptor is not initialized. link_addr must be initialized by using the proper bits right-shift to get the correct bits from the absolute address. _LDMA_CH_LINK_LINKADDR_SHIFT should be used for that operation:
desc.link_addr = ((int32_t)&next_desc) >> _LDMA_CH_LINK_LINKADDR_SHIFT;
The opposite bit shift (left) must be done if link_addr is read.
SL_HAL_LDMA_DESCRIPTOR_LINKABS_P2P#
#define SL_HAL_LDMA_DESCRIPTOR_LINKABS_P2PValue:
LDMA descriptor initializer for linked peripheral to peripheral word transfer.
Link address must be an absolute address.
Note
The link_addr member of the transfer descriptor is not initialized. link_addr must be initialized by using the proper bits right-shift to get the correct bits from the absolute address. _LDMA_CH_LINK_LINKADDR_SHIFT should be used for that operation:
desc.link_addr = ((int32_t)&next_desc) >> _LDMA_CH_LINK_LINKADDR_SHIFT;
The opposite bit shift (left) must be done if link_addr is read.
SL_HAL_LDMA_DESCRIPTOR_LINKREL_M2M#
#define SL_HAL_LDMA_DESCRIPTOR_LINKREL_M2MValue:
LDMA descriptor initializer for linked peripheral to peripheral word transfer.
Link address must be an absolute address.
Note
The link_addr member of the transfer descriptor is initialized to 4 (regular descriptor) or 7 (extended descriptor), assuming that the next descriptor immediately follows this descriptor (in memory).
SL_HAL_LDMA_DESCRIPTOR_LINKREL_P2M#
#define SL_HAL_LDMA_DESCRIPTOR_LINKREL_P2MValue:
LDMA descriptor initializer for linked peripheral to memory transfer.
SL_HAL_LDMA_DESCRIPTOR_LINKREL_M2P#
#define SL_HAL_LDMA_DESCRIPTOR_LINKREL_M2PValue:
LDMA descriptor initializer for linked memory to peripheral transfer.
SL_HAL_LDMA_DESCRIPTOR_LINKREL_P2P#
#define SL_HAL_LDMA_DESCRIPTOR_LINKREL_P2PValue:
LDMA descriptor initializer for linked peripheral to peripheral transfer.
SL_HAL_LDMA_DESCRIPTOR_SINGLE_WRITE#
#define SL_HAL_LDMA_DESCRIPTOR_SINGLE_WRITEValue:
LDMA descriptor initializer for Immediate WRITE transfer.
SL_HAL_LDMA_DESCRIPTOR_LINKABS_WRITE#
#define SL_HAL_LDMA_DESCRIPTOR_LINKABS_WRITEValue:
LDMA descriptor initializer for Immediate WRITE transfer.
Link address must be an absolute address.
Link address must be an absolute address.
Note
The link_addr member of the transfer descriptor is not initialized. link_addr must be initialized by using the proper bits right-shift to get the correct bits from the absolute address. _LDMA_CH_LINK_LINKADDR_SHIFT should be used for that operation:
desc.link_addr = ((int32_t)&next_desc) >> _LDMA_CH_LINK_LINKADDR_SHIFT;
The opposite bit shift (left) must be done if link_addr is read.
SL_HAL_LDMA_DESCRIPTOR_LINKREL_WRITE#
#define SL_HAL_LDMA_DESCRIPTOR_LINKREL_WRITEValue:
LDMA descriptor initializer for Immediate WRITE transfer.
SL_HAL_LDMA_DESCRIPTOR_SINGLE_SYNC#
#define SL_HAL_LDMA_DESCRIPTOR_SINGLE_SYNCValue:
LDMA descriptor initializer for SYNC transfer.
SL_HAL_LDMA_DESCRIPTOR_LINKABS_SYNC#
#define SL_HAL_LDMA_DESCRIPTOR_LINKABS_SYNCValue:
LDMA descriptor initializer for SYNC transfer.
Link address must be an absolute address.
Note
The link_addr member of the transfer descriptor is not initialized. link_addr must be initialized by using the proper bits right-shift to get the correct bits from the absolute address. _LDMA_CH_LINK_LINKADDR_SHIFT should be used for that operation:
desc.link_addr = ((int32_t)&next_desc) >> _LDMA_CH_LINK_LINKADDR_SHIFT;
The opposite bit shift (left) must be done if link_addr is read.
SL_HAL_LDMA_DESCRIPTOR_LINKREL_SYNC#
#define SL_HAL_LDMA_DESCRIPTOR_LINKREL_SYNCValue:
LDMA descriptor initializer for SYNC transfer.
SL_HAL_LDMA_DESCRIPTOR_EXTEND_DST_IL_CFG#
#define SL_HAL_LDMA_DESCRIPTOR_EXTEND_DST_IL_CFGValue:
Initializer for the destination interleaving portion of the LDMA extended descriptor.
SL_HAL_LDMA_DESCRIPTOR_SINGLE_M2M_EXTEND#
#define SL_HAL_LDMA_DESCRIPTOR_SINGLE_M2M_EXTENDValue:
LDMA descriptor initializer for single memory to memory transfer.
SL_HAL_LDMA_DESCRIPTOR_SINGLE_P2M_EXTEND#
#define SL_HAL_LDMA_DESCRIPTOR_SINGLE_P2M_EXTENDValue:
LDMA descriptor initializer for single peripheral to memory transfer.
SL_HAL_LDMA_DESCRIPTOR_SINGLE_M2P_EXTEND#
#define SL_HAL_LDMA_DESCRIPTOR_SINGLE_M2P_EXTENDValue:
LDMA descriptor initializer for single memory to peripheral transfer.
SL_HAL_LDMA_DESCRIPTOR_LINKABS_M2M_EXTEND#
#define SL_HAL_LDMA_DESCRIPTOR_LINKABS_M2M_EXTENDValue:
LDMA descriptor initializer for linked memory to memory transfer.
Link address must be an absolute address.
Note
The link_addr member of the transfer descriptor is not initialized. link_addr must be initialized by using the proper bits right-shift to get the correct bits from the absolute address. _LDMA_CH_LINK_LINKADDR_SHIFT should be used for that operation:
desc.link_addr = ((int32_t)&next_desc) >> _LDMA_CH_LINK_LINKADDR_SHIFT;
The opposite bit shift (left) must be done if link_addr is read.
SL_HAL_LDMA_DESCRIPTOR_LINKABS_P2M_EXTEND#
#define SL_HAL_LDMA_DESCRIPTOR_LINKABS_P2M_EXTENDValue:
LDMA descriptor initializer for linked peripheral to memory transfer.
Link address must be an absolute address.
Note
The link_addr member of the transfer descriptor is not initialized. link_addr must be initialized by using the proper bits right-shift to get the correct bits from the absolute address. _LDMA_CH_LINK_LINKADDR_SHIFT should be used for that operation:
desc.link_addr = ((int32_t)&next_desc) >> _LDMA_CH_LINK_LINKADDR_SHIFT;
The opposite bit shift (left) must be done if link_addr is read.
SL_HAL_LDMA_DESCRIPTOR_LINKABS_M2P_EXTEND#
#define SL_HAL_LDMA_DESCRIPTOR_LINKABS_M2P_EXTENDValue:
LDMA descriptor initializer for linked memory to peripheral word transfer.
Link address must be an absolute address.
Note
The link_addr member of the transfer descriptor is not initialized. link_addr must be initialized by using the proper bits right-shift to get the correct bits from the absolute address. _LDMA_CH_LINK_LINKADDR_SHIFT should be used for that operation:
desc.link_addr = ((int32_t)&next_desc) >> _LDMA_CH_LINK_LINKADDR_SHIFT;
The opposite bit shift (left) must be done if link_addr is read.
SL_HAL_LDMA_DESCRIPTOR_LINKREL_M2M_EXTEND#
#define SL_HAL_LDMA_DESCRIPTOR_LINKREL_M2M_EXTENDValue:
LDMA descriptor initializer for linked memory to memory transfer.
Link address is a relative address.
Note
The link_addr member of the transfer descriptor is initialized to 4 (regular descriptor) or 7 (extended descriptor), assuming that the next descriptor immediately follows this descriptor (in memory).
SL_HAL_LDMA_DESCRIPTOR_LINKREL_P2M_EXTEND#
#define SL_HAL_LDMA_DESCRIPTOR_LINKREL_P2M_EXTENDValue:
LDMA descriptor initializer for linked peripheral to memory transfer.
SL_HAL_LDMA_DESCRIPTOR_LINKREL_M2P_EXTEND#
#define SL_HAL_LDMA_DESCRIPTOR_LINKREL_M2P_EXTENDValue:
LDMA descriptor initializer for linked memory to peripheral transfer.