Event System#

A publish/subscribe inter-process communication system.

The source files for the event system software module are present under platform/common.

Overview#

The event system is a software component enabling the development of event-driven software systems for Simplicity SDK based firmware's by managing publisher creation, event dispatching/filtering and event listening.

The event system has multiple types of event classes that subscribers can listen to. Event classes identify the event source from which the event originates such as Bluetooth or Zigbee. See sl_event_class_t.

Subclasses further refine the event by offering information related to a particular functionality. A unique bit is assigned to each subclass which will have a specific meaning for each event publisher.

Initialization#

The initialization of the event system occurs during the general system initialization. This happens when the application calls the sl_system_init() function. All the basic event system data structures will be initialized along with every publisher available in your project.

Event subscription#

The event subscription takes place when the user establishes a communication pipeline between the listener and the publisher by calling sl_event_subscribe. The user shall provide the type of event class that he wants to listen to, an event mask to further refine the set of events that he wants to listen to. Finally, an event queue must be created and initialized by the event listening code by using sl_event_queue_create which will allocate the necessary memory and initialize an event system event queue. This queue is the main communication channel between the publisher and the listener.

Event notification#

When a new event is generated, the publisher will enqueue it in the event listener provided queue. At this point, the listener will be able to recover this event by calling sl_event_queue_get function. In the case where no event is ready for processing the calling process will pend on the message queue for a predetermined amount of time. After consuming the event, the @sl_event_process function must be called for each event instance. This will ensure that the memory and resources used by the event data structure is properly deallocated.

Supervisor Mode#

Supervisor mode allows users to subscribe to all events from all classes. There is an internal queue that will receive all events published by any publisher. When a publisher is registered, the supervisor queue will subscribe to it automatically. To get an event from the supervisor queue, the user must call the function sl_event_supervisor_queue_get.

Modules#

sl_event_subscriber_t

sl_event_publisher_t

sl_event_t

Enumerations#

enum
SL_EVENT_CLASS_IRQ
SL_EVENT_CLASS_BLUETOOTH
SL_EVENT_CLASS_ZIGBEE
SL_EVENT_CLASS_BLUETOOTH_MESH
SL_EVENT_CLASS_WISUN
SL_EVENT_CLASS_MAX
}

Typedefs#

typedef osMessageQueueId_t

TYPEDEFS ***********************************.

typedef void(*

Functions#

void

PROTOTYPES ***********************************.

sl_event_publisher_register(sl_event_publisher_t *publisher, sl_event_class_t event_class, sl_event_free_data_cb_t free_data_callback)

Initialize a publisher context and register it in the event system with a given event class.

sl_event_publisher_unregister(sl_event_publisher_t *publisher)

Unregister a publisher context from its event class.

sl_event_publish(sl_event_publisher_t *publisher, uint32_t event_mask, uint8_t event_prio, void *event_data)

Publish an event, with data, within the event class of the publisher.

sl_event_publish_static(sl_event_publisher_t *publisher, uint32_t event_mask, uint8_t event_prio, sl_event_t *event, void *event_data)

Publish an event, with data, with a pre-allocated event handle, within the event class of the publisher.

sl_event_subscribe(sl_event_class_t event_class, uint32_t event_mask, sl_event_queue_t event_queue)

Subscribe to one or more events for a given event class.

sl_event_unsubscribe(sl_event_class_t event_class, uint32_t event_mask, sl_event_queue_t event_queue)

Unsubscribe from one or more events for a given event class.

sl_event_process(sl_event_t **event)

Signal to the event system that a subscriber has processed an event.

sl_event_queue_create(uint32_t event_count, sl_event_queue_t *event_queue)

Create an event queue.

sl_event_queue_delete(sl_event_queue_t event_queue)

Delete an event queue.

sl_event_queue_get(sl_event_queue_t event_queue, uint8_t *event_prio, uint32_t timeout, sl_event_t **event)

Get an event from an event queue.

uint32_t
sl_event_queue_get_count(sl_event_queue_t event_queue)

Get the current number of events in queue.

size_t

Get the size of the event publisher structure.

sl_event_publisher_alloc(sl_event_publisher_t **publisher)

Allocate the publisher structure to the heap using the common memory manager with a long-term lifespan.

sl_event_publisher_free(sl_event_publisher_t *publisher)

Free a publisher context structure from the heap, as well as its list of subscriber entries using the common memory manager.

size_t

Get the size of the event structure.

sl_event_alloc(sl_event_t **event)

Allocate the event structure to the heap using the common memory manager with a long-term lifespan.

sl_event_free(sl_event_t *event)

Free an event structure from the heap using the common memory manager.

Enumeration Documentation#

sl_event_class_t#

sl_event_class_t
Enumerator
SL_EVENT_CLASS_IRQ
SL_EVENT_CLASS_BLUETOOTH
SL_EVENT_CLASS_ZIGBEE
SL_EVENT_CLASS_BLUETOOTH_MESH
SL_EVENT_CLASS_WISUN
SL_EVENT_CLASS_MAX

Typedef Documentation#

sl_event_queue_t#

typedef osMessageQueueId_t sl_event_queue_t

TYPEDEFS ***********************************.


sl_event_free_data_cb_t#

typedef void(* sl_event_free_data_cb_t) (void *data) )(void *data)

Function Documentation#

sl_event_system_init#

void sl_event_system_init (void )

PROTOTYPES ***********************************.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Initialize the event system.


sl_event_publisher_register#

sl_status_t sl_event_publisher_register (sl_event_publisher_t * publisher, sl_event_class_t event_class, sl_event_free_data_cb_t free_data_callback)

Initialize a publisher context and register it in the event system with a given event class.

Parameters
TypeDirectionArgument NameDescription
sl_event_publisher_t *[in]publisher

Pointer to a publisher context.

sl_event_class_t[in]event_class

The class of events published by the publisher.

sl_event_free_data_cb_t[in]free_data_callback

Callback to free the publisher's event data.

@description Only one publisher context is allowed per event class.

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.


sl_event_publisher_unregister#

sl_status_t sl_event_publisher_unregister (sl_event_publisher_t * publisher)

Unregister a publisher context from its event class.

Parameters
TypeDirectionArgument NameDescription
sl_event_publisher_t *[in]publisher

Pointer to a publisher context.

@description When a publisher context is unregistered, it can no longer publish messages until it is registered again. After a publisher context is unregistered, the event class it was registered with can be reused.

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.


sl_event_publish#

sl_status_t sl_event_publish (sl_event_publisher_t * publisher, uint32_t event_mask, uint8_t event_prio, void * event_data)

Publish an event, with data, within the event class of the publisher.

Parameters
TypeDirectionArgument NameDescription
sl_event_publisher_t *[in]publisher

Pointer to a publisher context.

uint32_t[in]event_mask

Event mask corresponding to the type of event.

uint8_t[in]event_prio

The priority of the event published.

void *[in]event_data

The event data.

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.


sl_event_publish_static#

sl_status_t sl_event_publish_static (sl_event_publisher_t * publisher, uint32_t event_mask, uint8_t event_prio, sl_event_t * event, void * event_data)

Publish an event, with data, with a pre-allocated event handle, within the event class of the publisher.

Parameters
TypeDirectionArgument NameDescription
sl_event_publisher_t *[in]publisher

Pointer to a publisher context.

uint32_t[in]event_mask

Event mask corresponding to the type of event.

uint8_t[in]event_prio

The priority of the event published.

sl_event_t *[in]event

The pre-allocated event structure handle

void *[in]event_data

The event data.

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.


sl_event_subscribe#

sl_status_t sl_event_subscribe (sl_event_class_t event_class, uint32_t event_mask, sl_event_queue_t event_queue)

Subscribe to one or more events for a given event class.

Parameters
TypeDirectionArgument NameDescription
sl_event_class_t[in]event_class

The class of events to subscribe to.

uint32_t[in]event_mask

The event(s) to subscribe to.

sl_event_queue_t[in]event_queue

The identifier of an event queue.

@description The subscribed event(s) is/are placed in the queue identified by event_queue.

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.


sl_event_unsubscribe#

sl_status_t sl_event_unsubscribe (sl_event_class_t event_class, uint32_t event_mask, sl_event_queue_t event_queue)

Unsubscribe from one or more events for a given event class.

Parameters
TypeDirectionArgument NameDescription
sl_event_class_t[in]event_class

The class of events to subscribe to.

uint32_t[in]event_mask

The event(s) to subscribe to.

sl_event_queue_t[in]event_queue

The identifier of an event queue.

@description The unsubscribed event(s) will no longer be placed in the queue identified by event_queue.

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.


sl_event_process#

sl_status_t sl_event_process (sl_event_t ** event)

Signal to the event system that a subscriber has processed an event.

Parameters
TypeDirectionArgument NameDescription
sl_event_t **[in]event

Pointer to an event reference.

@description This must be called by subscribers after consuming an event so that the event data may eventually be freed. The event reference passed to this function is nullified before returning.

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.


sl_event_queue_create#

sl_status_t sl_event_queue_create (uint32_t event_count, sl_event_queue_t * event_queue)

Create an event queue.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]event_count

The maximum number of events in the event queue.

sl_event_queue_t *[out]event_queue

The event queue that is created.

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.


sl_event_queue_delete#

sl_status_t sl_event_queue_delete (sl_event_queue_t event_queue)

Delete an event queue.

Parameters
TypeDirectionArgument NameDescription
sl_event_queue_t[in]event_queue

The event queue to delete.

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.

Note

  • In the process of deleting an event queue, all events that the queue was subscribed to will be unsubscribed from.


sl_event_queue_get#

sl_status_t sl_event_queue_get (sl_event_queue_t event_queue, uint8_t * event_prio, uint32_t timeout, sl_event_t ** event)

Get an event from an event queue.

Parameters
TypeDirectionArgument NameDescription
sl_event_queue_t[in]event_queue

The identifier of an event queue.

uint8_t *[in]event_prio

The priority of event(s) to get.

uint32_t[in]timeout

Maximum time to pend on the event queue.

sl_event_t **[out]event

The event reference retrieved from the event queue.

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.


sl_event_queue_get_count#

uint32_t sl_event_queue_get_count (sl_event_queue_t event_queue)

Get the current number of events in queue.

Parameters
TypeDirectionArgument NameDescription
sl_event_queue_t[in]event_queue

The identifier of an event queue.

Returns

  • The current number of events in the queue.


sl_event_publisher_get_size#

size_t sl_event_publisher_get_size (void )

Get the size of the event publisher structure.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Size of the event publisher structure.


sl_event_publisher_alloc#

sl_status_t sl_event_publisher_alloc (sl_event_publisher_t ** publisher)

Allocate the publisher structure to the heap using the common memory manager with a long-term lifespan.

Parameters
TypeDirectionArgument NameDescription
sl_event_publisher_t **[in]publisher

address of a pointer to a publisher context

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.


sl_event_publisher_free#

sl_status_t sl_event_publisher_free (sl_event_publisher_t * publisher)

Free a publisher context structure from the heap, as well as its list of subscriber entries using the common memory manager.

Parameters
TypeDirectionArgument NameDescription
sl_event_publisher_t *[in]publisher

address of a pointer to a publisher context

@description Using this function to free a publisher context will also free its list of subscribers, which will cause subscribers to no longer receive events from the publisher context's event class.

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.


sl_event_get_size#

size_t sl_event_get_size (void )

Get the size of the event structure.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Size of the event structure.


sl_event_alloc#

sl_status_t sl_event_alloc (sl_event_t ** event)

Allocate the event structure to the heap using the common memory manager with a long-term lifespan.

Parameters
TypeDirectionArgument NameDescription
sl_event_t **[in]event

address of a pointer to an event struct

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.


sl_event_free#

sl_status_t sl_event_free (sl_event_t * event)

Free an event structure from the heap using the common memory manager.

Parameters
TypeDirectionArgument NameDescription
sl_event_t *[in]event

address of a pointer to an event struct.

Note

  • Freeing an event structure that has not yet been processed by all subscribers will result in undefined behavior.

Returns

  • SL_STATUS_OK if successful, otherwise an error code is returned.