SYSTEM CONFIGURATION#
System Configuration (SYSCFG) peripheral API.
The SYSCFG module provides access to various system configuration registers including chip revision information, system tick clock configuration, and memory controller settings.
Modules#
Enumerations#
AHBHOST masters that can use alternate MPAHBRAM ports.
AHB port given priority.
Functions#
Reads CHIPREV register.
Enables the external clock for the SysTick timer.
Disables the external clock source for the SysTick timer.
Configure Error Correcting Code (ECC).
Set MPAHBRAM port to use to access DMEM.
Set MPAHBRAM port priority for arbitration when multiple concurrent transactions to DMEM.
Get MPAHBRAM port arbitration priority selection.
Reads the DMEM0RETNCTRL register.
Applies a mask to the DMEM0RETNCTRL register.
Sets the DMEM0RETNCTRL register to zero.
Macros#
Bit mask used to extract the part number value without the new naming bitfield.
xG26 chips incorporate 2 memory banks including ECC support.
Default syscfg ecc_config initialization.
Enumeration Documentation#
sl_hal_syscfg_dmem_master_t#
sl_hal_syscfg_dmem_master_t
AHBHOST masters that can use alternate MPAHBRAM ports.
| Enumerator | |
|---|---|
| SL_HAL_SYSCFG_DMEM_MASTER_LDMA | LDMA master. |
| SL_HAL_SYSCFG_DMEM_MASTER_SRWAES | SRWAES master. |
| SL_HAL_SYSCFG_DMEM_MASTER_AHBSRW | AHBSRW master. |
| SL_HAL_DMEM_MASTER_SRWECA0 | SRWECA0 master. |
| SL_HAL_DMEM_MASTER_SRWECA1 | SRWECA1 master. |
| SL_HAL_DMEM_MASTER_MVPAHB_DATA0 | MVPAHB_DATA0 master. |
| SL_HAL_DMEM_MASTER_MVPAHB_DATA1 | MVPAHB_DATA1 master. |
| SL_HAL_DMEM_MASTER_MVPAHB_DATA2 | MVPAHB_DATA2 master. |
sl_hal_syscfg_port_priority_t#
sl_hal_syscfg_port_priority_t
AHB port given priority.
| Enumerator | |
|---|---|
| SL_HAL_SYSCFG_PORT_PRIORITY_NONE | Priority none. |
| SL_HAL_SYSCFG_PORT_PRIORITY_PORT0 | Priority is given to port 0. |
| SL_HAL_SYSCFG_PORT_PRIORITY_PORT1 | Priority is given to port 1. |
| SL_HAL_SYSCFG_PORT_PRIORITY_PORT2 | Priority is given to port 2. |
| SL_HAL_SYSCFG_PORT_PRIORITY_PORT3 | Priority is given to port 3. |
Function Documentation#
sl_hal_syscfg_read_chip_rev#
uint32_t sl_hal_syscfg_read_chip_rev (void )
Reads CHIPREV register.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The current value of the CHIPREV register, containing chip revision information.
sl_hal_syscfg_set_systicextclken_cfgsystic#
void sl_hal_syscfg_set_systicextclken_cfgsystic (void )
Enables the external clock for the SysTick timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_hal_syscfg_clear_systicextclken_cfgsystic#
void sl_hal_syscfg_clear_systicextclken_cfgsystic (void )
Disables the external clock source for the SysTick timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
sl_hal_syscfg_ecc_set_config#
void sl_hal_syscfg_ecc_set_config (const sl_hal_syscfg_ecc_config_t * ecc_config)
Configure Error Correcting Code (ECC).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_hal_syscfg_ecc_config_t * | [in] | ecc_config | ECC configuration. |
This function configures ECC support according to the configuration input parameter. If the user requests enabling ECC for a given RAM bank this function will initialize ECC memory (syndromes) for the bank by reading and writing the existing values in memory. I.e. all data is preserved. The initialization process runs in a critical section disallowing interrupts and thread scheduling, and will consume a considerable amount of clock cycles. Therefore the user should carefully assess where to call this function. The user can consider to increase the clock frequency in order to reduce the execution time. This function makes use of 2 DMA channels to move data to/from RAM in an efficient way. The user can select which 2 DMA channels to use in order to avoid conflicts with the application. However the user must make sure that no other DMA operations takes place while this function is executing. If the application has been using the DMA controller prior to calling this function, the application will need to reinitialize DMA registers after this function has completed.
Note
This function protects the ECC initialization procedure from interrupts and other threads by using a critical section (defined by sl_core.h) When running on RTOS the user may need to override CORE_EnterCritical CORE_ExitCritical.
sl_hal_syscfg_set_dmem_port_map#
void sl_hal_syscfg_set_dmem_port_map (sl_hal_syscfg_dmem_master_t master, uint8_t port)
Set MPAHBRAM port to use to access DMEM.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_hal_syscfg_dmem_master_t | [in] | master | AHBHOST master to be configured. |
| uint8_t | [in] | port | AHBHOST slave port to use. |
This function configures which MPAHBRAM slave port is used to access DMEM. Depending on the use case, it might improve performance by spreading the load over the N ports (N is usually 2 or 4),instead of starving because a port is used by another master.
sl_hal_syscfg_set_port_priority#
void sl_hal_syscfg_set_port_priority (sl_hal_syscfg_port_priority_t port_priority)
Set MPAHBRAM port priority for arbitration when multiple concurrent transactions to DMEM.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_hal_syscfg_port_priority_t | [in] | port_priority | AHBHOST slave port having elevated priority. |
This function configures which MPAHBRAM slave port will have priority. The AHB port arbitration default scheme, round-robin arbitration, is selected when port_priority == SL_HAL_SYSCFG_PORT_PRIORITY_NONE.
Note
Doing this can potentially starve the others AHB port(s).
sl_hal_syscfg_get_port_priority#
sl_hal_syscfg_port_priority_t sl_hal_syscfg_get_port_priority (void )
Get MPAHBRAM port arbitration priority selection.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Returns the AHBHOST slave port given priority or none.
This function returns the AHBHOST slave with raised priority.
sl_hal_syscfg_read_dmem0retnctrl#
uint32_t sl_hal_syscfg_read_dmem0retnctrl (void )
Reads the DMEM0RETNCTRL register.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
The current value of the DMEM0RETNCTRL register.
This function retrieves the current value of the DMEM0RETNCTRL register, which is used to control the retention settings for DMEM0 memory blocks.
sl_hal_syscfg_mask_dmem0retnctrl#
void sl_hal_syscfg_mask_dmem0retnctrl (uint32_t mask)
Applies a mask to the DMEM0RETNCTRL register.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | mask | The bit mask to apply to the DMEM0RETNCTRL register. |
This function performs a bitwise OR operation between the current value of the DMEM0RETNCTRL register and the provided mask, setting specific bits in the register.
sl_hal_syscfg_zero_dmem0retnctrl#
void sl_hal_syscfg_zero_dmem0retnctrl (void )
Sets the DMEM0RETNCTRL register to zero.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function clears all bits in the DMEM0RETNCTRL register by setting its value to 0. This effectively disables all retention settings for DMEM0 memory blocks.