Synchronous mode initialization structure.

Public Attributes#

bool

Select if to operate in master or slave mode.

bool

Select if to send most or least significant bit first.

bool

Enable CS invert.

bool

Enable AUTOTX mode.

bool

Auto CS enabling.

bool

Enable USART Rx via PRS.

uint8_t

Select PRS channel for USART Rx. (Only valid if prs_rx_enable is true).

uint8_t

Auto CS hold time in baud cycles.

uint8_t

Auto CS setup time in baud cycles.

uint32_t

Desired Clock Divider.

Number of data bits in frame.

Clock polarity/phase mode.

Public Attribute Documentation#

master#

bool sl_hal_usart_sync_init_t::master

Select if to operate in master or slave mode.


msb_first#

bool sl_hal_usart_sync_init_t::msb_first

Select if to send most or least significant bit first.


cs_invert#

bool sl_hal_usart_sync_init_t::cs_invert

Enable CS invert.

By default, chip select is active low. Set to true to make chip select active high.


auto_tx#

bool sl_hal_usart_sync_init_t::auto_tx

Enable AUTOTX mode.

Transmits as long as RX is not full. Generates underflows if TX is empty.


auto_cs_enable#

bool sl_hal_usart_sync_init_t::auto_cs_enable

Auto CS enabling.


prs_rx_enable#

bool sl_hal_usart_sync_init_t::prs_rx_enable

Enable USART Rx via PRS.


prs_rx_channel#

uint8_t sl_hal_usart_sync_init_t::prs_rx_channel

Select PRS channel for USART Rx. (Only valid if prs_rx_enable is true).


auto_cs_hold#

uint8_t sl_hal_usart_sync_init_t::auto_cs_hold

Auto CS hold time in baud cycles.


auto_cs_setup#

uint8_t sl_hal_usart_sync_init_t::auto_cs_setup

Auto CS setup time in baud cycles.


clock_div#

uint32_t sl_hal_usart_sync_init_t::clock_div

Desired Clock Divider.


data_bits#

sl_hal_usart_data_bits_t sl_hal_usart_sync_init_t::data_bits

Number of data bits in frame.


clock_mode#

sl_hal_usart_clock_mode_t sl_hal_usart_sync_init_t::clock_mode

Clock polarity/phase mode.