UART advanced initialization structure.

Public Attributes#

bool

Enable the collision Detection feature.

bool

If true, data will be sent with most significant bit first.

bool

Enable DMA requests blocking while framing or parity errors.

bool

Enable automatic tristating of transmitter output when there is nothing to transmit.

bool

Enable Multiprocessor mode. Address and data filtering using the 9th bit.

bool

Multiprocessor address bit value. If true, 9th bit of address frame must be 1, 0 otherwise.

bool

Enable EUSART capability to use a PRS channel as an input data line for the receiver.

uint8_t

PRS Channel used to transmit data from PRS to the EUSART.

uint8_t

Start frame that will enable RX operation. 0x00 Disable this feature.

Enable inversion of RX and/or TX signals.

Auto TX delay in baud cycles before new transfers. Frames sent back-to-back are not delayed.

Interrupt and status level of the Receive FIFO.

Interrupt and status level of the Transmit FIFO.

uint8_t

Timeout in number of frames between RX frames. 0 disables this feature.

Public Attribute Documentation#

collision_detect#

bool sl_hal_eusart_uart_advanced_init_t::collision_detect

Enable the collision Detection feature.

Internal (setting loopback_enable) or external loopback must be done to use this feature.


msb_first#

bool sl_hal_eusart_uart_advanced_init_t::msb_first

If true, data will be sent with most significant bit first.


dma_halt_on_error#

bool sl_hal_eusart_uart_advanced_init_t::dma_halt_on_error

Enable DMA requests blocking while framing or parity errors.


tx_auto_tristate#

bool sl_hal_eusart_uart_advanced_init_t::tx_auto_tristate

Enable automatic tristating of transmitter output when there is nothing to transmit.


multi_processor_enable#

bool sl_hal_eusart_uart_advanced_init_t::multi_processor_enable

Enable Multiprocessor mode. Address and data filtering using the 9th bit.


multi_processor_address_bit_high#

bool sl_hal_eusart_uart_advanced_init_t::multi_processor_address_bit_high

Multiprocessor address bit value. If true, 9th bit of address frame must be 1, 0 otherwise.


prs_rx_enable#

bool sl_hal_eusart_uart_advanced_init_t::prs_rx_enable

Enable EUSART capability to use a PRS channel as an input data line for the receiver.

PRS channel and RX GPIO must be configured separately using PRS/GPIO API.


prs_rx_channel#

uint8_t sl_hal_eusart_uart_advanced_init_t::prs_rx_channel

PRS Channel used to transmit data from PRS to the EUSART.


start_frame#

uint8_t sl_hal_eusart_uart_advanced_init_t::start_frame

Start frame that will enable RX operation. 0x00 Disable this feature.


hw_flow_control_mode#

sl_hal_eusart_hw_flow_control_t sl_hal_eusart_uart_advanced_init_t::hw_flow_control_mode

Hardware flow control mode.


invert_io#

sl_hal_eusart_invert_io_t sl_hal_eusart_uart_advanced_init_t::invert_io

Enable inversion of RX and/or TX signals.


auto_tx_delay#

sl_hal_eusart_auto_tx_delay_t sl_hal_eusart_uart_advanced_init_t::auto_tx_delay

Auto TX delay in baud cycles before new transfers. Frames sent back-to-back are not delayed.


rx_fifo_watermark#

sl_hal_eusart_fifo_interrupt_watermark_t sl_hal_eusart_uart_advanced_init_t::rx_fifo_watermark

Interrupt and status level of the Receive FIFO.


tx_fifo_watermark#

sl_hal_eusart_fifo_interrupt_watermark_t sl_hal_eusart_uart_advanced_init_t::tx_fifo_watermark

Interrupt and status level of the Transmit FIFO.


rx_timeout#

uint8_t sl_hal_eusart_uart_advanced_init_t::rx_timeout

Timeout in number of frames between RX frames. 0 disables this feature.