Silicon Labs Cryptograpy Hardware Acceleration Drivers#

The Simplicity SDK includes PSA device drivers and ALT plugins for selected PSA Crypto and Mbed TLS library functions to support acceleration of cryptographic algorithms and support secure key storage. peripherals depending on the capabilities of the target device. All PSA Crypto drivers and Mbed TLS ALT "legacy" plugins in the Simplicity SDK support bare metal, RTOS and multi-threaded applications.

The ALT plugins support the "legacy" ALT(ernative) crypto APIs of Mbed TLS which receive key material in plaintext format, and hence do not support secure key handling, in contrast to the PSA Crypto APIs which supports importing and storing keys safely, and reference the keys by identifiers. The legacy crypto APIs will be removed in a future Mbed TLS version, and fully replaced by the PSA Crypto APIs.

Secure Key support#

The PSA Crypto APIs provides secure key support by importing and storing key material safely in a trusted format or storage. The PSA import key API function returns a key identifier which the user can subsequently apply to other PSA Crypto APIs , e.g. to encrypt some plaintext message.

  • Series-2 and Series-3 HSE Vault High devices support "wrapping" keys by encrypting the key material during the import function, then the "wrapped" key can be stored in untrusted RAM.

  • Series-2 HSE Vault Mid and VSE devices can enable TrustZone Secure Key Library (SKL) which will import and protect the plaintext keys in Secure RAM. For persistent keys stored in PSA ITS, the ITS driver will encrypt the plaintext keys before storing them securely in NVM3 which is located in NonSecure Flash. For more information on TZ SKL please refer to the application note AN1374 https://www.silabs.com/documents/public/application-notes/an1374-trustzone.pdf .

  • Series-3 HSE devices support importing keys into a Key Slot Unit (KSU) which can transfer keys efficiently and securely to SYMCRYPTO and LPWAES crypto engines for fast secure crypto operations. KSU support is faster than wrapped key support because wrapped keys need to be moved to the SE for every operation, compared to, once stored in the KSU the key can be used quickly multiple times.

Secure Engine (SE) Peripheral#

Series 2 and Series 3 devices with a Hardware Secure Engine (HSE) incorporate the SE peripheral for cryptographic hardware acceleration. In order to support the SE peripheral, the Simplicity SDK includes SE specific PSA Crypto drivers and ALT plugins for the "legacy" crypto APIs for Mbed TLS. For HSE Vault High devices the PSA SE Crypto drivers supports key wrapping for secure key support (opaque driver mode), in addition to plaintext key support (transparent driver mode). On HSE Vault Mid devices the SE does not support key wrapping, and hence the PSA SE drivers only work for plaintext keys (transparent driver mode). In order to support secure keys on Series-2 HSE Vault Mid the user can enable TrustZone Secure Key Library (TZ SKL) which will import and protect the plaintext keys in Secure RAM. For persistent keys stored in PSA ITS, the ITS driver will encrypt the plaintext keys before storing them securely in NVM3 which is located in NonSecure Flash. For more information on TZ SKL please refer to the application note AN1374 https://www.silabs.com/documents/public/application-notes/an1374-trustzone.pdf .

Note: The Secure Engine drivers are multi-thread capable, but do not support preemption. This means the application developer is responsible for not calling a driver-accelerated PSA Crypto API under conditions which would cause preemption of an already-running operation. For bare metal applications, this usually means not calling cryptographic operations from ISR. For RTOS-based applications, this boils down to not calling these SE-accelerated functions from either ISR or inside critical/atomic sections, since the underlying mutex acquisition would fail.

CRYPTOACC Peripheral#

Series 2 devices with a Virtual Secure Engine (VSE) incorporate the CRYPTOACC peripheral for cryptographic hardware acceleration. In order to support the CRYPTOACC peripheral, the Simplicity SDK includes CRYPTOACC specific PSA Crypto drivers and ALT plugins for the "legacy" crypto APIs of Mbed TLS. VSE devices do not support key wrapping, and hence the PSA CRYPTOACC drivers only work for plaintext keys (transparent driver mode). In order to support secure keys on Series-2 VSE the user can enable TrustZone Secure Key Library (TZ SKL) which will import and protect the plaintext keys in Secure RAM. For persistent keys stored in PSA ITS, the ITS driver will encrypt the plaintext keys before storing them securely in NVM3 which is located in NonSecure Flash. For more information on TZ SKL please refer to the application note AN1374 https://www.silabs.com/documents/public/application-notes/an1374-trustzone.pdf.

Note: The CRYPTOACC peripheral has not been hardened against side-channel analysis (SCA) attacks. Certain APIs in Mbed TLS might give the impression of being secured against this class of attack, but this is not necessarily true if the hardware acceleration plugins are used. For example: some APIs operating over elliptic curves will require an RNG function pointer and state to be passed as arguments in order to perform coordinate randomization. Since the CRYPTOACC peripheral does not allow for this type of acceleration, these parameters will not be used. However, it should be stated that timing based SCA attacks are more challenging to perform on hardware accelerated operations of this type – since they are significantly faster than their software implementation counterparts.

SYMCRYPTO, LPWAES and KSU Peripherals#

Series 3 devices incorporate the SYMCRYPTO and LPWAES peripherals for cryptographic hardware acceleration. The SYMCRYPTO and LPWAES can use keys provided in plaintext format or keys stored in the Key Slot Unit (KSU) for secure key support. SYMCRYPTO / LPWAES using KSU supports faster secure key operations than the SE wrapped key operations. However the SE wrapped key operations should be considered more secure than SYMCRYPTO/LPWAES since the SE AES engines have DFA countermeasures (which is not supported by SYMCRYPTO and LPWAES). The Simplicity SDK include PSA Crypto drivers in order to support the SYMCRYPTO peripheral. The LPWAES peripheral is reserved for internal Simplicity SDK components and is not supported by the PSA Crypto drivers.

Note: The KSU must not be used if the key is required to be protected by DFA countermeasures. Also note, if the key is required to be protected by DPA countermeasures, the user must ensure that the SYMCRYPTO DPA countermeasure is enabled and seeded for DPA protection to work properly. The SYMCRYPTO DPA seed can be loaded by the sli_crypto_countermeasure_reseed() function, and the initial seed can be performed by the sli_crypto_init() which is called by sl_main_init() during startup when the sli_crypto component labeled "Accelerated Crypto Primitives" is included in the application project. To prevent a key in a non-KSU location, e.g. SL_PSA_KEY_LOCATION_WRAPPED, from being copied to KSU with psa_copy_key, the user can apply the key usage flag called SLI_PSA_KSU_KEY_ATTR_DISALLOW_KSU.

Supported Features/Drivers for PSA Crypto#

In this section, all cryptographic primitives, algorithms, modes-of-operations, etc., that have dedicated drivers implemented will be listed. When including an SLC component that supports an algorithm in PSA Crypto, any corresponding driver usable for the current device will be automatically enabled.

Note: The fact that an algorithm is not explicitly listed in the below tables does not necessarily mean that it is unsupported through the PSA Crypto API: Mbed TLS provides software implementations for most algorithms supported by the PSA Crypto API specification. Also note that that 'composite algorithms' may be partially accelerated using the drivers—as an example, HKDF is not accelerated in its entirety, but the underlying HMAC operations are.

Encryption#

Algorithm

Key Sizes(Bits)

Multi-Part /Single-part

Plaintext Keys

Wrapped Keys

Built-in Keys

AES-ECB

128, 192, 256

Both

All Devices

Secure Vault High

AES-128 HSE Key

AES-CTR

128, 192, 256

Both

All Devices

Secure Vault High

AES-128 HSE Key

AES-CBC(W/O Padding)

128, 192, 256

Both

All Devices

Secure Vault High

AES-128 HSE Key

AES-CBC(PKCS#7 Padding)

128, 192, 256

Both

All Devices

Secure Vault High

AES-128 HSE Key

AES-OFB

128, 192, 256

Both

All Devices

Secure Vault High

AES-128 HSE Key

AES-CFB

128, 192, 256

Both

All Devices

Secure Vault High

AES-128 HSE Key

AES-CCM*(from IEEE 802.15.4)

128, 192, 256

Both

All Devices

Secure Vault High

AES-128 HSE Key

ChaCha20

256

Both

Secure Vault High , except xG301 device family

Secure Vault High , except xG301 device family

-

Authenticated Encryption#

Algorithm

Key Sizes(Bits)

Multi-Part/Single-Part

Plaintext Keys

Wrapped Keys

Built-in Keys

Limitations

AES-GCM

128, 192, 256

Both

All Devices

Secure Vault High

-

Only supports nonces of length equal to 12 bytes by default, support for other lengths must be explicitly enabled using SLC

AES-CCM

128, 192, 256

Both

All Devices

Secure Vault High

-

-

ChaCha20-Poly1305

256

Single-Part

Secure Vault High , except xG301 device family

Secure Vault High , except xG301 device family

-

Rejects truncated tag lengths; Only supports the nonce variant specified in RFC7539

Hash Functions#

Algorithm

Digest Sizes(Bits)

Multi-Part /Single-Part

Limitations

SHA-1

160

Both

-

SHA-2

224, 256, 384, 512

Both

Digest sizes greater than 256-bit are only available on Secure Vault High devices

Message Authentication Codes#

Algorithm

MAC Sizes(Bits)

Key Sizes(Bits)

Multi-Part/Single-Part

Plaintext Keys

Wrapped Keys

Built-In Keys

Limitations

HMAC

160, 224, 256, 384, 512 (Can be truncated)

Any multiple of 8 greater that zero

Both

All Devices

Secure Vault High

-

MAC sizes greater than 256-bit are only available on Secure Vault High devices; Wrapped keys can only be used for single-part operations

CMAC

128 (Can be truncated)

128, 192, 256

Both

All Devices

Secure Vault High

VSE PUF Key

-

CBC-MAC

128 (Can be truncated)

128, 192, 256

Both

xG21

xG21B

-

-

Signatures#

Algorithm

Curves

Plaintext Keys

Wrapped Keys

Built-In Keys

Limitations

ECDSA

Secp192r1, Secp224r1, Secp256r1, Secp384r1, Secp521r1, Secp256k1

All Devices

Secure Vault High

HSE Application Attestation Key, HSE System Attestation Key, HSE Secure Boot Key, HSE Secure Debug Key

Curves with parameter sizes greater than 256-bit are only available on Secure Vault High devices; Secp256k1 is only supported on Virtual Secure Engine devices; HSE Application Attestation is not supported on the xG301 device family

EdDSA

Edwards25519

HSE Devices

Secure Vault High

Only supports pure EdDSA (no pre-hashing)

Key Exchange#

Algorithm

Curves

Plaintext Keys

Wrapped Keys

Built-In Keys

Limitations

ECDH

Secp192r1, Secp224r1, Secp256r1, Secp384r1, Secp521r1, Secp256k1

All Devices

Secure Vault High

-

Curves with parameter sizes greater than 256-bit are only available on Secure Vault High devices; Secp256k1 is only supported on Virtual Secure Engine devices. The xG301 device family does not support Secp384r1, Secp521r1

X25519

Curve25519

Hardware Secure Engine Devices

Secure Vault High

-

Only supports pure EdDSA (no pre-hashing)