Common Token Manager Defines#
This module provides defines for the Common Token Manager (CTM).
The defines in this module are used for creating 32-bit token identifier to identify static device tokens, static secure tokens and dynamic tokens in the CTM.
Note
For more information on tokens and CTM refer to silabs application note 'AN1154: Using Tokens for Non-Volatile Data Storage'
Modules#
Macros#
Helper MACRO to get the size of a predefined token.
Helper MACRO to create a new static device token in 32-bit identifier format, the tokens created are stored in secure memory region and are mass erase protected, this MACRO can be used with sl_token_get_data() or sl_token_set_data() functions, for more information `sl_token_manager_defines.h`.
Helper MACRO to create a new static secure token in 32-bit identifier format, the tokens created are stored in dedicated flash region, with additional security measures and are not protected by mass/device erase, this MACRO can be used with sl_token_get_data() or sl_token_set_data() functions, for more information `sl_token_manager_defines.h`.
Helper MACRO to create dynamic token, user has to take care of providing the unique token for each NVM3 token created, the tokens created are stored in NVM3 region and are not protected by mass/device/nvm3 erase, this MACRO can be used with sl_token_get_data() or sl_token_set_data() functions, for more information `sl_token_manager_defines.h`.
Helper MACRO to create dynamic token for NVM3 secondary instance, user has to take care of providing the unique token for each NVM3 token created, the tokens created are stored in NVM3 region and are not protected by mass/device/nvm3 erase, this MACRO can be used with sl_token_get_data() or sl_token_set_data() functions, for more information `sl_token_manager_defines.h`.
Helper MACRO to create a NVM3 override key for static token, this MACRO can be used with sl_token_get_data() or sl_token_set_data() functions, the range for NVM3 Domain region for a static token override key is predefined for more information `sl_token_manager_defines.h`.