ACMP - Analog Comparator#
Analog comparator (ACMP) Peripheral API.
The Analog Comparator is used to compare voltage of two analog inputs with a digital output indicating which input voltage is higher. Inputs can either be one of the selectable internal references or from external pins. Response time and current consumption can be configured by altering the current supply to the comparator.
ACMP is available down to EM3 and is able to wake up the system when input signals pass a certain threshold. Use ACMP_IntEnable() to enable an edge interrupt to use this functionality.
This example shows how to use the em_acmp.h API for comparing an input pin to an internal 2.5 V reference voltage.
/* Initialize with default settings. */
ACMP_Init_TypeDef init = ACMP_INIT_DEFAULT;
ACMP_Init(ACMP0, &init);
/* In this example we want to compare an analog input to the 2.5 V
* internal reference. The default settings resets the divider for
* acmpInputVREFDIV2V5, which we can use as a 2.5 V reference. */
/* Now we select the two inputs to compare. Here we compare the acmpInputPD2
* input to the internal 2.5V reference. When acmpInputPD2 is lower than
* 2.5 V then the ACMP output is 0 and when acmpInputPD2 is is higher than
* 2.5 V then the ACMP output is 1. */
ACMP_ChannelSet(ACMP0, acmpInputVREFDIV2V5, acmpInputPD2);
/* Allocate CDEVEN0 to ACMP0 to be able to use the input. */
GPIO->CDBUSALLOC = GPIO_CDBUSALLOC_CDEVEN0_ACMP0;
/* To be able to probe the output we can send the ACMP output to a pin.
* The second argument to this function is the pin location which is
* device dependent. */
ACMP_GPIOSetup(ACMP0, gpioPortD, 1, true, false);
Note
ACMP can also be used to compare two separate input pins.
ACMP also contains specialized hardware for capacitive sensing. This module contains the ACMP_CapsenseInit() function to initialize ACMP for capacitive sensing and the ACMP_CapsenseChannelSet() function to select the current capsense channel.
For applications that require capacitive sensing it is recommended to use a library, such as cslib, which is provided by Silicon Labs.
Modules#
Enumerations#
Resistor values used for the internal capacitive sense resistor.
Hysteresis level.
Adjust ACMP performance for a given input voltage range.
ACMP accuracy mode.
ACMP Input Selection.
Functions#
Set up ACMP for use in capacitive sense applications.
Set the ACMP channel used for capacitive sensing.
Set which channels should be used in ACMP comparisons.
Disable ACMP.
Enable ACMP.
Sets up GPIO output from the ACMP.
Initialize ACMP.
Reset ACMP to the same state that it was in after a hardware reset.
Clear one or more pending ACMP interrupts.
Disable one or more ACMP interrupts.
Enable one or more ACMP interrupts.
Get pending ACMP interrupt flags.
Get enabled and pending ACMP interrupt flags.
Set one or more pending ACMP interrupts from software.
Convert GPIO port/pin to ACMP input selection.
Get state of ACMP output value.
Macros#
A default configuration for capacitive sense mode initialization.
Analog comparator reset value.
Capacitive sense mode configuration default values.
Default configuration for ACMP regular initialization.
Enumeration Documentation#
ACMP_CapsenseResistor_TypeDef#
ACMP_CapsenseResistor_TypeDef
Resistor values used for the internal capacitive sense resistor.
See data sheet for your device for details on each resistor value.
| Enumerator | |
|---|---|
| acmpResistor0 | Resistor value 0. |
| acmpResistor1 | Resistor value 1. |
| acmpResistor2 | Resistor value 2. |
| acmpResistor3 | Resistor value 3. |
| acmpResistor4 | Resistor value 4. |
| acmpResistor5 | Resistor value 5. |
| acmpResistor6 | Resistor value 6. |
ACMP_HysteresisLevel_TypeDef#
ACMP_HysteresisLevel_TypeDef
Hysteresis level.
See data sheet for your device for details on each level.
| Enumerator | |
|---|---|
| acmpHysteresisDisabled | Mode DISABLED for ACMP_CFG. |
| acmpHysteresis10Sym | Mode HYST10SYM for ACMP_CFG. |
| acmpHysteresis20Sym | Mode HYST20SYM for ACMP_CFG. |
| acmpHysteresis30Sym | Mode HYST30SYM for ACMP_CFG. |
| acmpHysteresis10Pos | Mode HYST10POS for ACMP_CFG. |
| acmpHysteresis20Pos | Mode HYST20POS for ACMP_CFG. |
| acmpHysteresis30Pos | Mode HYST30POS for ACMP_CFG. |
| acmpHysteresis10Neg | Mode HYST10NEG for ACMP_CFG. |
| acmpHysteresis20Neg | Mode HYST20NEG for ACMP_CFG. |
| acmpHysteresis30Neg | Mode HYST30NEG for ACMP_CFG. |
ACMP_InputRange_TypeDef#
ACMP_InputRange_TypeDef
Adjust ACMP performance for a given input voltage range.
| Enumerator | |
|---|---|
| acmpInputRangeFull | Input can be from 0 to VDD. |
| acmpInputRangeReduced | Input can be from 0 to VDD-0.7 V. |
ACMP_Accuracy_TypeDef#
ACMP_Accuracy_TypeDef
ACMP accuracy mode.
| Enumerator | |
|---|---|
| acmpAccuracyLow | Low-accuracy mode which consumes less current. |
| acmpAccuracyHigh | High-accuracy mode which consumes more current. |
ACMP_Channel_TypeDef#
ACMP_Channel_TypeDef
ACMP Input Selection.
| Enumerator | |
|---|---|
| acmpInputVSS | Select VSS. |
| acmpInputVREFDIVAVDD | Select Divided AVDD. |
| acmpInputVREFDIVAVDDLP | Select Low-Power Divided AVDD. |
| acmpInputVREFDIV1V25 | Select Divided 1V25 reference. |
| acmpInputVREFDIV1V25LP | Select Low-power Divided 1V25 reference. |
| acmpInputVREFDIV2V5 | Select Divided 2V5 reference. |
| acmpInputVREFDIV2V5LP | Select Low-power Divided 2V5 reference. |
| acmpInputVSENSE01DIV4 | Select VSENSE0 divided by 4. |
| acmpInputVSENSE01DIV4LP | Select Low-power VSENSE0 divided by 4. |
| acmpInputVSENSE11DIV4 | VSENSE1 divided by 4. |
| acmpInputVSENSE11DIV4LP | Low-power VSENSE1 divided by 4. |
| acmpInputCAPSENSE | Select Low-Power Divided AVDD. |
| acmpInputEXTPA | Select external interface, base is PA0. |
| acmpInputEXTPB | Select external interface, base is PB0. |
| acmpInputEXTPC | Select external interface, base is PC0. |
| acmpInputEXTPD | Select external interface, base is PD0. |
| acmpInputPA0 | Select Port A Pin0. |
| acmpInputPA1 | Select Port A Pin1. |
| acmpInputPA2 | Select Port A Pin2. |
| acmpInputPA3 | Select Port A Pin3. |
| acmpInputPA4 | Select Port A Pin4. |
| acmpInputPA5 | Select Port A Pin5. |
| acmpInputPA6 | Select Port A Pin6. |
| acmpInputPA7 | Select Port A Pin7. |
| acmpInputPA8 | Select Port A Pin8. |
| acmpInputPA9 | Select Port A Pin9. |
| acmpInputPA10 | Select Port A Pin10. |
| acmpInputPA11 | Select Port A Pin11. |
| acmpInputPA12 | Select Port A Pin12. |
| acmpInputPA13 | Select Port A Pin13. |
| acmpInputPA14 | Select Port A Pin14. |
| acmpInputPA15 | Select Port A Pin15. |
| acmpInputPB0 | Select Port B Pin0. |
| acmpInputPB1 | Select Port B Pin1. |
| acmpInputPB2 | Select Port B Pin2. |
| acmpInputPB3 | Select Port B Pin3. |
| acmpInputPB4 | Select Port B Pin4. |
| acmpInputPB5 | Select Port B Pin5. |
| acmpInputPB6 | Select Port B Pin6. |
| acmpInputPB7 | Select Port B Pin7. |
| acmpInputPB8 | Select Port B Pin8. |
| acmpInputPB9 | Select Port B Pin9. |
| acmpInputPB10 | Select Port B Pin10. |
| acmpInputPB11 | Select Port B Pin11. |
| acmpInputPB12 | Select Port B Pin12. |
| acmpInputPB13 | Select Port B Pin13. |
| acmpInputPB14 | Select Port B Pin14. |
| acmpInputPB15 | Select Port B Pin15. |
| acmpInputPC0 | Select Port C Pin0. |
| acmpInputPC1 | Select Port C Pin1. |
| acmpInputPC2 | Select Port C Pin2. |
| acmpInputPC3 | Select Port C Pin3. |
| acmpInputPC4 | Select Port C Pin4. |
| acmpInputPC5 | Select Port C Pin5. |
| acmpInputPC6 | Select Port C Pin6. |
| acmpInputPC7 | Select Port C Pin7. |
| acmpInputPC8 | Select Port C Pin8. |
| acmpInputPC9 | Select Port C Pin9. |
| acmpInputPC10 | Select Port C Pin10. |
| acmpInputPC11 | Select Port C Pin11. |
| acmpInputPC12 | Select Port C Pin12. |
| acmpInputPC13 | Select Port C Pin13. |
| acmpInputPC14 | Select Port C Pin14. |
| acmpInputPC15 | Select Port C Pin15. |
| acmpInputPD0 | Select Port D Pin0. |
| acmpInputPD1 | Select Port D Pin1. |
| acmpInputPD2 | Select Port D Pin2. |
| acmpInputPD3 | Select Port D Pin3. |
| acmpInputPD4 | Select Port D Pin4. |
| acmpInputPD5 | Select Port D Pin5. |
| acmpInputPD6 | Select Port D Pin6. |
| acmpInputPD7 | Select Port D Pin7. |
| acmpInputPD8 | Select Port D Pin8. |
| acmpInputPD9 | Select Port D Pin9. |
| acmpInputPD10 | Select Port D Pin10. |
| acmpInputPD11 | Select Port D Pin11. |
| acmpInputPD12 | Select Port D Pin12. |
| acmpInputPD13 | Select Port D Pin13. |
| acmpInputPD14 | Select Port D Pin14. |
| acmpInputPD15 | Select Port D Pin15. |
Function Documentation#
ACMP_CapsenseInit#
void ACMP_CapsenseInit (ACMP_TypeDef * acmp, const ACMP_CapsenseInit_TypeDef * init)
Set up ACMP for use in capacitive sense applications.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
| const ACMP_CapsenseInit_TypeDef * | [in] | init | A pointer to the initialization structure used to configure ACMP for capacitive sensing operation. |
This function sets up ACMP for use in capacitive sense applications. To use the capacitive sense functionality in the ACMP, use the PRS output of the ACMP module to count the number of oscillations in the capacitive sense circuit (possibly using a TIMER).
Note
A basic example of capacitive sensing can be found in the STK BSP (capsense demo).
A call to ACMP_CapsenseInit will enable and disable the ACMP peripheral, which can cause side effects if it was previously set up.
ACMP_CapsenseChannelSet#
void ACMP_CapsenseChannelSet (ACMP_TypeDef * acmp, ACMP_Channel_TypeDef channel)
Set the ACMP channel used for capacitive sensing.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
| ACMP_Channel_TypeDef | [in] | channel | The ACMP channel to use for capacitive sensing (Possel). |
Note
A basic example of capacitive sensing can be found in the STK BSP (capsense demo).
Can only be called when the peripheral is enabled.
ACMP_ChannelSet#
void ACMP_ChannelSet (ACMP_TypeDef * acmp, ACMP_Channel_TypeDef negSel, ACMP_Channel_TypeDef posSel)
Set which channels should be used in ACMP comparisons.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
| ACMP_Channel_TypeDef | N/A | negSel | A channel to use on the negative input to the ACMP. |
| ACMP_Channel_TypeDef | N/A | posSel | A channel to use on the positive input to the ACMP. |
Note
Can only be called when the peripheral is enabled.
If GPIO is used for both posSel and negSel, they cannot both use even or odd pins.
ACMP_Disable#
void ACMP_Disable (ACMP_TypeDef * acmp)
Disable ACMP.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
ACMP_Enable#
void ACMP_Enable (ACMP_TypeDef * acmp)
Enable ACMP.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
ACMP_GPIOSetup#
void ACMP_GPIOSetup (ACMP_TypeDef * acmp, GPIO_Port_TypeDef port, unsigned int pin, bool enable, bool invert)
Sets up GPIO output from the ACMP.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | Pointer to the ACMP peripheral register block. |
| GPIO_Port_TypeDef | N/A | port | The GPIO port to use. |
| unsigned int | N/A | pin | The GPIO pin to use. |
| bool | N/A | enable | Enable or disable pin output. |
| bool | N/A | invert | Invert output. |
Note
GPIO must be enabled in the CMU before this function call, i.e.
CMU_ClockEnable(cmuClock_GPIO, true);
ACMP_Init#
void ACMP_Init (ACMP_TypeDef * acmp, const ACMP_Init_TypeDef * init)
Initialize ACMP.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
| const ACMP_Init_TypeDef * | [in] | init | A pointer to the initialization structure used to configure ACMP. |
Note
A call to ACMP_Init can cause side effects since it can enable/disable the peripheral.
ACMP_Reset#
void ACMP_Reset (ACMP_TypeDef * acmp)
Reset ACMP to the same state that it was in after a hardware reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
Note
The GPIO ACMP ROUTE register is NOT reset by this function to allow for centralized setup of this feature.
The peripheral may be enabled and disabled during reset.
ACMP_IntClear#
void ACMP_IntClear (ACMP_TypeDef * acmp, uint32_t flags)
Clear one or more pending ACMP interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
| uint32_t | [in] | flags | Pending ACMP interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IFC_EDGE or ACMP_IFC_WARMUP. |
ACMP_IntDisable#
void ACMP_IntDisable (ACMP_TypeDef * acmp, uint32_t flags)
Disable one or more ACMP interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
| uint32_t | [in] | flags | ACMP interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IEN_EDGE or ACMP_IEN_WARMUP. |
ACMP_IntEnable#
void ACMP_IntEnable (ACMP_TypeDef * acmp, uint32_t flags)
Enable one or more ACMP interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
| uint32_t | [in] | flags | ACMP interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IEN_EDGE or ACMP_IEN_WARMUP. |
Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using ACMP_IntClear() prior to enabling if a pending interrupt should be ignored.
ACMP_IntGet#
uint32_t ACMP_IntGet (ACMP_TypeDef * acmp)
Get pending ACMP interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
Note
This function does not clear event bits.
Returns
Pending ACMP interrupt sources. A bitwise logic OR combination of valid interrupt flags for the ACMP module. The pending interrupt sources can be, for instance, ACMP_IF_EDGE or ACMP_IF_WARMUP.
ACMP_IntGetEnabled#
uint32_t ACMP_IntGetEnabled (ACMP_TypeDef * acmp)
Get enabled and pending ACMP interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
Useful for handling more interrupt sources in the same interrupt handler.
Note
This function does not clear interrupt flags.
Returns
Pending and enabled ACMP interrupt sources. The return value is the bitwise AND combination of
the OR combination of enabled interrupt sources in ACMPx_IEN_nnn register (ACMPx_IEN_nnn) and
the OR combination of valid interrupt flags of the ACMP module (ACMPx_IF_nnn).
ACMP_IntSet#
void ACMP_IntSet (ACMP_TypeDef * acmp, uint32_t flags)
Set one or more pending ACMP interrupts from software.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
| uint32_t | [in] | flags | ACMP interrupt sources to set as pending. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IFS_EDGE or ACMP_IFS_WARMUP. |
ACMP_PortPinToInput#
ACMP_Channel_TypeDef ACMP_PortPinToInput (GPIO_Port_TypeDef port, uint8_t pin)
Convert GPIO port/pin to ACMP input selection.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| GPIO_Port_TypeDef | [in] | port | GPIO port |
| uint8_t | [in] | pin | GPIO pin |
Returns
ACMP input selection
ACMP_OutputGet#
bool ACMP_OutputGet (ACMP_TypeDef * acmp)
Get state of ACMP output value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ACMP_TypeDef * | [in] | acmp | A pointer to the ACMP peripheral register block. |
Returns
State of ACMP output value
Macro Definition Documentation#
PM5507_ACMP_CFG_BIAS_DEFAULT#
#define PM5507_ACMP_CFG_BIAS_DEFAULTValue:
0x00000004UL
A default configuration for capacitive sense mode initialization.
Analog comparator CFG with initial bias value
PM5507_ACMP_CFG_RESETVALUE#
#define PM5507_ACMP_CFG_RESETVALUEValue:
0x00000004UL
Analog comparator reset value.
ACMP_CAPSENSE_INIT_DEFAULT#
#define ACMP_CAPSENSE_INIT_DEFAULTValue:
Capacitive sense mode configuration default values.
ACMP_INIT_DEFAULT#
#define ACMP_INIT_DEFAULTValue:
Default configuration for ACMP regular initialization.