Private CPC system endpoint primary. For internal use by other parts of CPC but not to be used by external users.

License#

Copyright 2023 Silicon Laboratories Inc. www.silabs.com

SPDX-License-Identifier: Zlib

The licensor of this software is Silicon Laboratories Inc.

This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.

Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:

  1. The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.

  2. Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.

  3. This notice may not be removed or altered from any source distribution.

/***************************************************************************/ 
#ifndef SLI_CPC_SYSTEM_PRIMARY_H
#define SLI_CPC_SYSTEM_PRIMARY_H

#include "sl_common.h"
#include "sl_enum.h"
#include "sli_cpc_system_common.h"
#include "sli_cpc_timer.h"

#ifdef __cplusplus
extern "C"
{
#endif

#define SLI_CPC_SYSTEM_COMMAND_FLAG_IS_FIRST_TRY        (0x01 << 0)
#define SLI_CPC_SYSTEM_COMMAND_FLAG_BEING_TRANSMITTED   (0x01 << 1)
#define SLI_CPC_SYSTEM_COMMAND_FLAG_RECEIVED_REPLY      (0x01 << 2)

typedef struct {
  bool is_first_try : 1;
  bool being_transmitted : 1;
  bool received_reply : 1;
} sli_cpc_system_command_flag_t;

typedef struct  {
  sl_slist_node_t node_commands;
  sl_slist_node_t node_retries;
  sli_cpc_system_cmd_t command;
  void *on_final;
  void *on_final_arg;
  uint8_t retry_count;
  sli_cpc_system_ep_frame_type_t frame_type;
  uint32_t retry_timeout_tick;
  sl_status_t error_status;
  sli_cpc_timer_handle_t timer;
  sli_cpc_system_command_flag_t flags;
} sli_cpc_system_command_handle_t;

typedef struct sli_cpc_system_endpoint {
  // IAR is not happy when the struct is empty, so for now just add a dummy
  // element in the struct in order to compile. Later on, that will be replaced
  // by actual primary's variables.
  sl_cpc_endpoint_handle_t dummy;
} sli_cpc_system_endpoint_t;

/***************************************************************************/
typedef void (*sli_cpc_system_noop_cmd_callback_t)(sl_status_t status);

/***************************************************************************/
typedef void (*sli_cpc_system_reset_cmd_callback_t)(sl_status_t command_status,
                                                    sl_cpc_system_status_t reset_status);

/***************************************************************************/
typedef void (*sli_cpc_system_property_get_set_cmd_callback_t)(sli_cpc_property_id_t property_id,
                                                               void *property_value,
                                                               size_t property_length,
                                                               void *reply_arg,
                                                               sl_status_t status);

/***************************************************************************/
sl_status_t sli_cpc_system_cmd_noop(sli_cpc_system_noop_cmd_callback_t on_noop_reply,
                                    void *on_noop_reply_arg,
                                    uint8_t retry_count_max,
                                    uint32_t retry_timeout_ms);

/***************************************************************************/
sl_status_t sli_cpc_system_cmd_property_get(sli_cpc_system_property_get_set_cmd_callback_t on_property_get_reply,
                                            void *on_property_get_reply_arg,
                                            sli_cpc_property_id_t property_id,
                                            uint8_t retry_count_max,
                                            uint32_t retry_timeout_ms,
                                            sli_cpc_system_ep_frame_type_t frame_type);

/***************************************************************************/
sl_status_t sli_cpc_system_cmd_property_set(sli_cpc_system_property_get_set_cmd_callback_t on_property_set_reply,
                                            void *on_property_set_reply_arg,
                                            sli_cpc_property_id_t property_id,
                                            uint8_t retry_count_max,
                                            uint32_t retry_timeout_ms,
                                            const void *value,
                                            size_t value_length,
                                            sli_cpc_system_ep_frame_type_t frame_type);

/***************************************************************************/
sl_status_t sli_cpc_system_cmd_reboot(sli_cpc_system_reset_cmd_callback_t on_reset_reply,
                                      void *on_reset_reply_arg,
                                      uint8_t retry_count_max,
                                      uint32_t retry_timeout_ms);

/***************************************************************************/
void sli_cpc_system_notify_reset(sl_cpc_system_status_t reset_reason);

/***************************************************************************/
bool sli_cpc_system_is_ready(void);

#ifdef __cplusplus
}
#endif

#endif /* SLI_CPC_SYSTEM_PRIMARY_H */

Modules#

sli_cpc_system_command_flag_t

sli_cpc_system_command_handle_t

sli_cpc_system_endpoint

Typedefs#

typedef void(*

This callback is called when the PRIMARY receives the reply from the SECONDARY.

typedef void(*
sli_cpc_system_reset_cmd_callback_t)(sl_status_t command_status, sl_cpc_system_status_t reset_status)

This callback is called when the PRIMARY receives the reply from the SECONDARY.

typedef void(*
sli_cpc_system_property_get_set_cmd_callback_t)(sli_cpc_property_id_t property_id, void *property_value, size_t property_length, void *reply_arg, sl_status_t status)

Functions#

sl_status_t
sli_cpc_system_cmd_noop(sli_cpc_system_noop_cmd_callback_t on_noop_reply, void *on_noop_reply_arg, uint8_t retry_count_max, uint32_t retry_timeout_ms)

This command can be seen like a ping command. Like its name implies, this command does nothing except generating a bidirectional transaction to assert the link is functional.

sl_status_t
sli_cpc_system_cmd_property_get(sli_cpc_system_property_get_set_cmd_callback_t on_property_get_reply, void *on_property_get_reply_arg, sli_cpc_property_id_t property_id, uint8_t retry_count_max, uint32_t retry_timeout_ms, sli_cpc_system_ep_frame_type_t frame_type)

This command sends a property-get request to the SECONDARY.

sl_status_t
sli_cpc_system_cmd_property_set(sli_cpc_system_property_get_set_cmd_callback_t on_property_set_reply, void *on_property_set_reply_arg, sli_cpc_property_id_t property_id, uint8_t retry_count_max, uint32_t retry_timeout_ms, const void *value, size_t value_length, sli_cpc_system_ep_frame_type_t frame_type)

This command sends a property-set request to the SECONDARY.

sl_status_t
sli_cpc_system_cmd_reboot(sli_cpc_system_reset_cmd_callback_t on_reset_reply, void *on_reset_reply_arg, uint8_t retry_count_max, uint32_t retry_timeout_ms)

This command sends a reset request to the SECONDARY.

void
sli_cpc_system_notify_reset(sl_cpc_system_status_t reset_reason)

Macro Definition Documentation#

SLI_CPC_SYSTEM_COMMAND_FLAG_IS_FIRST_TRY#

#define SLI_CPC_SYSTEM_COMMAND_FLAG_IS_FIRST_TRY
Value:
(0x01 << 0)

SLI_CPC_SYSTEM_COMMAND_FLAG_BEING_TRANSMITTED#

#define SLI_CPC_SYSTEM_COMMAND_FLAG_BEING_TRANSMITTED
Value:
(0x01 << 1)

SLI_CPC_SYSTEM_COMMAND_FLAG_RECEIVED_REPLY#

#define SLI_CPC_SYSTEM_COMMAND_FLAG_RECEIVED_REPLY
Value:
(0x01 << 2)

Typedef Documentation#

sli_cpc_system_endpoint_t#

typedef struct sli_cpc_system_endpoint sli_cpc_system_endpoint_t

sli_cpc_system_noop_cmd_callback_t#

typedef void(* sli_cpc_system_noop_cmd_callback_t) (sl_status_t status) )(sl_status_t status)

This callback is called when the PRIMARY receives the reply from the SECONDARY.

Callback for the no-op command.


sli_cpc_system_reset_cmd_callback_t#

typedef void(* sli_cpc_system_reset_cmd_callback_t) (sl_status_t command_status, sl_cpc_system_status_t reset_status) )(sl_status_t command_status, sl_cpc_system_status_t reset_status)

This callback is called when the PRIMARY receives the reply from the SECONDARY.

Parameters
TypeDirectionArgument NameDescription
[in]status

The SECONDARY will return STATUS_OK if the reset will occur in the desired mode. STATUS_FAILURE will be returned otherwise.

Callback for the reset command.


sli_cpc_system_property_get_set_cmd_callback_t#

typedef void(* sli_cpc_system_property_get_set_cmd_callback_t) (sli_cpc_property_id_t property_id, void *property_value, size_t property_length, void *reply_arg, sl_status_t status) )(sli_cpc_property_id_t property_id, void *property_value, size_t property_length, void *reply_arg, sl_status_t status)
Parameters
TypeDirectionArgument NameDescription
[in]property_id

The ID of the property from the previously issued property-get/set.

Callback for the property-get or set command.

[in] property_value A pointer to the value returned by the SECONDARY. Has to be casted to an appropriate value in function of the property ID.

[in] property_length The length of the property value in bytes.

[in] reply_arg Value passed as on_property_set_reply_arg or on_property_get_reply_arg in sli_cpc_system_cmd_property_set or sli_cpc_system_cmd_property_get respectively.


Function Documentation#

sli_cpc_system_cmd_noop#

sl_status_t sli_cpc_system_cmd_noop (sli_cpc_system_noop_cmd_callback_t on_noop_reply, void * on_noop_reply_arg, uint8_t retry_count_max, uint32_t retry_timeout_ms)

This command can be seen like a ping command. Like its name implies, this command does nothing except generating a bidirectional transaction to assert the link is functional.

Parameters
TypeDirectionArgument NameDescription
sli_cpc_system_noop_cmd_callback_t[in]on_noop_reply

The callback upon receiving the reply of the command.

void *N/Aon_noop_reply_arg
uint8_tN/Aretry_count_max
uint32_tN/Aretry_timeout_ms

Send no-operation command query.

Send no-operation command query


sli_cpc_system_cmd_property_get#

sl_status_t sli_cpc_system_cmd_property_get (sli_cpc_system_property_get_set_cmd_callback_t on_property_get_reply, void * on_property_get_reply_arg, sli_cpc_property_id_t property_id, uint8_t retry_count_max, uint32_t retry_timeout_ms, sli_cpc_system_ep_frame_type_t frame_type)

This command sends a property-get request to the SECONDARY.

Parameters
TypeDirectionArgument NameDescription
sli_cpc_system_property_get_set_cmd_callback_t[in]on_property_get_reply

The callback upon receiving the reply of the command.

void *N/Aon_property_get_reply_arg
sli_cpc_property_id_tN/Aproperty_id
uint8_tN/Aretry_count_max
uint32_tN/Aretry_timeout_ms
sli_cpc_system_ep_frame_type_tN/Aframe_type

Send a property-get query.

Note

  • Only one property-get/set can be issued a a time. Otherwise SL_STATUS_BUSY is returned.

  • retry_count_max must be 0 for I-Frame.

[in] property_id The ID of the property to get.

Send a property-get query


sli_cpc_system_cmd_property_set#

sl_status_t sli_cpc_system_cmd_property_set (sli_cpc_system_property_get_set_cmd_callback_t on_property_set_reply, void * on_property_set_reply_arg, sli_cpc_property_id_t property_id, uint8_t retry_count_max, uint32_t retry_timeout_ms, const void * value, size_t value_length, sli_cpc_system_ep_frame_type_t frame_type)

This command sends a property-set request to the SECONDARY.

Parameters
TypeDirectionArgument NameDescription
sli_cpc_system_property_get_set_cmd_callback_t[in]on_property_set_reply

The callback upon receiving the reply of the command.

void *N/Aon_property_set_reply_arg
sli_cpc_property_id_tN/Aproperty_id
uint8_tN/Aretry_count_max
uint32_tN/Aretry_timeout_ms
const void *N/Avalue
size_tN/Avalue_length
sli_cpc_system_ep_frame_type_tN/Aframe_type

Send a property-set request to the SECONDARY.

Note

  • Only one property-get/set can be issued a a time. Otherwise SL_STATUS_BUSY is returned.

  • retry_count_max must be 0 for I-Frame.

[in] property_id The ID of the property to get.

[in] value The value of the property to set.

[in] value_length The length of the value.

Send a property-set query


sli_cpc_system_cmd_reboot#

sl_status_t sli_cpc_system_cmd_reboot (sli_cpc_system_reset_cmd_callback_t on_reset_reply, void * on_reset_reply_arg, uint8_t retry_count_max, uint32_t retry_timeout_ms)

This command sends a reset request to the SECONDARY.

Parameters
TypeDirectionArgument NameDescription
sli_cpc_system_reset_cmd_callback_t[in]on_reset_reply

The callback upon receiving the reply of the command.

void *N/Aon_reset_reply_arg
uint8_tN/Aretry_count_max
uint32_tN/Aretry_timeout_ms

Send a reset query.

Note

  • Prior to a reboot, the PROP_BOOTLOADER_REBOOT_MODE must be set to the desired reboot mode.

Send a reset query


sli_cpc_system_notify_reset#

void sli_cpc_system_notify_reset (sl_cpc_system_status_t reset_reason)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_system_status_t[in]reset_reason

reset reason sent by the secondary

Notify primary's system endpoint that a reset occurred on the secondary

Notify users that a reset has happened by going through the list of event listeners.


sli_cpc_system_is_ready#

bool sli_cpc_system_is_ready (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Check if the system endpoint is ready for normal operations (ie. it's connected to the secondary and the reboot sequence is finished).

Returns

  • true if ready, false otherwise

Check if the system endpoint is connected and reboot sequence is done.