SMU - Security Management Unit#

Security Management Unit (SMU) Peripheral API.

SMU forms the control and status/reporting component of bus-level security in EFM32/EFR32 devices.

Peripheral-level protection is provided via the Peripheral Protection Unit (PPU). PPU provides hardware access barrier to any peripheral that is configured to be protected. When an attempt is made to access a peripheral without the required privilege/security level, PPU detects the fault and intercepts the access. No write or read of the peripheral register space occurs, and an all-zero value is returned if the access is a read.

Modules#

sl_hal_smu_privileged_t

sl_hal_smu_init_t

Enumerations#

enum
SL_HAL_SMU_EMU = _SMU_PPUPATD0_EMU_SHIFT
SL_HAL_SMU_CMU = _SMU_PPUPATD0_CMU_SHIFT
SL_HAL_SMU_HFXO = 32 + _SMU_PPUPATD1_HFXO0_SHIFT
SL_HAL_SMU_HFRCO0 = _SMU_PPUPATD0_HFRCO0_SHIFT
SL_HAL_SMU_FSRCO = _SMU_PPUPATD0_FSRCO_SHIFT
SL_HAL_SMU_DPLL0 = _SMU_PPUPATD0_DPLL0_SHIFT
SL_HAL_SMU_LFXO = _SMU_PPUPATD0_LFXO_SHIFT
SL_HAL_SMU_LFRCO = _SMU_PPUPATD0_LFRCO_SHIFT
SL_HAL_SMU_ULFRCO = _SMU_PPUPATD0_ULFRCO_SHIFT
SL_HAL_SMU_MSC = _SMU_PPUPATD0_MSC_SHIFT
SL_HAL_SMU_ICACHE0 = _SMU_PPUPATD0_ICACHE0_SHIFT
SL_HAL_SMU_PRS = _SMU_PPUPATD0_PRS_SHIFT
SL_HAL_SMU_GPIO = _SMU_PPUPATD0_GPIO_SHIFT
SL_HAL_SMU_LDMA = _SMU_PPUPATD0_LDMA_SHIFT
SL_HAL_SMU_LDMAXBAR = _SMU_PPUPATD0_LDMAXBAR_SHIFT
SL_HAL_SMU_TIMER0 = _SMU_PPUPATD0_TIMER0_SHIFT
SL_HAL_SMU_TIMER1 = _SMU_PPUPATD0_TIMER1_SHIFT
SL_HAL_SMU_TIMER2 = _SMU_PPUPATD0_TIMER2_SHIFT
SL_HAL_SMU_TIMER3 = _SMU_PPUPATD0_TIMER3_SHIFT
SL_HAL_SMU_TIMER4 = _SMU_PPUPATD0_TIMER4_SHIFT
SL_HAL_SMU_USART0 = _SMU_PPUPATD0_USART0_SHIFT
SL_HAL_SMU_BURTC = _SMU_PPUPATD0_BURTC_SHIFT
SL_HAL_SMU_I2C1 = _SMU_PPUPATD0_I2C1_SHIFT
SL_HAL_SMU_CHIPTESTCTRL = _SMU_PPUPATD0_CHIPTESTCTRL_SHIFT
SL_HAL_SMU_SYSCFGCFGNS = _SMU_PPUPATD0_SYSCFGCFGNS_SHIFT
SL_HAL_SMU_SYSCFG = _SMU_PPUPATD0_SYSCFG_SHIFT
SL_HAL_SMU_BURAM = _SMU_PPUPATD0_BURAM_SHIFT
SL_HAL_SMU_GPCRC = _SMU_PPUPATD0_GPCRC_SHIFT
SL_HAL_SMU_DCDC = _SMU_PPUPATD0_DCDC_SHIFT
SL_HAL_SMU_HOSTMAILBOX = _SMU_PPUPATD0_HOSTMAILBOX_SHIFT
SL_HAL_SMU_EUSART0 = 32 + _SMU_PPUPATD1_EUSART0_SHIFT
SL_HAL_SMU_EUSART1 = _SMU_PPUPATD0_EUSART1_SHIFT
SL_HAL_SMU_EUSART2 = _SMU_PPUPATD0_EUSART2_SHIFT
SL_HAL_SMU_SYSRTC = 32 + _SMU_PPUPATD1_SYSRTC_SHIFT
SL_HAL_SMU_LCD = 32 + _SMU_PPUPATD1_LCD_SHIFT
SL_HAL_SMU_KEYSCAN = 32 + _SMU_PPUPATD1_KEYSCAN_SHIFT
SL_HAL_SMU_DMEM = 32 + _SMU_PPUPATD1_DMEM_SHIFT
SL_HAL_SMU_LCDRF = 32 + _SMU_PPUPATD1_LCDRF_SHIFT
SL_HAL_SMU_PFMXPPRF = 32 + _SMU_PPUPATD1_PFMXPPRF_SHIFT
SL_HAL_SMU_VDAC0 = 32 + _SMU_PPUPATD1_VDAC0_SHIFT
SL_HAL_SMU_PCNT = 32 + _SMU_PPUPATD1_PCNT_SHIFT
SL_HAL_SMU_LESENSE = 32 + _SMU_PPUPATD1_LESENSE_SHIFT
SL_HAL_SMU_HFRCO1 = 32 + _SMU_PPUPATD1_HFRCO1_SHIFT
SL_HAL_SMU_HFXO0 = 32 + _SMU_PPUPATD1_HFXO0_SHIFT
SL_HAL_SMU_LETIMER0 = 32 + _SMU_PPUPATD1_LETIMER0_SHIFT
SL_HAL_SMU_IADC0 = 32 + _SMU_PPUPATD1_IADC0_SHIFT
SL_HAL_SMU_ACMP0 = 32 + _SMU_PPUPATD1_ACMP0_SHIFT
SL_HAL_SMU_ACMP1 = 32 + _SMU_PPUPATD1_ACMP1_SHIFT
SL_HAL_SMU_I2C0 = 32 + _SMU_PPUPATD1_I2C0_SHIFT
SL_HAL_SMU_WDOG0 = 32 + _SMU_PPUPATD1_WDOG0_SHIFT
SL_HAL_SMU_WDOG1 = 32 + _SMU_PPUPATD1_WDOG1_SHIFT
SL_HAL_SMU_AMUXCP0 = 32 + _SMU_PPUPATD1_AMUXCP0_SHIFT
SL_HAL_SMU_RADIOAES = 32 + _SMU_PPUPATD1_RADIOAES_SHIFT
SL_HAL_SMU_SMU = 32 + _SMU_PPUPATD1_SMU_SHIFT
SL_HAL_SMU_SMUCFGNS = 32 + _SMU_PPUPATD1_SMUCFGNS_SHIFT
SL_HAL_SMU_AHBRADIO = 32 + _SMU_PPUPATD1_AHBRADIO_SHIFT
SL_HAL_SMU_SEMAILBOX = 32 + _SMU_PPUPATD1_SEMAILBOX_SHIFT
SL_HAL_SMU_END
}

SMU peripheral identifiers.

Functions#

void

Enable or disable PPU of SMU.

void
sl_hal_smu_init(const sl_hal_smu_init_t *init)

Initialize PPU of SMU.

void
sl_hal_smu_set_privileged_access(sl_hal_smu_peripheral_id_t peripheral, bool privileged)

Change access settings for a peripheral.

Get the ID of the peripheral that caused an access fault.

void
sl_hal_smu_int_clear(uint32_t flags)

Clear one or more pending SMU interrupts.

void
sl_hal_smu_int_disable(uint32_t flags)

Disable one or more SMU interrupts.

void
sl_hal_smu_int_enable(uint32_t flags)

Enable one or more SMU interrupts.

uint32_t

Get pending SMU interrupts.

uint32_t

Get enabled and pending SMU interrupt flags.

void
sl_hal_smu_int_set(uint32_t flags)

Set one or more pending SMU interrupts from SW.

void

SMU secure IRQ Handler.

Macros#

#define

Default SMU initialization structure settings.

Enumeration Documentation#

sl_hal_smu_peripheral_id_t#

sl_hal_smu_peripheral_id_t

SMU peripheral identifiers.

Enumerator
SL_HAL_SMU_EMU

SMU peripheral identifier for EMU

SL_HAL_SMU_CMU

SMU peripheral identifier for CMU

SL_HAL_SMU_HFXO

SMU peripheral identifier for HFXO0

SL_HAL_SMU_HFRCO0

SMU peripheral identifier for HFRCO0

SL_HAL_SMU_FSRCO

SMU peripheral identifier for FSRCO

SL_HAL_SMU_DPLL0

SMU peripheral identifier for DPLL0

SL_HAL_SMU_LFXO

SMU peripheral identifier for LFXO

SL_HAL_SMU_LFRCO

SMU peripheral identifier for LFRCO

SL_HAL_SMU_ULFRCO

SMU peripheral identifier for ULFRCO

SL_HAL_SMU_MSC

SMU peripheral identifier for MSC

SL_HAL_SMU_ICACHE0

SMU peripheral identifier for ICACHE0

SL_HAL_SMU_PRS

SMU peripheral identifier for PRS

SL_HAL_SMU_GPIO

SMU peripheral identifier for GPIO

SL_HAL_SMU_LDMA

SMU peripheral identifier for LDMA

SL_HAL_SMU_LDMAXBAR

SMU peripheral identifier for LDMAXBAR

SL_HAL_SMU_TIMER0

SMU peripheral identifier for TIMER0

SL_HAL_SMU_TIMER1

SMU peripheral identifier for TIMER1

SL_HAL_SMU_TIMER2

SMU peripheral identifier for TIMER2

SL_HAL_SMU_TIMER3

SMU peripheral identifier for TIMER3

SL_HAL_SMU_TIMER4

SMU peripheral identifier for TIMER4

SL_HAL_SMU_USART0

SMU peripheral identifier for USART0

SL_HAL_SMU_BURTC

SMU peripheral identifier for BURTC

SL_HAL_SMU_I2C1

SMU peripheral identifier for I2C1

SL_HAL_SMU_CHIPTESTCTRL

SMU peripheral identifier for CHIPTESTCTRL.

SL_HAL_SMU_SYSCFGCFGNS

SMU peripheral identifier for SYSCFGCFGNS.

SL_HAL_SMU_SYSCFG

SMU peripheral identifier for SYSCFG

SL_HAL_SMU_BURAM

SMU peripheral identifier for BURAM

SL_HAL_SMU_GPCRC

SMU peripheral identifier for GPCRC

SL_HAL_SMU_DCDC

SMU peripheral identifier for DCDC

SL_HAL_SMU_HOSTMAILBOX

SMU peripheral identifier for HOSTMAILBOX.

SL_HAL_SMU_EUSART0

SMU peripheral identifier for EUSART0

SL_HAL_SMU_EUSART1

SMU peripheral identifier for EUSART1

SL_HAL_SMU_EUSART2

SMU peripheral identifier for EUSART2

SL_HAL_SMU_SYSRTC

SMU peripheral identifier for SYSRTC

SL_HAL_SMU_LCD

SMU peripheral identifier for LCD

SL_HAL_SMU_KEYSCAN

SMU peripheral identifier for KEYSCAN

SL_HAL_SMU_DMEM

SMU peripheral identifier for DMEM

SL_HAL_SMU_LCDRF

SMU peripheral identifier for LCDRF

SL_HAL_SMU_PFMXPPRF

SMU peripheral identifier for PFMXPPRF

SL_HAL_SMU_VDAC0

SMU peripheral identifier for VDAC0

SL_HAL_SMU_PCNT

SMU peripheral identifier for PCNT

SL_HAL_SMU_LESENSE

SMU peripheral identifier for LESENSE

SL_HAL_SMU_HFRCO1

SMU peripheral identifier for HFRCO1

SL_HAL_SMU_HFXO0

SMU peripheral identifier for HFXO0

SL_HAL_SMU_LETIMER0

SMU peripheral identifier for LETIMER

SL_HAL_SMU_IADC0

SMU peripheral identifier for IADC0

SL_HAL_SMU_ACMP0

SMU peripheral identifier for ACMP0

SL_HAL_SMU_ACMP1

SMU peripheral identifier for ACMP1

SL_HAL_SMU_I2C0

SMU peripheral identifier for I2C0

SL_HAL_SMU_WDOG0

SMU peripheral identifier for WDOG0

SL_HAL_SMU_WDOG1

SMU peripheral identifier for WDOG1

SL_HAL_SMU_AMUXCP0

SMU peripheral identifier for AMUXCP0

SL_HAL_SMU_RADIOAES

SMU peripheral identifier for RADIOAES

SL_HAL_SMU_SMU

SMU peripheral identifier for SMU

SL_HAL_SMU_SMUCFGNS

SMU peripheral identifier for SMUCFGNS

SL_HAL_SMU_AHBRADIO

SMU peripheral identifier for AHBRADIO

SL_HAL_SMU_SEMAILBOX

SMU peripheral identifier for SEMAILBOX.

SL_HAL_SMU_END

SMU peripheral end.


Function Documentation#

sl_hal_smu_enable_ppu#

void sl_hal_smu_enable_ppu (bool enable)

Enable or disable PPU of SMU.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable

Set to true to enable PPU; set to false otherwise.


sl_hal_smu_init#

void sl_hal_smu_init (const sl_hal_smu_init_t * init)

Initialize PPU of SMU.

Parameters
TypeDirectionArgument NameDescription
const sl_hal_smu_init_t *[in]init

Pointer to initialization structure that defines which peripherals should only be accessed from privileged mode, and if PPU should be enabled.


sl_hal_smu_set_privileged_access#

void sl_hal_smu_set_privileged_access (sl_hal_smu_peripheral_id_t peripheral, bool privileged)

Change access settings for a peripheral.

Parameters
TypeDirectionArgument NameDescription
sl_hal_smu_peripheral_id_t[in]peripheral

ID of the peripheral to change access settings for.

bool[in]privileged

Set to true if the peripheral should only be accessed from privileged mode; set to false otherwise.

Set to limit access of a peripheral from privileged mode.


sl_hal_smu_get_faulting_peripheral#

sl_hal_smu_peripheral_id_t sl_hal_smu_get_faulting_peripheral (void )

Get the ID of the peripheral that caused an access fault.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • The return value is only valid if SMU_IF_PPUPRIV interrupt flag is set.

Returns

  • ID of the peripheral that caused an access fault.


sl_hal_smu_int_clear#

void sl_hal_smu_int_clear (uint32_t flags)

Clear one or more pending SMU interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

Bitwise logic OR of SMU interrupt sources to clear.


sl_hal_smu_int_disable#

void sl_hal_smu_int_disable (uint32_t flags)

Disable one or more SMU interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

SMU interrupt sources to disable.


sl_hal_smu_int_enable#

void sl_hal_smu_int_enable (uint32_t flags)

Enable one or more SMU interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

SMU interrupt sources to enable.

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using SMU_IntClear() prior to enabling the interrupt.


sl_hal_smu_int_get#

uint32_t sl_hal_smu_int_get (void )

Get pending SMU interrupts.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • SMU interrupt sources pending.


sl_hal_smu_int_get_enabled#

uint32_t sl_hal_smu_int_get_enabled (void )

Get enabled and pending SMU interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Interrupt flags are not cleared by this function.

Returns

  • Pending and enabled SMU interrupt sources. The return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in SMU_IEN register and

    • the OR combination of valid interrupt flags in SMU_IF register.


sl_hal_smu_int_set#

void sl_hal_smu_int_set (uint32_t flags)

Set one or more pending SMU interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

SMU interrupt sources to set to pending.


SMU_SECURE_IRQHandler#

void SMU_SECURE_IRQHandler (void )

SMU secure IRQ Handler.

Parameters
TypeDirectionArgument NameDescription
voidN/A

When a PPU detects an access to a secure peripheral at its non-secure address or an access to a non-secure peripheral at its secure address, PPUSECIF in SMU_IF is set and the ID of the peripheral being accessed is written to SMU_PPUFS. If PPUSECIEN is set and the SMU's Secure IRQ enabled, the CPU will be interrupted and SMU_SECURE_IRQHandler Will handle the interrupt.


Macro Definition Documentation#

SMU_INIT_DEFAULT#

#define SMU_INIT_DEFAULT
Value:
{ \
{ { 0 } }, /* No peripherals access protected. */ \
true /* Enable SMU.*/ \
}

Default SMU initialization structure settings.