Simplicity SDK Platform - Platform MCU Version 6.0.2 - Release Notes (May 4, 2026)#

Simplicity SDK Platform Version 6.0.2

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 6.0.1#

  • sl_main: New application hook app_init_post_platform called after platform/driver/service init and before stack init.

  • Linker: TrustZone workspaces can use remaining flash and RAM without specifying memory_flash_size or memory_ram_size.

Added in 6.0.0#

  • Auto PCLK divider selection now defaults to datasheet-compliant values.

  • Power Manager adds EM0/EM1 voltage scaling and power optimizations.

  • Clock Manager validation and oscillator configuration options expanded.

API Changes#

Changed in 6.0.1#

sl_main: New application hook app_init_post_platform for initialization after platform, driver, and service init but before stack init.

Changed in 6.0.0#

  • Peripheral HAL init macros renamed to _INIT_DEFAULT with standardized init signatures.

  • UARTDRV adds UARTDRV_GetTransmitDepthExt and UARTDRV_GetReceiveDepthExt returning uint16_t depths.

  • Memory Manager and EMU DCDC APIs remove implicit enable/lock handling and tighten validation; DCDC Coulomb Counter calibration APIs deprecated in favor of HLD.

Bug Fixes#

Fixed in 6.0.1#

  • Clock Manager: Wrapped SE Manager calls during initialization in atomic sections.

  • Memory Manager: Fixed heap statistics underflow and memory pool corruption when the same block was freed twice.

  • Power Manager: Restored clock correctly when an EM1 requirement is added during sleep on SiXG301 devices.

  • RGB LED PWM driver: Fixed build issue for Series 3 devices.

  • NVM: Updated all NVM operations to use non-cacheable data-alias to avoid L1ICACHE returning outdated cached data.

Fixed in 6.0.0#

  • Clock Manager, IADC, EMU, LDMA, TIMER, and EUSART/UART fixes across Series 2 devices.

  • Linker and toolchain updates to enforce memory limits and avoid build warnings.

Chip Enablement#

Added in 6.0.1#

None.

Added in 6.0.0#

Added EFR32FG23L010F128GM40, EFR32FG23L020F128GM40 EFR32FG2DB010F512IM48, BGM270SC22SNA and MGM270SC22SNA support.

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

New Features#

Added in 6.0.1#

sl_main: Added application hook app_init_post_platform, called from sl_main_second_stage_init after sl_platform_init, sl_driver_init, and sl_service_init have completed and before sl_stack_init is called, allowing initialization that depends on platform components, drivers, and services but must run before stacks.

Added in 6.0.0#

  • Clock Manager: Added SL_CLOCK_MANAGER_PCLK_DIV_MIN option to automatically select the lowest compliant PCLK divider (default).

  • Power Manager: Added SL_POWER_MANAGER_ENABLE_EM01_VOLTAGE_SCALING to apply the lowest VSCALE in EM0/EM1 based on SYSCLK.

  • Power Manager: HCLK and PCLK division is now maximized after early EM2 wakeups to reduce EM1 power.

Enhancements#

Added in 6.0.1#

Linker: memory_flash_start can now be used without specifying memory_flash_size; if memory_flash_size is not specified, the application uses the remaining flash. Similarly, memory_ram_start can be used without memory_ram_size.

Added in 6.0.0#

  • Clock Manager: Added SLC validation to ensure SYSCLK, HCLK, and PCLK respect datasheet limits.

  • Clock Manager: Added SL_CLOCK_MANAGER_LFXO_GAIN configuration for LFXO gain selection.

  • Clock Manager: Added separate XI/XO CTUNE settings (SL_CLOCK_MANAGER_HFXO_CTUNEXIANA and SL_CLOCK_MANAGER_HFXO_CTUNEXOANA) with enable control.

  • Clock Manager: Added SL_CLOCK_MANAGER_HFXO_ENXIDCBIASANA to enable DC bias for AC-coupled external oscillators.

  • Linker: Relocated vma_ramfuncs to text_ram_vma to clarify stack sizing.

  • NVM3: Optimized repack size requirements for 4 KB and 8 KB page configurations, improving flash utilization and reducing repack frequency.

  • NVM3: Updated forced-repack logic to use a hard threshold instead of a soft threshold. The user repack threshold is now defined as forced threshold plus maximum object size, whereas previously it was identical to the forced threshold.

Removed Features#

None.

Deprecated Features#

None.

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

Added in 6.0.1#

New API Signature

Deprecated API replaced by this (if any)

void app_init_post_platform(void)

None

Added in 6.0.0#

New API Signature

Deprecated API replaced by this (if any)

Ecode_t UARTDRV_GetTransmitDepthExt(UARTDRV_Handle_t handle, uint16_t *depth)

None

Ecode_t UARTDRV_GetReceiveDepthExt(UARTDRV_Handle_t handle, uint16_t *depth)

None

Modified APIs#

Modified in 6.0.1#

None.

Modified in 6.0.0#

Old API

Modified

Peripheral HAL init macros SL_HAL_<peripheral>_CONFIG_DEFAULT and init prototypes void sl_hal_<peripheral>_init(const sl_hal_<peripheral>_config_t *config)

Renamed to SL_HAL_<peripheral>_INIT_DEFAULT with standardized prototypes void sl_hal_<peripheral>_init(const sl_hal_<peripheral>_init_t *init) across low-level drivers (for example, SL_HAL_TIMER_INIT_DEFAULT).

sl_memory_init returned SL_STATUS_OK on repeated calls

Now returns SL_STATUS_ALREADY_INITIALIZED when invoked after initialization.

Removed APIs#

None.

Deprecated APIs#

Deprecated in 6.0.1#

None.

Deprecated in 6.0.0#

Deprecated API Name

Planned Removal Date

sl_hal_dcdc_coulomb_counter_cal_init

12/09/2026

sl_hal_dcdc_coulomb_counter_cal_start

12/09/2026

sl_hal_dcdc_coulomb_counter_cal_stop

12/09/2026

sl_hal_dcdc_coulomb_counter_get_cal_reference_freq

12/09/2026

Bug Fixes#

Fixed in 6.0.1#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
Services
1589194 Clock Manager: Added atomic sections around some SE Manager function calls during Clock Manager initialization to avoid using RTOS constructs before the kernel is started. 00338665 SiXG301 devices
1574895 Memory Manager: Fixed an issue in the statistics APIs where the reported used heap value could underflow. None All
1574016 Memory Manager: Fixed an issue where freeing the same memory pool allocation twice would corrupt the memory pool, making it impossible to delete the memory pool. None All
1525962 Power Manager: Add missing clock restoration when an EM1 requirement is added during sleep with SYSCLK switch from SOCPLL to HFXO. 00333452 SiXG301 Devices
1589197 NVM: Updated all NVM operations to use non-cacheable data-alias to avoid L1ICACHE returning outdated cached data. None SiXG301 devices
Peripherals
1577673 hal_ldma: Fixed misclassification of multiple sl_hal_ldma functions that are called from interrupt context in DMADRV; they are now correctly placed in RAM on Series 3 devices. None SiXG301 Devices
1563576 hal_ldma: Fixed an issue where the CHDONE flag for a given channel was not being cleared before starting a new transfer with the sl_hal_ldma_start_transfer API. None All
1611330 RGB LED PWM driver: Fixed the build issue for Series 3 devices. None SiXG301 devices

Fixed in 6.0.0#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
Services
1533447, 1512518, 1479008, 1455259 clock_manager/device_init: Aligned HFRCO and DPLL defaults for xG22 devices by setting HFRCO to 38 MHz on limited parts, fixing DPLL max frequency to 38 MHz, and updating Device Init for BG22/FG22/L22 OPNs with reduced calibrated bands. Setting HRFRCO to 80MHz fails
  • BGM220SC12WGA
  • EFR32FG22
  • EFR32BG22C112F352GM32/GM40
  • EFR32BG22L122F352GM32
1505125 clock_manager: Set SL_CLOCK_MANAGER_DEFAULT_HF_CLOCK_SOURCE_AUTO to HFRCODPLL for xG21 devices to match wireless stack expectations. None EFR32xG21
1529640 sl_main: Removed duplicate weak definitions when upgrading sl_system projects to sl_main to avoid conflicts in app_init and app_process_action. None Projects using sl_system_compatibility.
1528625 Token Manager: Fixed virtual EUI token (TOKEN_MFG_EUI_64) read logic. When a read request is made for the virtual EUI token (TOKEN_MFG_EUI_64), the system first checks the override token TOKEN_MFG_CUSTOM_EUI_64 (if the override feature is enabled). If an override value exists, it returns the overridden TOKEN_MFG_CUSTOM_EUI_64 data. If no override exists, it returns the static TOKEN_MFG_CUSTOM_EUI_64 data. If that is also unavailable, it falls back to the TOKEN_MFG_EMBER_EUI_64 token (Silicon Labs device info register) and returns the DevInfo value. Note: The virtual EUI token (TOKEN_MFG_EUI_64) itself cannot be overridden because it is not an actual physical token. None All
1449079 NVM3: Fixed an issue where, on bootup, the NVM3 handler would advance the next object address to the following page if the last stored object was fragmented. The handler now properly accounts for fragmented objects, ensuring optimal page utilization. None Series 2 and 3 Devices
1488094 Clock Manager: Fixed incorrect labeling of the RTCCCLK clock source in Clock Manager configuration files. The RTCCCLK source (SL_CLOCK_MANAGER_RTCCCLK_SOURCE) was mislabeled as EM23GRPACLK. This resulted in the Clock Manager UI displaying duplicate EM23GRPACLK branches and prevented users from correctly identifying the RTCC clock source. The configuration files across the SDK have been updated to remove the duplication and restore accurate UI behavior for RTCCCLK source selection. None All
1528263 NVM3: Fixed static analysis warnings in NVM3. Removed unnecessary loop condition during NVM3 data copy on write failure for Series-3. Fixed an issue where, if the first page was invalid, fifofirstObj was not updated to the next valid page, causing getFreeSize() to enter an infinite loop in case of a write failure. None Series 3 Devices
Common
1529446 linker: Added an assert when code size exceeds the SIXX301 code region to fail builds early. None SiMG301
1412916 linker: Removed zero-sized .noinit sections to prevent arm-none-eabi-objcopy warnings when the section is empty. 00325319 GCC projects with unused .noinit
Peripherals
1531716 hal_ldma: Fixed pending interrupt flag and enable handling for sl_hal_ldma_get_enabled_pending_interrupts and sl_hal_ldma_transfer_is_done on SiMG301. None SiMG301
1468177 hal_timer: Restored compare and top buffer values after re-enabling TIMER channels in sl_hal_timer_channel_init. None All
1505880 uartdrv: Corrected abort transfer callbacks to report transferred items instead of remaining items when DMA transfers are aborted. 00332923 Series 2 Devices
1453195 em_usart: Fixed clock divider calculation in USART_BaudrateSyncSet for synchronous mode. None All
1505263, 1505518 em_iadc: Corrected OFFSETANA1HIACC casting and reference voltage handling in high-precision mode, improving accuracy by up to 5 LSB. None Series 2 Devices
1450028 em_iadc: Added missing iadcPosInputVbat and iadcNegInputVbat inputs for EFR32xG27 devices. None EFR32xG27
1486153 em_emu: Added WFI after EM4 entry sequence to ensure devices enter EM4 reliably. None All
1474641 hal_eusart: Updated sl_hal_eusart_reset to avoid bus faults if the bus clock is disabled immediately after reset. None All
1436872 em_eusart: EUSART_SpiInit now honors the init.eusartDisable parameter to keep the peripheral disabled when requested. None All

Chip Enablement#

Added in 6.0.2#

Chip Family OPNs / Boards / OPN Combinations Supported Software Variants (if applicable) Supported Modes Supported Host Interfaces
EFR32FG2D
  • OPN: EFR32FG2DB010F512IM48
  • OPN: EFR32FG2DB020F512IM48
  • OPN: EFR32FG2DB010F512IM40
  • OPN: EFR32FG2DA010F256IM40
  • OPN: EFR32FG2DA020F256IM48
  • OPN: EFR32FG2DA010F256IM48
  • Board: BRD4277A
  • Board: BRD4278A
  • Board: BRD2611A
All All All
WPK Main Board
  • Board: BRD4002B
All All All

Added in 6.0.1#

None.

Added in 6.0.0#

Chip Family OPNs / Boards / OPN Combinations Supported Software Variants (if applicable) Supported Modes Supported Host Interfaces
EFR32FG23L
  • OPN: EFR32FG23L010F128GM40
  • OPN: EFR32FG23L020F128GM40
All All All
EFR32FG2D
  • OPN: EFR32FG2DB010F512IM48
  • Board: BRD4277A
All All All
BGM270S
  • OPN: BGM270SC22SNA4
All All All
MGM270S
  • OPN: MGM270SC22SNA4
  • Board: BRD2715A
  • Board: BRD4356A
All All All

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

Example Name Changes Supported Software Variants if applicable Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces

Platform - RHT UniDriver Bare-metal

See README.

This example demonstrates the RHT UniDriver API with the on-board Si70xx (for example, Wireless Pro Kit BRD4002A) or SHT4x (WPK BRD4002B). It prints discovery information, optional API status codes, and periodic relative humidity and temperature data over VCOM. NA SoC Series 2 Devices VCOM

Modified Examples#

Example Name Changes Supported Software Variants if applicable Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces

Platform - Segment LCD Tempsensor

See README.

This project demonstrates how to use the on-board RHT sensor (Si70xx or SHT4x via the RHT UniDriver) to measure and record temperature values and how to use the Segment LCD to display those values. NA SoC Series 2 and 3 Devices VCOM

Removed Examples#

None.

Deprecated Examples#

None.

Known Issues and Limitations#

None.