DMA channel transfer descriptor flags.
Public Attributes#
uint32_t
Indicates if the descriptor was internally allocated by the driver.
uint32_t
Indicates if a callback should be called on descriptor completion.
uint32_t
Public Attribute Documentation#
driver_allocated#
uint32_t sl_dma_channel_xfer_descriptor_flags_t::driver_allocated
Indicates if the descriptor was internally allocated by the driver.
callback_on_complete#
uint32_t sl_dma_channel_xfer_descriptor_flags_t::callback_on_complete
Indicates if a callback should be called on descriptor completion.