SYSRTC - System RTC#


Example#

This example demonstrates how to configure and use the System Real-Time Counter (SYSRTC) to generate periodic interrupts.

#include "sl_hal_sysrtc.h"
#include "sl_clock_manager.h"
#include "sl_interrupt_manager.h"

// SYSRTC group 0 compare 0 interrupt handler
void SYSRTC_APP_IRQHandler(void)
{
  uint32_t flags = sl_hal_sysrtc_get_group_interrupts(0);
  if (flags & SYSRTC_GRP0_IF_CMP0) {
    // Handle compare match 0 interrupt
    sl_hal_sysrtc_clear_group_interrupts(0, SYSRTC_GRP0_IF_CMP0);
    // Add your application code here (e.g., toggle an LED)
  }
}

void sysrtc_example(void)
{
  // Enable SYSRTC clock
  sl_clock_manager_enable_bus_clock(SL_BUS_CLOCK_SYSRTC0);

  // Initialize SYSRTC with default config
  sl_hal_sysrtc_init_t sysrtc_init = SL_HAL_SYSRTC_INIT_DEFAULT;
  sl_hal_sysrtc_init(&sysrtc_init);

  // Initialize group 0 and enable compare channel 0 with config
  sl_hal_sysrtc_group_init_t group_init = SL_HAL_SYSRTC_GROUP_INIT_DEFAULT;
  sl_hal_sysrtc_group_channel_compare_config_t compare0_config = SL_HAL_SYSRTC_GROUP_CHANNEL_COMPARE_INIT_DEFAULT;
  group_init.compare_channel0_enable = true;
  group_init.p_compare_channel0_config = &compare0_config;
  sl_hal_sysrtc_init_group(0, &group_init);

  // Set compare value for group 0, channel 0
  sl_hal_sysrtc_set_group_compare_channel_value(0, 0, 1000);

  // Enable group 0 compare 0 interrupt
  sl_hal_sysrtc_enable_group_interrupts(0, SYSRTC_GRP0_IF_CMP0);

  // Enable SYSRTC interrupt in NVIC
  sl_interrupt_manager_clear_irq_pending(SYSRTC_APP_IRQn);
  sl_interrupt_manager_enable_irq(SYSRTC_APP_IRQn);

  // Start SYSRTC
  sl_hal_sysrtc_enable();
  sl_hal_sysrtc_wait_sync();

  // Application main loop
  while (1) {
    // Read current counter value if needed
    uint32_t count = sl_hal_sysrtc_get_counter();
    // Sleep or perform other tasks
  }
}

Modules#

sl_hal_sysrtc_group_channel_compare_config_t

sl_hal_sysrtc_group_channel_capture_config_t

sl_hal_sysrtc_group_init_t

sl_hal_sysrtc_pretrigger_config_t

sl_hal_sysrtc_group_pretrigger_config_t

sl_hal_sysrtc_init_t

Enumerations#

enum
SL_HAL_SYSRTC_CAPTURE_EDGE_RISING = 0
SL_HAL_SYSRTC_CAPTURE_EDGE_FALLING
SL_HAL_SYSRTC_CAPTURE_EDGE_BOTH
}

Capture input edge select.

enum
SL_HAL_SYSRTC_COMPARE_MATCH_OUT_ACTION_CLEAR = 0
SL_HAL_SYSRTC_COMPARE_MATCH_OUT_ACTION_SET
SL_HAL_SYSRTC_COMPARE_MATCH_OUT_ACTION_PULSE
SL_HAL_SYSRTC_COMPARE_MATCH_OUT_ACTION_TOGGLE
SL_HAL_SYSRTC_COMPARE_MATCH_OUT_ACTION_CMPIF
}

Compare match output action mode.

Functions#

void

Waits for the SYSRTC to complete all synchronization of register changes and commands.

uint32_t

Gets SYSRTC STATUS register value.

uint32_t

Gets SYSRTC counter value.

void
sl_hal_sysrtc_wait_sync_group(uint8_t group_number)

Waits for the SYSRTC group to complete all synchronization of register changes and commands.

void
sl_hal_sysrtc_init_group(uint8_t group_number, sl_hal_sysrtc_group_init_t const *group_init)

Initializes the selected SYSRTC group.

void
sl_hal_sysrtc_group_enable_compare_channel(uint8_t group_number, uint8_t channel, bool enable)

Enables or disables a compare channel for the specified group at runtime.

void
sl_hal_sysrtc_group_set_compare_channel_action(uint8_t group_number, uint8_t channel, sl_hal_sysrtc_compare_match_out_action_t action)

Sets the compare match out action for a compare channel at runtime.

void
sl_hal_sysrtc_group_enable_capture_channel(uint8_t group_number, uint8_t channel, bool enable)

Enables or disables a capture channel for the specified group at runtime.

void
sl_hal_sysrtc_group_set_capture_channel_edge(uint8_t group_number, uint8_t channel, sl_hal_sysrtc_capture_edge_t edge)

Sets the capture input edge for a capture channel at runtime.

void
sl_hal_sysrtc_enable_group_interrupts(uint8_t group_number, uint32_t flags)

Enables one or more SYSRTC interrupts for the given group.

void
sl_hal_sysrtc_disable_group_interrupts(uint8_t group_number, uint32_t flags)

Disables one or more SYSRTC interrupts for the given group.

void
sl_hal_sysrtc_clear_group_interrupts(uint8_t group_number, uint32_t flags)

Clears one or more pending SYSRTC interrupts for the given group.

uint32_t

Gets pending SYSRTC interrupt flags for the given group.

uint32_t

Gets enabled and pending SYSRTC interrupt flags for the given group.

void
sl_hal_sysrtc_set_group_interrupts(uint8_t group_number, uint32_t flags)

Sets one or more pending SYSRTC interrupts for the given group from Software.

uint32_t
sl_hal_sysrtc_get_group_compare_channel_value(uint8_t group_number, uint8_t channel)

Gets SYSRTC compare register value for selected channel of given group.

void
sl_hal_sysrtc_set_group_compare_channel_value(uint8_t group_number, uint8_t channel, uint32_t value)

Sets SYSRTC compare register value for selected channel of given group.

uint32_t

Gets SYSRTC input capture register value for capture channel of given group.

void
sl_hal_sysrtc_set_group_pretrigger(uint8_t group_number, sl_hal_sysrtc_group_pretrigger_config_t const *group_pretrigger_config)

Sets the pre-triggers for a given group.

uint32_t

Gets the status of the pre-triggers for a given group.

void
sl_hal_sysrtc_clear_group_pretrigger_status(uint8_t group_number, uint32_t flags)

Clears the status of the pre-triggers for a given group.

void
sl_hal_sysrtc_init(const sl_hal_sysrtc_init_t *init)

Initializes SYSRTC module.

void

Enables the SYSRTC module and starts the counter.

void

Stops the counter and disables the SYSRTC.

void

Waits for the SYSRTC to complete resetting or disabling procedure.

void

Starts SYSRTC counter.

void

Stops the SYSRTC counter.

void

Restores SYSRTC to its reset state.

void

Locks SYSRTC registers.

void

Unlocks SYSRTC registers.

void

Sets the SYSRTC counter value.

Macros#

#define

Minimum compare channels for SYSRTC group.

#define

Maximum compare channels for SYSRTC group.

#define

Minimum capture channels for SYSRTC group.

#define

Maximum capture channels for SYSRTC group.

#define
SYSRTC_INST SYSRTC0

SYSRTC instance.

#define

Number of SYSRTC groups.

#define

Validation of valid SYSRTC group for assert statements.

#define

Suggested default values for compare channel configuration structure.

#define

Compare channel configuration for starting HFXO using PRS.

#define

Suggested default values for capture channel configuration structure.

#define

Suggested default values for SYSRTC group configuration structure.

#define

Suggested default values for pre-trigger configuration structure.

#define

Suggested default values for group pre-trigger configuration structure.

#define

Suggested default values for SYSRTC configuration structure.

Enumeration Documentation#

sl_hal_sysrtc_capture_edge_t#

sl_hal_sysrtc_capture_edge_t

Capture input edge select.

Enumerator
SL_HAL_SYSRTC_CAPTURE_EDGE_RISING

Rising edges detected.

SL_HAL_SYSRTC_CAPTURE_EDGE_FALLING

Falling edges detected.

SL_HAL_SYSRTC_CAPTURE_EDGE_BOTH

Both edges detected.


sl_hal_sysrtc_compare_match_out_action_t#

sl_hal_sysrtc_compare_match_out_action_t

Compare match output action mode.

Enumerator
SL_HAL_SYSRTC_COMPARE_MATCH_OUT_ACTION_CLEAR

Clear output.

SL_HAL_SYSRTC_COMPARE_MATCH_OUT_ACTION_SET

Set output.

SL_HAL_SYSRTC_COMPARE_MATCH_OUT_ACTION_PULSE

Generate a pulse.

SL_HAL_SYSRTC_COMPARE_MATCH_OUT_ACTION_TOGGLE

Toggle output.

SL_HAL_SYSRTC_COMPARE_MATCH_OUT_ACTION_CMPIF

Export CMPIF.


Function Documentation#

sl_hal_sysrtc_wait_sync#

void sl_hal_sysrtc_wait_sync (void )

Waits for the SYSRTC to complete all synchronization of register changes and commands.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Wait for synchronization of register changes to low frequency domain.

Note

  • This function will stall execution until the synchronization is complete.


sl_hal_sysrtc_get_status#

uint32_t sl_hal_sysrtc_get_status (void )

Gets SYSRTC STATUS register value.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Current STATUS register value.


sl_hal_sysrtc_get_counter#

uint32_t sl_hal_sysrtc_get_counter (void )

Gets SYSRTC counter value.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Current SYSRTC counter value.


sl_hal_sysrtc_wait_sync_group#

void sl_hal_sysrtc_wait_sync_group (uint8_t group_number)

Waits for the SYSRTC group to complete all synchronization of register changes and commands.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.


sl_hal_sysrtc_init_group#

void sl_hal_sysrtc_init_group (uint8_t group_number, sl_hal_sysrtc_group_init_t const * group_init)

Initializes the selected SYSRTC group.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

sl_hal_sysrtc_group_init_t const *[in]group_init

Pointer to group initialization structure variable.


sl_hal_sysrtc_group_enable_compare_channel#

void sl_hal_sysrtc_group_enable_compare_channel (uint8_t group_number, uint8_t channel, bool enable)

Enables or disables a compare channel for the specified group at runtime.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

uint8_t[in]channel

Compare channel number (0-2).

bool[in]enable

Enable state for the compare channel.


sl_hal_sysrtc_group_set_compare_channel_action#

void sl_hal_sysrtc_group_set_compare_channel_action (uint8_t group_number, uint8_t channel, sl_hal_sysrtc_compare_match_out_action_t action)

Sets the compare match out action for a compare channel at runtime.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

uint8_t[in]channel

Compare channel number (0-2).

sl_hal_sysrtc_compare_match_out_action_t[in]action

Compare match out action.


sl_hal_sysrtc_group_enable_capture_channel#

void sl_hal_sysrtc_group_enable_capture_channel (uint8_t group_number, uint8_t channel, bool enable)

Enables or disables a capture channel for the specified group at runtime.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

uint8_t[in]channel

Capture channel number (currently only 0 is valid).

bool[in]enable

Enable state for the capture channel.

Note

  • Currently only capture channel 0 is supported by hardware, but the API is designed to be future-proof for additional capture channels.


sl_hal_sysrtc_group_set_capture_channel_edge#

void sl_hal_sysrtc_group_set_capture_channel_edge (uint8_t group_number, uint8_t channel, sl_hal_sysrtc_capture_edge_t edge)

Sets the capture input edge for a capture channel at runtime.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

uint8_t[in]channel

Capture channel number (currently only 0 is valid).

sl_hal_sysrtc_capture_edge_t[in]edge

Capture input edge selection.

Note

  • Currently only capture channel 0 is supported by hardware, but the API is designed to be future-proof for additional capture channels.


sl_hal_sysrtc_enable_group_interrupts#

void sl_hal_sysrtc_enable_group_interrupts (uint8_t group_number, uint32_t flags)

Enables one or more SYSRTC interrupts for the given group.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

uint32_t[in]flags

SYSRTC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the given SYSRTC group.

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using sl_hal_sysrtc_clear_group_interrupts() prior to enabling the interrupt.


sl_hal_sysrtc_disable_group_interrupts#

void sl_hal_sysrtc_disable_group_interrupts (uint8_t group_number, uint32_t flags)

Disables one or more SYSRTC interrupts for the given group.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

uint32_t[in]flags

SYSRTC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for the given SYSRTC group.


sl_hal_sysrtc_clear_group_interrupts#

void sl_hal_sysrtc_clear_group_interrupts (uint8_t group_number, uint32_t flags)

Clears one or more pending SYSRTC interrupts for the given group.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

uint32_t[in]flags

SYSRTC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the given SYSRTC group.


sl_hal_sysrtc_get_group_interrupts#

uint32_t sl_hal_sysrtc_get_group_interrupts (uint8_t group_number)

Gets pending SYSRTC interrupt flags for the given group.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

Note

  • Event bits are not cleared by using this function.

Returns

  • Pending SYSRTC interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the SYSRTC group.


sl_hal_sysrtc_get_group_enabled_interrupts#

uint32_t sl_hal_sysrtc_get_group_enabled_interrupts (uint8_t group_number)

Gets enabled and pending SYSRTC interrupt flags for the given group.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Interrupt flags are not cleared by using this function.

Returns

  • Pending and enabled SYSRTC interrupt sources. The return value is the bitwise AND of

    • the enabled interrupt sources in SYSRTC_GRPx_IEN and

    • the pending interrupt flags SYSRTC_GRPx_IF.


sl_hal_sysrtc_set_group_interrupts#

void sl_hal_sysrtc_set_group_interrupts (uint8_t group_number, uint32_t flags)

Sets one or more pending SYSRTC interrupts for the given group from Software.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

uint32_t[in]flags

SYSRTC interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the SYSRTC group.


sl_hal_sysrtc_get_group_compare_channel_value#

uint32_t sl_hal_sysrtc_get_group_compare_channel_value (uint8_t group_number, uint8_t channel)

Gets SYSRTC compare register value for selected channel of given group.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

uint8_t[in]channel

Channel selector.

Returns

  • Compare register value.


sl_hal_sysrtc_set_group_compare_channel_value#

void sl_hal_sysrtc_set_group_compare_channel_value (uint8_t group_number, uint8_t channel, uint32_t value)

Sets SYSRTC compare register value for selected channel of given group.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

uint8_t[in]channel

Channel selector.

uint32_t[in]value

Compare register value.


sl_hal_sysrtc_get_group_capture_channel_value#

uint32_t sl_hal_sysrtc_get_group_capture_channel_value (uint8_t group_number)

Gets SYSRTC input capture register value for capture channel of given group.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

Returns

  • Capture register value.


sl_hal_sysrtc_set_group_pretrigger#

void sl_hal_sysrtc_set_group_pretrigger (uint8_t group_number, sl_hal_sysrtc_group_pretrigger_config_t const * group_pretrigger_config)

Sets the pre-triggers for a given group.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

sl_hal_sysrtc_group_pretrigger_config_t const *[in]group_pretrigger_config

Pointer to group pre-trigger configuration structure variable.


sl_hal_sysrtc_get_group_pretrigger_status#

uint32_t sl_hal_sysrtc_get_group_pretrigger_status (uint8_t group_number)

Gets the status of the pre-triggers for a given group.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

Returns

  • Pre-trigger status flags for a given group.


sl_hal_sysrtc_clear_group_pretrigger_status#

void sl_hal_sysrtc_clear_group_pretrigger_status (uint8_t group_number, uint32_t flags)

Clears the status of the pre-triggers for a given group.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]group_number

SYSRTC group number to use.

uint32_t[out]flags

Pre-trigger status flags for a given group.

The ACTIVE status must be cleared from Software.


sl_hal_sysrtc_init#

void sl_hal_sysrtc_init (const sl_hal_sysrtc_init_t * init)

Initializes SYSRTC module.

Parameters
TypeDirectionArgument NameDescription
const sl_hal_sysrtc_init_t *[in]init

A pointer to the SYSRTC initialization structure variable.

@Note that the compare values must be set separately with (sl_hal_sysrtc_set_group_compare_channel_value()), which should probably be done prior to the use of this function if configuring the SYSRTC to start when initialization is completed.


sl_hal_sysrtc_enable#

void sl_hal_sysrtc_enable (void )

Enables the SYSRTC module and starts the counter.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_hal_sysrtc_disable#

void sl_hal_sysrtc_disable (void )

Stops the counter and disables the SYSRTC.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_hal_sysrtc_wait_ready#

void sl_hal_sysrtc_wait_ready (void )

Waits for the SYSRTC to complete resetting or disabling procedure.

Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_hal_sysrtc_start#

void sl_hal_sysrtc_start (void )

Starts SYSRTC counter.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function will send a start command to the SYSRTC peripheral. The SYSRTC peripheral will use some LF clock ticks before the command is executed. The sl_hal_sysrtc_wait_sync() function can be used to wait for the start command to be executed.

Note

  • This function requires the SYSRTC to be enabled.


sl_hal_sysrtc_stop#

void sl_hal_sysrtc_stop (void )

Stops the SYSRTC counter.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function will send a stop command to the SYSRTC peripheral. The SYSRTC peripheral will use some LF clock ticks before the command is executed. The sl_hal_sysrtc_wait_sync() function can be used to wait for the stop command to be executed.

Note

  • This function requires the SYSRTC to be enabled.


sl_hal_sysrtc_reset#

void sl_hal_sysrtc_reset (void )

Restores SYSRTC to its reset state.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • On devices without a software reset SYSRTC_SWRST register, the reset is done manually by writing reset values to all IO registers. Read-only registers are not modified.


sl_hal_sysrtc_lock#

void sl_hal_sysrtc_lock (void )

Locks SYSRTC registers.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • When SYSRTC registers are locked SYSRTC_EN, SYSRTC_CFG, SYSRTC_CMD, SYSRTC_SWRST, SYSRTC_CNT and SYSRTC_TOPCNT registers cannot be written to.


sl_hal_sysrtc_unlock#

void sl_hal_sysrtc_unlock (void )

Unlocks SYSRTC registers.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • When SYSRTC registers are locked SYSRTC_EN, SYSRTC_CFG, SYSRTC_CMD, SYSRTC_SWRST, SYSRTC_CNT and SYSRTC_TOPCNT registers cannot be written to.


sl_hal_sysrtc_set_counter#

void sl_hal_sysrtc_set_counter (uint32_t value)

Sets the SYSRTC counter value.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]value

The new SYSRTC counter value.


Macro Definition Documentation#

SYSRTC_GROUP_MIN_CHANNEL_COMPARE#

#define SYSRTC_GROUP_MIN_CHANNEL_COMPARE
Value:
1u

Minimum compare channels for SYSRTC group.


SYSRTC_GROUP_MAX_CHANNEL_COMPARE#

#define SYSRTC_GROUP_MAX_CHANNEL_COMPARE
Value:
3u

Maximum compare channels for SYSRTC group.


SYSRTC_GROUP_MIN_CHANNEL_CAPTURE#

#define SYSRTC_GROUP_MIN_CHANNEL_CAPTURE
Value:
0u

Minimum capture channels for SYSRTC group.


SYSRTC_GROUP_MAX_CHANNEL_CAPTURE#

#define SYSRTC_GROUP_MAX_CHANNEL_CAPTURE
Value:
1u

Maximum capture channels for SYSRTC group.


SYSRTC_INST#

#define SYSRTC_INST
Value:
SYSRTC0

SYSRTC instance.


SYSRTC_GROUP_NUMBER#

#define SYSRTC_GROUP_NUMBER
Value:
1u

Number of SYSRTC groups.


SYSRTC_GROUP_VALID#

#define SYSRTC_GROUP_VALID
Value:
(group)

Validation of valid SYSRTC group for assert statements.


SL_HAL_SYSRTC_GROUP_CHANNEL_COMPARE_INIT_DEFAULT#

#define SL_HAL_SYSRTC_GROUP_CHANNEL_COMPARE_INIT_DEFAULT
Value:
{ \
SL_HAL_SYSRTC_COMPARE_MATCH_OUT_ACTION_PULSE \
}

Suggested default values for compare channel configuration structure.


SL_HAL_SYSRTC_GROUP_CHANNEL_COMPARE_CONFIG_EARLY_WAKEUP#

#define SL_HAL_SYSRTC_GROUP_CHANNEL_COMPARE_CONFIG_EARLY_WAKEUP
Value:
{ \
SL_HAL_SYSRTC_COMPARE_MATCH_OUT_ACTION_CMPIF \
}

Compare channel configuration for starting HFXO using PRS.


SL_HAL_SYSRTC_GROUP_CHANNEL_CAPTURE_INIT_DEFAULT#

#define SL_HAL_SYSRTC_GROUP_CHANNEL_CAPTURE_INIT_DEFAULT
Value:
{ \
SL_HAL_SYSRTC_CAPTURE_EDGE_RISING \
}

Suggested default values for capture channel configuration structure.


SL_HAL_SYSRTC_GROUP_INIT_DEFAULT#

#define SL_HAL_SYSRTC_GROUP_INIT_DEFAULT
Value:
{ \
true, /* Enable compare channel 0. */ \
false, /* Disable compare channel 1. */ \
false, /* Disable compare channel 2. */ \
false, /* Disable capture channel 0. */ \
NULL, /* NULL Pointer to configuration structure for compare channel 0. */ \
NULL, /* NULL Pointer to configuration structure for compare channel 1. */ \
NULL, /* NULL Pointer to configuration structure for compare channel 2. */ \
NULL /* NULL Pointer to configuration structure for capture channel 0. */ \
}

Suggested default values for SYSRTC group configuration structure.


SL_HAL_SYSRTC_PRETRIGGER_INIT_DEFAULT#

#define SL_HAL_SYSRTC_PRETRIGGER_INIT_DEFAULT
Value:
{ \
false, /* Disable the pre-trigger. */ \
0, /* The pre-trigger occurs 0 LF ticks before the compare. */ \
}

Suggested default values for pre-trigger configuration structure.


SL_HAL_SYSRTC_GROUP_PRETRIGGER_INIT_DEFAULT#

#define SL_HAL_SYSRTC_GROUP_PRETRIGGER_INIT_DEFAULT
Value:
{ \
SL_HAL_SYSRTC_PRETRIGGER_INIT_DEFAULT, /* Default pre-trigger configuration to wake up EMU. */ \
SL_HAL_SYSRTC_PRETRIGGER_INIT_DEFAULT, /* Default pre-trigger configuration to start HFXO. */ \
0 /* Compare channel used by the pre-triggers. */ \
}

Suggested default values for group pre-trigger configuration structure.


SL_HAL_SYSRTC_INIT_DEFAULT#

#define SL_HAL_SYSRTC_INIT_DEFAULT
Value:
{ \
false, /* Disable updating during debug halt. */ \
}

Suggested default values for SYSRTC configuration structure.