CPC#

Modules#

sl_cpc_endpoint_handle_t

sl_cpc_endpoint_debug_counters_t

sl_cpc_core_debug_counters_t

Enumerations#

enum
SL_CPC_JOURNAL_ERROR_LEVEL = 0x00
SL_CPC_JOURNAL_WARNING_LEVEL = 0x40
SL_CPC_JOURNAL_INFO_LEVEL = 0x80
SL_CPC_JOURNAL_DEBUG_LEVEL = 0xC0
SL_CPC_JOURNAL_TRACE_LEVEL = 0xC0
}

Enumeration of journal entry levels.

enum
SL_CPC_ENDPOINT_USER_ID_0 = 90
SL_CPC_ENDPOINT_USER_ID_1 = 91
SL_CPC_ENDPOINT_USER_ID_2 = 92
SL_CPC_ENDPOINT_USER_ID_3 = 93
SL_CPC_ENDPOINT_USER_ID_4 = 94
SL_CPC_ENDPOINT_USER_ID_5 = 95
SL_CPC_ENDPOINT_USER_ID_6 = 96
SL_CPC_ENDPOINT_USER_ID_7 = 97
SL_CPC_ENDPOINT_USER_ID_8 = 98
SL_CPC_ENDPOINT_USER_ID_9 = 99
}

Enumeration representing user endpoint.

enum
SL_CPC_STATE_FREED = 0
SL_CPC_STATE_OPEN
SL_CPC_STATE_CLOSED
SL_CPC_STATE_CLOSING
SL_CPC_STATE_CONNECTING
SL_CPC_STATE_CONNECTED
SL_CPC_STATE_SHUTTING_DOWN
SL_CPC_STATE_SHUTDOWN
SL_CPC_STATE_REMOTE_SHUTDOWN
SL_CPC_STATE_DISCONNECTED
SL_CPC_STATE_ERROR_DESTINATION_UNREACHABLE
SL_CPC_STATE_ERROR_SECURITY_INCIDENT
SL_CPC_STATE_ERROR_FAULT
}

Enumeration representing the possible endpoint state.

enum
SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE = 0
SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE_ARG
SL_CPC_ENDPOINT_ON_IFRAME_WRITE_COMPLETED
SL_CPC_ENDPOINT_ON_ERROR
SL_CPC_ENDPOINT_ON_ERROR_ARG
SL_CPC_ENDPOINT_ON_CONNECT
SL_CPC_ENDPOINT_ON_CONNECT_ARG
SL_CPC_ENDPOINT_SHUTDOWN_TIMEOUT
SL_CPC_ENDPOINT_WRITE_TIMEOUT
SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE
SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE_ARG
SL_CPC_ENDPOINT_ON_UFRAME_WRITE_COMPLETED
SL_CPC_ENDPOINT_ON_FINAL
SL_CPC_ENDPOINT_ON_FINAL_ARG
}

Enumeration representing the possible configurable options for an endpoint.

Typedefs#

typedef void(*
sl_cpc_on_write_completed_t)(sl_cpc_user_endpoint_id_t endpoint_id, void *buffer, void *arg, sl_status_t status)
typedef void(*
sl_cpc_on_data_reception_t)(uint8_t endpoint_id, void *arg)
typedef void(*
sl_cpc_on_error_callback_t)(uint8_t endpoint_id, void *arg)
typedef void(*
sl_cpc_on_connect_callback_t)(uint8_t endpoint_id, void *arg, sl_status_t status)

Functions#

const char *
bool
sl_cpc_user_is_ok_to_run(const char *primary_app_version, const char *secondary_app_version)
sl_status_t
sl_cpc_get_fwu_chunk(uint8_t *const chunk_buffer, const size_t index, const size_t chunk_size, size_t *size, bool *last)
void

PUBLIC FUNCTIONS.

void
sl_cpc_journal_record_internal(sl_cpc_journal_level_t level, const char *string, uint32_t value)

Push an entry in the Journal.

void
sl_cpc_journal_record(sl_cpc_journal_level_t level, const char *string, uint32_t value)

Record a Journal Entry.

void
sl_cpc_journal_print(bool print_csv_header, sl_iostream_t *stream)

Print the contents of the CPC journal via the default IOStream.

void
sl_cpc_journal_print_cmd_handler(sl_cli_command_arg_t *arguments)

Command Handler to Print the Journal Contents.

sl_status_t
sl_status_t
sl_cpc_init_user_endpoint(sl_cpc_endpoint_handle_t *endpoint_handle, sl_cpc_user_endpoint_id_t id, uint8_t flags)
sl_status_t
sl_cpc_connect_endpoint(sl_cpc_endpoint_handle_t *endpoint_handle, uint8_t flags)
sl_status_t
sl_cpc_open_user_endpoint(sl_cpc_endpoint_handle_t *endpoint_handle, sl_cpc_user_endpoint_id_t id, uint8_t flags, uint8_t tx_window_size)
sl_status_t
sl_cpc_listen_endpoint(sl_cpc_endpoint_handle_t *endpoint_handle, uint8_t flags)
sl_status_t
sl_cpc_close_endpoint(sl_cpc_endpoint_handle_t *endpoint_handle)
sl_status_t
sl_cpc_set_endpoint_option(sl_cpc_endpoint_handle_t *endpoint_handle, sl_cpc_endpoint_option_t option, void *value)
sl_status_t
sl_cpc_shutdown_endpoint(sl_cpc_endpoint_handle_t *endpoint_handle, uint8_t flags)
sl_status_t
sl_cpc_terminate_endpoint(sl_cpc_endpoint_handle_t *endpoint_handle, uint8_t flags)
sl_status_t
sl_cpc_free_endpoint(sl_cpc_endpoint_handle_t *endpoint_handle)
sl_status_t
sl_cpc_abort_read(sl_cpc_endpoint_handle_t *endpoint_handle)
sl_status_t
sl_cpc_read(sl_cpc_endpoint_handle_t *endpoint_handle, void **data, uint16_t *data_length, uint32_t timeout, uint8_t flags)
sl_status_t
sl_cpc_write(sl_cpc_endpoint_handle_t *endpoint_handle, void *data, uint16_t data_length, uint8_t flags, void *on_write_completed_arg)
sl_cpc_get_endpoint_state(sl_cpc_endpoint_handle_t *endpoint_handle)
bool
sl_cpc_get_endpoint_encryption(sl_cpc_endpoint_handle_t *endpoint_handle)
sl_status_t
uint16_t
sl_cpc_get_tx_max_payload_length(sl_cpc_endpoint_handle_t *endpoint_handle)
sl_power_manager_on_isr_exit_t

Macros#

#define

Record a CPC journal entry.

#define
#define
#define
#define

sl cpc open endpoint flag none

#define

sl cpc open endpoint flag disable encryption

#define
SL_CPC_OPEN_ENDPOINT_FLAG_NONE SL_CPC_ENDPOINT_FLAG_NONE
#define
SL_CPC_OPEN_ENDPOINT_FLAG_DISABLE_ENCRYPTION SL_CPC_ENDPOINT_FLAG_DISABLE_ENCRYPTION
#define
SL_CPC_USER_ENDPOINT_ID_START ((uint8_t)SL_CPC_ENDPOINT_USER_ID_0)

Struct representing a core debug.

#define
SL_CPC_USER_ENDPOINT_ID_END ((uint8_t)SL_CPC_ENDPOINT_USER_ID_9)

sl cpc user endpoint id end.

#define
SL_CPC_USER_ENDPOINT_MAX_COUNT (SL_CPC_USER_ENDPOINT_ID_END - SL_CPC_USER_ENDPOINT_ID_START + 1)

maximum simultaneous user endpoint.

#define

sl cpc flag no block.

#define

sli cpc security tag length.

#define

sli cpc ldma desciptor max size.

#define

sli cpc header size.

#define

sli cpc payload crc size.

#define
SL_CPC_TX_PAYLOAD_MAX_LENGTH ((2 * SLI_CPC_LDMA_DESCRIPTOR_MAX_SIZE) - SLI_CPC_HEADER_SIZE - SLI_CPC_PAYLOAD_CRC_SIZE)

sl cpc tx payload max length.

#define
SL_CPC_TX_PAYLOAD_MAX_LENGTH_WITH_SECURITY (SL_CPC_TX_PAYLOAD_MAX_LENGTH - SLI_CPC_SECURITY_TAG_LENGTH)

sl cpc tx payload max lenght with security.

#define

sl cpc transmit window min size.

#define

sl cpc transmit window max size.

Enumeration Documentation#

sl_cpc_journal_level_t#

sl_cpc_journal_level_t

Enumeration of journal entry levels.

Enumerator
SL_CPC_JOURNAL_ERROR_LEVEL
SL_CPC_JOURNAL_WARNING_LEVEL
SL_CPC_JOURNAL_INFO_LEVEL
SL_CPC_JOURNAL_DEBUG_LEVEL
SL_CPC_JOURNAL_TRACE_LEVEL

sl_cpc_user_endpoint_id_t#

sl_cpc_user_endpoint_id_t

Enumeration representing user endpoint.

Enumerator
SL_CPC_ENDPOINT_USER_ID_0

User endpoint ID 0.

SL_CPC_ENDPOINT_USER_ID_1

User endpoint ID 1.

SL_CPC_ENDPOINT_USER_ID_2

User endpoint ID 2.

SL_CPC_ENDPOINT_USER_ID_3

User endpoint ID 3.

SL_CPC_ENDPOINT_USER_ID_4

User endpoint ID 4.

SL_CPC_ENDPOINT_USER_ID_5

User endpoint ID 5.

SL_CPC_ENDPOINT_USER_ID_6

User endpoint ID 6.

SL_CPC_ENDPOINT_USER_ID_7

User endpoint ID 7.

SL_CPC_ENDPOINT_USER_ID_8

User endpoint ID 8.

SL_CPC_ENDPOINT_USER_ID_9

User endpoint ID 9.


sl_cpc_endpoint_state_t#

sl_cpc_endpoint_state_t

Enumeration representing the possible endpoint state.

Enumerator
SL_CPC_STATE_FREED

State freed.

SL_CPC_STATE_OPEN

State open.

SL_CPC_STATE_CLOSED

State close.

SL_CPC_STATE_CLOSING

State closing.

SL_CPC_STATE_CONNECTING

Connecting to remote's endpoint.

SL_CPC_STATE_CONNECTED

Connected to remote's endpoint.

SL_CPC_STATE_SHUTTING_DOWN

Transmissions shutting down.

SL_CPC_STATE_SHUTDOWN

Transmissions shutdown.

SL_CPC_STATE_REMOTE_SHUTDOWN

Remote transmissions shutdown.

SL_CPC_STATE_DISCONNECTED

Connection terminated.

SL_CPC_STATE_ERROR_DESTINATION_UNREACHABLE

Error state, destination unreachable.

SL_CPC_STATE_ERROR_SECURITY_INCIDENT

Error state, security incident.

SL_CPC_STATE_ERROR_FAULT

Error state, fault.


sl_cpc_endpoint_option_t#

sl_cpc_endpoint_option_t

Enumeration representing the possible configurable options for an endpoint.

Enumerator
SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE

Set callback for iframe received notification.

SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE_ARG

Set callback argument for iframe received notification.

SL_CPC_ENDPOINT_ON_IFRAME_WRITE_COMPLETED

Set callback for write complete notification.

SL_CPC_ENDPOINT_ON_ERROR

Set callback for error notification.

SL_CPC_ENDPOINT_ON_ERROR_ARG

Set callback argument for error notification.

SL_CPC_ENDPOINT_ON_CONNECT

Set callback when host/primary connects to endpoint.

SL_CPC_ENDPOINT_ON_CONNECT_ARG

Set callback argument for connect notification.

SL_CPC_ENDPOINT_SHUTDOWN_TIMEOUT

Set shutdown timeout, in ticks.

SL_CPC_ENDPOINT_WRITE_TIMEOUT

Set the timeout time for blocking write in ticks.

SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE

Set callback for uframe received notification.

SL_CPC_ENDPOINT_ON_UFRAME_RECEIVE_ARG

Set callback argument for uframe received notification.

SL_CPC_ENDPOINT_ON_UFRAME_WRITE_COMPLETED

Set callback for write complete notification.

SL_CPC_ENDPOINT_ON_FINAL

Set callback for on final notification.

SL_CPC_ENDPOINT_ON_FINAL_ARG

Set callback argument for on final notification.


Typedef Documentation#

sl_cpc_on_write_completed_t#

typedef void(* sl_cpc_on_write_completed_t) (sl_cpc_user_endpoint_id_t endpoint_id, void *buffer, void *arg, sl_status_t status) )(sl_cpc_user_endpoint_id_t endpoint_id, void *buffer, void *arg, sl_status_t status)
Parameters
TypeDirectionArgument NameDescription
N/Aendpoint_id

Endpoint ID

N/Abuffer

Pointer to data buffer.

N/Aarg

Transaction user's argument.

N/Astatus

Status indicating the transaction result: SL_STATUS_OK Remote should have receive the frame SL_STATUS_TRANSMIT_INCOMPLETE Remote has not received the frame.

Typedef for the user - supplied callback function which is called when CPC is done with the provided buffer.

The callback must be non-blocking and efficient: it should return quickly and must not perform long-running operations, busy-waiting, or blocking on RTOS primitives or slow I/O. In general, application code must not invoke CPC API functions from within this callback, unless an API is explicitly documented as safe to use from callbacks. Any substantial work, including further CPC operations, should be deferred to another execution context (for example by posting to a queue or signaling a task).


sl_cpc_on_data_reception_t#

typedef void(* sl_cpc_on_data_reception_t) (uint8_t endpoint_id, void *arg) )(uint8_t endpoint_id, void *arg)
Parameters
TypeDirectionArgument NameDescription
N/Aendpoint_id

Endpoint ID

N/Aarg

User-specific argument .

Typedef for the user - supplied callback function which is called when CPC receive data on an endpoint.

The callback must be non-blocking and efficient: it should return quickly and must not perform long-running operations, busy-waiting, or blocking on RTOS primitives or slow I/O. In general, application code must not invoke CPC API functions from within this callback, unless an API is explicitly documented as safe to use from callbacks. Any substantial work, including further CPC operations, should be deferred to another execution context (for example by posting to a queue or signaling a task).


sl_cpc_on_error_callback_t#

typedef void(* sl_cpc_on_error_callback_t) (uint8_t endpoint_id, void *arg) )(uint8_t endpoint_id, void *arg)
Parameters
TypeDirectionArgument NameDescription
N/Aendpoint_id

Endpoint ID

N/Aarg

User-specific argument .

Typedef for the user-supplied callback function which is called when CPC detects a fatal error on an endpoint.

The callback must be non-blocking and efficient: it should return quickly and must not perform long-running operations, busy-waiting, or blocking on RTOS primitives or slow I/O. In general, application code must not invoke CPC API functions from within this callback, unless an API is explicitly documented as safe to use from callbacks. Any substantial work, including further CPC operations, should be deferred to another execution context (for example by posting to a queue or signaling a task).


sl_cpc_on_connect_callback_t#

typedef void(* sl_cpc_on_connect_callback_t) (uint8_t endpoint_id, void *arg, sl_status_t status) )(uint8_t endpoint_id, void *arg, sl_status_t status)
Parameters
TypeDirectionArgument NameDescription
N/Aendpoint_id

Endpoint ID

N/Aarg

User-specific argument.

N/Astatus

Indicate if the connection was successful or not: SL_STATUS_OK successfully connected SL_STATUS_TIMEOUT operation timed out SL_STATUS_NOT_READY secondary's endpoint is not ready

Typedef for the user-supplied callback function which is called when CPC connection to a secondary completes, successfully or not.

The callback must be non-blocking and efficient: it should return quickly and must not perform long-running operations, busy-waiting, or blocking on RTOS primitives or slow I/O. In general, application code must not invoke CPC API functions from within this callback, unless an API is explicitly documented as safe to use from callbacks. Any substantial work, including further CPC operations, should be deferred to another execution context (for example by posting to a queue or signaling a task).

Note

  • If several users connect to the same endpoint on the host side, this callback will only be called only when the first connection occurs.


Function Documentation#

sl_cpc_secondary_app_version#

const char * sl_cpc_secondary_app_version (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Called when secondary app version is requested. The format is up to the user. The string should be null terminated.


sl_cpc_primary_app_version#

const char * sl_cpc_primary_app_version (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Called when primary app version is requested. The format is up to the user. The string should be null terminated.

Note

  • : CPC source code contains a weak definition that default to returning "UNDEFINED". If the user provides a strong definition of this function, the user shall return a static string.

Returns

  • : String that represents the application version.

Called when primary app version is requested. The format is up to the user. The string should be null terminated.


sl_cpc_user_is_ok_to_run#

bool sl_cpc_user_is_ok_to_run (const char * primary_app_version, const char * secondary_app_version)
Parameters
TypeDirectionArgument NameDescription
const char *N/Aprimary_app_version
const char *N/Asecondary_app_version

Callback implemented by the user to verify if the secondary application version is compatible with this primary version.

Note

  • : If this function is not implemented, then no version check will be performed and CPC API will always be available after the startup sequence.

  • : The function prototype is declared as weak. No default weak definition exist.

Returns

  • bool : true : CPC is authorized to start normally false : The user decided that the application versions are not compatible. CPC API will be blocked and only a firmware upgrade will be possible


sl_cpc_get_fwu_chunk#

sl_status_t sl_cpc_get_fwu_chunk (uint8_t *const chunk_buffer, const size_t index, const size_t chunk_size, size_t * size, bool * last)
Parameters
TypeDirectionArgument NameDescription
uint8_t *const[in]chunk_buffer

: 128 bytes buffer into which the user must copy the chunk

const size_t[in]index

: The byte index of the chunk being requested. When the FWU starts, the index starts at 0 and will increment by 128 (chunk size) after each time the user submits a chunk.

const size_t[in]chunk_size

: This will always be 128 (chunk size) and is the number of bytes the user must copy into the chunk_buffer. The only exception is for the last chunk; if the last chunk is less than 128 bytes, then the user must copy the the remaining bytes and return the size of the last chunk in the 'size' out parameter.

size_t *[out]size

: This is the number of bytes the user has copied into the chunk buffer. For all chunks except the last one, this value is expected to be 128 bytes, and some value between 1-128 for the last chunk.

bool *[out]last

: false if the chunk is not the last chunk. The firmware update state machine will continue fetching chunks from the user as long as the user does not return true on the last chunk.

Fetch the next firmware update image chunk from the user.

Note

  • : The prototype is declared as weak and no weak definition exist in CPC code. Not providing an implementation by the user is valid, although if the user asks to perform a firmware upgrade, sl_firmware_upgrade_start() will return SL_STATUS_NOT_AVAILABLE

Returns

  • sl_status_t : Whether or not the user has written a valid chunk. In the case where the user does not have the requested chunk in hand when this function is called and does not want to block (for example, fetching is from a serial link or an external storage), SL_STATUS_NOT_READY would be returned. The firmware update state machine will retry later to ask the user for the chunk. The index will remain the same at the next call. When a value of SL_STATUS_OK is returned, the state machine will go ahead and send the chunk to the secondary.


sl_cpc_journal_init#

void sl_cpc_journal_init (void )

PUBLIC FUNCTIONS.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Initialize the CPC Journal Module.

This function sets up the journal's circular buffers and configures the maximum number of entries. The journal supports four log levels: Error, Warning, Info, and Debug.

Note

  • To prevent overwriting critical log entries, Debug logs are stored in a separate circular buffer.


sl_cpc_journal_record_internal#

void sl_cpc_journal_record_internal (sl_cpc_journal_level_t level, const char * string, uint32_t value)

Push an entry in the Journal.

Parameters
TypeDirectionArgument NameDescription
sl_cpc_journal_level_t[in]level

The level of the entry (Error, Warning, Info, Debug).

const char *[in]string

The message string to log.

uint32_t[in]value

The value associated with the message.

This function logs a journal entry with a specified severity level, message string, and associated value.


sl_cpc_journal_record#

static void sl_cpc_journal_record (sl_cpc_journal_level_t level, const char * string, uint32_t value)

Record a Journal Entry.

Parameters
TypeDirectionArgument NameDescription
sl_cpc_journal_level_t[in]level

The level of the entry (Error, Warning, Info, Debug).

const char *[in]string

The message string to log.

uint32_t[in]value

The value associated with the message.

Note

  • If the provided journal level is superior to the configured max level, the journal entry will be ignored.


sl_cpc_journal_print#

void sl_cpc_journal_print (bool print_csv_header, sl_iostream_t * stream)

Print the contents of the CPC journal via the default IOStream.

Parameters
TypeDirectionArgument NameDescription
bool[in]print_csv_header

Whether to print a CSV header.

sl_iostream_t *[in]stream

The IOStream used to print the journal entries.

Note

  • Journal entries will be consumed when called


sl_cpc_journal_print_cmd_handler#

void sl_cpc_journal_print_cmd_handler (sl_cli_command_arg_t * arguments)

Command Handler to Print the Journal Contents.

Parameters
TypeDirectionArgument NameDescription
sl_cli_command_arg_t *[in]arguments

CLI arguments.

This function handles a command to print the contents of the CPC journal.

Note

  • Journal entries will be consumed when this function is called.


sl_cpc_init#

sl_status_t sl_cpc_init (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Initialize CPC module.

Initialize CPC module.


sl_cpc_init_permanent_allocations#

sl_status_t sl_cpc_init_permanent_allocations (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Initialize and allocate permanent memory for CPC

Initialize permanent memory for CPC


sl_cpc_process_action#

void sl_cpc_process_action (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

The bare metal process action function.

Tick step function, iterate over all instances and process them one by one.


sl_cpc_init_user_endpoint#

sl_status_t sl_cpc_init_user_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, sl_cpc_user_endpoint_id_t id, uint8_t flags)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[inout]endpoint_handle

Endpoint handle.

sl_cpc_user_endpoint_id_t[in]id

Endpoint ID [90 to 99].

uint8_t[in]flags

Initialization flags. Reserved for future used

Dynamically allocate and initialize a user endpoint. Following the successful initialization of an endpoint, successive attempts to initialize an endpoint of the same ID will fail until the endpoint is freed.

Initialize a CPC user endpoint


sl_cpc_connect_endpoint#

sl_status_t sl_cpc_connect_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, uint8_t flags)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

uint8_t[in]flags

Optional flags: SL_CPC_FLAG_NO_BLOCK Cause the function to return SL_STATUS_IN_PROGRESS immediately in RTOS.

Connect endpoint to remote. (CPC Primary only)

When an RTOS is present and no flag is specified, this function will block until the remote connects. In baremetal this function will return immediately.


sl_cpc_open_user_endpoint#

sl_status_t sl_cpc_open_user_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, sl_cpc_user_endpoint_id_t id, uint8_t flags, uint8_t tx_window_size)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

sl_cpc_user_endpoint_id_t[in]id

Endpoint ID [90 to 99].

uint8_t[in]flags

Endpoint type flags. SL_CPC_OPEN_ENDPOINT_FLAG_NONE Default behaviors SL_CPC_OPEN_ENDPOINT_FLAG_DISABLE_ENCRYPTION Disable encryption on the endpoint

uint8_t[in]tx_window_size

The maximum number of packets that can be sent before waiting for an acknowledge from the primary. Currently, only a value of 1 is supported.

Dynamically allocate and open a user endpoint.

Note

  • This function will be deprecated in the future. Use sl_cpc_init_user_endpoint() and sl_cpc_listen_endpoint() instead.


sl_cpc_listen_endpoint#

sl_status_t sl_cpc_listen_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, uint8_t flags)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

uint8_t[in]flags

Optional flags: SL_CPC_FLAG_NO_BLOCK Cause the function to return SL_STATUS_IN_PROGRESS immediately in RTOS.

Put an endpoint in listening mode, waiting for the remote to connect to it.

When an RTOS is present and no flag is specified, this function will block until the remote connects. In baremetal this function will return immediately.


sl_cpc_close_endpoint#

sl_status_t sl_cpc_close_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

Close endpoint.

Note

  • This function will be deprecated in the future. Use sl_cpc_terminate_endpoint() and sl_cpc_free_endpoint() instead.


sl_cpc_set_endpoint_option#

sl_status_t sl_cpc_set_endpoint_option (sl_cpc_endpoint_handle_t * endpoint_handle, sl_cpc_endpoint_option_t option, void * value)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

sl_cpc_endpoint_option_t[in]option

Endpoint Option.

void *[in]value

Pointer to the option value.

Set endpoint option.

Returns

  • Status code.

Return values

  • SL_STATUS_OK: Set endpoint option successfully.

  • Other: sl_status_t if error occurred.

Note

  • Public options are: SL_CPC_ENDPOINT_NAME: Set endpoint name. value must be a null-terminated string. The string is not copied, only the pointer. Caller must make sure the string is persistent for the lifetime of the endpoint.

SL_CPC_ENDPOINT_ON_CONNECT: Set a callback that will be called when connection is established with the remote.

SL_CPC_ENDPOINT_ON_CONNECT_ARG: Set an on connect argument.

SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE: Set an on iframe receive callback. value is a sl_cpc_on_data_reception_t type.

SL_CPC_ENDPOINT_ON_IFRAME_RECEIVE_ARG: Set an on iframe receive argument.

SL_CPC_ENDPOINT_ON_IFRAME_WRITE_COMPLETED: Set an on iframe write completed callback. value is a sl_cpc_on_write_completed_t type.

SL_CPC_ENDPOINT_ON_ERROR: Set an on error callback. value is a sl_cpc_on_error_callback_t type.

SL_CPC_ENDPOINT_ON_ERROR_ARG: Set an on error callback argument.

SL_CPC_ENDPOINT_SHUTDOWN_TIMEOUT: (RTOS Only) Set shutdown handshake timeout, in ticks.

SL_CPC_ENDPOINT_WRITE_TIMEOUT: (RTOS Only) Set the timeout time for blocking write in ticks.

Set endpoint option


sl_cpc_shutdown_endpoint#

sl_status_t sl_cpc_shutdown_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, uint8_t flags)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

uint8_t[in]flags

Optional flags: SL_CPC_FLAG_NO_BLOCK Cause the function to return SL_STATUS_IN_PROGRESS immediately in RTOS data still pending TX.

Shutdown endpoint connection. Any pending TX frame will attempt to be transmitted.

Note

  • In RTOS, this function is blocking by default. Use the SL_CPC_FLAG_NO_BLOCK flag to execute without blocking.

Shutdown endpoint's connection


sl_cpc_terminate_endpoint#

sl_status_t sl_cpc_terminate_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle, uint8_t flags)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

uint8_t[in]flags

Termination flags. Reserved for future use

Terminate an endpoint, effectively dropping any pending TX and RX frame.

In RTOS, this function will always block until all frames have been dropped.

Note

  • This function must be called before attempting to reconnect an endpoint to the remote.

Terminate endpoint


sl_cpc_free_endpoint#

sl_status_t sl_cpc_free_endpoint (sl_cpc_endpoint_handle_t * endpoint_handle)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

Free the memory associated to an endpoint so it can be reused.

Free endpoint


sl_cpc_abort_read#

sl_status_t sl_cpc_abort_read (sl_cpc_endpoint_handle_t * endpoint_handle)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

Abort read; Allow unblocking task in blocked by a read.

Note

  • This function can be called from an ISR.


sl_cpc_read#

sl_status_t sl_cpc_read (sl_cpc_endpoint_handle_t * endpoint_handle, void ** data, uint16_t * data_length, uint32_t timeout, uint8_t flags)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

void **[out]data

Address of the variable that will receive the data pointer.

uint16_t *[out]data_length

Length of the data contained in the buffer.

uint32_t[in]timeout

Timeout in ticks for the read operation. (Requires RTOS). Note: No effect if SL_CPC_FLAG_NO_BLOCK is provided as a flag

uint8_t[in]flags

Optional flags: SL_CPC_FLAG_NO_BLOCK Cause the function to return SL_STATUS_EMPTY immediately in RTOS if no data available.

Read data.

Read data from an endpoint


sl_cpc_write#

sl_status_t sl_cpc_write (sl_cpc_endpoint_handle_t * endpoint_handle, void * data, uint16_t data_length, uint8_t flags, void * on_write_completed_arg)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

void *[in]data

Pointer to data buffer.

uint16_t[in]data_length

Length of the data contained in the buffer.

uint8_t[in]flags

Optional flags: SL_CPC_FLAG_NO_BLOCK Cause the function to return SL_STATUS_NO_MORE_RESOURCE immediately in RTOS when out of resources.

void *[in]on_write_completed_arg

Argument that will be passed to on_write_completed().

Write data.

Note

  • This function cannot be called from an ISR.

  • When the write buffer is encrypted, the original content is lost and replaced by its encrypted counterpart.

Write data from an endpoint


sl_cpc_get_endpoint_state#

sl_cpc_endpoint_state_t sl_cpc_get_endpoint_state (sl_cpc_endpoint_handle_t * endpoint_handle)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

Get endpoint state.

Returns

  • Endpoint state.

Get endpoint status


sl_cpc_get_endpoint_encryption#

bool sl_cpc_get_endpoint_encryption (sl_cpc_endpoint_handle_t * endpoint_handle)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *[in]endpoint_handle

Endpoint handle.

Get endpoint encryption state.

Returns

  • Endpoint encryption state.

Get endpoint encryption


sl_cpc_free_rx_buffer#

sl_status_t sl_cpc_free_rx_buffer (void * data)
Parameters
TypeDirectionArgument NameDescription
void *[in]data

Pointer to data buffer to free.

Free buffer returned by sl_cpc_read().

Free rx buffer returned by sl_cpc_read().


sl_cpc_get_tx_max_payload_length#

uint16_t sl_cpc_get_tx_max_payload_length (sl_cpc_endpoint_handle_t * endpoint_handle)
Parameters
TypeDirectionArgument NameDescription
sl_cpc_endpoint_handle_t *N/Aendpoint_handle

handle of the endpoint for which the query is made

Get the maximum payload length that the remote can receive.

Returns

  • the maximum tx payload length in function of whether the encryption is enabled on the endpoint or not

Retrieve the maximum payload length that can be transmitted

Returns

  • the maximum tx payload length in function of whether the encryption is enabled on the endpoint or not


sl_cpc_is_ok_to_sleep#

bool sl_cpc_is_ok_to_sleep (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_cpc_sleep_on_isr_exit#

sl_power_manager_on_isr_exit_t sl_cpc_sleep_on_isr_exit (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Macro Definition Documentation#

SL_CPC_JOURNAL_RECORD_ERROR#

#define SL_CPC_JOURNAL_RECORD_ERROR
Value:
(string, value)

Record a CPC journal entry.


SL_CPC_JOURNAL_RECORD_WARNING#

#define SL_CPC_JOURNAL_RECORD_WARNING
Value:
(string, value)

SL_CPC_JOURNAL_RECORD_INFO#

#define SL_CPC_JOURNAL_RECORD_INFO
Value:
(string, value)

SL_CPC_JOURNAL_RECORD_DEBUG#

#define SL_CPC_JOURNAL_RECORD_DEBUG
Value:
(string, value)

SL_CPC_ENDPOINT_FLAG_NONE#

#define SL_CPC_ENDPOINT_FLAG_NONE
Value:
0

sl cpc open endpoint flag none


SL_CPC_ENDPOINT_FLAG_DISABLE_ENCRYPTION#

#define SL_CPC_ENDPOINT_FLAG_DISABLE_ENCRYPTION
Value:
(0x01 << 3)

sl cpc open endpoint flag disable encryption


SL_CPC_OPEN_ENDPOINT_FLAG_NONE#

#define SL_CPC_OPEN_ENDPOINT_FLAG_NONE
Value:
SL_CPC_ENDPOINT_FLAG_NONE

SL_CPC_OPEN_ENDPOINT_FLAG_DISABLE_ENCRYPTION#

#define SL_CPC_OPEN_ENDPOINT_FLAG_DISABLE_ENCRYPTION
Value:
SL_CPC_ENDPOINT_FLAG_DISABLE_ENCRYPTION

SL_CPC_MAJOR_VERSION#

#define SL_CPC_MAJOR_VERSION
Value:
4

SL_CPC_MINOR_VERSION#

#define SL_CPC_MINOR_VERSION
Value:
9

SL_CPC_PATCH_VERSION#

#define SL_CPC_PATCH_VERSION
Value:
1

SL_CPC_USER_ENDPOINT_ID_START#

#define SL_CPC_USER_ENDPOINT_ID_START
Value:
((uint8_t)SL_CPC_ENDPOINT_USER_ID_0)

Struct representing a core debug.

sl cpc endpoint id start.


SL_CPC_USER_ENDPOINT_ID_END#

#define SL_CPC_USER_ENDPOINT_ID_END
Value:
((uint8_t)SL_CPC_ENDPOINT_USER_ID_9)

sl cpc user endpoint id end.


SL_CPC_USER_ENDPOINT_MAX_COUNT#

#define SL_CPC_USER_ENDPOINT_MAX_COUNT
Value:
(SL_CPC_USER_ENDPOINT_ID_END - SL_CPC_USER_ENDPOINT_ID_START + 1)

maximum simultaneous user endpoint.


SL_CPC_FLAG_NO_BLOCK#

#define SL_CPC_FLAG_NO_BLOCK
Value:
0x01

sl cpc flag no block.


SLI_CPC_SECURITY_TAG_LENGTH#

#define SLI_CPC_SECURITY_TAG_LENGTH
Value:
8

sli cpc security tag length.


SLI_CPC_LDMA_DESCRIPTOR_MAX_SIZE#

#define SLI_CPC_LDMA_DESCRIPTOR_MAX_SIZE
Value:
2048

sli cpc ldma desciptor max size.


SLI_CPC_HEADER_SIZE#

#define SLI_CPC_HEADER_SIZE
Value:
7

sli cpc header size.


SLI_CPC_PAYLOAD_CRC_SIZE#

#define SLI_CPC_PAYLOAD_CRC_SIZE
Value:
2

sli cpc payload crc size.


SL_CPC_TX_PAYLOAD_MAX_LENGTH#

#define SL_CPC_TX_PAYLOAD_MAX_LENGTH
Value:
((2 * SLI_CPC_LDMA_DESCRIPTOR_MAX_SIZE) - SLI_CPC_HEADER_SIZE - SLI_CPC_PAYLOAD_CRC_SIZE)

sl cpc tx payload max length.


SL_CPC_TX_PAYLOAD_MAX_LENGTH_WITH_SECURITY#

#define SL_CPC_TX_PAYLOAD_MAX_LENGTH_WITH_SECURITY
Value:
(SL_CPC_TX_PAYLOAD_MAX_LENGTH - SLI_CPC_SECURITY_TAG_LENGTH)

sl cpc tx payload max lenght with security.


SL_CPC_TRANSMIT_WINDOW_MIN_SIZE#

#define SL_CPC_TRANSMIT_WINDOW_MIN_SIZE
Value:
1

sl cpc transmit window min size.


SL_CPC_TRANSMIT_WINDOW_MAX_SIZE#

#define SL_CPC_TRANSMIT_WINDOW_MAX_SIZE
Value:
1

sl cpc transmit window max size.