CPC system endpoint secondary part.

License#

Copyright 2019 Silicon Laboratories Inc. www.silabs.com

SPDX-License-Identifier: Zlib

The licensor of this software is Silicon Laboratories Inc.

This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.

Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:

  1. The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.

  2. Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.

  3. This notice may not be removed or altered from any source distribution.

/***************************************************************************/ 
#ifndef SLI_CPC_SYSTEM_SECONDARY_H
#define SLI_CPC_SYSTEM_SECONDARY_H

#include "sl_common.h"
#include "sl_compiler.h"
#include "sli_cpc_system_common.h"
#include "sli_cpc_timer.h"

/***************************************************************************/
#define SLI_CPC_SYSTEM_COMMAND_BUFFER_SIZE \
  (sizeof(sli_cpc_system_cmd_context_t)    \
   - PAYLOAD_LENGTH_MAX                    \
   + SLI_CPC_SYSTEM_COMMAND_PAYLOAD_LENGTH_MAX)

typedef struct sli_cpc_system_endpoint {
  sl_cpc_endpoint_handle_t handle;

  sli_cpc_system_primary_version_t primary_version;

  bool stop_flag;
  bool reset_sequence_done;

  uint32_t enter_irq_end_ms;
  sli_cpc_timer_handle_t enter_irq_timer;

  bool process_uframes_flag;

  uint32_t fc_validation_value;
} sli_cpc_system_endpoint_t;

/***************************************************************************/
typedef struct {
  sli_cpc_system_endpoint_t         *ep;
  void                              *on_complete_arg;
  uint8_t                           ep_id;

  // due to its definition, sli_cpc_system_cmd_t alignment is two bytes,
  // but some casts in the system endpoint expects it to be word-aligned.
  __ALIGNED(4) sli_cpc_system_cmd_t command;
} sli_cpc_system_cmd_context_t;

SL_NORETURN void cpc_system_reset(sli_cpc_system_reboot_mode_t reboot_mode);

sl_cpc_system_status_t cpc_get_reset_reason(void);

void cpc_get_bootloader_info(sli_cpc_system_bootloader_info_t *infos);

/***************************************************************************/
sl_status_t sli_cpc_system_secondary_on_poll(sli_cpc_system_endpoint_t *system_ep,
                                             sli_cpc_system_ep_frame_type_t frame_type,
                                             void *poll_data,
                                             uint32_t poll_data_length, // Rx buffer is freed once this on_poll function return
                                             void **reply_data,
                                             uint32_t *reply_data_length,
                                             sli_cpc_system_cmd_context_t **context);

#endif

Modules#

sli_cpc_system_endpoint

sli_cpc_system_cmd_context_t

Macros#

#define

Each command buffer must be big enough to hold the metadata around the command and the command itself (command_id, seq, length, and payload). Considering PAYLOAD_MAX_LENGTH is already accounted for in sizeof(system_cmd_context), it must be substracted to avoid allocating extra space.

Functions#

SL_NORETURN void
cpc_system_reset(sli_cpc_system_reboot_mode_t reboot_mode)
void
cpc_get_bootloader_info(sli_cpc_system_bootloader_info_t *infos)
sl_status_t
sli_cpc_system_secondary_on_poll(sli_cpc_system_endpoint_t *system_ep, sli_cpc_system_ep_frame_type_t frame_type, void *poll_data, uint32_t poll_data_length, void **reply_data, uint32_t *reply_data_length, sli_cpc_system_cmd_context_t **context)

Macro Definition Documentation#

SLI_CPC_SYSTEM_COMMAND_BUFFER_SIZE#

#define SLI_CPC_SYSTEM_COMMAND_BUFFER_SIZE
Value:
(sizeof(sli_cpc_system_cmd_context_t) \
- PAYLOAD_LENGTH_MAX \
+ SLI_CPC_SYSTEM_COMMAND_PAYLOAD_LENGTH_MAX)

Each command buffer must be big enough to hold the metadata around the command and the command itself (command_id, seq, length, and payload). Considering PAYLOAD_MAX_LENGTH is already accounted for in sizeof(system_cmd_context), it must be substracted to avoid allocating extra space.


Typedef Documentation#

sli_cpc_system_endpoint_t#

typedef struct sli_cpc_system_endpoint sli_cpc_system_endpoint_t

Function Documentation#

cpc_system_reset#

SL_NORETURN void cpc_system_reset (sli_cpc_system_reboot_mode_t reboot_mode)
Parameters
TypeDirectionArgument NameDescription
sli_cpc_system_reboot_mode_tN/Areboot_mode

Reset system; Should not return


cpc_get_reset_reason#

sl_cpc_system_status_t cpc_get_reset_reason (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Get system reset reason.


cpc_get_bootloader_info#

void cpc_get_bootloader_info (sli_cpc_system_bootloader_info_t * infos)
Parameters
TypeDirectionArgument NameDescription
sli_cpc_system_bootloader_info_t *N/Ainfos

Return bootloader informations

Return bootloader


sli_cpc_system_secondary_on_poll#

sl_status_t sli_cpc_system_secondary_on_poll (sli_cpc_system_endpoint_t * system_ep, sli_cpc_system_ep_frame_type_t frame_type, void * poll_data, uint32_t poll_data_length, void ** reply_data, uint32_t * reply_data_length, sli_cpc_system_cmd_context_t ** context)
Parameters
TypeDirectionArgument NameDescription
sli_cpc_system_endpoint_t *N/Asystem_ep
sli_cpc_system_ep_frame_type_tN/Aframe_type
void *N/Apoll_data
uint32_tN/Apoll_data_length
void **N/Areply_data
uint32_t *N/Areply_data_length
sli_cpc_system_cmd_context_t **N/Acontext

Invoked when a frame with the Poll/Final flag is set.

Returns

  • Status code.

Called by CPC core when uframe/poll is received