EMU - Energy Management Unit#

Energy Management Unit (EMU) Peripheral API.

This module contains functions to control the EMU peripheral of Silicon Labs 32-bit MCUs and SoCs. The EMU handles the different low energy modes in Silicon Labs microcontrollers.

Modules#

EMU_EM23Init_TypeDef

EMU_EM4Init_TypeDef

Enumerations#

enum
emuBODMode_Active
emuBODMode_Inactive
}

BOD threshold setting selector, active or inactive mode.

enum
emuEM4Shutoff = 0
emuEM4Hibernate = 1
}

EM4 modes.

enum
emuPinRetentionDisable = EMU_EM4CTRL_EM4IORETMODE_DISABLE
emuPinRetentionEm4Exit = EMU_EM4CTRL_EM4IORETMODE_EM4EXIT
emuPinRetentionLatch = EMU_EM4CTRL_EM4IORETMODE_SWUNLATCH
}

EM4 Pin Retention Type.

enum
emuPowerConfig_DcdcToDvdd
}

Power configurations.

enum
emuVreginCmpThreshold_2v0 = 0
emuVreginCmpThreshold_2v1 = 1
emuVreginCmpThreshold_2v2 = 2
emuVreginCmpThreshold_2v3 = 3
}

VREGIN comparator threshold.

Functions#

void
EMU_EM23Init(const EMU_EM23Init_TypeDef *em23Init)

Update the EMU module with Energy Mode 2 and 3 configuration.

void

Energy mode 2/3 pre-sleep hook function.

void

Energy mode 2/3 post-sleep hook function.

void

EFP's Energy mode 2/3 pre-sleep hook function.

void

EFP's Energy mode 2/3 post-sleep hook function.

void
EMU_EnterEM2(bool restore)

Enter energy mode 2 (EM2).

void
EMU_EnterEM3(bool restore)

Enter energy mode 3 (EM3).

void
EMU_Save(void)

Save the CMU HF clock select state, oscillator enable, and voltage scaling (if available) before EMU_EnterEM2() or EMU_EnterEM3() are called with the restore parameter set to false.

void

Restore CMU HF clock select state, oscillator enable, and voltage scaling (if available) after EMU_EnterEM2() or EMU_EnterEM3() are called with the restore parameter set to false.

void
EMU_EM4Init(const EMU_EM4Init_TypeDef *em4Init)

Update the EMU module with Energy Mode 4 configuration.

void

Energy mode 4 pre-sleep hook function.

void

EFP's Energy mode 4 pre-sleep hook function.

void

Enter energy mode 4 (EM4).

void

Enter energy mode 4 (EM4).

void

Enter energy mode 4 hibernate (EM4H).

void

Enter energy mode 4 shutoff (EM4S).

void
EMU_RamPowerDown(uint32_t start, uint32_t end)

Power down RAM memory blocks.

void

Power up all available RAM memory blocks.

float

Get temperature in degrees Celsius.

void

Executes WFI with required memory barriers.

void

Enter energy mode 1 (EM1).

void
EMU_IntClear(uint32_t flags)

Clear one or more pending EMU interrupts.

void
EMU_IntDisable(uint32_t flags)

Disable one or more EMU interrupts.

void
EMU_IntEnable(uint32_t flags)

Enable one or more EMU interrupts.

uint32_t

Get pending EMU interrupt flags.

uint32_t

Get enabled and pending EMU interrupt flags.

void
EMU_IntSet(uint32_t flags)

Set one or more pending EMU interrupts.

void
EMU_Lock(void)

Lock EMU registers in order to protect them against unintended modification.

void

Unlock the EMU so that writing to locked registers again is possible.

void

When EM4 pin retention is set to emuPinRetentionLatch, then pins are retained through EM4 entry and wakeup.

bool

Temperature measurement ready status.

Macros#

#define

Default initialization of EM2 and 3 configuration.

#define

Default initialization of EM4 configuration (Series 1 without VSCALE).

#define

Zero degrees Celcius in Kelvin.

Enumeration Documentation#

EMU_BODMode_TypeDef#

EMU_BODMode_TypeDef

BOD threshold setting selector, active or inactive mode.

Enumerator
emuBODMode_Active

Configure BOD threshold for active mode.

emuBODMode_Inactive

Configure BOD threshold for inactive mode.


EMU_EM4State_TypeDef#

EMU_EM4State_TypeDef

EM4 modes.

Enumerator
emuEM4Shutoff

EM4 Shutoff.

emuEM4Hibernate

EM4 Hibernate.


EMU_EM4PinRetention_TypeDef#

EMU_EM4PinRetention_TypeDef

EM4 Pin Retention Type.

Enumerator
emuPinRetentionDisable

No Retention: Pads enter reset state when entering EM4.

emuPinRetentionEm4Exit

Retention through EM4: Pads enter reset state when exiting EM4.

emuPinRetentionLatch

Retention through EM4 and wakeup: call EMU_UnlatchPinRetention() to release pins from retention after EM4 wakeup.


EMU_PowerConfig_TypeDef#

EMU_PowerConfig_TypeDef

Power configurations.

DCDC-to-DVDD is currently the only supported mode.

Enumerator
emuPowerConfig_DcdcToDvdd

DCDC is connected to DVDD.


EMU_VreginCmpThreshold_TypeDef#

EMU_VreginCmpThreshold_TypeDef

VREGIN comparator threshold.

Enumerator
emuVreginCmpThreshold_2v0

Comparator threshold is 2.0V.

emuVreginCmpThreshold_2v1

Comparator threshold is 2.1V.

emuVreginCmpThreshold_2v2

Comparator threshold is 2.2V.

emuVreginCmpThreshold_2v3

Comparator threshold is 2.3V.


Function Documentation#

EMU_EM23Init#

void EMU_EM23Init (const EMU_EM23Init_TypeDef * em23Init)

Update the EMU module with Energy Mode 2 and 3 configuration.

Parameters
TypeDirectionArgument NameDescription
const EMU_EM23Init_TypeDef *[in]em23Init

Energy Mode 2 and 3 configuration structure.


EMU_EM23PresleepHook#

void EMU_EM23PresleepHook (void )

Energy mode 2/3 pre-sleep hook function.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function is called by EMU_EnterEM2() and EMU_EnterEM3() functions just prior to execution of the WFI instruction. The function implementation does not perform anything, but it is SL_WEAK so that it can be re- implemented in application code if actions are needed.


EMU_EM23PostsleepHook#

void EMU_EM23PostsleepHook (void )

Energy mode 2/3 post-sleep hook function.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function is called by EMU_EnterEM2() and EMU_EnterEM3() functions just after wakeup from the WFI instruction. The function implementation does not perform anything, but it is SL_WEAK so that it can be re- implemented in application code if actions are needed.


EMU_EFPEM23PresleepHook#

void EMU_EFPEM23PresleepHook (void )

EFP's Energy mode 2/3 pre-sleep hook function.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function is similar to EMU_EM23PresleepHook() but is reserved for EFP usage.

Note

  • The function is primarily meant to be used in systems with EFP circuitry. (EFP = Energy Friendly Pmic (PMIC = Power Management IC)). In such systems there is a need to drive certain signals to EFP pins to notify about energy mode transitions.


EMU_EFPEM23PostsleepHook#

void EMU_EFPEM23PostsleepHook (void )

EFP's Energy mode 2/3 post-sleep hook function.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function is similar to EMU_EM23PostsleepHook() but is reserved for EFP usage.

Note

  • The function is primarily meant to be used in systems with EFP circuitry. (EFP = Energy Friendly Pmic (PMIC = Power Management IC)). In such systems there is a need to drive certain signals to EFP pins to notify about energy mode transitions.


EMU_EnterEM2#

void EMU_EnterEM2 (bool restore)

Enter energy mode 2 (EM2).

Parameters
TypeDirectionArgument NameDescription
bool[in]restore
  • true - save and restore oscillators, clocks and voltage scaling, see function details.

  • false - do not save and restore oscillators and clocks, see function details.

When entering EM2, high-frequency clocks are disabled, i.e., HFXO, HFRCO and AUXHFRCO (for AUXHFRCO, see exception note below). When re-entering EM0, HFRCO is re-enabled and the core will be clocked by the configured HFRCO band. This ensures a quick wakeup from EM2.

However, prior to entering EM2, the core may have been using another oscillator than HFRCO. The restore parameter gives the user the option to restore all HF oscillators according to state prior to entering EM2, as well as the clock used to clock the core. This restore procedure is handled by SW. However, since handled by SW, it will not be restored before completing the interrupt function(s) waking up the core!

Note

  • If restoring core clock to use the HFXO oscillator, which has been disabled during EM2 mode, this function will stall until the oscillator has stabilized. Stalling time can be reduced by adding interrupt support detecting stable oscillator, and an asynchronous switch to the original oscillator. See CMU documentation. Such a feature is however outside the scope of the implementation in this function.

  • If ERRATA_FIX_EMU_E110_ENABLE is active, the core's SLEEPONEXIT feature can not be used.

  • This function is incompatible with the Power Manager module. When the Power Manager module is present, it must be the one deciding at which EM level the device sleeps to ensure the application properly works. Using both at the same time could lead to undefined behavior in the application.

  • If HFXO is re-enabled by this function, and NOT used to clock the core, this function will not wait for HFXO to stabilize. This must be considered by the application if trying to use features relying on that oscillator upon return.

  • If a debugger is attached, the AUXHFRCO will not be disabled if enabled upon entering EM2. It will thus remain enabled when returning to EM0 regardless of the restore parameter.

  • If HFXO autostart and select is enabled by using CMU_HFXOAutostartEnable(), the automatic starting and selecting of the core clocks will be done, regardless of the restore parameter, when waking up on the wakeup sources corresponding to the autostart and select setting.

  • If voltage scaling is supported, the restore parameter is true and the EM0 voltage scaling level is set higher than the EM2 level, then the EM0 level is also restored.

  • On Series 2 Config 2 devices (EFRxG22), this function will also relock the DPLL if the DPLL is used and restore is true.

Note that the hardware will automatically update the HFRCO frequency in the case where voltage scaling is used in EM2/EM3 and not in EM0/EM1. When the restore argument to this function is true then software will restore the original HFRCO frequency after EM2/EM3 wake up. If the restore argument is false then the HFRCO frequency is 19 MHz when coming out of EM2/EM3 and all wait states are at a safe value.

  • The restore option should only be used if all clock control is done via the CMU API.


EMU_EnterEM3#

void EMU_EnterEM3 (bool restore)

Enter energy mode 3 (EM3).

Parameters
TypeDirectionArgument NameDescription
bool[in]restore
  • true - save and restore oscillators, clocks and voltage scaling, see function details.

  • false - do not save and restore oscillators and clocks, see function details.

When entering EM3, the high-frequency clocks are disabled by hardware, i.e., HFXO, HFRCO, and AUXHFRCO (for AUXHFRCO, see exception note below). In addition, the low-frequency clocks, i.e., LFXO and LFRCO are disabled by software. When re-entering EM0, HFRCO is re-enabled and the core will be clocked by the configured HFRCO band. This ensures a quick wakeup from EM3.

However, prior to entering EM3, the core may have been using an oscillator other than HFRCO. The restore parameter gives the user the option to restore all HF/LF oscillators according to state prior to entering EM3, as well as the clock used to clock the core. This restore procedure is handled by software. However, since it is handled by software, it will not be restored before completing the interrupt function(s) waking up the core!

Note

  • If restoring core clock to use an oscillator other than HFRCO, this function will stall until the oscillator has stabilized. Stalling time can be reduced by adding interrupt support detecting stable oscillator, and an asynchronous switch to the original oscillator. See CMU documentation. This feature is, however, outside the scope of the implementation in this function.

  • If ERRATA_FIX_EMU_E110_ENABLE is active, the core's SLEEPONEXIT feature can't be used.

  • This function is incompatible with the Power Manager module. When the Power Manager module is present, it must be the one deciding at which EM level the device sleeps to ensure the application properly works. Using both at the same time could lead to undefined behavior in the application.

  • If HFXO/LFXO/LFRCO are re-enabled by this function, and NOT used to clock the core, this function will not wait for those oscillators to stabilize. This must be considered by the application if trying to use features relying on those oscillators upon return.

  • If a debugger is attached, the AUXHFRCO will not be disabled if enabled upon entering EM3. It will, therefore, remain enabled when returning to EM0 regardless of the restore parameter.

  • If voltage scaling is supported, the restore parameter is true and the EM0 voltage scaling level is set higher than the EM3 level, then the EM0 level is also restored.

  • On Series 2 Config 2 devices (EFRxG22), this function will also relock the DPLL if the DPLL is used and restore is true.

  • The restore option should only be used if all clock control is done via the CMU API.


EMU_Save#

void EMU_Save (void )

Save the CMU HF clock select state, oscillator enable, and voltage scaling (if available) before EMU_EnterEM2() or EMU_EnterEM3() are called with the restore parameter set to false.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Calling this function is equivalent to calling EMU_EnterEM2() or EMU_EnterEM3() with the restore parameter set to true, but it allows the state to be saved without going to sleep. The state can be restored manually by calling EMU_Restore().


EMU_Restore#

void EMU_Restore (void )

Restore CMU HF clock select state, oscillator enable, and voltage scaling (if available) after EMU_EnterEM2() or EMU_EnterEM3() are called with the restore parameter set to false.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Calling this function is equivalent to calling EMU_EnterEM2() or EMU_EnterEM3() with the restore parameter set to true, but it allows the application to evaluate the wakeup reason before restoring state.


EMU_EM4Init#

void EMU_EM4Init (const EMU_EM4Init_TypeDef * em4Init)

Update the EMU module with Energy Mode 4 configuration.

Parameters
TypeDirectionArgument NameDescription
const EMU_EM4Init_TypeDef *[in]em4Init

Energy Mode 4 configuration structure.


EMU_EM4PresleepHook#

void EMU_EM4PresleepHook (void )

Energy mode 4 pre-sleep hook function.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function is called by EMU_EnterEM4() just prior to the sequence of writes to put the device in EM4. The function implementation does not perform anything, but it is SL_WEAK so that it can be re-implemented in application code if actions are needed.


EMU_EFPEM4PresleepHook#

void EMU_EFPEM4PresleepHook (void )

EFP's Energy mode 4 pre-sleep hook function.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function is similar to EMU_EM4PresleepHook() but is reserved for EFP usage.

Note

  • The function is primarily meant to be used in systems with EFP circuitry. (EFP = Energy Friendly Pmic (PMIC = Power Management IC)). In such systems there is a need to drive certain signals to EFP pins to notify about energy mode transitions.


EMU_EnterEM4#

__NO_RETURN void EMU_EnterEM4 (void )

Enter energy mode 4 (EM4).

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function never returns. It waits after the EM4 entry request to make sure the CPU is properly shutdown by calling WFI.

Note

  • Only a power on reset or external reset pin can wake the device from EM4. Device which is configured in Boost DC-DC mode can not enter EM4.


EMU_EnterEM4Wait#

void EMU_EnterEM4Wait (void )

Enter energy mode 4 (EM4).

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function never returns. It waits after the EM4 entry request to make sure the CPU is properly shutdown by calling WFI.

Note

  • Only a power on reset or external reset pin can wake the device from EM4.


EMU_EnterEM4H#

void EMU_EnterEM4H (void )

Enter energy mode 4 hibernate (EM4H).

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function never returns. It waits after the EM4 entry request to make sure the CPU is properly shutdown by calling WFI.

Note

  • Retention of clocks and GPIO in EM4 can be configured using EMU_EM4Init before calling this function.


EMU_EnterEM4S#

void EMU_EnterEM4S (void )

Enter energy mode 4 shutoff (EM4S).

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function never returns. It waits after the EM4 entry request to make sure the CPU is properly shutdown by calling WFI.

Note

  • Retention of clocks and GPIO in EM4 can be configured using EMU_EM4Init before calling this function.


EMU_RamPowerDown#

void EMU_RamPowerDown (uint32_t start, uint32_t end)

Power down RAM memory blocks.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]start

The start address of the RAM region to power down. This address is inclusive.

uint32_t[in]end

The end address of the RAM region to power down. Except for xg27, It can only have two values: 0 or more than RAM0_END. Any other valid RAM address will just do nothing without any error or indication that nothing happened. This address is exclusive. If this parameter is 0, all RAM blocks contained in the region from start to the upper RAM address will be powered down.

This function will power down all the RAM blocks that are within a given range. The RAM block layout is different between device families, so this function can be used in a generic way to power down a RAM memory region which is known to be unused.

This function will power down blocks from start to the end of RAM. For xg27, it will shut off blocks which are completely enclosed by the memory range given by [start, end].

This is an example to power down all RAM blocks except the first one. The first RAM block is special in that it cannot be powered down by the hardware. The size of the first RAM block is device-specific. See the reference manual to find the RAM block sizes.

EMU_RamPowerDown(SRAM_BASE, SRAM_BASE + SRAM_SIZE);

Note

  • The specified memory block(s) will stay off until a call to EMU_RamPowerUp() is done.


EMU_RamPowerUp#

void EMU_RamPowerUp (void )

Power up all available RAM memory blocks.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function will power up all the RAM blocks on a device, this means that the RAM blocks are retained in EM2/EM3. Note that this functionality is not supported on Series 0 devices. Only a reset will power up the RAM blocks on a series 0 device.


EMU_DCDCPowerOff#

bool EMU_DCDCPowerOff (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

EMU_TemperatureGet#

float EMU_TemperatureGet (void )

Get temperature in degrees Celsius.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Temperature in degrees Celsius


EMU_CallWFI#

void EMU_CallWFI (void )

Executes WFI with required memory barriers.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Calls __DSB() and __ISB() before __WFI() to ensure instruction and data synchronization before entering sleep mode.


EMU_EnterEM1#

void EMU_EnterEM1 (void )

Enter energy mode 1 (EM1).

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • This function is incompatible with the Power Manager module. When the Power Manager module is present, it must be the one deciding at which EM level the device sleeps to ensure the application properly works. Using both at the same time could lead to undefined behavior in the application.


EMU_IntClear#

void EMU_IntClear (uint32_t flags)

Clear one or more pending EMU interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

Pending EMU interrupt sources to clear. Use one or more valid interrupt flags for the EMU module (EMU_IFC_nnn or EMU_IF_nnn).


EMU_IntDisable#

void EMU_IntDisable (uint32_t flags)

Disable one or more EMU interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

EMU interrupt sources to disable. Use one or more valid interrupt flags for the EMU module (EMU_IEN_nnn).


EMU_IntEnable#

void EMU_IntEnable (uint32_t flags)

Enable one or more EMU interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

EMU interrupt sources to enable. Use one or more valid interrupt flags for the EMU module (EMU_IEN_nnn).

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using EMU_IntClear() prior to enabling the interrupt.


EMU_IntGet#

uint32_t EMU_IntGet (void )

Get pending EMU interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Event bits are not cleared by the use of this function.

Returns

  • EMU interrupt sources pending. Returns one or more valid interrupt flags for the EMU module (EMU_IF_nnn).


EMU_IntGetEnabled#

uint32_t EMU_IntGetEnabled (void )

Get enabled and pending EMU interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Interrupt flags are not cleared by the use of this function.

Returns

  • Pending and enabled EMU interrupt sources Return value is the bitwise AND of

    • the enabled interrupt sources in EMU_IEN and

    • the pending interrupt flags EMU_IF.


EMU_IntSet#

void EMU_IntSet (uint32_t flags)

Set one or more pending EMU interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

EMU interrupt sources to set to pending. Use one or more valid interrupt flags for the EMU module (EMU_IFS_nnn).


EMU_Lock#

void EMU_Lock (void )

Lock EMU registers in order to protect them against unintended modification.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • If locking EMU registers, they must be unlocked prior to using any EMU API functions modifying EMU registers, excluding interrupt control and regulator control if the architecture has a EMU_PWRCTRL register. An exception to this is the energy mode entering API (EMU_EnterEMn()), which can be used when the EMU registers are locked.


EMU_Unlock#

void EMU_Unlock (void )

Unlock the EMU so that writing to locked registers again is possible.

Parameters
TypeDirectionArgument NameDescription
voidN/A

EMU_UnlatchPinRetention#

void EMU_UnlatchPinRetention (void )

When EM4 pin retention is set to emuPinRetentionLatch, then pins are retained through EM4 entry and wakeup.

Parameters
TypeDirectionArgument NameDescription
voidN/A

The pin state is released by calling this function. The feature allows peripherals or GPIO to be re-initialized after EM4 exit (reset), and when initialization is done, this function can release pins and return control to the peripherals or GPIO.


EMU_TemperatureReady#

bool EMU_TemperatureReady (void )

Temperature measurement ready status.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • True if temperature measurement is ready


Macro Definition Documentation#

EMU_EM23INIT_DEFAULT#

#define EMU_EM23INIT_DEFAULT
Value:
{ \
false, /* Reduced voltage regulator drive strength in EM2/3.*/ \
}

Default initialization of EM2 and 3 configuration.


EMU_EM4INIT_DEFAULT#

#define EMU_EM4INIT_DEFAULT
Value:
{ \
false, /* Retain LFXO configuration upon EM4 entry. */ \
false, /* Retain LFRCO configuration upon EM4 entry. */ \
false, /* Retain ULFRCO configuration upon EM4 entry. */ \
emuEM4Shutoff, /* Use EM4 shutoff state. */ \
emuPinRetentionDisable, /* Do not retain pins in EM4. */ \
}

Default initialization of EM4 configuration (Series 1 without VSCALE).


EMU_TEMP_ZERO_C_IN_KELVIN#

#define EMU_TEMP_ZERO_C_IN_KELVIN
Value:
(273.15f)

Zero degrees Celcius in Kelvin.