Utilities#
Device initialisation, debug lock, upgrade functionality, user data...
API for managing the Secure Engine or Root code on a device. Upload and read device configuration.
Modules#
Enumerations#
Lifecycle event flags keep track of certain events and state changes by setting a one-time irreversible flag in the OTP.
OTP key types.
Typedefs#
SE tamper signal levels.
SE tamper signals.
SE tamper filter timeout period.
Number of tamper counts to trigger the filter signal.
SE certificate types.
SE Debug lock flags.
SE challenge storage.
Functions#
Validate SE firmware image.
Apply SE firmware image.
Get upgrade status of SE firmware image.
Validate Host firmware image.
Apply Host firmware image.
Get upgrade status of Host firmware image.
Initialize key to be stored in the SE OTP flash.
Read a public key stored in the SE.
Initialize and commit SE OTP configuration to OTP.
Read the OTP firmware version of the SE module.
Read SE OTP configuration.
Read the SE firmware version.
Returns the current debug lock configuration.
Enables the debug lock for the part.
Writes data to User Data section in MTP.
Retrieves the data from the user data section in MTP.
Returns the number of remaining writes to the user data section in MTP that can be performed before the static token data write limit is reached.
Returns the current boot status, versions and system configuration.
Read the serial number of the SE module.
Read the EMU->RSTCAUSE after a tamper reset.
Read the latest cached tamper reset cause.
Reads out traceable lifecycle event flags from the OTP.
Utility for checking if a certain lifecycle event flag is set.
Enables the secure debug functionality.
Disables the secure debug functionality.
Set debug options.
Performs a device mass erase and debug unlock.
Disabled device erase functionality.
Request challenge from SE which can be used to open debug access.
Invalidate current challenge and make a new challenge.
Unlock debug access using certificate and signed challenge.
Temporarily disable tamper configuration using certificate and signed challenge.
Read size of stored certificates in SE.
Read stored certificates in SE.
Enter SE active mode.
Exit SE active mode.
Read the OTP rollback counter.
Increment the OTP rollback counter.
Reads back the stored upgrade file version.
Records a new upgrade file version.
Macros#
Size of the USER_DATA element.
Default configuration for OTP initialisation structure.
SE Challenge size.
Certificate key size.
Certificate signature size.
Batch ID certificate.
SE ID certificate.
Host ID certificate.
Enumeration Documentation#
sl_se_lifecycle_event_flag_t#
sl_se_lifecycle_event_flag_t
Lifecycle event flags keep track of certain events and state changes by setting a one-time irreversible flag in the OTP.
This enum contains information on what the separate event flags indicate. The lifecycle state flags can be fetched using sl_se_get_lifecycle_event_flags. The utility sl_se_lifecycle_event_flag_is_set can be used to check if any specific flag has been set.
| Enumerator | |
|---|---|
| SL_SE_LIFECYCLE_EVENT_HOST_UNSECURE_UNLOCKED | Host has been unsecure-unlocked. |
| SL_SE_LIFECYCLE_EVENT_HOST_SECURE_UNLOCKED | Host has been secure-unlocked. |
| SL_SE_LIFECYCLE_EVENT_SE_SECURE_UNLOCKED | SE has been secure-unlocked. |
| SL_SE_LIFECYCLE_EVENT_INITIAL_DEBUG_LOCK_SET | Initial debug lock token has been set in MTP. |
| SL_SE_LIFECYCLE_EVENT_HOST_SECURE_DEBUG_ENABLED | Host secure debug has been enabled. |
| SL_SE_LIFECYCLE_EVENT_HOST_SECURE_DEBUG_DISABLED | Host secure debug has been disabled. |
| SL_SE_LIFECYCLE_EVENT_HOST_DEBUG_LOCKED | Host has been debug locked. |
| SL_SE_LIFECYCLE_EVENT_AXIP_NONCE_ROLL_DISABLED | AXiP nonce rolling has been disabled. |
sl_se_device_key_type_t#
sl_se_device_key_type_t
OTP key types.
| Enumerator | |
|---|---|
| SL_SE_KEY_TYPE_IMMUTABLE_BOOT | |
| SL_SE_KEY_TYPE_IMMUTABLE_AUTH | |
| SL_SE_KEY_TYPE_IMMUTABLE_AES_128 | |
| SL_SE_KEY_TYPE_IMMUTABLE_ATTESTATION | |
| SL_SE_KEY_TYPE_IMMUTABLE_SE_ATTESTATION | |
Typedef Documentation#
sl_se_tamper_filter_period_t#
typedef uint8_t sl_se_tamper_filter_period_t
SE tamper filter timeout period.
sl_se_tamper_filter_threshold_t#
typedef uint8_t sl_se_tamper_filter_threshold_t
Number of tamper counts to trigger the filter signal.
sl_se_challenge_t#
typedef uint8_t sl_se_challenge_t[SL_SE_CHALLENGE_SIZE] [SL_SE_CHALLENGE_SIZE]
SE challenge storage.
Function Documentation#
sl_se_check_se_image#
sl_status_t sl_se_check_se_image (sl_se_command_context_t * cmd_ctx, void * image_addr)
Validate SE firmware image.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| void * | [in] | image_addr | Pointer to SE image to validate. |
Validate SE firmware image located at given address. This function is typically used before calling sl_se_apply_se_image.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_apply_se_image#
sl_status_t sl_se_apply_se_image (sl_se_command_context_t * cmd_ctx, void * image_addr)
Apply SE firmware image.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| void * | [in] | image_addr | Pointer to SE image to apply. |
Apply SE firmware image located at given address.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_get_upgrade_status_se_image#
sl_status_t sl_se_get_upgrade_status_se_image (sl_se_command_context_t * cmd_ctx, uint32_t * status, uint32_t * prev_version)
Get upgrade status of SE firmware image.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| uint32_t * | [in] | status | Pointer to 32-bit word where to return upgrade status. |
| uint32_t * | [in] | prev_version | Pointer to 32-bit word where to return previous version. |
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_check_host_image#
sl_status_t sl_se_check_host_image (sl_se_command_context_t * cmd_ctx, void * image_addr, uint32_t size)
Validate Host firmware image.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| void * | [in] | image_addr | Pointer to Host image to validate. |
| uint32_t | [in] | size | Size of Host image to validate. |
Validate Host firmware image located at given address. This function is typically used before calling sl_se_apply_host_image.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_apply_host_image#
sl_status_t sl_se_apply_host_image (sl_se_command_context_t * cmd_ctx, void * image_addr, uint32_t size)
Apply Host firmware image.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| void * | [in] | image_addr | Pointer to Host image to apply. |
| uint32_t | [in] | size | Size of Host image to apply. |
Apply Host firmware image located at given address.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_get_upgrade_status_host_image#
sl_status_t sl_se_get_upgrade_status_host_image (sl_se_command_context_t * cmd_ctx, uint32_t * status, uint32_t * prev_version)
Get upgrade status of Host firmware image.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| uint32_t * | [in] | status | Pointer to 32-bit word where to return upgrade status. |
| uint32_t * | [in] | prev_version | Pointer to 32-bit word where to return previous version. |
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_init_otp_key#
sl_status_t sl_se_init_otp_key (sl_se_command_context_t * cmd_ctx, sl_se_device_key_type_t key_type, void * key, uint32_t num_bytes)
Initialize key to be stored in the SE OTP flash.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| sl_se_device_key_type_t | [in] | key_type | ID of key type to initialize. |
| void * | [in] | key | Pointer to a buffer that contains the key. Public keys must be word aligned and have a length of 64 bytes. AES-128 keys must be word aligned and have length of 16 bytes. |
| uint32_t | [in] | num_bytes | Length of key buffer in bytes (16 or 64 bytes). |
Initialize key stored in the SE. The command can be used to write (sl_se_device_key_type_t):
SL_SE_KEY_TYPE_IMMUTABLE_BOOT
SL_SE_KEY_TYPE_IMMUTABLE_AUTH
SL_SE_KEY_TYPE_IMMUTABLE_AES_128
Note
These keys can not be overwritten, so this command can only be issued once per key per part.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_read_pubkey#
sl_status_t sl_se_read_pubkey (sl_se_command_context_t * cmd_ctx, sl_se_device_key_type_t key_type, void * key, uint32_t num_bytes)
Read a public key stored in the SE.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| sl_se_device_key_type_t | [in] | key_type | ID of key type to read. |
| void * | [out] | key | Pointer to a buffer to contain the returned public key. Must be word aligned and have a length of 64 bytes. |
| uint32_t | [in] | num_bytes | Length of pubkey buffer (64 bytes). |
Read out a public key stored in the SE. The command can be used to read (sl_se_device_key_type_t):
SL_SE_KEY_TYPE_IMMUTABLE_BOOT
SL_SE_KEY_TYPE_IMMUTABLE_AUTH
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_init_otp#
sl_status_t sl_se_init_otp (sl_se_command_context_t * cmd_ctx, sl_se_otp_init_t * otp_init)
Initialize and commit SE OTP configuration to OTP.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| sl_se_otp_init_t * | [in] | otp_init | Pointer to OTP initialization structure. |
Warnings
When this function succeeds the configuration is committed to OTP and cannot be changed.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passedSL_STATUS_ABORTwhen the operation is not attempted.
sl_se_get_otp_version#
sl_status_t sl_se_get_otp_version (sl_se_command_context_t * cmd_ctx, uint32_t * version)
Read the OTP firmware version of the SE module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| uint32_t * | [out] | version | Pointer to uint32_t word where version shall be returned. |
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognizedSL_STATUS_INVALID_CREDENTIALSwhen the command is not authorizedSL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_read_otp#
sl_status_t sl_se_read_otp (sl_se_command_context_t * cmd_ctx, sl_se_otp_init_t * otp_settings)
Read SE OTP configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| sl_se_otp_init_t * | [out] | otp_settings | Pointer to OTP initialization structure. |
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_COMMANDif OTP configuration isn't initializedSL_STATUS_ABORTwhen the operation is not attempted.
sl_se_get_se_version#
sl_status_t sl_se_get_se_version (sl_se_command_context_t * cmd_ctx, uint32_t * version)
Read the SE firmware version.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| uint32_t * | [out] | version | Pointer to uint32_t word where version shall be returned. |
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_OWNERSHIPwhen the ownership is already takenSL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognizedSL_STATUS_INVALID_CREDENTIALSwhen the command is not authorizedSL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_get_debug_lock_status#
sl_status_t sl_se_get_debug_lock_status (sl_se_command_context_t * cmd_ctx, sl_se_debug_status_t * status)
Returns the current debug lock configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| sl_se_debug_status_t * | [out] | status | Pointer to sl_se_debug_status_t structure to be filled out with the current status of the debug configuration. |
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_apply_debug_lock#
sl_status_t sl_se_apply_debug_lock (sl_se_command_context_t * cmd_ctx)
Enables the debug lock for the part.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
The debug port will be closed and the only way to open it is through device erase (if enabled) or through secure debug unlock (if enabled).
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfully
sl_se_write_user_data#
sl_status_t sl_se_write_user_data (sl_se_command_context_t * cmd_ctx, const void * data, size_t num_bytes)
Writes data to User Data section in MTP.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| const void * | [in] | data | Data to write to flash. |
| size_t | [in] | num_bytes | Number of bytes to write to flash. NB: Must be equal to SL_SE_USER_DATA_SIZE size |
The full MTP element is written every time, so length of write data (num_bytes) must always be equal to SL_SE_USER_DATA_SIZE.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_get_user_data#
sl_status_t sl_se_get_user_data (sl_se_command_context_t * cmd_ctx, void * output_data, size_t num_bytes)
Retrieves the data from the user data section in MTP.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| void * | [out] | output_data | Data to write to flash. Must be large enough to contain SL_SE_USER_DATA_SIZE bytes |
| size_t | [in] | num_bytes | Number of bytes to read from flash, NB: Must be equal to SL_SE_USER_DATA_SIZE size |
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passedSL_STATUS_NOT_INITIALIZEDif element is empty/unwritten
sl_se_get_user_data_remaining_writes#
sl_status_t sl_se_get_user_data_remaining_writes (sl_se_command_context_t * cmd_ctx, uint32_t * remaining_writes)
Returns the number of remaining writes to the user data section in MTP that can be performed before the static token data write limit is reached.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| uint32_t * | [out] | remaining_writes | Pointer to uint32_t word where remaining writes shall be returned. |
The write limit is enforced by the SE module and cannot be exceeded. The limit is enforced to ensure OTP bit consumption is not exceeded. See sli_se_write_user_data_force for more details.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_get_status#
sl_status_t sl_se_get_status (sl_se_command_context_t * cmd_ctx, sl_se_status_t * status)
Returns the current boot status, versions and system configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| sl_se_status_t * | [out] | status | SE_Status_t containing current SE status. |
Returns
One of the following sl_status_t codes:
SL_STATUS_OKupon command completion. Errors are encoded in the different parts of the returned status object.SL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognizedSL_STATUS_INVALID_CREDENTIALSwhen the command is not authorizedSL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_get_serialnumber#
sl_status_t sl_se_get_serialnumber (sl_se_command_context_t * cmd_ctx, void * serial)
Read the serial number of the SE module.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| void * | [out] | serial | Pointer to array of size 16 bytes. |
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognizedSL_STATUS_INVALID_CREDENTIALSwhen the command is not authorizedSL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_get_reset_cause#
sl_status_t sl_se_get_reset_cause (sl_se_command_context_t * cmd_ctx, uint32_t * reset_cause)
Read the EMU->RSTCAUSE after a tamper reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| uint32_t * | [out] | reset_cause | Pointer to uint32_t word where reset cause shall be returned. |
This function should be called if EMU->RSTCAUSE has been cleared upon boot.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognized
sl_se_get_tamper_reset_cause#
sl_status_t sl_se_get_tamper_reset_cause (sl_se_command_context_t * cmd_ctx, bool * was_tamper_reset, uint32_t * reset_cause)
Read the latest cached tamper reset cause.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| bool * | [out] | was_tamper_reset | Pointer to bool that indicates if a tamper event occurred. If the cached value is 0 this will be false, true otherwise. |
| uint32_t * | [out] | reset_cause | Pointer to a uint32_t where the cached reset cause value should be returned. |
The returned value is the index of the tamper source that caused a reset. Requires SE version 2.2.1 or above.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognizedSL_STATUS_INVALID_PARAMETERwhen cmd_ctx or reset_cause is NULL
sl_se_get_lifecycle_event_flags#
sl_status_t sl_se_get_lifecycle_event_flags (sl_se_command_context_t * cmd_ctx, uint64_t * event_flags)
Reads out traceable lifecycle event flags from the OTP.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| uint64_t * | [out] | event_flags | Pointer to an array of at least 8 bytes, to contain the trace flags |
See sl_se_lifecycle_event_flag_t for details on what the individual flag bits indicate.
Returns
SL_STATUS_OK upon successfull execution, error code elsewise
sl_se_lifecycle_event_flag_is_set#
bool sl_se_lifecycle_event_flag_is_set (uint64_t * flags, sl_se_lifecycle_event_flag_t flag_index)
Utility for checking if a certain lifecycle event flag is set.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint64_t * | [in] | flags | Pointer to an 8 byte array of lifecycle event flags (event_flags from sl_se_get_lifecycle_event_flags) |
| sl_se_lifecycle_event_flag_t | [in] | flag_index | Which bit (event flag) to check if is set |
Returns
true if event flag bit was set false if event flag bit was not set
sl_se_enable_secure_debug#
sl_status_t sl_se_enable_secure_debug (sl_se_command_context_t * cmd_ctx)
Enables the secure debug functionality.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
Enables the secure debug functionality that can be used to open a locked debug port through the Get challenge and Open debug commands. This command can only be executed before the debug port is locked, and after a secure debug public key has been installed in the SE.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfully
sl_se_disable_secure_debug#
sl_status_t sl_se_disable_secure_debug (sl_se_command_context_t * cmd_ctx)
Disables the secure debug functionality.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
Disables the secure debug functionality that can be used to open a locked debug port.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfully
sl_se_set_debug_options#
sl_status_t sl_se_set_debug_options (sl_se_command_context_t * cmd_ctx, const sl_se_debug_options_t * debug_options)
Set debug options.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| const sl_se_debug_options_t * | [in] | debug_options | Pointer to debug options structure. |
This function makes it possible to configure the Trust-Zone access permissions of the debug interface. For details please refer to sl_se_debug_options_t.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfully
sl_se_erase_device#
sl_status_t sl_se_erase_device (sl_se_command_context_t * cmd_ctx)
Performs a device mass erase and debug unlock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
Performs a device mass erase and resets the debug configuration to its initial unlocked state. Only available before DEVICE_ERASE_DISABLE has been executed.
Note
This command clears and verifies the complete flash and ram of the system, excluding the user data pages and one-time programmable commissioning information in the secure engine.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_COMMANDif device erase is disabled.
sl_se_disable_device_erase#
sl_status_t sl_se_disable_device_erase (sl_se_command_context_t * cmd_ctx)
Disabled device erase functionality.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
This command disables the device erase command. It does not lock the debug interface to the part, but it is a permanent action for the part. If device erase is disabled and the device is debug locked, there is no way to permanently unlock the part. If secure debug unlock is enabled, secure debug unlock can still be used to temporarily open the debug port.
Warnings
This command permanently disables the device erase functionality!
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfully
sl_se_get_challenge#
sl_status_t sl_se_get_challenge (sl_se_command_context_t * cmd_ctx, sl_se_challenge_t challenge)
Request challenge from SE which can be used to open debug access.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| sl_se_challenge_t | [out] | challenge | SE challenge storage. |
This command requests a challenge (16 bytes) which can be used to generate a certificate in order to open debug access, sl_se_open_debug.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_roll_challenge#
sl_status_t sl_se_roll_challenge (sl_se_command_context_t * cmd_ctx)
Invalidate current challenge and make a new challenge.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
This command requests the SE to invalidate it's current challenge (16bytes) and generate a new challenge.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfully
sl_se_open_debug#
sl_status_t sl_se_open_debug (sl_se_command_context_t * cmd_ctx, void * cert, uint32_t len, const sl_se_debug_options_t * debug_options)
Unlock debug access using certificate and signed challenge.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| void * | [in] | cert | Certificate for debug unlock and signed challenge. |
| uint32_t | [in] | len | Length of certificate in number of bytes. |
| const sl_se_debug_options_t * | [in] | debug_options | Debug options to open/unlock. |
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognizedSL_STATUS_INVALID_CREDENTIALSwhen the command is not authorizedSL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_disable_tamper#
sl_status_t sl_se_disable_tamper (sl_se_command_context_t * cmd_ctx, void * cert, uint32_t len, sl_se_tamper_signals_t tamper_signals)
Temporarily disable tamper configuration using certificate and signed challenge.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| void * | [in] | cert | Certificate for disabling tamper and signed challenge. |
| uint32_t | [in] | len | Length of certificate in number of bytes. |
| sl_se_tamper_signals_t | [in] | tamper_signals | Tamper signals to disable. Each signal represented by a bit. |
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_OPERATIONwhen the SE command ID is not recognizedSL_STATUS_INVALID_CREDENTIALSwhen the command is not authorizedSL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passed
sl_se_read_cert_size#
sl_status_t sl_se_read_cert_size (sl_se_command_context_t * cmd_ctx, sl_se_cert_size_type_t * cert_size)
Read size of stored certificates in SE.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| sl_se_cert_size_type_t * | [inout] | cert_size | Size of the certificates stored in SE. |
Returns
Status code, sl_status.h.
sl_se_read_cert#
sl_status_t sl_se_read_cert (sl_se_command_context_t * cmd_ctx, sl_se_cert_type_t cert_type, void * cert, uint32_t num_bytes)
Read stored certificates in SE.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| sl_se_cert_type_t | [in] | cert_type | Type of the certificate stored in SE. |
| void * | [inout] | cert | Buffer to read certificate. |
| uint32_t | [in] | num_bytes | Length of certificate in number of bytes. |
Returns
Status code, sl_status_t
sl_se_enter_active_mode#
sl_status_t sl_se_enter_active_mode (sl_se_command_context_t * cmd_ctx)
Enter SE active mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
SE will enter active mode. This will ensure SE is not powered down between operations, at the expense of increased power consumption.
Warnings
Active mode will prevent entry to EM2/3/4. To allow energy mode entry, exit active mode through sl_se_exit_active_mode().
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passedSL_STATUS_COMMAND_IS_INVALIDwhen already in active mode
sl_se_exit_active_mode#
sl_status_t sl_se_exit_active_mode (sl_se_command_context_t * cmd_ctx)
Exit SE active mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
SE will exit active mode.
Returns
One of the following sl_status_t codes:
SL_STATUS_OKwhen the command was executed successfullySL_STATUS_INVALID_PARAMETERwhen an invalid parameter was passedSL_STATUS_COMMAND_IS_INVALIDwhen already not in active mode
sl_se_get_rollback_counter#
sl_status_t sl_se_get_rollback_counter (sl_se_command_context_t * cmd_ctx, uint32_t * rollback_counter)
Read the OTP rollback counter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| uint32_t * | [out] | rollback_counter | Pointer to location where the rollback counter value will be returned. |
Returns
SL_STATUS_OK when the function executed successfully, else, a status code of type sl_status_t that indicates why the function was not successful, sl_status_t
sl_se_increment_rollback_counter#
sl_status_t sl_se_increment_rollback_counter (sl_se_command_context_t * cmd_ctx, uint32_t * rollback_counter)
Increment the OTP rollback counter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| uint32_t * | [out] | rollback_counter | Optional: Retrieve the rollback counter count after increment Set to NULL to ignore |
Returns
SL_STATUS_OK when the function executed successfully, else, a status code of type sl_status_t that indicates why the function was not successful, sl_status_t
sl_se_get_upgrade_file_version#
sl_status_t sl_se_get_upgrade_file_version (sl_se_command_context_t * cmd_ctx, uint32_t * version)
Reads back the stored upgrade file version.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| uint32_t * | [out] | version | The stored upgrade file version. |
Returns
SL_STATUS_OK when the function executed successfully, else, a status code of type sl_status_t that indicates why the function was not successful, sl_status_t
sl_se_set_upgrade_file_version#
sl_status_t sl_se_set_upgrade_file_version (sl_se_command_context_t * cmd_ctx, uint32_t version)
Records a new upgrade file version.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_se_command_context_t * | [in] | cmd_ctx | Pointer to an SE command context object. |
| uint32_t | [in] | version | New upgrade file version |
Returns
SL_STATUS_OK when the function executed successfully, else, a status code of type sl_status_t that indicates why the function was not successful, sl_status_t
Macro Definition Documentation#
SL_SE_OTP_INIT_DEFAULT#
#define SL_SE_OTP_INIT_DEFAULTValue:
Default configuration for OTP initialisation structure.