// Gecko Platform//Version 4.4.1 //Services ... /modified in a date format sl_sleeptimer_date_t. API : sl_status_t sl_sleeptimer_get_datetime(sl_ ... sl_sleeptimer_ms_to_tick(uint16_t time_ms)
... PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... Configure sl_se_command_context_t with sl_se_set_yield to yield the CPU core when the SE ...
Training ... 4.4.4 Gecko Platform# Gecko Platform is the common foundation for the Gecko SDK Suite. ... Table of Contents Gecko Platform Gecko Platform Components Version HistorySupportAbout ...