Silicon Labs
gecko-platform/hardware-driver/api/group-imu-fusion
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
Results 1-5 of 5 for gecko-platform/hardware-driver/api/group-imu-fusion in 0.60 seconds
Project Configurator and Gecko Platform
https://www.silabs.com/.../project-configuration-gecko-platform-training....
Driver for the Silicon Labs Si1133 ambient light and UV sensor ... Driver for the Silicon Labs Si7210 Hall effect sensor ... Platform Services Detail Device Initialization
Sleep Timer | API Documentation | Gecko Platform | v4.4.1 | Silicon Labs
https://docs.silabs.com/.../sleepti...
// Gecko Platform//Version 4.4.1 //Services ... The hardware timer peripheral must be properly clocked from the application. ... All API functions can be called from within interrupt handlers.
I/O Stream RTT - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-iostream-...
You are viewing documentation for version: 4.2 | Version History ... The control block references a ring buffer for each configured channel. ... You should avoid using it in production.
ProductMicrocontrollers Resource TypeSoftware API documentation
SE Manager | API Documentation | Platform | v5.0.1 | Silicon Labs
https://docs.silabs.com/.../sl-se-mana...
Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... Hardware block inside the SE used for generating random numbers.
AN1247: Anti-Tamper Protection Configuration and Use
https://www.silabs.com/.../an1247-efr32-secure-vault-tamper....
The SE Manager API document can be found at https://docs.silabs.com/gecko-platform/latest/service/api/group-sl-se-manager. ... (Note that this API is not available for EFR32xG21B-based parts).
Resource TypeApplication Notes
    Results 1-5 of 5 for gecko-platform/hardware-driver/api/group-imu-fusion