//API Reference //BGAPI headers You are viewing documentation for version: 3.3 BGAPI# BGAPI message header format# ... BGAPI protocol stores data in little endian. ... 0x06 3 GATT Database
// Bluetooth LE//Version 3.2 //API Reference ... Only (maximum BGAPI payload size - 3) amount of data can be read at once. ... See Bluetooth specification Vol 3, Part G, 7.2 for the values.
... at line 1249 of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h ... Bluetooth identity address in little endian format
... at line 1249 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h ... Bluetooth identity address in little endian format