Description Version API. Macros specifying the EMLIB and CMSIS version. ... #define _EMLIB_VERSION_PATCH 0 #define _CMSIS_VERSION 5.3.0 Version number of targeted CMSIS package.
ProductMicrocontrollersResource TypeSoftware API documentation
Core API, inititalizing of SE Manager and SE command context (Core) ... Configure sl_se_command_context_t with sl_se_set_yield to yield the CPU core when the SE Manager is waiting for the ...
You should avoid using it in production. ... sl_iostream_rtt_handle sl_iostream_instance_info_t sl_iostream_instance_rtt_info ... sl_iostream_instance_info_t sl_iostream_instance_rtt_info
ProductMicrocontrollersResource TypeSoftware API documentation
command (4 bytes) Tamper disable mask (4 bytes) Access certificate (156 bytes) ... 1.The value allows all debug options to be reset for secure debug. ... Private Command Key 3 Signed by
Resource TypeApplication Notes
Results 1-6 of 6 for gecko-platform/latest/emlib/api/efm32gg/struct-d-a-c-init-channel-type-def