EMU - Energy Management Unit
Description
Energy Management Unit (EMU) Peripheral API.
This module contains functions to control the EMU peripheral of Silicon Labs 32-bit MCUs and SoCs. The EMU handles the different low energy modes in Silicon Labs microcontrollers.
Data Structures | |
struct | EMU_EM01Init_TypeDef |
EM0 and 1 initialization structure. | |
struct | EMU_EM23Init_TypeDef |
EM2 and 3 initialization structure. | |
struct | EMU_EM4Init_TypeDef |
EM4 initialization structure. | |
struct | EMU_BUInit_TypeDef |
Backup Power Domain Initialization structure. | |
struct | EMU_DCDCInit_TypeDef |
DCDC initialization structure. | |
struct | EMU_VmonInit_TypeDef |
VMON initialization structure. | |
struct | EMU_VmonHystInit_TypeDef |
VMON Hysteresis initialization structure. | |
Functions | |
void | EMU_EM01Init (const EMU_EM01Init_TypeDef *em01Init) |
Update the EMU module with Energy Mode 0 and 1 configuration. | |
void | EMU_EM23Init (const EMU_EM23Init_TypeDef *em23Init) |
Update the EMU module with Energy Mode 2 and 3 configuration. | |
void | EMU_EM23PresleepHook (void) |
Energy mode 2/3 pre-sleep hook function. | |
void | EMU_EM23PostsleepHook (void) |
Energy mode 2/3 post-sleep hook function. | |
void | EMU_EFPEM23PresleepHook (void) |
EFP's Energy mode 2/3 pre-sleep hook function. | |
void | EMU_EFPEM23PostsleepHook (void) |
EFP's Energy mode 2/3 post-sleep hook function. | |
void | EMU_EnterEM2 (bool restore) |
Enter energy mode 2 (EM2). | |
void | EMU_EnterEM3 (bool restore) |
Enter energy mode 3 (EM3). | |
void | EMU_Save (void) |
Save the CMU HF clock select state, oscillator enable, and voltage scaling (if available) before EMU_EnterEM2() or EMU_EnterEM3() are called with the restore parameter set to false. | |
void | EMU_Restore (void) |
Restore CMU HF clock select state, oscillator enable, and voltage scaling (if available) after EMU_EnterEM2() or EMU_EnterEM3() are called with the restore parameter set to false. | |
void | EMU_EM4Init (const EMU_EM4Init_TypeDef *em4Init) |
Update the EMU module with Energy Mode 4 configuration. | |
void | EMU_EM4PresleepHook (void) |
Energy mode 4 pre-sleep hook function. | |
void | EMU_EFPEM4PresleepHook (void) |
EFP's Energy mode 4 pre-sleep hook function. | |
void | EMU_EnterEM4 (void) |
Enter energy mode 4 (EM4). | |
void | EMU_EnterEM4H (void) |
Enter energy mode 4 hibernate (EM4H). | |
void | EMU_EnterEM4S (void) |
Enter energy mode 4 shutoff (EM4S). | |
void | EMU_MemPwrDown (uint32_t blocks) |
Power down memory block. | |
void | EMU_RamPowerDown (uint32_t start, uint32_t end) |
Power down RAM memory blocks. | |
void | EMU_RamPowerUp (void) |
Power up all available RAM memory blocks. | |
void | EMU_PeripheralRetention (EMU_PeripheralRetention_TypeDef periMask, bool enable) |
Set EM2 3 peripheral retention control. | |
void | EMU_UpdateOscConfig (void) |
Update EMU module with CMU oscillator selection/enable status. | |
void | EMU_VScaleEM01ByClock (uint32_t clockFrequency, bool wait) |
Voltage scale in EM0 and 1 by clock frequency. | |
void | EMU_VScaleEM01 (EMU_VScaleEM01_TypeDef voltage, bool wait) |
Force voltage scaling in EM0 and 1 to a specific voltage level. | |
void | EMU_BUInit (const EMU_BUInit_TypeDef *buInit) |
Configure Backup Power Domain settings. | |
void | EMU_BUDisMaxCompSet (bool disableMainBuComparator) |
Disable Main Backup Power Domain comparator. | |
void | EMU_BUBuInactPwrConSet (EMU_BUBuInactPwrCon_TypeDef inactPwrCon) |
Configure power connection configuration when not in Backup mode. | |
void | EMU_BUBuActPwrConSet (EMU_BUBuActPwrCon_TypeDef actPwrCon) |
Configure power connection configuration when in Backup mode. | |
void | EMU_BUPwrResSet (EMU_BUPwrRes_TypeDef pwrRes) |
Power domain resistor selection. | |
void | EMU_BUVoutResSet (EMU_BUVoutRes_TypeDef resistorSel) |
B_VOUT resistor select. | |
void | EMU_BUBuVinProbeEnSet (bool enable) |
Enable BU_VIN probing. | |
void | EMU_BUStatEnSet (bool enable) |
Enable backup mode status export. | |
void | EMU_BUEnableSet (bool enable) |
Enable backup mode. | |
void | EMU_DCDCModeSet (EMU_DcdcMode_TypeDef dcdcMode) |
Set DCDC regulator operating mode. | |
bool | EMU_DCDCInit (const EMU_DCDCInit_TypeDef *dcdcInit) |
Configure the DCDC regulator. | |
void | EMU_DCDCModeEM23Set (EMU_DcdcModeEM23_TypeDef dcdcModeEM23) |
Set DCDC Mode EM23 operating mode. | |
void | EMU_DCDCConductionModeSet (EMU_DcdcConductionMode_TypeDef conductionMode, bool rcoDefaultSet) |
Set DCDC LN regulator conduction mode. | |
bool | EMU_DCDCOutputVoltageSet (uint32_t mV, bool setLpVoltage, bool setLnVoltage) |
Set the DCDC output voltage. | |
void | EMU_DCDCOptimizeSlice (uint32_t em0LoadCurrentmA) |
Optimize the DCDC slice count based on the estimated average load current in EM0. | |
void | EMU_DCDCLnRcoBandSet (EMU_DcdcLnRcoBand_TypeDef band) |
Set DCDC Low-noise RCO band. | |
void | EMU_VmonInit (const EMU_VmonInit_TypeDef *vmonInit) |
Initialize a VMON channel. | |
void | EMU_VmonHystInit (const EMU_VmonHystInit_TypeDef *vmonInit) |
Initialize a VMON channel with hysteresis (separate rise and fall triggers). | |
void | EMU_VmonEnable (EMU_VmonChannel_TypeDef channel, bool enable) |
Enable or disable a VMON channel. | |
bool | EMU_VmonChannelStatusGet (EMU_VmonChannel_TypeDef channel) |
Get the status of a voltage monitor channel. | |
float | EMU_TemperatureGet (void) |
Get temperature in degrees Celsius. | |
bool | EMU_LDOStatusGet (void) |
Check status of the internal LDO regulator. | |
void | EMU_EnterEM1 (void) |
Enter energy mode 1 (EM1). | |
void | EMU_VScaleWait (void) |
Wait for voltage scaling to complete. | |
EMU_VScaleEM01_TypeDef | EMU_VScaleGet (void) |
Get current voltage scaling level. | |
bool | EMU_VmonStatusGet (void) |
Get the status of the voltage monitor (VMON). | |
void | EMU_IntClear (uint32_t flags) |
Clear one or more pending EMU interrupts. | |
void | EMU_IntDisable (uint32_t flags) |
Disable one or more EMU interrupts. | |
void | EMU_IntEnable (uint32_t flags) |
Enable one or more EMU interrupts. | |
uint32_t | EMU_IntGet (void) |
Get pending EMU interrupt flags. | |
uint32_t | EMU_IntGetEnabled (void) |
Get enabled and pending EMU interrupt flags. | |
void | EMU_IntSet (uint32_t flags) |
Set one or more pending EMU interrupts. | |
void | EMU_BUReady (void) |
Halts until backup power functionality is ready. | |
void | EMU_Lock (void) |
Lock EMU registers in order to protect them against unintended modification. | |
void | EMU_Unlock (void) |
Unlock the EMU so that writing to locked registers again is possible. | |
void | EMU_PowerLock (void) |
Lock the EMU regulator control registers in order to protect against unintended modification. | |
void | EMU_PowerUnlock (void) |
Unlock the EMU power control registers so that writing to locked registers again is possible. | |
void | EMU_EM2Block (void) |
Block entering EM2 or higher number energy modes. | |
void | EMU_EM2UnBlock (void) |
Unblock entering EM2 or higher number energy modes. | |
void | EMU_UnlatchPinRetention (void) |
When EM4 pin retention is set to emuPinRetentionLatch, then pins are retained through EM4 entry and wakeup. | |
bool | EMU_TemperatureReady (void) |
Temperature measurement ready status. | |
bool | EMU_DCDCPowerOff (void) |
Power off the DCDC regulator. | |
Macros | |
#define | EMU_VSCALE_PRESENT |
Voltage scaling present. | |
#define | EMU_VSCALE_EM01_PRESENT |
Voltage scaling for EM01 present. | |
#define | EMU_SERIES1_DCDC_BUCK_PRESENT |
#define | emuDcdcLnHighEfficiency -1 |
High efficiency mode. | |
#define | emuDcdcLnFastTransient 160 |
Default reverse current for fast transient response mode (low noise). | |
#define | EMU_EM01INIT_DEFAULT |
Default initialization of EM0 and 1 configuration. | |
#define | EMU_EM23INIT_DEFAULT |
Default initialization of EM2 and 3 configuration. | |
#define | EMU_EM4INIT_DEFAULT |
Default initialization of EM4 configuration (Series 1 with VSCALE). | |
#define | EMU_BUINIT_DEFAULT |
Default Backup Power Domain configuration. | |
#define | EMU_DCDCINIT_DEFAULT |
Default DCDC initialization. | |
#define | EMU_VMONINIT_DEFAULT |
Default VMON initialization structure. | |
#define | EMU_VMONHYSTINIT_DEFAULT |
Default VMON Hysteresis initialization structure. | |
#define | EMU_TEMP_ZERO_C_IN_KELVIN (273.15f) |
Zero degrees Celcius in Kelvin. | |
Typedefs | |
typedef int16_t | EMU_DcdcLnReverseCurrentControl_TypeDef |
DCDC Forced CCM and reverse current limiter control. | |
Enumerations | |
enum | EMU_BUBuInactPwrCon_TypeDef { emuBuBuInactPwrCon_None = EMU_BUCTRL_BUINACTPWRCON_NONE, emuBuBuInactPwrCon_MainBu = EMU_BUCTRL_BUINACTPWRCON_MAINBU, emuBuBuInactPwrCon_BuMain = EMU_BUCTRL_BUINACTPWRCON_BUMAIN, emuBuBuInactPwrCon_NoDiode = EMU_BUCTRL_BUINACTPWRCON_NODIODE } |
Backup Power Domain power connection configuration when not in backup mode selection. | |
enum | EMU_BUBuActPwrCon_TypeDef { emuBuBuActPwrCon_None = EMU_BUCTRL_BUACTPWRCON_NONE, emuBuBuActPwrCon_MainBu = EMU_BUCTRL_BUACTPWRCON_MAINBU, emuBuBuActPwrCon_BuMain = EMU_BUCTRL_BUACTPWRCON_BUMAIN, emuBuBuActPwrCon_NoDiode = EMU_BUCTRL_BUACTPWRCON_NODIODE } |
Backup Power Domain power connection configuration in backup mode selection. | |
enum | EMU_BUPwrRes_TypeDef { emuBuPwrRes_Res0 = EMU_BUCTRL_PWRRES_RES0, emuBuPwrRes_Res1 = EMU_BUCTRL_PWRRES_RES1, emuBuPwrRes_Res2 = EMU_BUCTRL_PWRRES_RES2, emuBuPwrRes_Res3 = EMU_BUCTRL_PWRRES_RES3 } |
Backup Power Domain resistor selection. | |
enum | EMU_BUVoutRes_TypeDef { emuBuVoutRes_Dis = EMU_BUCTRL_VOUTRES_DIS, emuBuVoutRes_Weak = EMU_BUCTRL_VOUTRES_WEAK, emuBuVoutRes_Med = EMU_BUCTRL_VOUTRES_MED, emuBuVoutRes_Strong = EMU_BUCTRL_VOUTRES_STRONG } |
Resistance between backup domain power supply and BU_VOUT. | |
enum | EMU_BODMode_TypeDef { emuBODMode_Active, emuBODMode_Inactive } |
BOD threshold setting selector, active or inactive mode. | |
enum | EMU_EM4State_TypeDef { emuEM4Shutoff = 0, emuEM4Hibernate = 1 } |
EM4 modes. | |
enum | EMU_EM4PinRetention_TypeDef { emuPinRetentionDisable = EMU_EM4CTRL_EM4IORETMODE_DISABLE, emuPinRetentionEm4Exit = EMU_EM4CTRL_EM4IORETMODE_EM4EXIT, emuPinRetentionLatch = EMU_EM4CTRL_EM4IORETMODE_SWUNLATCH } |
EM4 Pin Retention Type. | |
enum | EMU_PowerConfig_TypeDef { emuPowerConfig_DcdcToDvdd } |
Power configurations. | |
enum | EMU_DcdcMode_TypeDef { emuDcdcMode_Bypass = EMU_DCDCCTRL_DCDCMODE_BYPASS, emuDcdcMode_LowNoise = EMU_DCDCCTRL_DCDCMODE_LOWNOISE, emuDcdcMode_LowPower = EMU_DCDCCTRL_DCDCMODE_LOWPOWER } |
DCDC operating modes. | |
enum | EMU_DcdcModeEM23_TypeDef { emuDcdcModeEM23_LowPower = EMU_DCDCCTRL_DCDCMODEEM23_EM23LOWPOWER, emuDcdcModeEM23_Sw = EMU_DCDCCTRL_DCDCMODEEM23_EM23SW } |
DCDC operating modes in EM2 or EM3. | |
enum | EMU_DcdcConductionMode_TypeDef { emuDcdcConductionMode_ContinuousLN, emuDcdcConductionMode_DiscontinuousLN } |
DCDC conduction modes. | |
enum | EMU_DcdcAnaPeripheralPower_TypeDef { emuDcdcAnaPeripheralPower_AVDD = EMU_PWRCTRL_ANASW_AVDD, emuDcdcAnaPeripheralPower_DCDC = EMU_PWRCTRL_ANASW_DVDD } |
DCDC to DVDD mode analog peripheral power supply select. | |
enum | EMU_DcdcLnRcoBand_TypeDef { emuDcdcLnRcoBand_3MHz = 0, emuDcdcLnRcoBand_4MHz = 1, emuDcdcLnRcoBand_5MHz = 2, emuDcdcLnRcoBand_6MHz = 3, emuDcdcLnRcoBand_7MHz = 4, emuDcdcLnRcoBand_8MHz = 5, emuDcdcLnRcoBand_9MHz = 6, emuDcdcLnRcoBand_10MHz = 7 } |
DCDC Low-noise RCO band select. | |
enum | EMU_DcdcLnCompCtrl_TypeDef { emuDcdcLnCompCtrl_1u0F, emuDcdcLnCompCtrl_4u7F } |
DCDC Low Noise Compensator Control register. | |
enum | EMU_VmonChannel_TypeDef { emuVmonChannel_AVDD, emuVmonChannel_ALTAVDD, emuVmonChannel_DVDD, emuVmonChannel_IOVDD0, emuVmonChannel_IOVDD1, emuVmonChannel_BUVDD } |
VMON channels. | |
enum | EMU_VScaleEM01_TypeDef { emuVScaleEM01_HighPerformance = _EMU_STATUS_VSCALE_VSCALE2, emuVScaleEM01_LowPower = _EMU_STATUS_VSCALE_VSCALE0 } |
Supported EM0/1 Voltage Scaling Levels. | |
enum | EMU_VScaleEM23_TypeDef { emuVScaleEM23_FastWakeup = _EMU_CTRL_EM23VSCALE_VSCALE2, emuVScaleEM23_LowPower = _EMU_CTRL_EM23VSCALE_VSCALE0 } |
Supported EM2/3 Voltage Scaling Levels. | |
enum | EMU_VScaleEM4H_TypeDef { emuVScaleEM4H_FastWakeup = _EMU_CTRL_EM4HVSCALE_VSCALE2, emuVScaleEM4H_LowPower = _EMU_CTRL_EM4HVSCALE_VSCALE0 } |