// Gecko Platform//Version 4.4.1 //Services ... A 64-bits tick counter is accessible through the ... All API functions can be called from within interrupt handlers. ... Description N/A handle
A template for this file, containing default values, is in the emdrv/config folder. ... [in] type Abort type – whether to abort only Tx, only Rx, or both.
ProductMicrocontrollersResource TypeSoftware API documentation
RTT module uses a control block structure located in RAM memory with a specific ID so that it can be discovered when a ... sl_status_t sl_iostream_rtt_init (void) RTT Stream init. Variables
ProductMicrocontrollersResource TypeSoftware API documentation
// Platform//Version 5.0.1 //Security ... PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... A counter in the tamper filter is increased.
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32gg11/struct-o-p-a-m-p-init-type-def